FS6510 Reading BIST Result needs a delay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS6510 Reading BIST Result needs a delay

跳至解决方案
4,021 次查看
Jamber_H
Contributor III

Hi, 

I read the BIST Register after power-on reset, the result is 0x0, it means all the 4 bits of BIST reault are NOTOK. But after a 8ms delay, I read this register again, it returns 0xD, it means ABIST2_VAUX is NOTOK, and other bits such as LBIST, ABIST1, ABIST2_FS1B are Normal. Why does it need a delay, what's the possible reason about it?

BIST延时.png

Best Regards,

Jamber

0 项奖励
回复
1 解答
4,010 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
1 回复
4,011 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jamber,

the 8ms is actually quite short delay time. According to the datasheet, the Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.

JozefKozon_0-1626871580793.png

With Best Regards,

Jozef

0 项奖励
回复