FS6510 Can't set IMPACT register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS6510 Can't set IMPACT register

ソリューションへジャンプ
2,782件の閲覧回数
Jamber_H
Contributor III

After Power-On, the SBC is in Init mode, I set INIT_VAUX_OVUV_IMPACT register as 0xA, after 200us, I read back it, but the result is 0x0, which is not equal to the value I set. What's the reason?Can't set IMPACT register.png

0 件の賞賛
返信
1 解決策
2,777件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Please try to close the INIT_FS with at least 1 good WD refresh and then read back the INIT_VAUX_OVUV_IMPACT register.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,764件の閲覧回数
Jamber_H
Contributor III

HI, could you help me?

0 件の賞賛
返信
2,778件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Please try to close the INIT_FS with at least 1 good WD refresh and then read back the INIT_VAUX_OVUV_IMPACT register.

Best regards,

Tomas

0 件の賞賛
返信
2,775件の閲覧回数
Jamber_H
Contributor III

Hi, Tomas,

I tried that, I read this register periodly after I set it in INIT phase. In Normal phase, the value is not 0x0, but it's a default value as 0xE.

2021-07-20_195751.png

Best regards,

Jamber

 

0 件の賞賛
返信