Problem with Secure Boot on P2041

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Secure Boot on P2041

1,553件の閲覧回数
saadahmad
Contributor I

Hi,

I am trying to activate secure boot on P2041RDB.

I am using (rcw_14g_sben_1500mhz.bin) RCW with secure boot and boot hold enabled

(without ITS=1).

I am following procedure from SDK documentation to add SRKH on runtime during boot hold (without blowing fuses):

Using CW TAP (USB)

Open CCS (On Ubuntu)

source IDcode.tcl (selected cw usb TAP)

# Connect to CCS and configure Config Chain

ccs::config_chain p2040

display ccs::get_config_chain

#Check Initial SNVS State and Value in SCRATCH Registers

ccs::display_mem 0 0xfe314014 4 0 1

ccs::display_mem 0 0xfe0e0200 4 0 4

#Wrie the SRK Hash Value in Mirror Registers

ccs::write_mem 0 0xfe0e807c 4 0 <SRKH1>

ccs::write_mem 0 0xfe0e8080 4 0 <SRKH2>

ccs::write_mem 0 0xfe0e8084 4 0 <SRKH3>

ccs::write_mem 0 0xfe0e8088 4 0 <SRKH4>

ccs::write_mem 0 0xfe0e808c 4 0 <SRKH5>

ccs::write_mem 0 0xfe0e8090 4 0 <SRKH6>

ccs::write_mem 0 0xfe0e8094 4 0 <SRKH7>

ccs::write_mem 0 0xfe0e8098 4 0 <SRKH8>

#Get the Core Out of Boot Hold-Off

ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001

The problem is on second debug command <which ever it is> I always get (scan timeout error)

But If I retry again the command works.

However when I read SSM_ST (Security State of SEC_MON), it goes to "Non-Secure" state.

The cores are still in boot hold but the security state changes to Non-Secure.

After releasing boot hold the ISBC gives error "SSM_CHECKSTS" (SEC_MON State Machine

not in CHECK state at start of ISBC) and SoC gets stuck (no output).

Thanks in advance for any help you are able to provide.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,217件の閲覧回数
bpe
NXP Employee
NXP Employee

Hello,

Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Support Case:

How to submit a new question for NXP Support

Be aware that to give you remote support through an SC, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SC and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Have a great day,
Platon

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信