P2020 LALE Output Delay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P2020 LALE Output Delay

跳至解决方案
1,357 次查看
stevenrendano
Contributor I

P2020EC Rev 2, Table 59, Enhanced Local Bus Timing Specifications - PLL Enabled Mode, does not provide output delay for LALE.  Associated Figure 37, Local Bus AC Timing Diagram (PLL Enabled), shows LALE output delay less than general output delay tLBKHOV.  Is this relationship guaranteed, i.e. is LALE output delay always less than or equal to tBKHOV?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,204 次查看
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,205 次查看
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

0 项奖励
回复