P2020 LALE Output Delay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 LALE Output Delay

ソリューションへジャンプ
1,356件の閲覧回数
stevenrendano
Contributor I

P2020EC Rev 2, Table 59, Enhanced Local Bus Timing Specifications - PLL Enabled Mode, does not provide output delay for LALE.  Associated Figure 37, Local Bus AC Timing Diagram (PLL Enabled), shows LALE output delay less than general output delay tLBKHOV.  Is this relationship guaranteed, i.e. is LALE output delay always less than or equal to tBKHOV?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,203件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,204件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

0 件の賞賛
返信