Hi,
I am using MPC8377E-RDBA powerpc board. I need to load image through tftp. Can anyone suggest what are all the things(environment variables, servers etc..) need to set up to load the image.
/Raghu
解決済! 解決策の投稿を見る。
Please check it at: http://www.imxdev.org/wiki/index.php?title=All_Boards_TFTP
Regards,
Fabio Estevam
I have found openSUSE very satisfactory for TFTP server. Just set a couple of parameters in YaST and it works.
Alternatively if you're hosting your files on a windows PC, you can use the tftp server executable included in the SDK tar (L2.6.31_09.12.00_SDK_SOURCE, which you can get from here) and point the Base Directory to the folder where your images are stored.
Please check it at: http://www.imxdev.org/wiki/index.php?title=All_Boards_TFTP
Regards,
Fabio Estevam