tftp environment setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tftp environment setup

Jump to solution
3,470 Views
mpc8377e
Contributor I

Hi,

 

I am using MPC8377E-RDBA powerpc board. I need to load image through tftp. Can anyone suggest what are all the things(environment variables, servers etc..) need to set up to load the image.

 

/Raghu

0 Kudos
Reply
1 Solution
2,498 Views
fabio_estevam
NXP Employee
NXP Employee
0 Kudos
Reply
3 Replies
2,498 Views
edss
Contributor I

I have found openSUSE very satisfactory for TFTP server.  Just set a couple of parameters in YaST and it works.

0 Kudos
Reply
2,498 Views
leper
Contributor II

Alternatively if you're hosting your files on a windows PC, you can use the tftp server executable included in the SDK tar (L2.6.31_09.12.00_SDK_SOURCE, which you can get from here) and point the Base Directory to the folder where your images are stored.

0 Kudos
Reply
2,499 Views
fabio_estevam
NXP Employee
NXP Employee

Please check it at: http://www.imxdev.org/wiki/index.php?title=All_Boards_TFTP

 

Regards,

 

Fabio Estevam

0 Kudos
Reply