tftp environment setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

tftp environment setup

跳至解决方案
3,476 次查看
mpc8377e
Contributor I

Hi,

 

I am using MPC8377E-RDBA powerpc board. I need to load image through tftp. Can anyone suggest what are all the things(environment variables, servers etc..) need to set up to load the image.

 

/Raghu

0 项奖励
回复
1 解答
2,504 次查看
fabio_estevam
NXP Employee
NXP Employee
0 项奖励
回复
3 回复数
2,504 次查看
edss
Contributor I

I have found openSUSE very satisfactory for TFTP server.  Just set a couple of parameters in YaST and it works.

0 项奖励
回复
2,504 次查看
leper
Contributor II

Alternatively if you're hosting your files on a windows PC, you can use the tftp server executable included in the SDK tar (L2.6.31_09.12.00_SDK_SOURCE, which you can get from here) and point the Base Directory to the folder where your images are stored.

0 项奖励
回复
2,505 次查看
fabio_estevam
NXP Employee
NXP Employee

Please check it at: http://www.imxdev.org/wiki/index.php?title=All_Boards_TFTP

 

Regards,

 

Fabio Estevam

0 项奖励
回复