tftp environment setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tftp environment setup

ソリューションへジャンプ
3,474件の閲覧回数
mpc8377e
Contributor I

Hi,

 

I am using MPC8377E-RDBA powerpc board. I need to load image through tftp. Can anyone suggest what are all the things(environment variables, servers etc..) need to set up to load the image.

 

/Raghu

0 件の賞賛
返信
1 解決策
2,502件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
0 件の賞賛
返信
3 返答(返信)
2,502件の閲覧回数
edss
Contributor I

I have found openSUSE very satisfactory for TFTP server.  Just set a couple of parameters in YaST and it works.

0 件の賞賛
返信
2,502件の閲覧回数
leper
Contributor II

Alternatively if you're hosting your files on a windows PC, you can use the tftp server executable included in the SDK tar (L2.6.31_09.12.00_SDK_SOURCE, which you can get from here) and point the Base Directory to the folder where your images are stored.

0 件の賞賛
返信
2,503件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Please check it at: http://www.imxdev.org/wiki/index.php?title=All_Boards_TFTP

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信