TEA1716T SNSMAINS pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TEA1716T SNSMAINS pin

跳至解决方案
67 次查看
KA1
Contributor II

 

We have a question about the connection of pin 2 (SNSMAINS) of the TEA1716T.

Is it possible to apply a bridge-rectified voltage to pin 2 (SNSMAINS)?

(Connection like the attached circuit diagram.)

This connection is the same as FIG. 26 in AN11179.

In FIG. 26 of AN11179, a diode-rectified voltage is applied to pin 2 (SNSMAINS).

KA1_0-1756792301412.pngKA1_1-1756792395413.png

 

 

标记 (1)
0 项奖励
回复
1 解答
57 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
58 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

0 项奖励
回复
47 次查看
KA1
Contributor II

Thanks for reply.

That's useful information for us.

Question solved.

0 项奖励
回复