TEA1716T SNSMAINS pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA1716T SNSMAINS pin

Jump to solution
68 Views
KA1
Contributor II

 

We have a question about the connection of pin 2 (SNSMAINS) of the TEA1716T.

Is it possible to apply a bridge-rectified voltage to pin 2 (SNSMAINS)?

(Connection like the attached circuit diagram.)

This connection is the same as FIG. 26 in AN11179.

In FIG. 26 of AN11179, a diode-rectified voltage is applied to pin 2 (SNSMAINS).

KA1_0-1756792301412.pngKA1_1-1756792395413.png

 

 

Tags (1)
0 Kudos
Reply
1 Solution
58 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

View solution in original post

0 Kudos
Reply
2 Replies
59 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

0 Kudos
Reply
48 Views
KA1
Contributor II

Thanks for reply.

That's useful information for us.

Question solved.

0 Kudos
Reply