TEA1716T SNSMAINS pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEA1716T SNSMAINS pin

ソリューションへジャンプ
69件の閲覧回数
KA1
Contributor II

 

We have a question about the connection of pin 2 (SNSMAINS) of the TEA1716T.

Is it possible to apply a bridge-rectified voltage to pin 2 (SNSMAINS)?

(Connection like the attached circuit diagram.)

This connection is the same as FIG. 26 in AN11179.

In FIG. 26 of AN11179, a diode-rectified voltage is applied to pin 2 (SNSMAINS).

KA1_0-1756792301412.pngKA1_1-1756792395413.png

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
59件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
60件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to apply a bridge-rectified voltage to the SNSMAINS pin, as shown in your schematic. This approach is valid and supported by the TEA1716T.

BRs, Tomas

0 件の賞賛
返信
49件の閲覧回数
KA1
Contributor II

Thanks for reply.

That's useful information for us.

Question solved.

0 件の賞賛
返信