PNEV7462 example uploading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PNEV7462 example uploading

2,912件の閲覧回数
xlivnenko_michael
Contributor I

Hi, I'm new in NXP and I have a problem with uploading the example to the board.

I have a PNEV7462C dev board and want to upload phExCcid example using a J-Link or a divece as a mass storage. I've upload support packege and open the example with MCUXpress IDE, if I run the debug - the device works fine, but if I want to upload with RUN after uploading nothing works. Also I've tried with mass storage, upload EEPROM file separetly and bin file that was creating while building and nothing works. 

 

0 件の賞賛
返信
8 返答(返信)

2,873件の閲覧回数
xlivnenko_michael
Contributor I

I succesfuly open the needed project, but the problem is that the example works only in debug mode. When I use program flash or uploading using mass storage nothing works

0 件の賞賛
返信

2,824件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @xlivnenko_michael 

Just checked the properties of this project, it programmed into flash.  it should work without debug.  But no print on debug console.

danielchen_0-1703730691909.pngdanielchen_0-1703730691909.png

 

 

Regards

Daniel

 

0 件の賞賛
返信

2,889件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Sorry I am not sure I catch your question,  I would suggest you take a look at the um10883: PN7462 Quick Start Guider,  it describes how to start and develop software and hardware with PN7462 family

https://www.nxp.com/docs/en/user-guide/UM10883.pdf

 

Regards

Daniel

0 件の賞賛
返信

2,872件の閲覧回数
xlivnenko_michael
Contributor I

I uploaded the code from this manual and succesfully run the needed example, but it works only in debug mode, if I program flash using JLink and MCUXpresso or using masstorage for uploading - nothing works

0 件の賞賛
返信

2,851件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @xlivnenko_michael 

 

which demo you are using, let me try to reproduce this issue on my side

 

Regards

Daniel

0 件の賞賛
返信

2,785件の閲覧回数
xlivnenko_michael
Contributor I

Hi, 

Any news?

0 件の賞賛
返信

2,781件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

This demo works without debugger,  but you can not see the debug output in MCUXpresso console, since you stopped debugging.   actually it works

0 件の賞賛
返信

2,846件の閲覧回数
xlivnenko_michael
Contributor I

Ccid example, for flashing JLink

0 件の賞賛
返信