PNEV7462 example uploading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PNEV7462 example uploading

2,939 Views
xlivnenko_michael
Contributor I

Hi, I'm new in NXP and I have a problem with uploading the example to the board.

I have a PNEV7462C dev board and want to upload phExCcid example using a J-Link or a divece as a mass storage. I've upload support packege and open the example with MCUXpress IDE, if I run the debug - the device works fine, but if I want to upload with RUN after uploading nothing works. Also I've tried with mass storage, upload EEPROM file separetly and bin file that was creating while building and nothing works. 

 

0 Kudos
Reply
8 Replies

2,900 Views
xlivnenko_michael
Contributor I

I succesfuly open the needed project, but the problem is that the example works only in debug mode. When I use program flash or uploading using mass storage nothing works

0 Kudos
Reply

2,851 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @xlivnenko_michael 

Just checked the properties of this project, it programmed into flash.  it should work without debug.  But no print on debug console.

danielchen_0-1703730691909.png

 

 

Regards

Daniel

 

0 Kudos
Reply

2,916 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

Sorry I am not sure I catch your question,  I would suggest you take a look at the um10883: PN7462 Quick Start Guider,  it describes how to start and develop software and hardware with PN7462 family

https://www.nxp.com/docs/en/user-guide/UM10883.pdf

 

Regards

Daniel

0 Kudos
Reply

2,899 Views
xlivnenko_michael
Contributor I

I uploaded the code from this manual and succesfully run the needed example, but it works only in debug mode, if I program flash using JLink and MCUXpresso or using masstorage for uploading - nothing works

0 Kudos
Reply

2,878 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @xlivnenko_michael 

 

which demo you are using, let me try to reproduce this issue on my side

 

Regards

Daniel

0 Kudos
Reply

2,812 Views
xlivnenko_michael
Contributor I

Hi, 

Any news?

0 Kudos
Reply

2,808 Views
danielchen
NXP TechSupport
NXP TechSupport

This demo works without debugger,  but you can not see the debug output in MCUXpresso console, since you stopped debugging.   actually it works

0 Kudos
Reply

2,873 Views
xlivnenko_michael
Contributor I

Ccid example, for flashing JLink

0 Kudos
Reply