LS1028A reference clocks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1028A reference clocks

跳至解决方案
1,559 次查看
mkraj
Contributor III

Dear NXP support team

In the NXP LS1028A reference design 100MHz LP-HCSL clock was used for SerDes 1&2 reference and PCIe reference.

Can these clocks be 100 MHz HCSL instead of LP-HCSL?

 

 

With Regards

Krishnam Raju M

标记 (1)
0 项奖励
回复
1 解答
1,548 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,549 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

0 项奖励
回复