LS1028A reference clocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A reference clocks

Jump to solution
1,557 Views
mkraj
Contributor III

Dear NXP support team

In the NXP LS1028A reference design 100MHz LP-HCSL clock was used for SerDes 1&2 reference and PCIe reference.

Can these clocks be 100 MHz HCSL instead of LP-HCSL?

 

 

With Regards

Krishnam Raju M

Tags (1)
0 Kudos
Reply
1 Solution
1,546 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

View solution in original post

0 Kudos
Reply
1 Reply
1,547 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

0 Kudos
Reply