LS1028A reference clocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A reference clocks

ソリューションへジャンプ
1,555件の閲覧回数
mkraj
Contributor III

Dear NXP support team

In the NXP LS1028A reference design 100MHz LP-HCSL clock was used for SerDes 1&2 reference and PCIe reference.

Can these clocks be 100 MHz HCSL instead of LP-HCSL?

 

 

With Regards

Krishnam Raju M

タグ(1)
0 件の賞賛
返信
1 解決策
1,544件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,545件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport

Hi @mkraj 

 

The clock selected should be as per the specification mentioned in section# 3.16.2 of the LS1028A datasheet. And I believe the HCSL clock is as per the specification required for the SerDes clock.

 

Thanks

Khushbu

0 件の賞賛
返信