Hi Parth,
It is better when you will create a new request for the questions which are not related to this case.
However, you can look at the AN2708 - An Introduction to the External Bus Interface on the HCS12X
https://www.nxp.com/docs/en/application-note/AN2708.pdf
The purpose of the external bus interface is the expansion of internal bus to enable connection of external memories/peripherals.
I hope it helps.
Best Regards,
Diana
Hello Parth,
Did you download the S12X Example pack?
https://community.nxp.com/docs/DOC-95116
There can be found the ADT examples:
XEP100 - ATD + GPIO - CW47
XEP100 - ATD and PIT - CW47
XEP100 - ATD Continuous conversion with interrupt - CW4
XEP100 - ATD multichannel - CW46
XEP100 - ATD Single conversion - CW46
And on this link can be found the FLASH examples.
https://community.nxp.com/docs/DOC-329209
You can use it as a reference.
I hope it helps.
Best Regards,
Diana
Hello,
Sorry I am late with replying.
I am using MC9S12X256, and code warrior version 5.1. I want to use some ADCs of this micro-controller to acquire some voltages and want to set output accordingly. I am studying Timers and interrupts, and also memory accessing. If you can help me on this, I will be very thankful.
Hello Parth,
If you give me more information such as a concrete type of MCU or what's causing you difficulty I can tell you more.
Do you have already installed CodeWarrior? If yes, which version?
For now, I would like to provide you some examples and documents:
S12X Examples Pack:
https://community.nxp.com/docs/DOC-339787
List of MagniV and S12(X) Examples and Documents (please, focus on the S12(X) section)
https://community.nxp.com/docs/DOC-341378
List of MagniV S12(X) Application notes
https://community.nxp.com/docs/DOC-341377
S12X PLL (Filter) Calculator
https://community.nxp.com/docs/DOC-103954
Also, important information can be found on the NXP site:
I hope it helps.
Best Regards,
Diana