Hi,pgo
1 my chip number is FXTH8709116T1
2 my debug and program tool is USBDM
3 my development tool is codewarrior 10.5
Now,when I try loading my .s19 file to the FXTH8709116T1, I got this
But when I create an new empty project, the .s19 file can be load by HCS08 programmer successfully.
When I use codewarrior 10.5, it can flash my target file successfully, but the target device seem not run successfully, I am very confused
.
Solved! Go to Solution.
Hi Xia,
I suspect you have erased the top sectors of the device somewhere along the way. This will result in a secured device.
When you try to read from a secured device you get all zeros.
If this is the case you have little choice but to do a mass erase and reprogram one of the file images provided on the previous link provided (above).
bye
Dear Xia,
When you created your project in Codewarrior did you change the memory map to avoid re-programming the semi-permanent information in the upper region of the chip? See the previous discussion thread.
Can you post the image file you are programming please?
bye
;
When I try to debug using USBDM, I got this
the attach file FXTH87xx11_Starter_Project_CW10.abs.s19 can not be programmed by HCS08 progarm;
the attach file 20151201.abs.s19 can be programmed by HCS08 progarm, but the progarm can not run.
Hi Xia,
The example files you provided appear to cover the correct memory ranges so I am unsure what is causing your problem.
It is possible that the upper ROM has been erased.
I suggest you program the chip with the file that programs OK and then use the memory dump program to read-back the entire memory image to check that upper region of the Flash has not been erased somewhere along the line.
Refer to this page for some more information:
Hi Xia,
I suspect you have erased the top sectors of the device somewhere along the way. This will result in a secured device.
When you try to read from a secured device you get all zeros.
If this is the case you have little choice but to do a mass erase and reprogram one of the file images provided on the previous link provided (above).
bye
hi
pgo, I do a mass erase and reprogram fxth870511_Image.sx, then load the .s19 file in the codewarrior 10.5 ,the chip can run sucessfully.
I download my file using the codewarrior 10.5 flash devices. but I can not download using hcs08 program. I am very happy, my chip can run successfully, thank you very munch!
Hi
pgo,
I load the image file FXTH870911_Image.sx already.
When I loaded my .s19 file, I set in codewarrior about " EraseSelective" already and build my project, creat .s19 file.
I select EraseSelective on the stand-alone HCS08 Programmer,but I got this,Why?
I use USBDM 4.12.1.30,
when I click " Program Flash", I got this.
看你的中文XP系统,就直接给你打中文的算了,早在半年前我就尝试了CW配合USBDM开发 FXTH87xx11,但是也是一直无法调试这款芯片,不过能够直接下载代码,但是感觉下载进去的程序并没有运行,建议使用好点的仿真器开发。
谢谢!中文看起来更顺啊!哈哈!本想用中文发表,但是怕中国人少,回复的也少,能讲中文真舒服啊。
现在我可以烧写新建的工程,但是以前的工程烧写不了。
提示烧写区域不在芯片ROM内。
但是烧写进去的程序貌似并没有跑起来。
所以,我也快要放弃了,用这个烧写器搞不好了。
Dear pgo,
I restart my computer, the target can be connected finally,.
The flash programmer can load an empty project,but it can not load my own project. i got this:
Do I need these files:
how can I get the files above?
Dear pgo,
1、Where can I get the image file?
2、 Do you mean this kind of file? Such as your FXTH870511_Image.sx
3、I don’t change the memory map when I creat project in codewarrior.
Now I met an new program, I can not connect the target in any case, I check the hardware , it is no problem, I try two target, the problem is same. Now, I need to solve it firstly.