NXP FTF 2016 - 培训演示

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP FTF 2016 - Training Presentations

讨论

排序依据:
This beginning hands-on session will walk you through the steps to configure the device and boot U-Boot. Learn how to configure the device reset control word (RCW), flash the device, and debug U-Boot. This session will use the CodeWarrior Development Studio for ARM®v8 ISA to boot the QorIQ LS1021A Reference Design Board (RDB).
查看全文
With the trend of frequent and remote software updates on the vehicle, the need of managing this properly at the microcontroller is critical. This session will present the challenges on microcontroller reprogramming and how our S32K144 microcontroller properly addresses it safe and efficiently.
查看全文
The CodeWarrior Development Suite for the QorIQ LS series includes a variety of tools targeted at analyzing the operation and performance of a multicore Linux system. Tools utilitize hardware trace and system logs to monitor operation and performance. CodeWarrior Development Suite includes tools for performance analysis with the Hierarchical Profiler, Flat Profiler and CodeCoverage; path analysis with Timeline and CallTree; real-time monitoring with DebugPrint and TraceCommander in addition to interval profiling.
查看全文
The I2C bus has expanded from its humble beginnings in 1980s home electronics to both small and large scale systems in the modern world. Applications range from Smartphones to Server farms, and while they're true to the original simple signaling protocol other I2C bus components are needed to expand, adapt or buffer those signals. We take an in depth technical look at the simple Bus Buffer. Often needed, and seldom understood. Watch Video Presentation
查看全文
Designer have a simple way to achieve functional safety standards with NXP's functional safety microcontroller portfolio. During this session we will cover how functional safety applies to both the automotive and industrial markets and the support NXP offers in each step. Watch Video Presentation
查看全文
From solving a simple problem - How did a 1980s TV 'talk' to your new Video Cassette Recorder (VCR)? - The Inter-Integrated Bus has solved many of today's low speed communication problems. Known affectionately as the I2C (pronounced eye-squared-see) bus, just two wires can connect a variety of electronic components that help us enjoy many products from Smartphones to Cloud Server farms. In industry the I2C bus is a simple and reliable link for sensors, indicators, human interface, and behind-the-scenes equipment set up and control. We talk about how it works, and what it can do for your next electronics project. Watch Video Presentation
查看全文
This is an overview of the next generation S32K microcontrollers family and the system solution benefits using the latest MCU features. Watch Video Presentation
查看全文
Deep dive into the vision processing architecture of the i.MX 8 family. Learn how to access the advanced processing features, the vision SDK, and the vision-based applications enabled by the i.MX 8 processor. This class provides an introduction to understanding the unique way in which machine vision is handled by i.MX 8. It forms a basic introduction class that is a precursor to the more advanced "Call Your Shot!" pool table demo class. Watch Video Presentation
查看全文
The standard CAN protocol has been extended into CAN Flexible Data (FD) to provide higher bandwidth while keeping the physical characteristics that have made it the most popular automotive in-vehicle communications protocol . This presentation will provide an overview of the changes to the standard as well as address the challenges faced while rolling out and implementing the technology. Watch Video Presentation
查看全文
White box switches are network switches that are sold independent of the software that will run on them. Open Network Linux (ONL) is used as the basis for the "network operating systems" that run on the switches. Open Network Install Environment (ONIE) is used to create the software used to install the networking operation system onto the switch. This presentation highlights NXP's involvement in ONL/ONIE on the QorIQ P2041 and QorIQ T2080 platforms as well as the roadmap for LS2085. This session will expand on NXP's approach to ONL/ONIE and the white box market. Watch Video Presentation
查看全文
Aimed to be a hands-on the exercise would consist in using a vision processor to run CNN on various pictures to recognize traffic signals (Stop, Turn, Yield, etc). First we will cover basic concepts on machine learning for the algorithms to be used. After the class part is over, we will use a vision processor to run CNN to recognize between traffic signs and no traffic signs.
查看全文
Hands-on training for ZigBee-3.0 with NXP lowest power Wireless MCU, using evaluation kit. Quickest and fastest way to develop a smart home product using ZigBee-3.0 such as sensors, monitoring device panels, router devices and Gateway solutions.
查看全文
The hottest topic in automotive design today is the concept of the eCockpit -- where all visual functions in the car are controlled across multiple screens and fully integrated for the driver’s convenience. The key technology that enables eCockpit to run on a single processor also offers new capabilities in industrial, embedded and consumer products such as drones, manufacturing HMI interfaces and smart displays. This class will cover the fundamental technologies and architectural techniques in the i.MX 8 processor which enables rich eCockpit functionality, how NXP has implemented the world’s most significant full chip virtualization capabilities in an ARM-based processor and breaks down the eCockpit demo from the Tech Lab.  Watch Video Presentation
查看全文
Solid state RF energy provides cooking appliance OEMs the opportunity to create differentiated cooking appliances. When combined with emerging food services, these appliances can enable greater levels of consumer convenience while delivering consistent cooking results. This session will cover the underlying basics of how solid state RF cooking is performed, its benefits, and how it can be combined in an IoT appliance to deliver even further differentiation. Watch Video Presentation
查看全文
In this session, a panel of multi-disciplinary experts will describe and discuss the challenges of securing the connected world around us. The session will cover three major facets of creating secure solutions, addressing the challenges and emerging trends for: *Device Security - Securing edge nodes, smart cards, certifications *Network Security - Secure data transmission, security protocols *Internet of Things Security -Trust, crypto, tamper Subject matter experts will present an overview of each of these topics, followed by an interactive dialogue with the audience. It is hoped that the audience will gain a high-level understanding of the multi-faceted challenges of securing end to end solutions, and how semiconductor companies will work with ecosystem partners, innovators, and policy makers to address those challenges.  
查看全文
By adding NFC to a door lock, the same smartcard technology that protects some of the world’s most valuable objects can now be brought to everyday places like homes, apartment buildings, and hotels. An NFC-enabled smartphone can be used to configure the lock, so homeowners can grant temporary access to a specific person or group. This hands-on session demonstrates how the latest NFC controller solution with customizable firmware, the PN7462, can be used for access applications. For the demonstration the PN7462 development kit will be used together with the software example to develop a door access application.
查看全文
Virtual network functions offer a great deal of flexibility, allowing for dynamic provisioning of network services. Handling network services within a VM and meeting performance requirements can be challenging. It's essential to utilize specialized hardware accelerators to meet the desired performance targets. ODP/DPDK are becoming defacto standard for NFV abstracting the hardware accelerator interfaces from VNF applications. In order to leverage the data plane capability of underlying platform the hardware acceleration can be exposed to the VMs via proprietary interfaces through direct-assignment or standardized interfaces. In this session we discuss how we can leverage the hardware acceleration on QorIQ platforms for developing optimized virtual network functions with DPDK/ODP.
查看全文
This session provides an overview of the new opportunities and challenges opened by applying Automotive Ethernet in in-vehicle Networks. We will describe how the NXP portfolio of PHYs and Switches addresses these challenges and outline the new opportunities arising from the combined portfolios after the merger. The presentation will also address ways of using the Automotive Ethernet portfolio in the industrial and automation markets. Watch Video Presentation
查看全文
Roadside Units (RSUs) will play a critical role in helping connected and automated vehicles meet their potential for increased safety, decreased commute times, and energy savings. Learn how smart RSUs could become, how secure they must be, and their relationship to the vehicles, broadband connectivity, and the cloud. Watch Video Presentation
查看全文
While many look for hypervisor based solutions when separating multiple operating systems running on multiple cores in the new embedded devices from NXP, an easier solution is often overlooked. This session will describe ARM TrustZone as a technology currently found in the ARM Cortex A family of the devices, but being introduced by ARM in other variants. A few use cases will be presented - these include secure gateway on a Layerscape LS1021 device, and an automotive instrument cluster on an i.MX6 dual core device.
查看全文