p2020rdb-pca, example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

p2020rdb-pca, example

2,626 次查看
velvettear
Contributor I

hello,

I purchased p2020rdb-pca, where can I get example windriver source?

Or is there any reference material?

标签 (2)
0 项奖励
回复
1 回复

2,562 次查看
bpe
NXP Employee
NXP Employee

Based on the information on Wind River public Website, there are multiple
Wind River products that support P2020. However, all support to Wind River
products is done by Wind River. Please contact that company directly to obtain any BSP or
example software. Available from  NXP is only a Linux-based SDK


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复