p2020rdb-pca, example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p2020rdb-pca, example

2,579件の閲覧回数
velvettear
Contributor I

hello,

I purchased p2020rdb-pca, where can I get example windriver source?

Or is there any reference material?

ラベル(2)
0 件の賞賛
返信
1 返信

2,515件の閲覧回数
bpe
NXP Employee
NXP Employee

Based on the information on Wind River public Website, there are multiple
Wind River products that support P2020. However, all support to Wind River
products is done by Wind River. Please contact that company directly to obtain any BSP or
example software. Available from  NXP is only a Linux-based SDK


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信