NFC PN7150 : Sleep Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC PN7150 : Sleep Issue

3,808 Views
karthikeyanraju
Contributor III

Hi,

 

I have used PN7150 module integrated with android Nougat 7.1.2

Followed below mentioned procedure provided by NXP.

GitHub - NXPNFCLinux/nxpnfc_android_pie: Android patches for support of PN7150 NCI based NXP NFC Con... 

Now, The read functionality is working fine.

But, There is sleep and wake-up in the NFC module when the android device goes to sleep and wake-up.

Is it possible to maintain the nfc module always ON mode ? even the android device goes to sleep mode ?

Please provide the feedback as soon as possible, since our product is in critical situation.

0 Kudos
Reply
4 Replies

3,698 Views
jimmychan
NXP TechSupport
NXP TechSupport

Basically NFC module can run autonomously, after it has been configured by host, to poll for card or remote reader while supplies (VBAT, VANT, PVDD) are kept and I2C interface is available. Indeed, when a detection occurs the host must be able to handle the notification and take action otherwise the NFC function will be locked until NFC module reset.

0 Kudos
Reply

3,698 Views
karthikeyanraju
Contributor III

Hi Jimmychan,

Thanks for your response.

Is it possible to maintain the nfc module always ON mode ? even the android device goes to sleep mode ?

Is NXP has the support for my requirement ?

0 Kudos
Reply

3,698 Views
jimmychan
NXP TechSupport
NXP TechSupport

There are four different power states. (please refer to PN7150 power states in datasheet)

The host controller control this.

0 Kudos
Reply

3,698 Views
karthikeyanraju
Contributor III

Please provide feedback on this.

Thanks and Regards,

Karthikeyan.

0 Kudos
Reply