Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

1,402 次查看
854648943
Contributor III

Hi,

When i let the router go into the network many times and leave the network, there is a situation where  return

ZPS_NWK_ENUM_INVALID_REQUEST when the router join the network through function ZPS_eAplZdoJoinNetwork( )

I looked at some of the documents and found that there was very little introduction to this problems, So i could't well

locate the cause of the problem , so i hope you can help provides some more information about the occurrence of this

problem.

The SDK is SW-4170, The coordinator uses the JN-AN-1216,Router uses the JN-AN-1217.

标记 (1)
0 项奖励
回复
1 回复

1,348 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Han, I hope you're doing well!

 

If the request is not properly formatted sometimes it could result in an error, could you please check the format and values in the request to see if it's being formed correctly?

 

After the ZPS_NWK_ENUM_INVALID_REQUEST status is returned, are you able to connect the device when trying again? After how many requests are you getting this error?

 

Could you please provide a sniffer log showing the command and responses?

 

Best regards,

Sebastian

0 项奖励
回复