Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

1,350件の閲覧回数
854648943
Contributor III

Hi,

When i let the router go into the network many times and leave the network, there is a situation where  return

ZPS_NWK_ENUM_INVALID_REQUEST when the router join the network through function ZPS_eAplZdoJoinNetwork( )

I looked at some of the documents and found that there was very little introduction to this problems, So i could't well

locate the cause of the problem , so i hope you can help provides some more information about the occurrence of this

problem.

The SDK is SW-4170, The coordinator uses the JN-AN-1216,Router uses the JN-AN-1217.

タグ(1)
0 件の賞賛
返信
1 返信

1,296件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Han, I hope you're doing well!

 

If the request is not properly formatted sometimes it could result in an error, could you please check the format and values in the request to see if it's being formed correctly?

 

After the ZPS_NWK_ENUM_INVALID_REQUEST status is returned, are you able to connect the device when trying again? After how many requests are you getting this error?

 

Could you please provide a sniffer log showing the command and responses?

 

Best regards,

Sebastian

0 件の賞賛
返信