Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee Router Join the network return ZPS_NWK_ENUM_INVALID_REQUEST

1,351 Views
854648943
Contributor III

Hi,

When i let the router go into the network many times and leave the network, there is a situation where  return

ZPS_NWK_ENUM_INVALID_REQUEST when the router join the network through function ZPS_eAplZdoJoinNetwork( )

I looked at some of the documents and found that there was very little introduction to this problems, So i could't well

locate the cause of the problem , so i hope you can help provides some more information about the occurrence of this

problem.

The SDK is SW-4170, The coordinator uses the JN-AN-1216,Router uses the JN-AN-1217.

Tags (1)
0 Kudos
Reply
1 Reply

1,297 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Han, I hope you're doing well!

 

If the request is not properly formatted sometimes it could result in an error, could you please check the format and values in the request to see if it's being formed correctly?

 

After the ZPS_NWK_ENUM_INVALID_REQUEST status is returned, are you able to connect the device when trying again? After how many requests are you getting this error?

 

Could you please provide a sniffer log showing the command and responses?

 

Best regards,

Sebastian

0 Kudos
Reply