NTAG 424 DNA Change NDEF File Settings problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG 424 DNA Change NDEF File Settings problem

ソリューションへジャンプ
2,999件の閲覧回数
MarkShen
Contributor I

I successfully modified the file settings according to the AN12196.pdf document, but an error occurred when I wanted to customize the CmdData.

The following is my CmdData:

40 00 E0 D1 F1 21 1F 00 00 44 00 00 44 00 00 40 00 00 8A 00 00 80 80 80 80 80 80 80 80 80 80 80

Received 91 7E

my ndef url data is https://my424dna.com/?picc_data=00000000000000000000000000000000&enc=7878787878787878787878787878787... 

I want to modify it to look like the picture below. What should CmdData be?

ntag.png

0 件の賞賛
返信
1 解決策
2,987件の閲覧回数
MarkShen
Contributor I

I have solved the problem

the CmdData should be 40 00 E0 D1 F1 21 1F 00 00 44 00 00 44 00 00 40 00 00 8A 00 00 80 00 00 00 00 00 00 00 00 00 00

the padding should be 80 00 00 00 00 00 00 00 00 00 00 instead of 80 80 80 80 80 80 80 80 80 80 80

元の投稿で解決策を見る

2 返答(返信)
2,988件の閲覧回数
MarkShen
Contributor I

I have solved the problem

the CmdData should be 40 00 E0 D1 F1 21 1F 00 00 44 00 00 44 00 00 40 00 00 8A 00 00 80 00 00 00 00 00 00 00 00 00 00

the padding should be 80 00 00 00 00 00 00 00 00 00 00 instead of 80 80 80 80 80 80 80 80 80 80 80

2,985件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @MarkShen ,

 

Thanks for the solution!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信