Write NT3H2211 NFC Command timing tACK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write NT3H2211 NFC Command timing tACK

1,525 Views
gb31
Contributor I

Hi

When I use WRITE or FAST WRITE command NFC in order to write a page in NT3H2211 eeprom, how much time is the tACK time ( please see datasheet at page 55 ) ?

As the eeprom write is 4,7ms long, will I receive the ack of the write command after these 4,7ms or before? 

In other words, when I receive an ack from the NFC write command sent by my app, am I sure that the data is correctlly written in the eeprom or no?

 

Thanks

0 Kudos
Reply
1 Reply

1,508 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello.

Please refer to the 10.2 Timing of the datasheet. And for the more information please refer to 

1. NFC Forum - Type 2 Tag Specification 1.0
Technical Specification
2. ISO/IEC 14443 - Identification cards - Contactless integrated circuit cards - Proximity
cards
International Standard.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply