MFRC522 Multiple SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFRC522 Multiple SPI

Jump to solution
3,369 Views
kita
Contributor I

#MFRC522  Multi SPI

Connect SPI communication (MISO / MOSI / SCK / SS) with the microcomputer
I would like to do multi-control,
When multiple units are connected,
Even if you select the device you want to communicate with the SS terminal,
Other If the MISO port of the device is output "Low"
If the selected MISO output level goes down and the communication
It will not be possible.

Is MFRC 522 supported only 1: 1 SPI?

Tags (1)
0 Kudos
Reply
1 Solution
3,151 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,152 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,151 Views
kita
Contributor I

Hello,

Thank you for answering.

◆When MFRC 522 is used in 1 (Master): N (Slave)
I plan to communicate by switching the SS terminal and MISO port to the device I want to communicate with.
Is there not a problem?

※N (Slave) unit MOSI / SCK / RST ports share.

◆Does MFRC-630 support 1 (Master): N (Slave) communication?

Best Regards,

Kan_Li

0 Kudos
Reply