MFRC522 Multiple SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,370件の閲覧回数
kita
Contributor I

#MFRC522  Multi SPI

Connect SPI communication (MISO / MOSI / SCK / SS) with the microcomputer
I would like to do multi-control,
When multiple units are connected,
Even if you select the device you want to communicate with the SS terminal,
Other If the MISO port of the device is output "Low"
If the selected MISO output level goes down and the communication
It will not be possible.

Is MFRC 522 supported only 1: 1 SPI?

タグ(1)
0 件の賞賛
返信
1 解決策
3,152件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,153件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,152件の閲覧回数
kita
Contributor I

Hello,

Thank you for answering.

◆When MFRC 522 is used in 1 (Master): N (Slave)
I plan to communicate by switching the SS terminal and MISO port to the device I want to communicate with.
Is there not a problem?

※N (Slave) unit MOSI / SCK / RST ports share.

◆Does MFRC-630 support 1 (Master): N (Slave) communication?

Best Regards,

Kan_Li

0 件の賞賛
返信