Does the SW32K3_IPCF_4.2.0_D2412 support the S32K328 chip _0-1764664238042.png Based on S32DS 3.6.3 and using the SW32K3_IPCF_4.2.0_D2412 package, I encountered the issue shown above when configuring IPCF on the S32K328 chip: the core type and core index cannot be configured. Could you please explain what is causing this? Are there any other IPCF software packages that support the #S32K328 chip Re: Does the SW32K3_IPCF_4.2.0_D2412 support the S32K328 chip Hello,
Looking at release notes, it does not support S32K328 directly.
petervlna_0-1764669786577.png
But I see no issue to use S32K358 instead.
I have also check the IPCF_S32K3_4.2.0_ReleaseNotes_Updated_D2502.pdf, but the result is the same. Since the only difference is lockstep I see no issue going with S32K358 instead.
I have no info what is the reason S32K328 is not supported directly in IPCF releases.
Best regards,
Peter
Re: Does the SW32K3_IPCF_4.2.0_D2412 support the S32K328 chip Is there any version of the IPCF software package that supports the S32K328? If not, and if a project is fully configured for the S32K324, can it run on an S32K328-based project? Re: Does the SW32K3_IPCF_4.2.0_D2412 support the S32K328 chip Hello,
Use direct derivative which is S32K358 for S32K328 to keep compatibility.
Best regards,
Peter
記事全体を表示