A Question about MPU s32k144 I have a question about MPU. In the S32K144 demo about MPU, another light will turn on after pressing the button, and then the error register of port 0 will capture the error information. My question is why the error register of port 2 will also capture this information. Is the address I visited not the FLASH address? Why does this port of SRAM_L catch this error Re: A Question about MPU s32k144 Yes, that’s expected behavior in the MPU demo. Pressing the button triggers an access violation, which is logged in the error register and indicated by the second LED. Re: A Question about MPU s32k144 image.png /* * Copyright 2020 NXP * All rights reserved. * * NXP Confidential. This software is owned or controlled by NXP and may only be * used strictly in accordance with the applicable license terms. By expressly * accepting such terms or by downloading, installing, activating and/or otherwise * using the software, you are agreeing that you have read, and that you agree to * comply with and are bound by, such license terms. If you do not agree to be * bound by the applicable license terms, then you may not retain, install, * activate or otherwise use the software. The production use license in * Section 2.3 is expressly granted for this software. */ /* ################################################################### ** Filename : main.c ** Project : mpu_memory_protection_s32k144 ** Processor : s32k144 ** Abstract : ** Main module. ** This module contains user's application code. ** Settings : ** Contents : ** No public methods ** ** ###################################################################*/ /*! ** @file main.c ** @brief ** Main module. ** This module contains user's application code. */ /*! ** @addtogroup main_module main module documentation ** @{ */ /* MODULE main */ /* Including necessary configuration files. */ #include "sdk_project_config.h" volatile int exit_code = 0; /* User includes */ /* This example is setup to work by default with EVB. To use it with other boards please comment the following line */ #define EVB #ifdef EVB #define ON 0U /* LED ON */ #define OFF 1U /* LED OFF */ #define LED_GPIO PTD /* LED GPIO type */ #define LED_RED 15U /* pin PTD15 - LED RGB on DEV-KIT */ #define LED_GREEN 16U /* pin PTD16 - LED RGB on DEV-KIT */ #define SW_GPIO PTC /* SW GPIO type */ #define SW 12U /* pin PTC12 - SW2_BTN0 on DEV-KIT */ #else #define ON 0U /* LED ON */ #define OFF 1U /* LED OFF */ #define LED_GPIO PTC /* LED GPIO type */ #define LED_RED 0U /* pin PTC0 - LED0 on Motherboard */ #define LED_GREEN 1U /* pin PTC1 - LED1 on Motherboard */ #define SW_GPIO PTC /* SW GPIO type */ #define SW 12U /* pin PTC12 - SW2_BTN0 on Motherboard */ #endif /* Protected address in Flash memory */ #define ADDRESS_PROTECT 0x0007FF04U /*! \brief The main function for the project. \details The startup initialization sequence is the following: * - startup asm routine * - main() */ /* Expected error */ mpu_access_err_info_t expectedError = { .master = FEATURE_MPU_MASTER_CORE, /* Error Core master */ .attributes = MPU_DATA_ACCESS_IN_SUPERVISOR_MODE, /* Error data access in supervisor mode */ .accessType = MPU_ERR_TYPE_READ, /* Error read access */ .accessCtr = 0xA000U, /* Error occurs on region 0 and region 2 */ .addr = ADDRESS_PROTECT, /* Error address */ #if FEATURE_MPU_HAS_PROCESS_IDENTIFIER .processorIdentification = 0U /* Error processor identifier */ #endif }; /*! * @brief The error comparator * * @Param[in] error1 The error access. * @Param[in] error2 The error access. * @return Status * - true : The errors are the same. * - false: The errors are different. */ bool ErrorCompare(mpu_access_err_info_t error1, mpu_access_err_info_t error2) { bool status = false; if ((error1.master == error2.master) && (error1.attributes == error2.attributes) && (error1.accessType == error2.accessType) && (error1.accessCtr == error2.accessCtr) && (error1.addr == error2.addr)) { status = true; #if FEATURE_MPU_HAS_PROCESS_IDENTIFIER if(error1.processorIdentification != error2.processorIdentification) { status = false; } #endif } return status; } /* HardFault Handler */ void HardFault_Handler(void) { /* Enables region 3 to grant Core read permission */ MPU_DRV_EnableRegion(MPU_INST, 3U, true); } /*! \brief The main function for the project. \details The startup initialization sequence is the following: * - startup asm routine * - main() */ int main(void) { /* Write your local variable definition here */ bool status = false; uint32_t switchStatus = 0; status_t returnCode = STATUS_ERROR; volatile uint32_t test = 0U; mpu_access_err_info_t reportedError; /* ARM Disable Debug Exception and Monitor Control Register */ *(uint32_t *)0xE000EDFC = 0x1000000; /* Initialize clock module */ CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT); CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT); /* Initialize LEDs and Button configuration */ PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0); /* LEDs off */ PINS_DRV_WritePin(LED_GPIO, LED_RED, OFF); PINS_DRV_WritePin(LED_GPIO, LED_GREEN, OFF); /* Check the initial state of the button */ switchStatus = PINS_DRV_ReadPins(SW_GPIO) & (1U << SW); /* Initialize MPU module */ returnCode = MPU_DRV_Init(MPU_INST, MPU_NUM_OF_REGION_CFG0, MPU_Cfg0); /* Check initialization */ if (returnCode == STATUS_SUCCESS) { /* Turn on LED_GREEN */ PINS_DRV_WritePin(LED_GPIO, LED_GREEN, ON); } /* Infinite loop */ for(;;) { /* Check button */ if (switchStatus != (PINS_DRV_ReadPins(SW_GPIO) & (1U << SW))) { /* Disable region 3 to ignore Core read permission */ MPU_DRV_EnableRegion(MPU_INST, 3U, false); } /* Read address in flash memory where protected by MPU */ test = *((uint32_t *)ADDRESS_PROTECT); /* Casting to void to avoid "Set but unused warnings" */ (void)test; /* Get the detail of error access on slave port 0 */ status = MPU_DRV_GetDetailErrorAccessInfo(MPU_INST, FEATURE_MPU_SLAVE_FLASH_BOOTROM, &reportedError); /* Check error status */ if (status) { /* Compare with expected error */ status = ErrorCompare(reportedError, expectedError); /* If true */ if (status) { /* Turn on LED_RED and turn off LED_GREEN */ PINS_DRV_WritePin(LED_GPIO, LED_RED, ON); PINS_DRV_WritePin(LED_GPIO, LED_GREEN, OFF); break; } } } for(;;) { if(exit_code != 0) { break; } } return exit_code; } /* END main */ /*! ** @} */ This is the program from the official example of S32K144. The screenshot above shows the registers, and both EAR0 and EAR3 have captured this error Re: A Question about MPU s32k144 Could you specify used example code and clarify a question a bit? Thanks
記事全体を表示