示例 MPC5676R-eQADC_DECFILTER_integrator_eTPU CW210 ******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and cyclically converts PMC * internal channel as specified by macros CHOOSEN_PMC_ADC_CHNL, * CHOOSEN_PMC_ADC_SCALE and CHOOSEN_PMC_ADC_COMMAND to check particular voltage * level, displaying it into terminal window. * Example configures decimation filter to scale signal down by 1/16, this is * achieved by FIR filter (user could choose real filter by proper coeficient * selection). * Example also sums filtered samples by integrator that is configured to be * triggered and zeroed by eTPU signal (for simplicity it uses general purpose * outputs). Integrated values are displayed in terminal window as well. * No external connection required excluding terminal via eSCI. * ------------------------------------------------------------------------------ * Test HW: XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU: PPC5676RDMVY1 3N23A * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys: 180MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: RAM, internal_FLASH * EVB connection: default ******************************************************************************** ******************************************************************************** * 详细说明: * 初始化 eQADC 模块,执行校准并循环转换 PMC * 由宏 CHOOSEN_PMC_ADC_CHNL 指定的内部通道, * CHOOSEN_PMC_ADC_SCALE 和 CHOOSEN_PMC_ADC_COMMAND 用于检查特定电压 * 级别,并将其显示到终端窗口中。 * 示例配置抽取滤波器将信号缩小 1/16,这是 * 由 FIR 滤波器实现(用户可以通过适当的系数选择实际滤波器 * 选择)。 * 示例还通过配置为 * 由 eTPU 信号触发并归零(为简单起见,它使用通用 * 输出)。积分值也显示在终端窗口中。 * 除通过 eSCI 的终端外,无需任何外部连接。 * ---------------------------------------------------------------------------------------------- * 测试硬件:XPC567XKIT516 - MPC567xADAT516 Rev.D、MPC567XEVBFXMB Rev.C * 微控制器: PPC5676RDMVY1 3N23A * 终端:19200-8-无奇偶校验-1 停止位-eSCI_A 上无流量控制 *系统频率:180MHz * 调试器:Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * 目标:RAM、internal_FLASH * EVB连接:默认 ********************************************************************************
記事全体を表示