Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY Hello NXP Support, We are investigating low-latency HEVC decoding on an i.MX8MP EVK. Could you confirm whether the G2 decoder supports incremental input of one picture, where complete slices are submitted before the remaining slices of that picture arrive? We are not requesting partial-picture display. We only want decoding to overlap with reception, and to output the complete picture after all slices have been decoded. 1. Platform - Hardware: i.MX8MP EVK - SoC revision reported by Linux: 1.1 - BSP: Linux 6.12.49, Walnascar - Decoder package: imx-vpu-hantro 1.39.0-ea804d0 - G2 ASIC ID: 0x67323088 - Decoder API: HevcDecDecode() - Device: /dev/mxc_hantro 2. Expected behavior The i.MX8MP Reference Manual, Rev. 3, section 16.2.5.1.8.3, describes supplying another stream buffer when the current buffer is insufficient to finish a picture, with at least one slice/VP provided for HEVC. The SDK also contains DEC_BUF_EMPTY / HEVCDEC_BUFFER_EMPTY handling and a hardware continuation path. Our expected sequence is: - Submit one complete HEVC slice from a multi-slice picture. - Receive DEC_BUF_EMPTY while preserving the current decoding state. - Submit subsequent slices of the same picture. - Receive the correctly decoded complete picture. 3. Actual behavior We reproduced the issue using a small native application calling the decoder SDK directly, without GStreamer, RTSP, camera capture, or display. Test stream: - HEVC Main, 8-bit, 1920x1080 at 60 fps - Initial IDR followed by P pictures - 17 independent CTU-row slices per picture - No B pictures Complete-AU control: All 120 pictures decode correctly. Every visible NV12 frame SHA256 matches an independent software-decoder reference. Partial-picture input: After decoding the initial IDR as a complete AU, submitting only 1, 2, 8, or 16 complete slices of the next P picture fails. DEC_BUF_EMPTY is never returned. A temporary read-only kernel diagnostic captured the actual hardware IRQ status before the ISR cleared it: - Complete picture: 0x00001100 - Incomplete picture: 0x00040100 Thus, the hardware reports timeout bit 18, not buffer-empty bit 14. The public API subsequently returns DEC_PIC_CONSUMED (13), without a decoded P picture. 4. Additional checks - Partial decoding does start: output-buffer comparisons show correct pixels for most of the supplied slice area before failure. - Disabling SAO and deblocking does not fix it. - CTU sizes 64, 32, and 16 do not fix it. - Separately generated, software-validated tile and dependent-slice streams also pass complete-AU decoding but fail partial-picture input. - We also tested the official testbench NextPacket() splitting logic in an isolated harness, with the same failure. - The published IMX8MP_1P33A Rev. 2.1 errata does not appear to describe this specific G2 input-exhaustion behavior. 5. Questions a) Is HEVC partial-picture input with BUFFER_EMPTY continuation supported on this exact G2 ASIC / i.MX8MP configuration? b) If supported, could you provide a minimal working example and the required SDK, driver, and configuration? c) Are there specific requirements for input-buffer alignment, padding, NAL boundaries, ring-buffer mode, prefetch settings, or slice organization? d) Is there a known SDK/driver limitation or silicon restriction that requires supplying a complete HEVC picture? We can provide a small test stream, the native reproducer, pixel-validation results, and IRQ logs upon request. Thank you. i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY Hello, Unfortunately, this is not documented at that level, and we need to check with internal team and there are no working example or validated SDK/driver available.  Could you please raise a ticket with your information to start with the scalation? Best regards. Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY Hello, Please check it here: Support Tickets Confidential assistance with an NXP support professional. Submit a ticket Best regards. Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY Hello Jorge, Thank you for checking. We would like to open a technical support ticket for escalation to the internal team. Could you please provide the appropriate ticket submission link and advise which product/category we should select? Please also let us know what information and attachments are required. We can provide the i.MX8MP EVK hardware details, BSP/kernel and decoder library versions, a minimal reproducer, an HEVC sample stream, and logs comparing successful complete-picture input with the hardware timeout observed during incremental slice input. Our requirement is to start decoding complete slices before the remaining slices of the same picture arrive, and output the picture only after decoding is complete. We are not requesting partial-picture display. Please also advise how to link the ticket to this forum discussion and route it to the appropriate internal decoder team. Once submitted, I will share the ticket number here. Best regards.
View full article
i.MX8MP G2 HEVC 切片输入超时,而不是 BUFFER_EMPTY 您好,NXP技术支持, 我们正在研究 i.MX8MP EVK 上的低延迟 HEVC 解码。请确认 G2 解码器是否支持单幅图像的增量输入,即先提交完整的图像切片,然后再提交该图像的其余切片? 我们并未要求显示部分图片。我们只希望解码与接收重叠,并在所有切片解码完成后输出完整的图像。 1. 平台 - 硬件:i.MX8MP EVK Linux 报告的 SoC 版本:1.1 - BSP:Linux 6.12.49,沃尔纳斯卡 - 解码器软件包:imx-vpu-hantro 1.39.0-ea804d0 - G2 ASIC ID:0x67323088 - 解码器 API:HevcDecDecode() - 设备:/dev/mxc_hantro 2. 预期行为 i.MX8MP 参考手册,修订版 3,第 16.2.5.1.8.3 节描述了当当前缓冲区不足以完成一帧画面时,如何提供另一个流缓冲区,并为 HEVC 提供至少一个切片/VP。 SDK 还包含 DEC_BUF_EMPTY / HEVCDEC_BUFFER_EMPTY 处理和硬件延续路径。 我们预期的序列是: - 从多切片图像中提交一个完整的 HEVC 切片。 - 接收 DEC_BUF_EMPTY,同时保持当前解码状态。 - 提交同一张图片的后续切片。 - 接收到正确解码的完整图像。 3. 实际行为 我们使用一个直接调用解码器 SDK 的小型原生应用程序重现了该问题,没有使用 GStreamer、RTSP、摄像头捕获或显示。 测试流: - HEVC 主视频,8 位,1920x1080 分辨率,60 帧/秒 - 初始IDR,随后是P图片 每张图片包含 17 个独立的 CTU 行切片 - 没有B图片 完全AU控制: 全部120张图片均解码正确。每个可见的 NV12 帧的 SHA256 值都与一个独立的软件解码器参考值相匹配。 局部图像输入: 将初始 IDR 解码为完整的 AU 后,仅提交下一个 P 图片的 1、2、8 或 16 个完整切片均会失败。DEC_BUF_EMPTY 永远不会返回。 在中断服务例程 (ISR) 清除中断请求 (IRQ) 之前,一个临时的只读内核诊断程序捕获了实际的硬件 IRQ 状态: - 完整图片:0x00001100 - 图片不完整:0x00040100 因此,硬件报告的是超时位 18,而不是缓冲区为空位 14。随后,公共 API 返回 DEC_PIC_CONSUMED (13),但没有解码后的 P 图片。 4. 附加检查 - 部分解码开始:输出缓冲区比较显示,在失败之前,大部分提供的切片区域像素都是正确的。 - 禁用 SAO 和解除阻塞并不能解决问题。 - CTU 尺寸 64、32 和 16 都无法解决这个问题。 - 单独生成的、经过软件验证的图块流和相关切片流也能通过完整的 AU 解码,但无法通过部分图像输入。 - 我们还在一个独立的测试环境中测试了官方测试平台 NextPacket() 的拆分逻辑,结果出现了同样的故障。 - 已发布的 IMX8MP_1P33A Rev. 2.1 勘误表似乎没有描述这种特定的 G2 输入耗尽行为。 5. 问题 a) 此 G2 ASIC / i.MX8MP 配置是否支持带有 BUFFER_EMPTY 延续的 HEVC 部分图像输入? b) 如果支持,能否提供一个最小可运行示例以及所需的 SDK、驱动程序和配置? c) 对输入缓冲区对齐、填充、NAL 边界、环形缓冲区模式、预取设置或切片组织是否有具体要求? d) 是否存在已知的 SDK/驱动程序限制或芯片限制,需要提供完整的 HEVC 图像? 我们可以根据要求提供小型测试流、原生复现程序、像素验证结果和 IRQ 日志。 谢谢! i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY 你好, 遗憾的是,这方面没有文档说明,我们需要咨询内部团队,目前没有可用的示例或经过验证的SDK/驱动程序。 请您提交一份包含相关信息的工单,以便我们启动升级流程。 顺祝商祺! Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY 你好,豪尔赫, 感谢您的核实。我们希望提交一份技术支持工单,以便将问题升级至内部团队。 请问能否提供相应的工单提交链接,并告知我们应该选择哪个产品/类别?请也与我们联系,告知需要哪些信息和附件。 我们可以提供 i.MX8MP EVK 硬件详情、电路板支持包。/内核和解码器库版本、最小复现程序、HEVC 样本流以及日志,以比较成功的完整图像输入与增量切片输入期间观察到的硬件超时。 我们的要求是,在同一幅图像的其余切片到达之前,开始解码已完成的切片,并且仅在解码完成后才输出图像。我们不要求显示部分图像。 请问如何将此工单链接到此论坛讨论并将其转交给相应的内部解码团队?提交后,我会在这里分享票号。 顺祝商祺! Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY 你好, 请点击此处查看: 支持工单 获取恩智浦支持专家提供的保密帮助。 提交工单 顺祝商祺!
View full article
lpx43xx usb0 主机 HID 键盘 你好 我正在使用LPX4357,并且已经成功完成了通过USB HID的键盘接口连接。但是当我连接条码扫描器时,扫描后出现硬故障……只读取/检测到一个字节,然后就出现硬故障……请问这是什么原因造成的?或者有什么建议吗? 请大家帮忙! LPC43xx 外设 USB Re: lpx43xx usb0 host HID keyboard 你好, 我正在尝试连接USB条形码扫描器。我正在使用 LPCOpen 键盘主机示例。连接USB键盘时,系统能够正确接收到输入的任何数据。但是使用条形码扫描器时,扫描的条形码数据仅在开机时接收一次。这种情况有时也会发生,但并非总是如此。每次我从条码扫描器接收到数据后,下次扫描时总是收到HID_Host_IsReportReceived 标志为 false 的情况,导致之后无法从条码扫描器接收到数据。这是管道问题吗?我该如何解决? 控制器 LPC4337 条形码制作 Zebronics。 型号 BS2H1000 此致问候 Re: lpx43xx usb0 host HID keyboard 您好, 我正在尝试连接USB条形码扫描器。我正在使用 LPCOpen 键盘主机示例,我已经获取到键盘按键了。但是当我连接条形码扫描器时,它显示设备已枚举,但无法读取条形码数据。请问需要对键盘代码示例进行哪些修改才能读取条形码数据? 控制器 LPC4337 条形码制造新大陆。 型号 NLS-HR11 温暖的问候。 Re: lpx43xx usb0 host HID keyboard 问题已解决,谢谢。 Re: lpx43xx usb0 host HID keyboard 您的项目是基于lpcopen示例吗?如果是,是哪一个?需要修改吗? 请追踪出错的运行环节?是吗? 列举清楚了吗? Re: lpx43xx usb0 host HID keyboard 我正在使用 LPCUSBLIB 库将 USB 条码扫描器与 LPC4337 控制器连接起来。我想知道清除管道缓冲器的条件是什么。有时候我能正确收到完整的条形码。有时扫描第一个字符后就收不到任何数据,而且USB线还会卡住,导致之后多次扫描条形码都收不到任何数据。 Re: lpx43xx usb0 host HID keyboard 您好@RDGC_member 这个帖子是5年前创建的。我建议你在LPC论坛创建一个新帖子。NXP技术支持会为您提供帮助。 https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc 谢谢! 张军
View full article
RT1172は電源投入時に起動しない 皆さん、こんにちは。 弊社ではRT1172をベースにしたカスタム基板を製造しています。GUI FLASHツール(「実行時にターゲットをリセット」オプション付き)を使用する場合、またはデバッグモードでは、プログラムは期待どおりに起動し、動作します。しかし、ボードの電源を入れても、起動反応が全く見られません。XIP_BOOT_HEADER_ENABLE 定義が 1 に設定されている場合、IVT をイメージに追加する必要があります。このような問題をデバッグする方法について、何かアイデアをお持ちの方はいらっしゃいますか? ちなみに、RT1176をベースにした非常によく似た設計のボードももう1つあります。このボードは、(我々が確認した限りでは)RT1172ボードと同じ構成で、期待どおりに起動しています。 よろしくお願いいたします マティアス Re: RT1172 does not boot on Power up この問題は未解決のままですか? RT1172でも同様の現象が見られます。 RT1172のBootRom NXPコードにおいて、ITC RAMが64KB以上予約されている場合にFlexSPI-FlashからFlexRAMにロードする際に既知の問題があります。 Re: RT1172 does not boot on Power up こんにちは、 @ingdb さん、 最新情報をお知らせいただきありがとうございます。 あなたの抱えている問題について、もう少し明確にする必要があります。 1. J-Link 経由でプログラムをダウンロードしたとき (他のデバッガーは試していません)、ボードは動作し、アプリケーションは実行され、USB も動作し、すべてが期待どおりでした。 =>kerry: この方法をダウンロードする際、IDEを使用しますか、それとも使用しませんか?それとも、アプリケーションをダウンロードするためにJLINK CommanderやJflashだけを使うのでしょうか? あなたが使用しているアプリケーションプロジェクトは何ですか?問題のデバッグプロジェクトと同じアプリでしょうか? 2.しかし、ボードの電源を入れた際に、J-Linkを使用してプログラムをダウンロードして起動しない場合、アプリケーションは0x223104で停止してしまいました。 =>ケリー:JLINKを使ってダウンロードしない場合、JLINKは使用するものの、MCUXPresso IDEでJLINKデバッグを使用すると問題が発生するということですか? あなたが使用しているプロジェクトは何ですか?JLINKでダウンロードして動作確認済みのアプリですか? 3. 0x223104 は ROM アドレスです。プロジェクトのデバッグ構成でリセットの選択を解除してみてください。 以下のブログ記事もそれを証明しています。 https://www.cnblogs.com/henjay724/p/15725966.html よろしくお願いいたします。 kerry Re: RT1172 does not boot on Power up こんにちは、 J-Link経由でプログラムをダウンロードする際(他のデバッガーは試していません)、ボードは正常に動作し、アプリケーションも実行され、USBも正常に動作するなど、すべてが期待どおりです。 つまり、私のボードにはソフトウェアの問題もハードウェアの問題もありません。 しかし、ボードの電源を入れた際に、J-Linkを使用してプログラムをダウンロードして起動しない場合、アプリケーションは0x223104で停止してしまいました。(下記の私のコメントをご覧ください。) JTAG以外のブートユーティリティは試していません。ソフトウェアが動作していることから、XIPを使用しているためフラッシュメモリは正しくプログラムされていると想定しています。 よろしくお願いします マティアス Re: RT1172 does not boot on Power up こんにちは、 @ingdb さん、 最新情報をありがとうございます。 あなたはこう言いました:ボードが起動しています JLINK以外のデバッガーを使用した場合、どのように起動していると思いますか? SPTまたはMCUbootUtilityツールを使用してダウンロードを試みましたか?ツールを使ってアプリをダウンロードしましたが、それが起動するかどうかは関係ありませんか? また、あなたのプロジェクトがRT1172に適しているかどうかについても考えています。ハードウェアに問題がない場合は、ソフトウェアも確認する必要があります。 よろしくお願いいたします。 kerry Re: RT1172 does not boot on Power up こんにちは、ケリーさん。 ご協力ありがとうございます。しかし、ハードウェアの問題はありません。ボードは起動しますが、J-Linkでデバッグしている時だけで、ボードの電源を入れただけでは起動しません。ブートモードはFlexSPI1、Q-SPI、NOR-FLASHを使用した内部ブートモードとして構成されています。 よろしくお願いいたします。 マティアス   Re: RT1172 does not boot on Power up こんにちは、 @ingdb さん、 現在、どのデバッガーを使用していますか? まず、JLINKを使ってRT1172ボードを接続してみて、ARMコアが見つかるかどうか確認することをお勧めします。そうでない場合は、ハードウェアに問題があることを意味します。 はいの場合、RAMコードをチップにダウンロードして動作するかどうかを確認し、動作するまで繰り返します。次に、フラッシュにダウンロードできるかどうかを確認し、BOOT_CFG、BOOT_MODEピンも確認する必要があります。boot_cfgが使用するフラッシュの要件を満たしていること、およびboot_modeがシリアルダウンロードモードではなく内部ブートモードであることを確認してください。 お役に立てれば幸いです! よろしくお願いいたします。 kerry Re: RT1172 does not boot on Power up 電源投入後に起動しないターゲットを調べたところ、ここで止まっていることがわかりました。 Re: RT1172 does not boot on Power up この件に関して何か新しい情報はありませんか? これまではBoot Smallでこの問題が起きたので、待機状態にしています。今はもっと大きなブートが必要で、この問題がそれを阻んでいます。Segger社と共同で分析を行った結果、問題の原因はNXPブートローダーにあることが判明しました。 分析結果を添付しました。 よろしくお願いいたします Re: RT1172 does not boot on Power up 実は、問題点を見つけました(私のミスです)。間違ったブートヘッダーを使用していました。チケット内の私のコメントは無視して構いません。元のコメントのみを考慮する必要があります。誤解を招いてしまい申し訳ありません。 よろしくお願いいたします
View full article
Matter Stack 移植到 MIMXRT700-EVK (MIMXRT798S) — 持久存储初始化失败 您好, 我目前正在使用 MCUXpresso SDK 和 VS Code 将 NXP Matter 协议栈移植到 MIMXRT700-EVK (MIMXRT798S)板上。该板使用基于 IW612 芯片组的外部 Murata Type 2EL 无线模块。 开发设置和变更 我通过 VS Code 下载并设置了 Matter MCUXpresso SDK 工作区。该工作区位于matter_mcuxpresso/mcuxsdk 。 我针对RT700进行了以下方面的修改: Matter:修改了中间件/matter下的文件,用于 RT700 平台集成。 无线框架:增加了对外部 Murata Type 2EL (IW612) 无线模块的 RT700 特定平台支持和集成。 链接器脚本:使用 RT700 SDK 提供的MIMXRT798Sxxxx_cm33_core0_flash.ld作为参考,并根据 Matter 应用程序的内存布局和 NVS 存储配置对其进行了修改。 问题描述 Matter 应用程序构建成功,并且可以使用 LinkServer 进行编程。但是,运行时初始化失败,并在src/platform/nxp/common/NXPConfigNVS.cpp中的以下调用处出现CHIP_ERROR_PERSISTED_STORAGE_FAILED错误: flash_init(fa->fa_dev) CHIP_ERROR_PERSISTED_STORAGE_FAILED 链接器脚本附件 我将附上修改后的MIMXRT798Sxxxx_cm33_core0_flash.ld链接器脚本供您参考。该脚本基于 RT700 SDK 提供的链接器脚本,并针对 Matter 应用程序的内存布局和 NVS 存储配置进行了修改。 需要支持 请问您能否帮忙澄清一下: 如何在RT700-EVK上配置Matter持久存储的闪存设备和驱动程序? 是否还需要任何针对 RT700 的额外闪存驱动程序或 NVS 集成步骤? 修改后的链接器脚本或 NVS 内存布局是否会导致flash_init()失败? 我希望您能指导我如何解决这个问题。 谢谢! 评估板 Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure 嗨@Aparna1 , 谢谢你的提问! 我已审核提供的链接脚本。它目前引用了以下与 FlexSPI 相关的对象: *(EXCLUDE_FILE( ... *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o* ) .text*) 但是,MIMXRT700 使用的是 XSPI 控制器。请确认该应用程序已链接到正确的 RT700 XSPI 闪存后端,并且 fa->fa_dev 指的是该设备,而不是其他 i.MX RT 平台使用的 FlexSPI 后端。 另请检查映射文件中的 flash_init() 、闪存擦除/编程功能以及相关的 XSPI_* 功能。这些功能及其所需的配置数据应该位于 RAM 中,而不是 XIP 闪存区域中。 我们建议按以下顺序检查端口: 验证 SDK 中的官方 RT700 XSPI 或非 闪存示例; 确认 fa->fa_dev 使用正确的XSPI后端; 验证闪存操作代码是否确实从 RAM 中执行; 然后检查 NVS 地址、扇区对齐方式,以及驱动程序是否期望绝对地址或设备相对偏移量。 此致, 加文 Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure 嗨@Gavin_Jia 我已根据建议修改了链接器文件( MIMXRT798Sxxxx_cm33_core0_flash.ld ),并更新了与 XSPI 相关的配置。但是,问题仍然存在, flash_init()函数仍然失败。 我已将修改后的MIMXRT798Sxxxx_cm33_core0_flash.ld文件分享给您审核。请您检查一下链接器配置,并指导我还需要做哪些更改才能解决 XSPI 闪存初始化问题? 谢谢! Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure 嗨@Aparna1 , 谢谢你的更新。 我仍然建议使用 `mimxrt700evk_flash_component_octal_xspi_cm33_core0` 项目及其相关的链接器脚本(LD 文件)作为基准。请确保与闪存操作相关的代码已成功移植,然后再继续移植到 Matter。 仅凭链接器脚本无法对您的移植项目进行全面诊断,因此我只能提供一些建议。感谢您的理解。 以下是我审阅您的剧本后发现的一些问题: 1.XSPI 代码可能仍然链接到 XIP 区域 在 .text 部分,脚本首先排除 XSPI 和 NVS 相关对象文件: *(EXCLUDE_FILE( ……​​ *fsl_xspi_nor_flash.c* *mflash_drv.c.o* *fsl_xspi.c.o* ) 。文本*) 然而,脚本后面包含无条件规则:   *(。文本) *(。文本*) *(.rodata) *(.rodata*) 后面的规则可以再次收集先前排除的输入部分,并将它们放回位于外部 XSPI Flash 区域的 m_text 中。 因此,当前的 EXCLUDE_FILE 规则不能保证 XSPI/NVS 执行路径是从 RAM 运行的。 2. RAM 部分仍然包含 FlexSPI 对象,而不是 RT700 XSPI 对象。 .data 部分目前将以下代码放入 RAM 中: *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o*   然而,RT700 使用的是 XSPI 控制器。 3. fsl_xspi_nor_flash 常量并未始终如一地移至 RAM 中 fsl_xspi_nor_flash 包含在 .text* 排除列表中,但不包含在 .rodata* 排除列表中。 如果您对修改后的链接器脚本或最终图像有任何疑问,从映射文件中提取关键信息是一种值得尝试的调试方法。 此致, 加文 Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure 你好@Gavin_Jia 之前报告的 flash_init 问题( CHIP_ERROR_PERSISTED_STORAGE_FAILED )已解决。应用程序现在可以成功完成 flash 初始化过程。 但是,在使用外置 Murata Type 2EL (IW612) M.2 模块的 RT700-EVK 进行 IW612 Wi-Fi 初始化时,我目前遇到了一个新问题。 启动过程中会出现以下错误信息: [wifi_io] Error: SDIO - FW Ready Registers not set [wifi] Error: sd_wifi_init failed. status code -1 [wlcm] Error: wifi init/reinit failed. status code -1 ASSERT ERROR " WM_SUCCESS == ret " 请您协助我们调查此问题,并提出所需的 SDIO 配置、固件下载顺序或 IW612 初始化所需的任何 RT700 特定更改? 谢谢
View full article
Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi, I am currently working on porting the NXP Matter stack to the MIMXRT700-EVK (MIMXRT798S) using the MCUXpresso SDK and VS Code. The board uses an external Murata Type 2EL wireless module based on the IW612 chipset. Development Setup and Changes I downloaded and set up the Matter MCUXpresso SDK workspace through VS Code. The workspace is located at matter_mcuxpresso/mcuxsdk. I have made RT700-specific changes in the following areas: Matter: Modified files under middleware/matter for RT700 platform integration. Wireless framework: Added RT700-specific platform support and integration for the external Murata Type 2EL (IW612) wireless module. Linker script: Used the RT700 SDK-provided MIMXRT798Sxxxx_cm33_core0_flash.ld as the reference and modified it for the Matter application's memory layout and NVS storage configuration. Issue Description The Matter application builds successfully and can be programmed using LinkServer. However, runtime initialization fails with CHIP_ERROR_PERSISTED_STORAGE_FAILED at the following call in src/platform/nxp/common/NXPConfigNVS.cpp: flash_init(fa->fa_dev) CHIP_ERROR_PERSISTED_STORAGE_FAILED Linker Script Attachment I will attach the modified MIMXRT798Sxxxx_cm33_core0_flash.ld linker script for reference. It is based on the RT700 SDK-provided linker script and includes changes for the Matter application's memory layout and NVS storage configuration. Support Required Could you please help clarify: How should the flash device and driver be configured for Matter persistent storage on the RT700-EVK? Are any additional RT700-specific flash driver or NVS integration steps required? Could the modified linker script or NVS memory layout contribute to the flash_init() failure? I would appreciate your guidance on resolving this issue. Thank you. Evaluation Board Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi @Aparna1 , Thanks for your questions! I reviewed the provided linker script. It currently references the following FlexSPI-related objects: *(EXCLUDE_FILE( ... *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o* ) .text*) However, the MIMXRT700 uses the XSPI controller. Please confirm that the application is linked with the correct RT700 XSPI flash backend and that fa->fa_dev refers to this device, rather than to a FlexSPI backend used by other i.MX RT platforms. Please also check the map file for flash_init() , the flash erase/program functions, and the related XSPI_* functions. These functions and their required configuration data should be located in RAM rather than in the XIP flash region. We suggest checking the port in this order: Verify the official RT700 XSPI NOR flash example from the SDK; Confirm that fa->fa_dev uses the correct XSPI backend; Verify that the flash-operation code actually executes from RAM; Then check the NVS address, sector alignment, and whether the driver expects an absolute address or a device-relative offset. Best regards, Gavin Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure hi @Gavin_Jia  I have modified the linker (MIMXRT798Sxxxx_cm33_core0_flash.ld) file based on the suggested changes and updated the XSPI-related configuration. However, the issue still persists, and the flash_init() function continues to fail. I am sharing the modified MIMXRT798Sxxxx_cm33_core0_flash.ld file for your review. Could you please check the linker configuration and guide me on what additional changes are required to resolve the XSPI flash initialization issue? Thank you. Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi @Aparna1 , Thanks for your update. I still recommend using the `mimxrt700evk_flash_component_octal_xspi_cm33_core0` project—along with its associated linker script (LD file)—as a baseline. Please ensure that the code related to flash operations is successfully ported before moving on to Matter. It is not possible to fully diagnose your porting project based solely on the linker script, so I can only offer a few suggestions. Thank you for your understanding. Below are some issues I identified after reviewing your script: 1. The XSPI code may still be linked into the XIP region In the .text section, the script first excludes the XSPI and NVS-related object files: *(EXCLUDE_FILE( ... *fsl_xspi_nor_flash.c* *mflash_drv.c.o* *fsl_xspi.c.o* ) .text*) However, the script later contains unconditional rules:   *(.text) *(.text*) *(.rodata) *(.rodata*) These later rules can collect the previously excluded input sections again and place them back into m_text , which is located in the external XSPI Flash region. Therefore, the current EXCLUDE_FILE rules do not guarantee that the XSPI/NVS execution path is running from RAM. 2. The RAM section still contains FlexSPI objects instead of the RT700 XSPI objects The .data section currently places the following code into RAM: *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o*   However, RT700 uses the XSPI controller.  3. fsl_xspi_nor_flash constants are not consistently moved to RAM fsl_xspi_nor_flash is included in the .text* exclusion list, but it is not included in the .rodata* exclusion list. If you are uncertain about a modified linker script or the final image, extracting key information from the map file is a debugging approach worth trying. Best regards, Gavin Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hello @Gavin_Jia  The previously reported flash_init  issue (CHIP_ERROR_PERSISTED_STORAGE_FAILED) has been resolved. The application now successfully completes the flash initialization process. However, I am currently facing a new issue during IW612 Wi-Fi initialization on the RT700-EVK with the external Murata Type 2EL (IW612) M.2 module. The following error messages appear during startup: [wifi_io] Error: SDIO - FW Ready Registers not set [wifi] Error: sd_wifi_init failed. status code -1 [wlcm] Error: wifi init/reinit failed. status code -1 ASSERT ERROR " WM_SUCCESS == ret "  Could you please help us investigate this issue and suggest the required SDIO configuration, firmware download sequence, or any RT700-specific changes needed for IW612 initialization? Thank You 
View full article
lpx43xx usb0 host HID keyboard HI  i'm using lpx4357 and successfully completed keyboard interfacing using USB HID but when i connect a barcode scanner hard fault occurs after scanning .. only one byte read / detected and then it goes to hard fault.. can i get some ideas why this could be happen?? or any suggestions ? please help! LPC43xx Peripherals USB Re: lpx43xx usb0 host HID keyboard Hello, I am trying to interface the USB barcode scanner . I am using the LPCOpen Keyboard Host example. while connecting Usb key board ,system receives proper data what ever entered. but with barcode scanner, the barcode data scanned, is received only once at power on time . that is also happens sometimes not always. When ever i received data from barcode scanner , for the next scanning i  always receive HID_Host_IsReportReceived flag false. which causes no data receive from barcode after that.  Is there any pipiline issue? how can i resolve it?   Controller LPC4337 Barcode Make Zebronics. Model BS2H1000 Regards. Re: lpx43xx usb0 host HID keyboard Hi, I am trying to interface the USB barcode scanner. I am using the LPCOpen Keyboard Host example, I am getting the keyboard keys. But when I connect the barcode scanner, it shows device is enumerated, but now able to read the barcode data. Can you please let me know, what modification need to be done in the keyboard code example to read the barcode data.  Controller LPC4337 Barcode Make Newland. Model NLS-HR11 Warm regards. Re: lpx43xx usb0 host HID keyboard issue solved .. thank you.. Re: lpx43xx usb0 host HID keyboard Is your project based on lpcopen demo ? if yes which one? any revise ? Please track where runs to error? Does it enumerate well? Re: lpx43xx usb0 host HID keyboard Hi @RDGC_member  This thread was created 5 years ago. I suggest you to create a new thread in LPC forum. The NXP support will help you. https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc Thanks, Jun Zhang Re: lpx43xx usb0 host HID keyboard I am using LPCUSBLIB library for interfacing USB barcode scanner with LPC4337 controller. i wanted to know that which are the conditions cause to clear the  pipe buffer. some times i receive full barcode properly. some times after first character nothing is received also the usb line gets stuck so that after that nothing is received for several times barcode scanning. 
View full article
FRDM-A-S32K356)The PWM signal is not being output I am planning to change the MCU from the S32K344 to the S32K356 in order to reduce processing time. I ported an S32K344-based FOC project to the S32K356 using the FRDM-A-S32K356 evaluation board. However, I am unable to obtain any PWM output signals to drive the inverter. Could you please advise me on the possible causes and the settings I should check? Specifically, I expect the PWM signals to be output from the following pins on connector JA1: Pin 15 (PTA0) Pin 13 (PTA1) Pin 11 (PTA3) Pin 9 (PTA2) Pin 7 (PTD3) Pin 5 (PTD2) Steps to Reproduce the Issue: Open S32K_PMSM_Sensorless.pmpx. Set "Speed Required" to 100 rpm. Change "On/Off" from "Stop" to "Run". Check the PWM output signals on the specified JA1 pins. Expected behavior: PWM signals should be output from the specified JA1 pins. Actual behavior: No PWM signals are observed on the specified JA1 pins. Re: FRDM-A-S32K356)The PWM signal is not being output Hi @Tomato1  First, please note that S32K3_S32M27x Real-Time Drivers Version 3.0.0 P07 were not tested with the S32K356 devices. Therefore, we cannot guarantee proper functionality when using this version with the S32K356. Official support for the S32K356 was introduced starting with S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0. For this reason, we recommend using the latest software releases and development tools that support the S32K356 to ensure compatibility and avoid potential issues related to unsupported software versions. Additionally, as a reference for your motor-control development, there is an example application available that demonstrates sensorless Field-Oriented Control (FOC) of a Permanent Magnet Synchronous Motor (PMSM) with dual-shunt current sensing. This example is based on the NXP DEVKIT-MOTORGD and FRDM-A-S32K344 and can be accessed through the NXP Application Code Hub. BR, VaneB
View full article
RT1172 在开机时无法启动 大家好, 我们有一款基于 RT1172 的定制主板。使用 GUI Flash 工具(使用 " 执行时 RESET 目标 ")或处于调试模式时,程序将按预期启动和运行。但是在给主板加电时,我看不到任何启动反应。如果 XIP_BOOT_HEADER_ENABLE 定义设为 1,则应将 IVT 添加到图像中。有人知道如何调试这样的问题吗? 顺便说一句,我们还有另一种基于 RT1176 的非常相似的设计,该主板按预期启动,其配置(据我们所见)与 RT1172 主板相同。 顺祝商祺! 马蒂亚斯 Re: RT1172 does not boot on Power up 这个问题一直没有解决? 我在 RT1172 中观察到类似情况,当 ITC RAM 保留> 64 KBytes 时,从 FlexSPI 闪存加载到 FlexRAM 时,RT1172 的 BootRom NXP 代码存在一些已知问题? Re: RT1172 does not boot on Power up 你好@ingdb, 感谢您提供的最新信息。 还需要更清楚地了解您的问题。 1。通过 J-Link 下载程序时(我从未尝试过任何其他调试器),主板正在运行,应用程序正在运行,USB 正在运行等等,一切都如预期。 =>kerry:这种方法何时下载,是否有 IDE?还是只用 JLINK 指令器或 Jflash 下载应用程序? 您使用的应用项目是什么?是否与问题调试项目的应用程序相同? 2。但是,当开启主板而不使用 J-Link 下载和启动程序时,应用程序卡在 0x223104 =>Kerry:如果不使用 JLINK 下载,您的意思是,仍然使用 JLINK,只是使用 JLINK 调试与 MCUXPresso IDE 相结合的问题吗? 您使用的是什么项目?使用 JLINK 下载的应用程序是否可以正常工作? 3.0x223104 是 ROM 地址,我想你可以尝试在项目中取消选择 RESET,调试配置。 下面的博客也证明了这一点: https://www.cnblogs.com/henjay724/p/15725966.html 顺祝商祺! kerry Re: RT1172 does not boot on Power up 你好,通过 J-Link 下载程序 时(我从未尝试过任何其他调试器),主板正在运行,应用程序正在运行,USB 正在运行等等,一切都如预期。 因此,我的主板上没有软件,也没有硬件问题。 但是,当启动板而不使用J-Link下载和启动程序时,应用程序卡在0x223104。(见我下面的评论)。 除了 JTAG 之外,我没有尝试过任何其他启动工具,因为软件正在运行,我假设我在使用 XIP 时对闪存进行了正确的编程。 最诚挚的问候 Matthias Re: RT1172 does not boot on Power up 你好@ingdb、 感谢您提供的最新信息。 你提到:主板正在启动 使用其他调试器而不是 JLINK,你觉得它正在启动? 你是否尝试使用 SPT 或 mcubootUtilityt 工具下载,使用该工具下载应用程序,无论启动与否? 我还想知道,您的项目是否适合 RT1172?如果硬件没有问题,那么还需要检查软件。 顺祝商祺! kerry Re: RT1172 does not boot on Power up 嗨,凯瑞、 感谢你的帮助,但我们没有硬件问题,主板正在启动,但只有在使用 J-Link 进行调试时,启动主板时它才无法启动。使用 FlexSPI1、Q-SP I、或非-FLASH 将启动模式配置为内部启动模式 顺祝商祺! 马蒂亚斯   Re: RT1172 does not boot on Power up 你好@ingdb、 您现在使用哪个调试器? 不管你能不能找到 Arm 内核,我建议你先用 JLINK 来连接你的 RT1172 板?如果没有,说明硬件有问题。 如果是,你可以将 RAM 代码下载到芯片上,检查它是否能正常工作,直到它能正常工作,然后你可以检查它是否可以下载到闪存中,然后你还需要检查 BOOT_CFG、BOOT_MODE 引脚,确保 boot_cfg 满足你使用的闪存要求,boot_mode 应该是内部启动模式,而不是串行下载模式。 希望它能帮到你! 顺祝商祺! kerry Re: RT1172 does not boot on Power up 在检查加电后无法启动的目标时我发现它卡在这里了 Re: RT1172 does not boot on Power up 关于这个问题有什么新进展吗? 到目前为止,我还没有机会解决与此问题相关的 启动 较小的问题,所以我暂时搁置了这个问题。现在我需要更大的启动空间,但这个问题阻碍了我。我用Segger进行了一些分析,问题出在NXP引导加载程序上。 分析结果已附上。 问候 Re: RT1172 does not boot on Power up 实际上我已经找到问题所在了(是我的错)。我之前使用了错误的启动头文件。我的工单评论可以忽略,只有原始评论才需要考虑。很抱歉造成了误会。 问候
View full article
i.MX8MP G2 HEVCスライス入力タイムアウト(BUFFER_EMPTYではなく) こんにちは、NXPサポートの皆さん、 私たちはi.MX8MPのEVKで低レイテンシHEVCデコードを調査しています。G2デコーダが1枚の画像のインクリメンタル入力をサポートしているか確認してもらえますか?つまり、残りの画像の残りのスライスが届く前に完全なスライスを提出する形です。 部分的な画像表示を要求しているわけではありません。復号処理は受信処理と重複するようにし、すべてのスライスが復号された後に完全な画像を出力するようにしたい。 1. プラットフォーム - ハードウェア:i.MX8MP EVK - Linuxが報告したSoCリビジョン:1.1 - BSP:Linux 6.12.49、ウォルナスカー - デコーダパッケージ:imx-vpu-hantro 1.39.0-ea804d0 - G2 ASIC ID:0x67323088 - デコーダAPI:HevcDecDecode() - デバイス:/dev/mxc_hantro 2. 期待される動作 i.MX8MPリファレンスマニュアル、Rev. 3、セクション16.2.5.1.8.3では、現在のバッファが映像を完成させるのに不十分な場合、HEVC用に少なくとも1つのスライス/VPを提供する別のストリームバッファを提供する方法について説明しています。 SDKにはDEC_BUF_EMPTY/HEVCDEC_BUFFER_EMPTY処理とハードウェア継続パスも含まれています。 想定される手順は以下のとおりです。 ・複数スライス画像から、完全なHEVCスライスを1つ提出してください。 - 現在のデコード状態を維持したまま、DEC_BUF_EMPTYを受信します。 同じ画像の連続したスライスを提出してください。 正しくデコードされた完全な画像を受信する。 3. 実際の行動 私たちは、GStreamer、RTSP、カメラキャプチャ、ディスプレイを使わず、デコーダーSDKを直接呼び出す小さなネイティブアプリケーションを使って問題を再現しました。 テストストリーム: - HEVCメイン、8ビット、1920x1080、60fps - 初期IDRに続いてP画像 - 画像ごとに17個の独立したCTU行スライス - B画像なし 完全なAU制御: 120枚すべての画像が正しくデコードされました。見えるすべてのNV12フレームのSHA256は独立したソフトウェアデコーダ参照と一致します。 部分的な画像入力: 最初のIDRを完全なAUとしてデコードした後、次のPピクチャの完全なスライスを1つ、2つ、8つ、または16つだけ送信すると失敗します。DEC_BUF_EMPTY は決して返されません。 一時的な読み取り専用カーネル診断により、ISRがハードウェアIRQをクリアする前に、実際のハードウェアIRQステータスが取得されました。 - 完全な画像: 0x00001100 - 画像が不完全です: 0x00040100 したがって、ハードウェアはバッファが空であることを示すビット14ではなく、タイムアウトを示すビット18を報告する。その後、公開APIはデコードされたP画像なしでDEC_PIC_CONSUMED(13)を返します。 4. 追加チェック - 部分的なデコードが開始されます。出力バッファの比較では、エラーが発生する前に、指定されたスライス領域の大部分で正しいピクセルが示されています。 SAOを無効にしてブロックを解除しても、問題は解決しません。 - CTUサイズ64、32、16では解決しません。 - 別途生成され、ソフトウェアで検証されたタイルおよび依存スライスストリームも完全AUデコードは通過しますが、部分的なピクチャー入力には失敗します。 - また、公式テストベンチのNextPacket()分割ロジックを独立したハーネスでテストしましたが、同じエラーが発生しました。 公開されているIMX8MP_1P33A Rev. 2.1の正誤表には、この特定のG2入力枯渇動作については記載されていないようです。 5. 質問 a) このG2 ASIC / i.MX8MP構成において、BUFFER_EMPTY継続を伴うHEVC部分画像入力はサポートされていますか? b) もし対応しているなら、最低限の動作例と必要なSDKs、ドライバ、設定を提供していただけますか? c) 入力バッファのアライメント、パディング、NAL境界、リングバッファモード、プリフェッチ設定、またはスライスの構成に特定の要件があるか? d) 完全なHEVC画像を提供する必要がある既知のSDKsやドライバの制限、シリコン制限はありますか? ご要望に応じて、小規模なテストストリーム、ネイティブリプロダクション、ピクセル検証結果、IRQログを提供できます。 よろしくお願いします。 i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY こんにちは、 残念ながら、そのレベルでは文書化されておらず、社内チームに確認する必要がありますが、動作する例や検証済みのSDKs/ドライバは存在しません。 スカレーションの手続きを始めるために、あなたの情報を添えたチケットを提出していただけますか? よろしくお願いいたします。 Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY こんにちは、 こちらでご確認ください: サポート・チケット NXPのサポート担当者による機密厳守でのサポート。 チケットを送信 よろしくお願いいたします。 Re: i.MX8MP G2 HEVC slice input timeout instead of BUFFER_EMPTY こんにちは、ホルヘさん。 ご確認いただきありがとうございます。社内チームへのエスカレーションのために技術サポートチケットを開きたいと考えています。 適切なチケット提出リンクを教えていただけますか?どの製品やカテゴリーを選ぶべきか教えていただけますか?必要な情報や添付書類についてもお知らせください。 i.MX8MP EVKハードウェアの詳細、BSP/カーネルおよびデコーダライブラリのバージョン、最小限のリプロダクション、HEVCサンプルストリーム、そしてインクリメンタルスライス入力時に観察されたハードウェアタイムアウトと成功した完全画像入力を比較したログを提供できます。 我々の要求は、同じ画像の残りのスライスが到着する前に、完全なスライスのデコードを開始し、デコードが完了した後にのみ画像を出力することです。部分的な画像表示は要求していません。 また、このチケットをこのフォーラムの議論にリンクさせ、適切な社内デコーダーチームに転送する方法についても教えてください。送信後、チケット番号をこちらで共有します。 よろしくお願いいたします。
View full article
FRDM-A-S32K356)PWM信号未输出 我计划将 MCU 从 S32K344 更换为 S32K356,以减少处理时间。 我使用 FRDM-A-S32K356 评估板将基于 S32K344 的 FOC 项目移植到了 S32K356。但是,我无法获得任何 PWM 输出信号来驱动逆变器。请问您能否告知我可能的原因以及我应该检查哪些设置? 具体来说,我希望 PWM 信号从连接器 JA1 上的以下引脚输出: 引脚 15 (PTA0) 引脚 13 (PTA1) 引脚 11 (PTA3) 引脚 9 (PTA2) 引脚 7 (PTD3) 引脚 5 (PTD2) 重现问题的步骤: 打开S32K_PMSM_Sensorless.pmpx 。 将“所需速度”设置为100 rpm 。 将“开/关”从“停止”改为“运行” 。 检查指定 JA1 引脚上的 PWM 输出信号。 预期行为: PWM信号应从指定的JA1引脚输出。 实际行为: 在指定的 JA1 引脚上未观察到 PWM 信号。 Re: FRDM-A-S32K356)The PWM signal is not being output 嗨@Tomato1 首先,请注意 S32K3_S32M27x 实时驱动程序版本 3.0.0P07 没有与 S32K356 设备进行测试。因此,我们不能保证将此版本与 S32K356 一起使用时能够正常工作。从 S32K3_S32M27x 实时驱动程序 ASR R21-11 版本 6.0.0 开始,正式引入了对 S32K356 的支持。 因此,我们建议使用支持 S32K356 的最新软件版本和开发工具,以确保兼容性并避免与不支持的软件版本相关的潜在问题。 此外,作为您电机控制开发的参考,我们提供了一个示例应用程序,演示了采用双并联电流检测的永磁同步电机 (PMSM) 的无传感器磁场定向控制 (FOC)。本示例基于 NXP DEVKIT-MOTORGD 和 FRDM-A-S32K344,可通过NXP 应用程序代码中心访问。 BR,VaneB
View full article
IMX535 我目前还有一款产品在使用 MCU MCIMX535DVP1C2,但 PMIC MC34708 和 MC34709 现在都已经过时了。我计划使用 PMIC MMPF0100,因为它被推荐作为 MC34708 的替代品:是否有任何参考设计、原理图、应用文档或关于如何实现替代的建议? 谢谢! 米尔科 Re: IMX535 嗨,米尔科, 感谢您就 MCIMX535DVP1C2 设计的 PMIC 迁移事宜与我们联系。 如硬件评测中所述, 虽然 MMPF0100 是推荐的后续产品系列,但 由于 PF0100 的目标平台是 i.MX6 生态系统, 因此 NXP 没有提供可直接替换的参考板 。 如果您决定进行重新设计, 则需要重新封装电路板(QFN56 封装与 MAPBGA206 封装不同),并对 OTP 启动序列(AN4536)进行编程,使其与 i.MX53 的电源轨相匹配。 根据您的生产时间表,以及您是否愿意承担立即进行电路板重新设计/模具制造的成本,还是使用现有布局进行过渡版本生产,以下是我们目前的分配和元器件价格,供您比较: MCIMX535DVP1C2 (NXP Cortex-A8 微处理器): 39.80 美元/个 MC34708 (传统电源管理集成电路,原始布局): 5.00 美元/个 MC34709 (传统电源管理集成电路替代方案): 5.30 美元/个 MMPF0100 (下一代迁移 PMIC): 4.20 美元/个 如果您希望现有存货/保修批次的产品保持当前的PCB布局,短期内继续使用MC34708/MC34709可以避免非经常性工程费用和重新认证周期。如果您无论如何都要开始进行版本升级,那么过渡到MMPF0100(4.20美元)将提供长期稳定的供货保障。 您可以直接访问 (spacechips.tech)查看我们的完整产品线卡、可追溯性标准和技术库存更新。 请告知您的目标数量和批次计划,以便我预留配额或据此准备正式的形式发票。 顺祝商祺! 陈艾斯
View full article
IMX535 I have a product still using MCU MCIMX535DVP1C2, but the PMIC MC34708 and MC34709 are both obsolete now. I am planning to use PMIC MMPF0100 as it is a suggested replacement for MC34708: is there any reference design, schematic, application document or recommendation on how to implement the relacement ? Thank you. Mierko Re: IMX535 Hi Mierko, Thanks for reaching out regarding the PMIC migration for the MCIMX535DVP1C2 design. As noted in the hardware review, while the MMPF0100 is the recommended successor family, there is no direct drop-in reference board from NXP since the PF0100 was targeted at the i.MX6 ecosystem. If you decide to proceed with the redesign, you will need to re-spin the board (QFN56 vs. MAPBGA206) and program the OTP startup sequence (AN4536) to match the i.MX53 power rails. Depending on your production timeline and whether you want to absorb immediate board redesign/tooling costs versus running a bridge build with existing layouts, here is our current allocation and component pricing for comparison: MCIMX535DVP1C2 (NXP Cortex-A8 MPU): $39.80 / pc MC34708 (Legacy PMIC, original layout): $5.00 / pc MC34709 (Legacy PMIC alternative): $5.30 / pc MMPF0100 (Next-gen migration PMIC): $4.20 / pc If you prefer to maintain the current PCB layout for existing inventory/warranty batches, keeping the MC34708 / MC34709 in the short term avoids NRE and re-certification cycles. If you are starting a revision anyway, transitioning to the MMPF0100 ($4.20) will provide long-term supply stability. You can review our full line-card, traceability standards, and technical stock updates directly at (spacechips.tech) Let me know your target quantities and batch schedule, and I can reserve allocation or prepare the official Proforma Invoice accordingly. Best regards, Ace Chen
View full article
FRDM-A-S32K356)PWM信号が出力されていません プロセッシング時間を短縮するために、MCUをS32K344からS32K356に変更する予定です。 私はFRDM-A-S32K356評価ボードを使ってS32K344ベースのFOCプロジェクトをS32K356に移植しました。しかし、インバータを駆動するためのPWM出力信号を得ることができません。原因や確認すべき設定についてアドバイスをいただけますか? 具体的には、コネクタJA1の以下のピンからPWM信号が出力されることを想定しています。 ピン15(PTA0) ピン13(PTA1) ピン11(PTA3) ピン9(PTA2) ピン7(PTD3) ピン5(PTD2) 問題を再現する手順: S32K_PMSM_Sensorless.pmpxを開きます。 「必要回転数」を100rpmに設定してください。 「オン/オフ」を「停止」から「実行」に変更します。 指定されたJA1ピンのPWM出力信号を確認してください。 期待される動作: PWM信号は、指定されたJA1ピンから出力される必要があります。 実際の動作: 指定されたJA1ピンにはPWM信号は観測されませんでした。 Re: FRDM-A-S32K356)The PWM signal is not being output こんにちは、@Tomato1さん まず、S32K3_S32M27xリアルタイムドライバーバージョン3.0.0であることにご注意ください。P07はS32K356デバイスではテストされていません。したがって、このバージョンをS32K356と組み合わせて使用した場合、適切な機能を保証することはできません。S32K356の公式サポートは、リアルタイム・ドライバのASR R21-11バージョン6.0.0 S32K3_S32M27xから導入されました。 このため、互換性を確保し、サポートされていないソフトウェアバージョンに関連する潜在的な問題を避けるために、S32K356をサポートする最新のソフトウェアリリースや開発ツールの使用を推奨します。 さらに、モータ制御開発の参考として、デュアルシャント電流検知を備えた永久磁石同期モーター(PMSM)のセンサーレス場指向制御(FOC)を実証するアプリケーションの例があります。この例はNXP DEVKIT-MOTORGDおよびFRDM-A-S32K344に基づいており、 NXPアプリケーションコードハブを通じてアクセス可能です。 BR、VaneB
View full article
ZSDK BLEホスト認定に関するリファレンスは古くなっているようです nxp-zsdkのリリースノートに記載されているBLEホストの認定情報は、非常に古い認定情報に基づいています。 例:nxp-zsdk 4.4の状態; BLE ホスト、DN#: Q305748、リンク *: ホスト資格 BLEコントローラ、DN#:Q380314、リンク*:コントローラ資格 *: BLE SIGアカウントが必要です。 このホスト資格はBLE 5.4のサポートを指定しています。 コントローラはBLE 6.1サポートを指定しています。 コントローラのすべての機能をサポートするには、ホストは同じBLEレベルまたはそれ以上のレベルが必要です。 SO、リリースノートの参照が間違っていると思いますが、正しい参考文献を教えてもらえますか? 敬具 トニー Re: ZSDK BLE host qualification references seems obsolete これはNXP RW612です。 ありがとう、トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg どのBLE製品を使っているのか教えてもらえますか? ご提供いただいたリンクを確認しましたが、RW610とRW612のどちらかです。なので、RW610を使っているのか、それともRW612なのか確認したいです。 SO、CAN調べられるように。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg ご返信ありがとうございます。 あなたが言及したタグを確認しました。NXP Zephyrプロジェクトv4.4.0は 2026年5月11日にリリースされます。 そして、もう一つ新しいNXP Bluetooth Low EnergyホストスタックのZephyr DNが登場します。Q393055は 2026年7月30日に入手可能です。つまり、リリースノートで間違ったBLEホストQDIDを記載していないということです:nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk ·GitHub。 実際には、古い QDID 番号であるべきです: DN#: Q305748。 しかし、誤解を訂正したいのですが、ホストとコントローラは必ずしもBluetooth Core Specのバージョンが一致する必要はありません。ホストとコントローラは別々のBluetoothサブシステムとして認定されており、Core 5.4に適合したホストとCore 6.1に適合したコントローラを使用可能です。 このThreadで他に何か懸念があれば教えてください。 それ以外の場合は、このCASEの解決策として私の回答をマークしてください。ありがとうございます! BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティンさん。 お返事ありがとうございます。Bluetoothホストの認証について、追加の質問があります。 リリースノートはhttps://qualification.bluetooth.com/ListingDetails/227830にリンクしています。これは以下を示しています。 Bluetooth ホストソリューション Zephyr、2024-09-16(www.nxp.com) コア仕様:ホスト5.4、アクティブ これはBLE 5.4の2年前のホスト資格であり、コントローラはBLE 6.1の資格を持っています。これらのリスティングに対して製品を基準にすると、BLE 5.4を超えるものは請求できません。 BLE 6.3の新しいホスト認定について言及されていましたが、リリースノートにはそれに関する記述がありません。これによって2つの疑問が生じる。 コントローラが6.1に対応し、ホストが6.3に対応している場合、私たちの製品でどのBLEバージョンを主張できますか? リリースノートは代わりにZephyr Project / Linux Foundationのホスト資格(例えば https://qualification.bluetooth.com/ListingDetails/332380)を指すことはあり得ますか?ホストの推薦を含めるのは、自分の資格審査で使える場合に限ります。 事前に感謝いたします。 よろしくお願いします、 トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg コントローラが6.1に対応し、ホストが6.3に対応している場合、私たちの製品でどのBLEバージョンを主張できますか? ==>[クリスティン]:はい、おっしゃる通りです。あなたの製品は6.1の下位バージョンしか主張できないと思います。ただし、製品の認証を申請する際には、Bluetooth SigがホストやコントローラのICSの詳細やアプリケーションフォームに入力したプロファイルもチェックします。 リリースノートは代わりにZephyr Project / Linux Foundationのホスト資格(例えば https://qualification.bluetooth.com/ListingDetails/332380)を指すことはあり得ますか?ホストの推薦を含めるのは、自分の資格審査で使える場合に限ります。 ==>[Christine]:どのホストQDIDを参照できるかは、使用するZephyrホストスタックによって異なります。このリンクはLinux FoundationのZephyr RTOS LEホストにのみ適用可能です。もしあなたが言及しているのであれば、このリンクBluetooth Low Energy Host Stack Zephyrを指すのではなく、私たちのNXPのQDIDを参照することをお勧めします。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg このリンクのすべてのブランチを確認しました。nxp-zsdk/doc/wireless/release-notes/トピック/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk ·GitHub QDIDは既に各リリースノートに記載済みです。同じQDIDであっても、それは全てNXPの同じ認証に基づいていることを意味します。 ZephyrベースのQDIDは2つしかなく、1つは2024年、もう1つは2026年です。 そして、2026年のこの新しいQDID以降、私たちのGitHubには新たなリリースはありません。 NXP-ZSDK/DOC/Wireless/release-Notes/トピック/rw610rw612_release_notes.MD at NXP-V4.4-branch·nxp-zephyr/nxp-zsdk ·GitHub SO、FUTUREのnxp-Zephyrリリースでは、リリースノートを新しいQDIDに付けて修正するかもしれません。 他に何かご心配な点がありましたら、お知らせください。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティン NXPが4.4.0向けのBLE認証を更新したことは素晴らしい。リリースノートには記載されていないが。 もしそうなら、Zephyr BLEホストはZephyr 3.7と4.4.0の間で 変更 されましたが、nxp-zsdkのリリースには適用されていませんでした。 バージョン4.5.0以降の計画について教えてください。ホストが変更された場合は、各nxp-zsdkリリースに必ず認定済みのBLEホストを含める必要があります。 トニーより Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティンさん。 NXP RW612で使っているBLEホストはZephyrプロジェクトに搭載されているもので、ソースコードとして提供されています。NXPのソフトウェアではありません。 Zephyrはだいたい6ヶ月ごとに新作がリリースされ、BLEホストはリリースごとに通常変わります。NXPが認定したBLEホストのみを使える場合、Zephyrのバージョンは1つに縛られます。リリースノートには、現在2年以上前のバージョン(おそらくZephyr 3.7.0)について言及されています。それ以降のすべてのリリース、現在の4.5.0まで、多くのセキュリティおよび機能上のバグ修正が含まれています。3.7.0以降、Zephyrプロジェクトは61件のBluetoothセキュリティアドバイザリーを発表しており、そのうち43件はBLE向けです。 もしNXPの資格だけに頼るなら、NXPはZephyrの各リリースごとにホストを資格付けする必要があります。 各ZephyrリリースでどのQDIDを使うべきかの概要を教えていただけますか?Nordicは次のようなマトリックスを公開しています。例えば: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (Nordicのマトリックスでは、彼らのSDKsバージョン番号はZephyrのバージョン番号とは異なります。) よろしくお願いします、 トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティン NXPが4.4.0向けのBLE認証を更新したことは良いのですが、リリースノートにはそのことが記載されていません。 Zephyr BLEホストはZephyr 3.7と4.4.0の間で 変更 されました。しかし、その間のどのリリースにおいても、nxp-zsdk の認定は受けていませんでした。 バージョン4.5.0以降の計画について教えてください。ホストが変更された場合は、各nxp-zsdkリリースに必ず認定済みのBLEホストを含める必要があります。 トニーより Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg ご返信ありがとうございます。 はい、間違いなく、FUTUREのZephyr SDKの計画があります。詳細なスケジュールについては、社内チームに確認するため、少々お時間をいただきます。 情報が確認でき次第、お知らせします。 BR、 Christine。
View full article
ZSDK BLE主机资质参考似乎已过时 nxp-zsdk 版本说明中提到的 BLE 主机资格认证参考的是一个非常古老的资格认证。 例如nxp-zsdk 4.4状态; BLE主机,DN#: Q305748,链路*:主机资质 BLE 控制器, DN#: Q380314,链接*:控制器资质 *:需要 BLE SIG 帐户。 此主机资质要求支持 BLE 5.4。 控制器明确支持 BLE 6.1。 为了支持控制器的所有功能,主机需要相同或更高的 BLE 级别。 所以我认为版本说明中的参考有误,您能提供正确的参考吗? 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀, 感谢你的回复。我还有一个关于蓝牙主机认证的后续问题。 版本说明链接至https://qualification.bluetooth.com/ListingDetails/227830 ,这表明: Bluetooth Host Solution Zephyr,2024-09-16 ( www.nxp.com ) 核心规格:主机 5.4,活动 这是两年前针对 BLE 5.4 的主机认证,而控制器则针对 BLE 6.1 进行了认证。如果我们按照这些标准来评判我们的产品,我们就不能声称其性能高于 BLE 5.4。 您提到了 BLE 6.3 的新主机认证,但版本说明中没有引用它。这就引出了两个问题: 我们的控制器符合 6.1 版本标准,主机符合 6.3 版本标准,那么我们的产品可以声明为哪个 BLE 版本? 版本说明能否引用 Zephyr 项目/Linux 基金会主机认证信息(例如https://qualification.bluetooth.com/ListingDetails/332380 )?只有当我们能在自己的资质认证中使用它时,提供主办方参考信息才对我们有帮助。 提前谢谢您。 此致, 托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 感谢您的回复。 我查看了您提到的标签 ,NXP Zephyr 项目 v4.4.0将于2026 年 5 月 11 日版本。 我们还有另一个更新的 NXP 低功耗蓝牙 Host Stack Zephyr DN: Q393055,于2026-7-30获取。这意味着,我们在版本说明中没有列出错误的 BLE 主机 QDID: nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub 。 实际上应该是旧的 QDID 号码:DN#: Q305748。 但我想要纠正你的理解,主机和控制器不需要具有相同的蓝牙核心规范版本。主机和控制器被认定为独立的蓝牙子系统,符合 Core 5.4 标准的主机可以与符合 Core 6.1 标准的控制器一起使用。 如果您对此帖还有其他疑问,请告诉我。 否则,请随时将我的回答标记为此问题的解决方案,谢谢! BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 请问您使用的是哪款BLE产品? 我查看了您提供的链接,上面是RW610和RW612,所以我想和您确认一下您使用的是RW610还是RW612? 这样我就可以帮你查一下了。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 它的NXP RW612。 谢谢托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀, 我们与 NXP RW612 一起使用的 BLE 主机是 Zephyr 项目中的主机,以源代码形式提供。这不是恩智浦半导体(NXP)的软件。 Zephyr 大约每 6 个月发布一个新版本,而 BLE 主机通常每个版本都会发生变化。如果我们只能使用 NXP 认证的 BLE 主机,那么我们就只能使用一个 Zephyr 版本。发行说明中提到的版本现在已经超过两年了(可能是 Zephyr 3.7.0)。从那时到目前的 4.5.0 版本,每个版本都包含了许多网络安全和功能性错误修复。自 3.7.0 版本以来,Zephyr 项目已发布了 61 份蓝牙网络安全公告,其中 43 份针对 BLE。 如果我们只依赖 NXP 的认证,那么 NXP 需要对每个 Zephyr 版本中的主机进行认证。 能否提供一份概述,说明每个 Zephyr 版本应该使用哪个 QDID?例如,Nordic 发布了一份类似这样的矩阵: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (在 Nordic 的矩阵中,他们的 SDK 版本号与 Zephyr 版本号不同。) 此致, 托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 我查看了此链接中的所有分支: nxp-zsdk/doc/wireless/版本-notes/topics/rw610rw612_release_notes.md,位于 nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub 我们已经在每个版本说明中列出了 QDID。即使 QDID 相同,也意味着它们都基于我们 NXP 的相同认证。 我们只有 2 个基于 Zephyr 的 QDID,一个在 2024 年,另一个在 2026 年。 继 2026 年发布这个新的 QDID 之后,我们的 GitHub 上将不再发布任何其他新版本: nxp-zsdk/doc/wireless/版本-notes/topics/rw610rw612_release_notes.md 位于 nxp-v4.4-branch· nxp-zephyr/nxp-zsdk · GitHub 所以我认为在未来的 nxp-zephyr 版本中,我们可能会修改版本说明,以提及新的 QDID。 如果您还有其他疑问,请告诉我。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀 NXP 更新了 BLE 4.4.0 的认证信息,这很好。即使版本说明中没有提到这一点。 如果是这样,Zephyr BLE 主机在 Zephyr 3.7 和 4.4.0 之间发生了变化,但 nxp-zsdk 并未对中间的任何版本进行认证。 从 4.5.0 版本开始,你们有什么计划?我们需要每次发布 nxp-zsdk 版本时都包含一个合格的 BLE 主机,无论主机何时发生更改。 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 我们的控制器符合 6.1 版本标准,主机符合 6.3 版本标准,那么我们的产品可以声明为哪个 BLE 版本? ==>[克里斯汀]:是的,你说得对。我认为你们的产品只能用于 6.1 这个较低版本。但需要指出的是,当您申请产品认证时,蓝牙技术联盟还会检查主机和控制器的 ICS 详细信息以及您在申请表中输入的我的类型。 版本说明能否引用 Zephyr 项目/Linux 基金会主机认证信息(例如https://qualification.bluetooth.com/ListingDetails/332380 )?只有当我们能在自己的资质认证中使用它时,提供主办方参考信息才对我们有帮助。 ==>[Christine]:具体可以参考哪个主机 QDID 取决于您使用的 Zephyr 主机协议栈。此链接仅适用于Linux 基金会提供的 Zephyr RTOS LE 主机。如果您指的是 NXP 的低功耗蓝牙主机协议栈 Zephyr,那么我不建议您参考此链接,而是参考我们 NXP 的 QDID。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀 NXP 针对 4.4.0 版本更新了 BLE 认证,这很好,但是发行说明中没有提到这一点。 Zephyr BLE主机在Zephyr 3.7和4.4.0之间发生了变化,但在 nxp-zsdk 中,他没有资格参与中间的任何版本发布。 从 4.5.0 版本开始,你们有什么计划?我们需要每次发布 nxp-zsdk 版本时都包含一个合格的 BLE 主机,无论主机何时发生更改。 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 感谢您的回复。 是的,我们当然有针对未来 Zephyr SDK 的规划。但具体的日程安排,请允许我花些时间向我们的内部团队核实。 一旦得到确认信息,我会通知你。 BR, Christine。
View full article
ZSDK BLE host qualification references seems obsolete The BLE host qualification references in nxp-zsdk release notes refers to a very old qualification. E.g. nxp-zsdk  4.4 states; BLE Host, DN#: Q305748, Link *: Host qualification BLE Controller, DN#: Q380314, Link *: Controller qualification *: Requires BLE SIG account. This host qualification specifies BLE 5.4 support. The controller specifies BLE 6.1 support. To support all the features of the controller, the host would need the same BLE level or higher. So I think that the reference in the release notes are wrong, can you provide the correct references? Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Thanks for your reply. I checked the tag you mentioned NXP Zephyr project v4.4.0  is release on May 11 2026. And we have another newer NXP Bluetooth Low Energy Host Stack Zephyr DN: Q393055 is gotten on 2026-7-30. It means, we did not list the wrong BLE host QDID in the release note:nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub. It actually should be the old QDID number: DN#: Q305748. But I want to correct your understandings, Host and Controller does not need to have matched Bluetooth Core Spec version. The Host and Controller are qualified as separate Bluetooth subsystems, and a Host qualified against Core 5.4 can be used with a Controller qualified against Core 6.1. Please let me know whether still have any other concerns on this thread. Otherwise, please do not hesitate to mark my answer as a solution for this case, Thanks! BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine, Thank you for your reply. I have a follow-up question about the Bluetooth host qualification. The release note links to https://qualification.bluetooth.com/ListingDetails/227830, which shows: Bluetooth Host Solution Zephyr, 2024-09-16 (www.nxp.com) Core Specification: Host 5.4, Active This is a two-year-old host qualification at BLE 5.4, while the controller is qualified for BLE 6.1. If we qualify our product against these listings, we can’t claim anything higher than BLE 5.4. You mentioned a newer host qualification for BLE 6.3, but the release note doesn’t reference it. That raises two questions: With a controller qualified for 6.1 and a host qualified for 6.3, which BLE version can we claim for our product? Could the release notes refer to the Zephyr Project / Linux Foundation host qualification instead (for example https://qualification.bluetooth.com/ListingDetails/332380)? Including a host reference only helps us if we can use it in our own qualification. Thank you in advance. Best regards, Tonny Re: ZSDK BLE host qualification references seems obsolete Its NXP RW612. Thanks Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Can you please let me know which BLE product are you using? I checked in the link you provided, it is RW610 and RW612, so I prefer to confirm with you that you are using RW610 or RW612? So that I can check for you. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine, The BLE host we use with the NXP RW612 is the one in the Zephyr project, delivered as source code. It is not NXP software. Zephyr has a new release every 6 months or so, and the BLE host usually changes with each release. If we may only use BLE hosts that NXP has qualified, we are tied to one Zephyr version. The release notes refer to a version that is now more than two years old (probably Zephyr 3.7.0). Every release since then, up to the current 4.5.0, has included many security and functional bug fixes. Since 3.7.0, the Zephyr project has published 61 Bluetooth security advisories, 43 of them for BLE. If we are to rely only on NXP’s qualification, NXP would need to qualify the host for each Zephyr release. Could you send us an overview of which QDID to use for each Zephyr release? Nordic publishes a matrix like this, for example: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (In Nordic’s matrix, their SDK version numbers are different from the Zephyr version numbers.) Best regards, Tonny Re: ZSDK BLE host qualification references seems obsolete Hi Christine It is nice that NXP has an updated BLE qualification for 4.4.0, even though the release notes don’t mention it. If so, the Zephyr BLE host changed between Zephyr 3.7 and 4.4.0 but wasn’t qualified in nxp-zsdk for any of the releases in between. What are your plans from 4.5.0 onward? We need each nxp-zsdk release to include a qualified BLE host whenever the host has changed. Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  I checked all of the branches in this link, nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub we already listed the QDID in each Release note. Even it is the same QDID, it means all of them are based on our NXP's same certification. We only have 2 Zephyr based QDID, one is in 2024, another is in 2026. And after this new QDID in 2026, there is still no other new release on our github: nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub So I think in the future nxp-zephyr release, we might modify the release note to refer to the new QDID. If you have any other concerns, please let me know. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  With a controller qualified for 6.1 and a host qualified for 6.3, which BLE version can we claim for our product? ==>[Christine]:Yes, you are right. I think your product can only be claimed  for 6.1 as the lower version. But need to point out that when you apply for the certification for your product, the Bluetooth Sig will also check the details of host and Controller's ICS and what kind of profiles you input in the application form. Could the release notes refer to the Zephyr Project / Linux Foundation host qualification instead (for example https://qualification.bluetooth.com/ListingDetails/332380)? Including a host reference only helps us if we can use it in our own qualification. ==>[Christine]:Which host QDID can be referred to depends on which Zephyr Host Stack you are using.  This link is only applicable to Zephyr RTOS LE host from the Linux Foundation. If you are referring to NXP Bluetooth Low Energy Host Stack Zephyr, then I do not recommend you to refer this link, but our NXP's QDID. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine Its fine that NXP has an updated BLE qualification for 4.4.0, but the release note don’t mention it. The Zephyr BLE host changed between Zephyr 3.7 and 4.4.0, but wasn’t qualified in nxp-zsdk for any of the releases in between. What are your plans from 4.5.0 onward? We need each nxp-zsdk release to include a qualified BLE host whenever the host has changed. Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Thanks for your reply. Yes, for sure, we have plan for the future Zephyr SDK.  But for the detailed schedule, please allow me some time to check with our internal team. Once have confirmed info, I will let you know. BR, Christine.
View full article
i.MX 8M Quad Evk I2C interface I need to interface an AM/FM tuner module with the NXP i.MX 8M Quad EVK using the I2C interface for tuner configuration and control. Could you please guide me on how to establish this hardware interface. Additionally, does the i.MX 8M Quad EVK expose I2S signals that can be used to receive digital audio output from the tuner module? If so, could you please share the relevant connector details and pin mapping? Re: i.MX 8M Quad Evk I2C interface Hello, Yes, the MCIMX8M-EVK has J801 connector to access I2C2 of the processor. Regarding access to I2S interface will be a little bit more difficult since an adapter will be needed. These signals are connected to M.2 KEY-E J1401 connector or J1801 connector. Please check it in the next design file: Design Files for the i.MX 8M Evaluation Kit (EVKB) Best regards.
View full article
[KW45B41Z] J-Link GDB 服务器错误:无法连接到自定义硬件上的目标 亲爱的团队, 我遇到了上述问题。请帮我解决这个问题。 硬件:定制板,搭载 KW45B41Z 芯片;调试器:SEGGER J-Link;IDE:MCUXpresso 尝试对我的定制 KW45B41Z 板进行烧录/调试时,J-Link GDB 服务器抛出以下弹出错误:“J-Link GDB 服务器报告了一个错误。原因:错误:无法连接到目标。 我附上了我的IDE和错误弹出窗口的截图。当J-Link在自定义设计中连接失败时,针对这款特定的MCU,建议的故障排除步骤是什么?
View full article
#ftm_pwm_S32K116 こんにちは、NXPの同僚の皆様: ftm_pwm_s32k116プロジェクトについて助けを求めています。実際のところ、コードや設定をどう変えても、MCUはデフォルトチャネル(FTM0-チャネル0、つまりPTD15)。 これが私の手順です。 1.サンプルから新しいプロジェクトをインポートします。 2.コンパイルするとすべて合格し、ピンマルチプレクサとフレックスタイマーの設定を確認しましたが問題はありませんでした(実際にはNXPのサンプルからなので、完全に正しいと思います)。 3.次に、それをS32K116に書き込みます。 4.PTD15の波形を観察しましたが、何も見つかりませんでした。ほぼ2日間試しました。 私のプロジェクトのzipファイルは以下のとおりです。ありがとうございます。 Re: #ftm_pwm_S32K116 プロジェクトを添付してください Re: #ftm_pwm_S32K116 こんにちは、 @Tracy_Lu さん。 まず、プロセッサ Expertを使っているので、古いソフトウェアバージョンを使っているようですね。S32K1デバイスで開発を始める場合は、最新のソフトウェアとツール、現在S32K1_S32M24X リアルタイム・ドライバ AUTOSAR R21-11 バージョン3.0.0の使用をお勧めします(S32K1用のリアルタイム・ドライバ)とS32プラットフォーム向けのS32 Design Studio(S32 Design Studio |NXP Semiconductors)を共同で提供しています。 しかし、S32K1 SDKsを使い続けたい場合は、最新のSDKsバージョンがS32 Design Studio for S32 プラットフォーム 3.4に付属していました。 また、EVBを使っているのかカスタムボードなのか教えていただけますか? 現在のソフトウェア環境を維持したい場合は、使っている正確なS32K1 SDKバージョンも共有していただけると助かります。 BR、VaneB Re: #ftm_pwm_S32K116 こんにちは、NXPの同僚の皆様: 迅速かつプロフェッショナルなご回答ありがとうございます。サンプルから別のプロジェクトS32K116_Project_FTMに変更し、コードを修正しました(gemini AIの支援を受けて)。コンパイルとデバッグ中に問題が発生するエンジニアの方々が解決できるよう、以下の点を共有したいと思います。 1.私はFTM機能を使用して、PMIC(TPS650366)のESM(エラー信号モニタリング)に応答します。 2.at 最初にftm_pwm_S32k116プロジェクトを使い、約2日間コンパイルとデバッグに失敗しました。割り当てられたピンで出力PWMが見当たりません。そして、Gemini AIの助けを借りて正しい設定とデバッグをしているはずです。 3.次に、S32K116_Project_FTM という名前の別の例を見つけ、それを試してコンパイルしましたが、エラーはありませんでした。そして、PTD15(FTM0CH0)/16(FTM0CH1) という構成済みピンの出力が得られました。初期周波数は 1Hz/5Hz ですが、ゴールが近いことがわかりました。 4. 実はPWM周波数は40KHz付近で必要なので、次のステップはシステムの周波数プリスケーラ、MOD値、CnV(デューティサイクル)を変更することだと分かっていますが、MOD値は変更できません(値は変えるだけでMCUのルート場所に書き込めません)。何度も試して、役立つ情報を探しました。 5.最後に、MOD値を変更したい場合は、いくつかの前提条件を満たす必要があることがわかりました。たとえば、クロックを閉じ、書き込み保護を解除する必要があります...。 6.以下はコンパイル後の私のコードで、正常に動作します(PTD16で約48KHzの出力)。 int main(void) { /*! * 初期化: * ======================= */ WDOG_disable(); /* ウォッチドッグを無効にする */ SOSC_init_40MHz(); /* 40 MHz水晶発振器用のシステム発振器を初期化します */ RUN_mode_48MHz(); /* クロックを初期化: 48 MHz システム、コア、バス、 24 MHz フラッシュ。*/    FTM0_init(); /* 8 MHz SIRCDIV1_CLK を使用して FTM0 を初期化します */    //FTM0_CH0_OC_init();    /* FTM0 CH0、PTD15 を初期化 */   FTM0_CH1_PWM_init();    /* FTM0 CH1、PTD16 を初期化 */   FTM0_CH6_IC_init();    /* FTM0 CH6、PTE8 を初期化します  */ FTM1_Init(); FTM1_CH1_PWM_init(); PORT_init(); /* ポートの設定 */   start_FTM0_counter();  /* FTM0カウンタを開始 */   /*! * 無限: * ======================== */ のために(;;)   { //FTM0_CH0_output_compare();/* 出力比較が一致した場合: */   /* ピンの切り替え(ハードウェアによる自動切り替え) */   /* フラグ 8 をクリア */   /* リロードタイマー */ //FTM0_CH6_input_capture(); /* 入力がキャプチャされた場合:フラグをクリアし、タイマーを読み取る */   } } 7.インポートコードは以下のとおりです(FTM0_init()、FTM0_CH1_PWM_init()): void FTM0_init(void) {/** * FTM0 クロック: * ================================================== */ PCC->PCCn[PCC_FTM0_INDEX] &= ~PCC_PCCn_CGC_MASK; /* 設定のためにクロックが無効になっていることを確認します */ PCC->PCCn[PCC_FTM0_INDEX] |= PCC_PCCn_PCS(0b010) /* クロックソース=1、8 MHz SIRCDIV1_CLK */ | PCC_PCCn_CGC_MASK; /* FTMレジスタのクロックを有効にする */ /*! * FTM0 の初期化: * =================================================== */ // 1. 最初のステップ:FTM 時間钟彻底关闭(CLKS = 0)、この時点では完全に構成可能な状態です FTM0->SC = 0x00000000; // 2. 2 番目:写保护并开启 FTM 完全モード volatile uint32_t dummy = FTM0->MODE; FTM0->MODE |= FTM_MODE_WPDIS_MASK; /* 禁止用写保护 */ FTM0->MODE |= FTM_MODE_FTMEN_MASK; /* 开启 FTM 完全モード */ // 3. 第三步:時钟关闭の安全状態下、顺利ハンドルMODと比较值写进去 FTM0->CNTIN = 0U; FTM0->MOD = 166 - 1; /* 8MHz / 166 ≈ 48.19 kHz */ // 4. 4 番目: 構成チャネル 1 (PTD16) は周縁 PWM モードです FTM0->CONTROLS[1].CnSC = FTM_CnSC_MSB_MASK | FTM_CnSC_ELSB_MASK; FTM0->コントロール[1].CnV = 83; /* 50% 占空比 (83 < 165) */ // 5. 第五章:极性と組み合わせモード清零 FTM0->COMBINE = 0x00000000; FTM0->POL = 0x00000000; // 6. 最後の一步:すべてのパラメータ已经安稳書入後,才真正开启道输出和時間钟源! FTM0->SC = FTM_SC_PWMEN0_MASK | FTM_SC_PWMEN1_マスク | FTM_SC_PS(0) /* PS = 0 (不分周波数) */ | FTM_SC_CLKS(1); /* CLKS = 1 (最終启アニメーション计数器) */ } void FTM0_CH1_PWM_init(void) { /** * FTM0、PWMモードでのチャネル1: * ================================================== */ FTM0->CONTROLS[1].CnSC = FTM_CnSC_MSB_MASK |FTM_CnSC_ELSB_MASK;  /* FTM0 ch1: エッジアラインメント PWM、低真パルス */ /* CHIE (ちゃん割り込みエナ) = 0 (デフォルト) */ /* MSB:MSA (チャンネルモード選択)=0b10、エッジアラインPWM */ /* ELSB:ELSA (chan Edge/Level Select)=0b10、low true */   FTM0->CONTROLS[1].CnV =  46875; /* FTM0 ch1 比較値 (デューティサイクル約75%) */ }
View full article