Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
使いやすい8ビットのマイクロコントローラやアセンブリ言語はありますか? 実際の16進/バイナリコードが見られる8ビットのマイクロコントローラを探しています。大学で8051アセンブリ言語を学んでいるのですが、メモリ内の命令や値の一つ一つを見て理解できることが本当に大好きです。しかし、それらのマイクロコントローラは時代遅れで互換性のために多くの「ハック」が必要です。少なくとも、自分のコードを実際のハードウェアに書き込むたびに、そんな風に感じるんです。では、シンプルな8ビットアセンブリ言語で実際のチップを使った簡単な電子工学プロジェクトをプログラムできるものはありますか? Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? こんにちは; アセンブリを学ぶなら、良い出発点はS08PTデバイスです。 S08PT|8ビット5V EEPROMとTSIを備えたフル機能MCU |NXP Semiconductors。 使用可能なソフトウェアツールは、Windows 10/11向けに利用可能な CodeWarrior for MCUS (Eclipse IDE) v11.1 です。このツールではアセンブリコードでテストできます。アセンブリ内のデバッグビューが表示され、メモリを確認してコードの機能を理解することができます。 このデバイスには評価ボードS08PT60-EVK、[MC9S08PT60]、[興味があれば]、[S08PT60-EVK製品情報]と様々な周辺機器が搭載されており、コードから実際のハードウェアへの異なる構成をテストできます。 オンボードインターフェースにはRGB LED、6軸デジタル加速度計と磁力計、周囲温度センサ、2つの静電容量式タッチパッド、ポテンショメーター、2つのユーザープッシュボタン、IRDAトランシーバが含まれます。また、拡張ボード用のArduinoピン配列にも対応しています。 詳細はメインページでご覧いただけます: S08P MCUs 評価キット | NXP Semiconductors 敬具、ルイス
View full article
使用 Green Hills 工具链的 S32k344 如何重新定位向量段,使其将向量表存储在闪存的 0x00400000 地址处,但在运行时复制到 DTCM 内存并从那里运行?我该如何在 Greenhills 链接器文件中实现这一点? Re: S32k344 using green hills toolchain 嗨@XRen_Parker 由于这个问题与 Green Hills 工具链及其集成密切相关,我建议您直接联系 Green Hills。他们应该能够提供适当的指导和资源。 https://support.ghs.com/ 此致, Lukas
View full article
DSPの使い方MPC5644A こんにちは、MPC5644AでDSPの使い方と設定方法を知りたいです Re: How to use DSP for MPC5644A こんにちは、 MPC5644A専用のDSPペリフェラルやDSPコプロセッサは搭載されていません。DSP機能は、e200z4 CPUコアに統合された信号処理拡張(SPE)を通じて提供されます。個別のDSP設定は必要ありません。DSP機能を活用するには、アプリケーションをSPEサポートを有効にしてコンパイルし、SIMDやMAC操作などのSPE命令を使えるようにする必要があります。 よろしくお願いいたします。 ピーター
View full article
Is there a simple 8 bit microcontroller/assembly language that is nice to work with? I'm searching for an 8 bit microcontroller where I can look at the actual hex/binary code. I've been learning 8051 assembly in university and I absolutely love seeing and understand every single instruction and value in the memory. But those microcontrollers are antiquated and need a bunch of "hacks" for compatibility. At least that's what it feels like everytime I put my code onto real hardware. So is there a simple 8 bit assembly language with actual chips I can program simple electronics projects with ? Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? Hello; If you are learning assembly a good start point could be the S08PT device; S08PT|8-bit 5V Full-featured MCU with EEPROM and TSI | NXP Semiconductors. The software tool to use it is CodeWarrior for MCUs (Eclipse IDE) v11.1 available for windows 10/11.; in this tool you can test with assembly code as it have the tools view for debug in assembly and review the memory to understand the functionality of your code. This device have an evaluation board S08PT60-EVK, [MC9S08PT60] if you are interested, [S08PT60-EVK Product Information] with various peripherals, for you to test different configurations from your code onto real hardware. The onboard interfaces include an RGB LED, a 6-axis digital accelerometer and magnetometer, an ambient temperature sensor, two capacitive touch pads, a potentiometer, two user push-buttons, and IRDA transceiver. Also is compatible with the Arduino pin layout for expansions boards. You can read more about the features in the main page: S08P MCUs Evaluation Kit | NXP Semiconductors Best Regards, Luis
View full article
The TCP client in S32K358 is not receiving the handshake packet. I've created a TCP client thread. When the handshake function is executed, I can see the messages sent by the client to the server and the messages sent by the server to the client using Wireshark. However, in the final step, the TCP client doesn't return a frame. I've been monitoring the GMAC receive interrupt and found it's stuck in a loop. The MCU TCP client hasn't received the final acknowledgment frame, so it hasn't sent the final handshake acknowledgment frame. What could be the reason? Re: S32K358 中TCP 客户端握手包接收不到 Hello @sunshine88, Are you using the lwip example provided inside the RTD package? If yes, could you share your RTD version?  Can you also share which status is being returned to RxStatus?  As requested on your other community post (LWIP TCP/IP Server-Client Hands-On), I've sent you a private message with the Lwip_HandsOn project for S32K148. Best regards, Julián
View full article
如何使用 DSP 控制 MPC5644A 您好,我想了解如何在MPC5644A中使用和配置DSP。 Re: How to use DSP for MPC5644A 你好, MPC5644A 不包含专用 DSP 外设或 DSP 协处理器。DSP 功能是通过集成到 e200z4 CPU 内核中的信号处理扩展 (SPE) 提供的。无需单独配置DSP。要利用 DSP 功能,必须在编译时启用 SPE 支持,允许编译器或应用程序代码使用 SPE 指令,例如 SIMD 和 MAC 操作。 顺祝商祺! Peter
View full article
S32K358のTCPクライアントはハンドシェイクパケットを受信していません。 TCPクライアントスレッドを作成しました。ハンドシェイク関数が実行されると、Wiresharkを使用してクライアントからサーバーに送信されたメッセージとサーバーからクライアントに送信されたメッセージを確認できます。しかし、最終ステップでTCPクライアントはフレームを返しません。GMAC受信割り込みを監視していたところ、ループに陥っていることがわかりました。MCU TCPクライアントは最終確認フレームを受信していないため、最終ハンドシェイク確認フレームを送信していません。原因は何でしょうか? Re: S32K358 中TCP 客户端握手包接收不到 こんにちは、@sunshine88 さん。 RTDパッケージ内のlwip例を使っていますか?もしそうなら、RTDのバージョンを教えていただけますか? RxStatusに返却されるステータスも教えてもらえますか? 他のコミュニティ投稿(LWIP TCP/IP サーバー・クライアント・実践形式)でのご要望通り、Lwip_HandsOnプロジェクトのプライベートメッセージを送りました。S32K148。 よろしくお願いします、 ジュリアン
View full article
Is i.MX 9 "there yet"? I started a project in a few years ago and NXP's i.MX 9 line of MPUs were beginning to be released but they were largely unobtainable so I went with a beefy i.MX 8. At this stage, it's way more power than I need and I'd like to move to a much smaller MPU. I was planning on getting the smallest i.MX 8 but the i.MX91 is the smallest cpu they have. I was wondering if I would be better off with the 91 instead of a more mature 8. Thermals are my primary concern so I would assume new is always better, but I just don't know if they are "there yet" since they are still fairly new. A more apples to apples port moving to an 8 could also be a motivator. Re: Is i.MX 9 "there yet"? Hi @ceva156  What is the main purpose of your project? Which IMX8 series product are you currently using? B.R Re: Is i.MX 9 "there yet"? Hello, Don’t need the heavier multimedia GPU capabilities of the i.MX8, the i.MX91 could be a much better fit and give you a simpler, lower-power design. Re: Is i.MX 9 "there yet"? Hello, I’d lean toward the i.MX91 if thermals and size are your main priorities. 
View full article
i.MX 9 准备好了吗? 几年前我开始了一个项目,当时 NXP 的 i.MX 9 系列 MPU 开始发布,但它们基本上无法获得,所以我选择了性能强大的 i.MX 8。现阶段,它的性能远远超过我的需求,我想换用性能小得多的微处理器。我原本打算买最小的 i.MX 8,但他们最小的 CPU 是 i.MX91。我一直在想,如果选择91型而不是更成熟的8型,会不会更好。散热是我最关心的问题,所以我认为新的总是更好,但我不知道它们是否已经“达到标准”,因为它们还比较新。更公平的比较,例如将港口升级到 8 级,也可能是一个激励因素。 Re: Is i.MX 9 "there yet"? 你好@ceva156 您的项目的主要目的是什么?您目前使用的是哪款IMX8系列产品? BR Re: Is i.MX 9 "there yet"? 你好, 如果不需要 i.MX8 的强大多媒体 GPU 功能,i.MX91 可能更合适,并且能提供更简单、更低功耗的设计。 Re: Is i.MX 9 "there yet"? 您好,如果您最看重散热性能和尺寸,我会推荐 i.MX91。
View full article
How to use DSP for MPC5644A Hello, I would like to know how to use and configure DSP in MPC5644A Re: How to use DSP for MPC5644A Hello, MPC5644A does not contain a dedicated DSP peripheral or DSP coprocessor. DSP functionality is provided through the Signal Processing Extension (SPE) integrated into the e200z4 CPU core. There is no separate DSP configuration required. To utilize DSP features, the application must be compiled with SPE support enabled, allowing the compiler or application code to use SPE instructions such as SIMD and MAC operations. Best regards, Peter
View full article
Functional Safety in Motor Control with AMMCLib and ASCLib When developing motor control for automotive and industrial systems, functional safety is a core requirement to ensure a motor does not produce unintended torque or speed. However, implementing complex algorithms like Field-Oriented Control (FOC) as a functionally safe component introduces severe architectural complexity, significantly increases development effort, and degrades overall performance. To solve this, NXP utilizes a safety decomposition approach that divides the application into a non-safety-related part (QM) and a safety-related part (ASIL). For this approach, NXP plans to provide the Automotive Safety Checker Library (ASCLib), which delivers ready-to-use safety checkers for the safety part. This enables high safety compliance without requiring a redesign of the QM motor control (MC) part. The Perfect Match: AMMCLib (QM) + ASCLib (ASIL) Many applications use highly optimized NXP's Automotive Math and Motor Control Library (AMMCLib) for the motor control part. While AMMCLib delivers exceptional performance, it is a Quality Management (QM) level library. Compliance with safety standards (such as ISO 26262) required teams to build custom safety mechanisms around the QM-level AMMCLib, consuming significant time and effort. NXP's ASCLib solves this by providing standardized, production-ready safety checkers. This eliminates proprietary safety software development and significantly reduces time-to-certification. Untitled Diagram (1).png How AMMCLib and ASCLib Fit Together The block diagram below illustrates a standard FOC system using this concept. The blue motor control blocks represents the QM-level AMMCLib functions, while the green blocks represent the ASCLib checkers that monitor key points to ensure safety. This architecture is based on the IEEE Low Complexity Safety Concept for FOC PMSM. source-NXPcommunity5.drawio.png This reference architecture shows that integrating ASCLib requires no changes to the existing QM motor control architecture. Full data-type compatibility allows ASCLib checkers to map directly to AMMCLib signals, ensuring seamless interconnection. The architecture assumes that Freedom from Interference (FFI) between the safety-related and QM software components is ensured. While standard FOC is a common use case, ASCLib is not limited to it. Thanks to its modular, independent blocks, the library supports alternative topologies and advanced techniques - including sensorless FOC and single-shunt current measurement. Inside ASCLib: A Layered Safety Architecture The ASCLib features a highly structured, layered software model organized hierarchically into Layers and Packages: pavelsvadbik_0-1784127185062.png The Service Layer (Top Layer) Exposes high-level functionalities directly to the safety application through two independent packages: High-Level Checkers (HLC): Wide range of application-level safety checkers tailored for various motor control systems. Fault Manager (FMG): Sophisticated fault-handling component managing error synchronization, configuration, and application notifications. The Core Layer (Foundational Layer) Provides the low-level building blocks utilized by the Service Layer. It consists of two essential packages: Low-Level Checkers (LLC): Delivers fundamental mathematical and verification functions. Fault-Debouncing (FDB): Provides generic fault debouncing algorithms. Developer Tip: The entire library is fully modular, isolated, and independent. If your application requires a unique checker, you can easily build your own custom checkers using the existing low-level blocks inside the LLC and FDB packages. Furthermore, the Fault Management (FMG) package is entirely optional—you are not forced to use it and can implement your own application-level error handling instead.   Not Just For Automotive Don't let the name fool you. While ASCLib has "Automotive" in its title and natively supports ISO 26262 workflows, its safety principles are universal. ASCLib applies perfectly to industrial systems complying with IEC 61508. To fit seamlessly into your existing development workflow, ASCLib features a dual-delivery option: Pure C Source Files: For direct integration into any bare-metal or RTOS-based embedded project. BAM (Bit Accurate Models): Ready-to-use blocks for Model-Based Design (MBD), allowing you to drag, drop, and simulate your safety architecture directly in MATLAB®/Simulink®. Key Benefits for Developers AMMCLib Remains QM: Keep using your existing, highly optimized AMMCLib code for core motor control. Model-Based development: Accelerate your design cycle by building and simulating your entire safety part using dedicated ASCLib BAM directly in MATLAB®/Simulink® before generating target C code. Accelerated Certification: Pre-designed safety checkers and integrated fault management significantly simplify your safety compliance and auditing processes. Get Started and Share Your Thoughts ASCLib is designed to be completely MCU-independent, giving you the flexibility to deploy it across various NXP hardware platforms. To accelerate your development, it is planned to be fully verified and ready to integrate with NXP’s automotive and industrial MCUs. By separating control from safety, you get the best of both worlds: maximum motor performance and uncompromising safety. Working on an upcoming ISO 26262 or IEC 61508 motor control project? Let’s discuss in the comments how the AMMCLib + ASCLib approach can simplify your design. We would also highly appreciate it if you could take a moment to fill out our quick survey below to share your insights with us! This project has received national funding from the MEYS and the funding from European Union’s Horizon Europe research and innovation framework programme under grant agreement No. 101112274. The ISOLDE project, nr. 101112274 is supported by the Chips Joint Undertaking and its members Austria, Czechia, France, Germany, Italy, Romania, Spain, Sweden, Switzerland. Building functionally safe motor control systems doesn’t have to mean sacrificing performance or redesigning your architecture. Discover how NXP combines AMMCLib and ASCLib to separate safety from motor control, reduce development effort, and accelerate certification—without compromising efficiency. Motor Control Re: Functional Safety in Motor Control with AMMCLib and ASCLib does ASCLib ONLY works together with AMMCLib? when and how should we promote ASCLib? Re: Functional Safety in Motor Control with AMMCLib and ASCLib Hi, ASCLib is NOT limited only to AMMCLib. While ASCLib is fully compatible with AMMCLib at the data type level, it can technically be integrated with any other library or custom algorithms without any limitations.   Regarding the promotion: ASCLib is not officially released yet. However, we are actively sharing information about it to gather real-world feedback. We would highly appreciate customer feedback on what their current gaps are and how ASCLib could help fill them. Re: Functional Safety in Motor Control with AMMCLib and ASCLib Hi, looks like very powerful lib, is ASCLib plan to be a premium (paid) software? what materials can we use to discuss with customer? any plan to have a beta version?
View full article
AMMCLibとASCLibを用いたモーター制御における機能安全 オートモーティブやインダストリアルシステム向けのモータ制御を開発する際、機能安全は、モーターが意図しないトルクや速度を発生させないことを保証するための重要な要件です。 しかし、フィールド指向制御(FOC)のような複雑なアルゴリズムを機能的に安全なコンポーネントとして実装すると、アーキテクチャが著しく複雑化し、開発工数が大幅に増加し、全体的なパフォーマンスが低下します。 この問題を解決するために、NXPはセーフティ分解アプローチを採用しています。これにより、アプリケーションは安全関連以外の部分(QM)と安全関連の部分(ASIL)に分割されます。この枠組みの中で、NXPはASCLIB (オートモーティブ セーフティ チェッカーライブラリ)を提供しています。セーフティ部分向けのすぐに使えるセーフティチェッカーを提供することで、QMモータ制御部分を再設計することなく、高いセーフティ基準への準拠を実現できます。 完璧な組み合わせ:AMMCLIB(QM)+ASCLIB(ASIL) ほとんどの顧客は、コアとなるMC処理に、高度に最適化されたNXP AMMCLIB (自動車用数学およびモーター制御ライブラリ)を利用しています。AMMCLIBは優れたパフォーマンスを発揮するものの、品質管理(QM)レベルのライブラリである。 ISO 26262などの安全規格に準拠するためには、チームはQMレベルのAMMCLIBを中心に独自の安全機構を構築する必要があり、多大な時間と労力がかかった。このプロセスを効率化するため、NXPは標準化された、すぐに実用化可能なソリューションとしてASCLIBを提供しています。包括的な事前検証済み安全チェックツールを提供することで、独自の安全ソフトウェア開発の必要性を大幅に削減し、設計から認証までのサイクルを加速します。 AMMCLIBとASCLIBの連携方法 この概念が実際にどのように適用されるかを説明するために、以下のブロック図は標準的なフィールド指向制御(FOC)システムの例を示しています。このシナリオでは、モーター制御ブロックは既存のQMレベルのAMMCLIBコード上で動作し、ASCLIB安全チェッカーが重要なポイントを監視して安全性を確保します。このアーキテクチャは、 FOC PMSM向けのIEEE低複雑度セーフティコンセプトに基づいています。 このリファレンスアーキテクチャは、ASCLIBを統合する際に、既存のQMモータ制御アーキテクチャに変更を加える必要がないことを示しています。完全なデータ型互換性により、ASCLIBチェッカーはAMMCLIB信号に直接マッピングできるため、シームレスな相互接続が保証されます。 標準的なFOCは一般的な使用例ですが、ASCLIBはそれに限定されるものではありません。モジュール式で独立したブロックのおかげで、このライブラリは、センサーレスFOCやシングルシャント電流測定など、代替トポロジーや高度な技術をサポートしています。 ASCLIBの内部構造:階層型セーフティアーキテクチャ ASCLIBは、階層的にレイヤーとパッケージに整理された、高度に構造化された階層型ソフトウェアモデルを特徴としています。 サービス層(最上位層) 2つの独立したパッケージを通じて、高度な機能を安全アプリケーションに直接公開します。 高レベルチェッカー(HLC):さまざまなモータ制御システム向けにカスタマイズされた、幅広いアプリケーションのセーフティチェッカー。 障害マネージャ(FMG):エラーの同期、構成、およびアプリケーション通知を管理する高度な障害処理コンポーネント。 コア層(基礎層) サービス層で使用される低レベルの構成要素を提供します。これは2つの重要なパッケージで構成されています。 低レベルチェッカー(LLC):基本的な数学的機能と認証機能を提供します。 フォールトデバウンス(FDB):汎用的なフォールトデバウンスアルゴリズムを提供します。 💡 開発者向けヒント:ライブラリ全体は完全にモジュール化され、分離されており、独立しています。アプリケーションに独自のチェッカーが必要な場合は、LLCおよびFDBパッケージ内の既存の低レベルブロックを使用して、独自のカスタムチェッカーを簡単に構築できます。さらに、障害マネジメント(FMG)パッケージは完全にオプションであり、使用を強制されることはなく、代わりに独自のアプリケーションレベルのエラー処理を実装することも可能です。 オートモーティブに限らない 名前に惑わされないでください。ASCLIBは名称に「オートモーティブ」という言葉を含み、 ISO 26262ワークフローをネイティブにサポートし、そのセーフティ原則は普遍的なものです。ASCLIBは、IEC 61508に準拠したインダストリアルシステムに最適です。 既存の開発ワークフローにシームレスに統合できるよう、ASCLIBは2種類の配信オプションを提供しています。 純粋なC言語ソースファイル:ベアメタルまたはRTOSベースの組み込みプロジェクトに直接統合できます。 BAM(ビット精度モデル):モデルベース設計(MBD)用のすぐに使えるブロックで、セーフティアーキテクチャをMATLAB/Simulinkに直接ドラッグ&ドロップしてシミュレーションできます。 開発者にとっての主なメリット AMMCLIBは引き続きQM用です。コアMCには、既存の高度に最適化されたAMMCLIBコードを引き続き使用してください。 モデルベース開発:専用のASCLIB BAMを使用してMATLAB/Simulink内でセーフティ部品全体を構築およびシミュレーションしてからターゲットCコードを生成することで、設計サイクルを加速します。 認証手続きの迅速化:事前に設計されたセーフティブロックと統合された障害マネジメント機能により、セーフティ基準への準拠と監査プロセスが大幅に簡素化されます。 さあ、始めて、あなたの考えを共有しましょう ASCLIBは完全にMCUに依存しないように設計されているため、さまざまなハードウェアプラットフォームに柔軟に展開できます。開発を加速させるため、本製品は既に完全な検証済みであり、NXPのオートモーティブおよびインダストリアルMCUとの統合に対応しています。制御と安全性を分離することで、最高のモーター性能と妥協のない安全性という、両方の利点を享受できます。 近々、ISO 26262またはIEC 61508規格に準拠したモーター制御プロジェクトに取り組んでいますか?AMMCLIB + ASCLIB アプローチが設計をどのように簡素化できるかについて、コメント欄で議論しましょう。または、以下のフォームからフィードバックをお寄せください。[フォームへのリンク] 機能的に安全なモーター制御システムを構築することは、性能を犠牲にしたり、アーキテクチャを再設計したりすることを意味するものではありません。NXPがAMMCLIBとASCLIBを組み合わせることで、セーフティと制御を分離し、開発労力を削減し、認証を迅速化する方法を、効率性を損なうことなくご紹介します。 モータ制御 Re: Functional Safety in Motor Control with AMMCLib and ASCLib ASCLibはAMMCLibとの組み合わせでのみ動作するのでしょうか?ASCLibはいつ、どのように普及させるべきでしょうか? Re: Functional Safety in Motor Control with AMMCLib and ASCLib こんにちは、 ASCLibはAMMCLibだけに限定されるものではありません。ASCLibはデータ型レベルでAMMCLibと完全に互換性がありますが、技術的には他のライブラリやカスタムアルゴリズムとも制限なく統合可能です。   プロモーションについて: ASCLibはまだ正式にリリースされていません。しかし、私たちは実際の現場からのフィードバックを収集するために、積極的に情報共有を行っています。現在のギャップやASCLibがどのようにそれを埋められるかについて、お客様からのフィードバックを大変ありがたく思います。 Re: Functional Safety in Motor Control with AMMCLib and ASCLib こんにちは、とても強力なライブラリのようですが、ASCLibはプレミアム(有料)ソフトウェアになる予定ですか?お客様と話す際に使える資料は何でしょうか?ベータ版をリリースする予定はありますか?
View full article
使用 ammClib 和 ASClib 实现电机控制的功能安全 在为汽车和工业系统开发电机控制时,功能安全是确保电机不会产生意想不到的扭矩或速度的核心要求。 但是,将诸如磁场定向控制 (FOC) 之类的复杂算法作为功能安全的组件实现会带来严重的架构复杂性,显著增加开发工作量并降低整体性能。 为了解决这个问题,恩智浦采用了功能安全分解方法。这将应用程序分为非功能安全相关部分 (QM) 和功能安全相关部分 (ASIL)。在此框架内,恩智浦提供了 ASCLIB(汽车功能安全检查器库)。它为功能安全部分提供即用型功能安全检查器,使您无需重新设计 QM 电机控制部件即可实现高度的功能安全合规性。 完美匹配:AMMCLIB (QM) + ASCLIB (ASIL) 大多数客户依靠高度优化的恩智浦 AMMCLIB(汽车数学和电机控制库)来实现核心 MC。AMMCLIB 性能出众,是质量管理 (QM)级别的库。 遵守功能安全标准(例如ISO 26262)要求团队围绕质量管理级别的AMMCLIB建立自定义功能安全机制,这需要花费大量的时间和精力。为了简化这一流程,恩智浦现在提供 ASCLIB 作为标准化的生产就绪解决方案。通过提供一整套预先验证的功能安全检查器,它显著减少了对专有功能安全软件开发的需求,并加快了设计到认证的周期。 AMMCLIB 和 ASCLIB 如何配合使用 为了说明这一概念如何转化为实践,下面的方框图提供了标准磁场定向控制 (FOC) 系统的示例。在这种情况下,电机控制模块根据您现有的 QM 级 AMMCLIB 代码运行,而 ASCLIB 功能安全检查器则监测关键点以确保安全。该架构基于 FOC PMSM 的 IEEE 低复杂度功能安全概念。 该参考架构表明,集成 ASCLIB 无需更改现有的 QM 电机控制架构。全面的数据类型兼容性允许 ASCLIB 校验器直接映射到 AMMCLIB 信号,确保无缝互联。 虽然标准 FOC 是一种常见的用例,但 ASCLIB 并不局限于此。该库采用模块化独立模块,支持其他拓扑结构和先进技术,包括无传感器 FOC 和单并联电流测量。 ASCLIB 内部:分层功能安全架构 ASCLIB 具有高度结构化的分层软件模型,该模型按层次结构组织为层和包: 服务层(顶层) 通过两个独立的软件包将高级功能直接暴露给功能安全应用程序: 高级检查器 (HLC):为各种电机控制系统量身定制的各种应用级功能安全检查器。 故障管理器 (FMG):复杂的故障处理组件,用于管理错误同步、配置和应用程序通知。 核心层(基础层) 提供服务层使用的低级构造块。它由两个基本套餐组成: 低级检查程序(LLC):提供基本的数学和验证功能。 故障排除 (FDB):提供通用的故障排除算法。 💡 开发人员小贴士 整个程序库是完全模块化、孤立和独立的。如果您的应用程序需要一个独特的检查器,则可以使用 LLC 和 FDB 包中现有的低级块轻松构建自己的自定义检查器。此外,故障管理 (FMG) 包完全是可选的——您无需强制使用它,而是可以实现自己的应用程序级错误处理。 不仅用于汽车 别让名字骗了你。尽管ASCLIB的标题中有 " Automotive " 并且原生支持 ISO 26262 工作流程,但其功能安全原则是通用的。ASCLIB 完全适用于符合 IEC 61508 标准的工业系统。 为了与您现有的开发工作流程无缝衔接,ASCLIB 提供了双重交付选项: 纯 C 源文件:可直接集成到任何裸机或基于 RTOS 的嵌入式项目中。 BAM(位精确模型):用于基于模型的设计 (MBD) 的即用型模块,允许您直接在 MATLAB/Simulink 中拖放和仿真功能安全架构。 开发人员的主要优势 AMMCLIB 保留 QM:继续使用现有的、高度优化的 AMMCLIB 代码来处理核心 MC。 基于模型的开发:在生成目标 C 代码之前,直接在 MATLAB/Simulink 中使用专用 ASCLIB BAM 构建和仿真整个功能安全部件,从而加快设计周期。 加速认证:预先设计的功能安全模块和集成的故障管理可显著简化您的功能安全合规和审计流程。 开始并分享您的想法 ASCLIB 的设计完全独立于 MCU,因此您可以灵活地在各种硬件平台上部署它。为了加快您的开发,它已经过全面验证,可以与恩智浦的汽车和工业微控制器集成。通过将控制与功能安全分开,您可以获得两全其美的效果:最高的电机性能和毫不妥协的功能安全性。 正在执行即将到来的 ISO 26262 或 IEC 61508 电机控制项目?让我们在评论中讨论 AMMCLIB + ASCLIB 方法如何简化您的设计,或通过下面的表格分享您的反馈:[表格链接] 构建功能安全的电机控制系统并不意味着要牺牲性能或重新设计架构。了解恩智浦如何将AMMCLIB和ASCLIB相结合,在不影响效率的情况下将功能安全与控制分开,减少开发工作量并加快认证。 电机控制 Re: Functional Safety in Motor Control with AMMCLib and ASCLib ASCLib 是否只能与 AMMCLib 配合使用?我们应该何时以及如何推广 ASCLib? Re: Functional Safety in Motor Control with AMMCLib and ASCLib 您好, ASCLib 并不局限于 AMMCLib。虽然 ASCLib 在数据类型级别上与 AMMCLib 完全兼容,但从技术上讲,它可以与任何其他库或自定义算法集成,没有任何限制。   关于此次促销活动: ASCLib尚未正式发布。但是,我们正在积极分享相关信息,以收集真实世界的反馈。我们非常希望收到客户的反馈,了解他们目前存在哪些不足,以及 ASCLib 可以如何帮助他们弥补这些不足。 Re: Functional Safety in Motor Control with AMMCLib and ASCLib 您好,ASCLib 看起来是一个非常强大的库,请问它计划成为一款付费软件吗?我们可以使用哪些材料与客户进行讨论?有计划推出测试版吗?
View full article
MCUXpresso for VS Code: Create, Build, and Debug a new Project using AI     A step-by-step walkthrough of how to use Copilot chat to import a multi-task FreeRTOS example for the LPCXpresso55S69, building it, debugging it, and analyzing memory usage – all driven from a single natural-language prompt. Introduction This tutorial shows how GitHub Copilot AI, along with the MCUXpresso for VS Code extension, can drive a complete FreeRTOS workflow from natural-language prompts: importing an SDK example, building it, debugging it, and analyzing the resulting artifact.   Instead of clicking through views, wizards, and commands, an embedded software engineer describes the intended outcome in plain language and the agent orchestrates the extension's language model tools to carry out each step.   In this scenario, the engineer asks the MCUXpresso agent to accomplish an end-to-end task: Get started quickly with a FreeRTOS example from MCUXpresso SDK. Target the LPCXpresso55S69 board. Import the new project as a freestanding example into the VS Code workspace, then build it. Freestanding will prompt for a folder to save the project. Start debugging and automatically resume execution after 10 seconds. Analyze the build artifact to see how much memory is used. Open the linker file used to build the artifact. The MCUXpresso agent decomposes this request into a sequence of tool calls – discovering boards and SDK revisions, listing suitable examples, importing the chosen example, building all configurations, launching and resuming the debug session, opening the Image Info view, and finally opening the linker script. The sections below follow that same order. The MCUXpresso agent leverages skill files that outline how to perform actions through the extension's own tools, so the steps it takes maps directly to functionality you could also trigger manually from the MCUXpresso for VS Code UI. System Architecture FreeRTOS Multi-Task Example — LPCXpresso55S69 System Architecture Overview Hardware 💻 Host PC MCUXpresso for VS Code MCUXpresso Agent/Skills     USB 🔗 Debug Probe On-board LinkServer CMSIS-DAP     SWD TARGET 📟 LPCXpresso55S69 Runs FreeRTOS example   Component Description Host PC Runs VS Code with the MCUXpresso for VS Code extension and the Copilot AI agent and skills. The agent properly imports the SDK example, builds it, launches the debug session, and opens the Image Info and linker views. Debug Probe The on-board LinkServer / CMSIS-DAP debug probe on the LPCXpresso55S69. Bridges USB from the Host PC to the SWD debug interface of the target MCU, and hosts the GDB server used during debugging. LPCXpresso55S69 Target evaluation board (LPC55S69 dual-core Arm Cortex-M33). Runs the FreeRTOS example with multiple tasks. Getting started The engineer describes the whole goal to the MCUXpresso agent in a single natural-language prompt, and the agent carries out each step below in order. Prerequisites This tutorial assumes the environment has already been prepared with the MCUXpresso Installer, which was previously used to install all required dependencies. Before starting you should have: Visual Studio Code with the MCUXpresso for VS Code extension installed and activated, and GitHub Copilot Chat available. All toolchain and tooling dependencies installed via the MCUXpresso Installer: the Arm GNU toolchain, LinkServer debug probe support, CMake and Ninja, and the west / SDK management tooling. MCUXpresso SDK v26.06 installed via the extension. One LPCXpresso55S69 board connected to the Host PC over USB (using the on-board LinkServer / CMSIS-DAP debug probe). If any dependency is missing, the MCUXpresso agent can open the MCUXpresso Installer for you (see Troubleshooting).   Step 1 – Import a FreeRTOS example The engineer opens Copilot Chat and describes the whole goal to in a single prompt – the board, the preferred kind of example (FreeRTOS, multiple tasks), the SDK version, and the follow-up actions. The engineer states the complete goal in natural language.   To satisfy the request, the agent first establishes the context and locates a suitable example using the extension's discovery tools: mcuxpresso_listSupportedBoards – confirms the LPCXpresso55S69 is a supported board. mcuxpresso_listRemoteRevisions – selects the requested MCUXpresso SDK v26.06 revision. mcuxpresso_listSupportedExamples – finds a FreeRTOS example with multiple tasks (for example a freertos_generic example). mcuxpresso_browseFolder – lets the engineer pick the destination folder for the imported example. Choosing where the example will be imported.   The agent confirms the example selection before importing.   The example is fetched and imported into the workspace.   Step 2 – Build the project Once the example is imported, the agent builds it using mcuxpresso_buildProjectAllConfigs , which compiles all configured build configurations for the project. The agent triggers a build of all configurations.   After a successful build, the imported project is visible in the extension's Projects view, ready for debugging and further analysis. The built project appears in the Projects view.   Step 3 – Debug the project The agent starts a debug session with mcuxpresso_startDebug . This launches the GDB server against the LPCXpresso55S69 through the on-board LinkServer / CMSIS-DAP debug probe, flashes the artifact, and halts at the program entry.   Because the engineer asked to automatically resume execution after 10 seconds, the agent then calls mcuxpresso_continueDebug to resume the program, letting the FreeRTOS tasks run on the target. The debug session starts, then execution is resumed automatically. The complementary tool mcuxpresso_pauseDebug can halt the running program again if you want to inspect state after resuming.   Step 4 – Open Image Info To analyze how much memory the firmware uses, the agent opens the Image Info view with mcuxpresso_openImageInfo . This inspects the build artifact and reports the memory footprint – the sizes of the code and data regions and how they map onto the device's flash and RAM. Image Info reports the artifact's memory usage; the linker script is opened alongside it.   Step 5 – Open the Linker Script Finally, the agent opens the linker file used to build the artifact with mcuxpresso_openLinkerScript . The linker script defines the memory regions and section placement referenced by the Image Info analysis, so the engineer can correlate the reported memory usage with the actual linker configuration (shown in the same screenshot above). Verifying the Result  The workflow is successful when all of the following hold: The FreeRTOS example was imported and appears in the Projects view (you can also confirm with mcuxpresso_listProjectsFromWorkspace ). The build completed without errors and produced a build artifact. The debug session started and execution was resumed after the requested delay. The Image Info view shows the artifact's memory usage. The linker script used for the build is open in the editor. Videos The following videos capture the steps for creating and debugging a project using AI in the MCUXpresso for VS Code extension. 1. Create and import a freestanding SDK project for your NXP board using Copilot in VS Code. (function() { var wrapper = document.getElementById('lia-vid-6405639429112w960h540r214'); var videoEl = wrapper ? wrapper.querySelector('video-js') : null; if (videoEl) { if (window.videojs) { window.videojs(videoEl).ready(function() { this.on('loadedmetadata', function() { this.el().querySelectorAll('.vjs-load-progress div[data-start]').forEach(function(bar) { bar.setAttribute('role', 'presentation'); bar.setAttribute('aria-hidden', 'true'); }); }); }); } }})(); (view in My Videos) 2. Build, debug, and analyze memory usage for a FreeRTOS Hello World project with Copilot. (function() { var wrapper = document.getElementById('lia-vid-6405639049112w960h540r139'); var videoEl = wrapper ? wrapper.querySelector('video-js') : null; if (videoEl) { if (window.videojs) { window.videojs(videoEl).ready(function() { this.on('loadedmetadata', function() { this.el().querySelectorAll('.vjs-load-progress div[data-start]').forEach(function(bar) { bar.setAttribute('role', 'presentation'); bar.setAttribute('aria-hidden', 'true'); }); }); }); } }})(); (view in My Videos) Troubleshooting Most issues in this workflow come from missing or incomplete dependencies. In almost all cases the fix is to (re)run the MCUXpresso Installer – the MCUXpresso agent can open it for you with mcuxpresso_openInstaller .   Symptom Likely cause Suggested action Project was not imported A west tooling issue (missing or misconfigured SDK management tooling) Start the MCUXpresso Installer ( mcuxpresso_openInstaller ) and (re)install the SDK / west dependencies, then retry the import. Build error A west issue, or no Arm GNU toolchain installed Start the Installer to install or repair the Arm GNU toolchain and build tooling, then rebuild. No debug probe support LinkServer / debug probe support is not installed Start the Installer and install LinkServer / debug probe support, then reconnect the board. Debug session does not start GDB server failed to launch, or probe/toolchain support is missing Inspect the GDB server terminal output for errors. If probe or toolchain support is missing, start the Installer to install it, then start debugging again. Examples
View full article
Getting Started: MCUXpresso for VS Code Installation & Setup for AI Introduction This Getting Started guide explains how to configure MCUXpresso for VS Code so GitHub Copilot agents can use available AI skills and MCP servers effectively when developing with MCUXpresso software and tools. If you already have MCUXpresso for VS Code installed, you can skip to Step 2 to enable Agentic AI features.  Note: The AI support in the MCUXpresso for VS Code extension is currently an experimental option. Users must enable the support after the extension is installed. Install the Tools The MCUXpresso Installer installs everything you need from a single application. Work through the prerequisites and the two steps below to reach a system that is ready to evaluate the NXP Agentic AI features with GitHub Copilot in VS Code. Prerequisites   Prerequisite Version Link MCUXpresso Installer 26.09+ Download   Note: The MCUXpresso Installer will install ALL software required – VS Code, the extension, and other software dependencies. Follow the instructions below and a single step will establish the base setup.   Step 1 – Install MCUXpresso for VS Code Installer options Enter Administrator mode. On Windows, you may need to run the installer as an administrator to avoid permission-related installation issues. Download and install the MCUXpresso Installer utility.  Launch MCUXpresso Installer from your desktop. Select the following components to install: MCUXpresso SDK Developer Arm GNU Toolchain Standalone Toolchain Add-ons LinkServer MCUXpresso Configuration Tools Note: All other components in the Installer are not required for initial development but can be added later based on other use cases. Click the Install button. Note: The Show details button will expand the selected kits to reveal other items installed as dependencies.   A green check mark will appear next to each item once installation has successfully completed. Step 2 – Enable Experimental AI in MCUXpresso for VS Code Open VS Code Settings Open Settings for the MCUXpresso for VS Code extension to enable the experimental features that support Agentic AI development: Launch VS Code. Open Settings with the shortcut Ctrl + , (Ctrl and comma). Filter by typing mcupresso experimental copilot . Click the box to enable the MCUXpresso Agentic AI resources. Close and relaunch VS Code to finish Agentic AI setup. Done: Your system is now ready to begin evaluating the NXP Agentic AI features using GitHub Copilot in VS Code.   Step 3 – Set up GitHub Copilot AI in VS Code AI features in VS Code require the user to log in to a valid GitHub account. You can use a personal account and receive a Free license, or use a corporate account that may provide Business-level Copilot access.   Display the GitHub Copilot Chat pane. Click on the Right Pane icon in the upper-right corner. Click on the GitHub Copilot icon in the lower-right corner. Log in to a valid GitHub account and authorize VS Code to link with the account. Done: The GitHub Copilot AI features are now active in the Chat pane. Videos The following videos help cover the Getting Started process with GitHub Copilot in VS Code:  1. Connect a GitHub account to Copilot in VS Code and verify it with a simple AI prompt. (function() { var wrapper = document.getElementById('lia-vid-6405641613112w960h540r180'); var videoEl = wrapper ? wrapper.querySelector('video-js') : null; if (videoEl) { if (window.videojs) { window.videojs(videoEl).ready(function() { this.on('loadedmetadata', function() { this.el().querySelectorAll('.vjs-load-progress div[data-start]').forEach(function(bar) { bar.setAttribute('role', 'presentation'); bar.setAttribute('aria-hidden', 'true'); }); }); }); } }})(); (view in My Videos) 2. Use Copilot Chat agents, models, context, dictation, history, targets, and permissions in VS Code (function() { var wrapper = document.getElementById('lia-vid-6405640756112w960h540r272'); var videoEl = wrapper ? wrapper.querySelector('video-js') : null; if (videoEl) { if (window.videojs) { window.videojs(videoEl).ready(function() { this.on('loadedmetadata', function() { this.el().querySelectorAll('.vjs-load-progress div[data-start]').forEach(function(bar) { bar.setAttribute('role', 'presentation'); bar.setAttribute('aria-hidden', 'true'); }); }); }); } }})(); (view in My Videos) 3. Configure Copilot tools, skills, workspace access, models, and privacy settings in VS Code. (function() { var wrapper = document.getElementById('lia-vid-6405642238112w990h540r360'); var videoEl = wrapper ? wrapper.querySelector('video-js') : null; if (videoEl) { if (window.videojs) { window.videojs(videoEl).ready(function() { this.on('loadedmetadata', function() { this.el().querySelectorAll('.vjs-load-progress div[data-start]').forEach(function(bar) { bar.setAttribute('role', 'presentation'); bar.setAttribute('aria-hidden', 'true'); }); }); }); } }})(); (view in My Videos) Getting Started
View full article
Kinetis W:[主题] CoAP 基础知识和实践 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Thread 使用 UDP 上的单播和多播传输提供应用程序框架实现所需的基本服务。 线程规范仅关注网络层;由于它与应用层无关,因此可以设计许多应用层无问题运行。 在该实验室中,用户将使用该应用层的约束应用协议 (CoAP),因为 Thread 堆栈使用 CoAP 进行大多数多跳网络管理和调试消息。 受限应用协议 (CoAP) 是一种专门用于物联网中受限节点和受限网络的 Web 传输协议。它使用具有四种方法的二进制 RESTful 协议 邮政 得到 放 删除 CoAP 还使用 ACK 响应;可确认(请求 ACK)和不可确认的消息。 Thread 堆栈使用 CoAP 来处理大多数多跳网络管理和调试消息   目标 通过本实验用户将修改固件以实现以下列表: 添加2个新的COAP URI资源“/resource1”和“/resource2”。 如果按照 CoAP 标准的规定收到 CON 请求,则在“/resource1”中发送 ACK 消息。ACK 消息中包含默认有效载荷。 所有发往“/resource1”的数据包都将触发一个 NON POST 数据包回复(独立于预期的 ACK 数据包),该回复发往具有默认有效负载的“/resource2”URI 路径。 在 shell 中打印所有 CoAP 事务,以充分了解请求何时发送以及何时收到响应,并指明方法和资源,例如 如果收到了 CON POST,则在 shell 上打印“收到了‘NON’数据包,‘POST’带有有效载荷‘ ’ 如果发送了 NON POST,则在 shell 上打印“已发送‘NON’数据包,带有有效载荷‘ ’的‘POST’ 实验室期望的流程行为如图 1 所示。 图 1 实验室期望行为示意图   设置 在下面的列表中,带有破折号(—)的组件将用于创建此实验室。   2 FRDM-KW41Z —牧师一个 来自最新 NXP 版本的 连接软件 。 — Thread Router 合格设备项目 串行终端 — TeraTerm   图2 FRDM-KW41Z   修改固件 将在 router_eligible_device_app.c 文件 中进行以下更改 。 1.定义在 shell 中用于访问资源的 URI 路径名。 #定义APP_RESOURCE1_URI_PATH“/resource1” #定义 APP_RESOURCE2_URI_PATH“/resource2” 2. 使用 coapUriPath_t 声明 URI 资源。使用此结构时,用户必须输入 URI 路径的长度和上一步创建的路径。 const coapUriPath_t gAPP_RESOURCE1_URI_PATH = {SizeOfString(APP_RESOURCE1_URI_PATH), APP_RESOURCE1_URI_PATH}; const coapUriPath_t gAPP_RESOURCE2_URI_PATH = {SizeOfString(APP_RESOURCE2_URI_PATH), APP_RESOURCE2_URI_PATH}; 3.创建资源的回调。此回调将处理接收到的数据包并根据接收到的 COAP 方法类型执行所需的操作。 static void APP_CoapResource1Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); static void APP_CoapResource2Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); 4. 为接收到的数据包添加回调处理程序,在此函数中将定义根据接收到的 COAP 方法类型执行哪些操作。 APP_CoapResource1Cb 静态无效APP_CoapResource1Cb ( coapSessionStatus_t 会话状态, 无效* pData, coapSession_t *pSession, uint32_t 数据长度 ) { 静态 uint8_t pMySessionPayload[3]={0x31,0x32,0x33}; 静态uint32_t pMyPayloadSize = 3; coapSession_t *pMySession = NULL; pMySession = COAP_OpenSession(mAppCoapInstId); COAP_AddOptionToList(pMySession,COAP_URI_PATH_OPTION,APP_RESOURCE2_URI_PATH,SizeOfString(APP_RESOURCE2_URI_PATH)); 如果(gCoapConfirmable_c == pSession->msgType) { 如果(gCoapGET_c == pSession->代码) { shell_write("'CON' 数据包已接收 'GET',有效载荷为:"); } 如果(gCoapPOST_c == pSession->代码) { shell_write("'CON' 数据包已接收带有有效载荷的 'POST':"); } 如果(gCoapPUT_c == pSession->代码) { shell_write("'CON' 数据包已接收 'PUT',有效载荷为:"); } 如果(gCoapFailure_c!=sessionStatus) { COAP_Send(pSession,gCoapMsgTypeAckSuccessChanged_c,pMySessionPayload,pMyPayloadSize); } } 否则,如果(gCoapNonConfirmable_c == pSession->msgType) { 如果(gCoapGET_c == pSession->代码) { shell_write("'NON' 数据包已接收 'GET',有效载荷为:"); } 如果(gCoapPOST_c == pSession->代码) { shell_write("'NON' 数据包接收到了带有有效载荷的 'POST': "); } 如果(gCoapPUT_c == pSession->代码) { shell_write("'NON' 数据包已接收 'PUT',有效载荷为:"); } } shell_writeN(pData,dataLen); shell_write("\r\n"); pMySession->msgType=gCoapNonConfirmable_c; pMySession->代码=gCoapPOST_c; pMySession->pCallback =NULL; FLib_MemCpy(&pMySession->remoteAddr,&gCoapDestAddress,sizeof(ipAddr_t)); COAP_SendMsg(pMySession,pMySessionPayload,pMyPayloadSize); shell_write("'NON' 数据包以 'POST' 形式发送,有效载荷为:"); shell_writeN((char*)pMySessionPayload,pMyPayloadSize); shell_write("\r\n"); } 每个 UDP 端口可以有一个 COAP 实例,如果应用程序只使用一个端口,则一个实例就足够了。 每个实例可以有多个 COAP 会话,每个数据包/事务都有一个 COAP 会话。在这种情况下,由于期望的结果是获得不同的 ACK 响应,因此需要使用新资源创建新的会话。 APP_CoapResource2Cb   静态无效APP_CoapResource2Cb ( coapSessionStatus_t 会话状态, 无效* pData, coapSession_t *pSession, uint32_t 数据长度 ) { 如果(gCoapNonConfirmable_c == pSession->msgType) { shell_write("'NON' 数据包接收到了带有有效载荷的 'POST': "); shell_writeN(pData,dataLen); shell_write("\r\n"); } } 5. 创建回调后,必须在函数APP_InitCoapDemo(void)中将其注册到 CoAP 回调数组中。 {APP_CoapResource1Cb, (coapUriPath_t*)&gAPP_RESOURCE1_URI_PATH}, {APP_CoapResource2Cb,(coapUriPath_t*)&gAPP_RESOURCE2_URI_PATH},   关于 CoAP 库的使用,有一些事情需要提及,这些事情在本实验室中没有使用,但可能对其他类型的应用程序有用。 当使用COAP_SendMsg()时,会话将默认自动关闭,除非使用pSession->autoClose进行指示。 发送消息时有两个选项: 可确认( CON ) :等待 ACK 回复,直到收到消息后才会关闭会话,或者在重传次数耗尽时关闭会话。 不可确认( NON ) :对于 NON,在发送消息后立即生效。 如果发送了一条消息但没有得到响应,则会在每个 COAP_ACK_TIMEOUT (以毫秒为单位)后发送一次重新传输,重新传输将以指数方式发送:首先在随机(2,3)秒后,接下来将超时时间加倍,依此类推,直到 达到 COAP_MAX_RETRANSMIT 。 重传停止后,会话将自动关闭并通知应用程序失败,应用程序回调将以状态 gCoapFailure_c 调用 。 当调用回调时当前会话仍然有效,但退出函数后CoAP会话将关闭它。有两种不同的解决方法: 必须创建一个新会话 设置pSession->autoClose = FALSE 。如果 autoClose 设置为 FALSE,请不要忘记使用COAP_CloseSession()从应用程序关闭会话。     运行演示 1.下载修改后的固件到开发板 2. 为每块板子打开一个串口终端,波特率为115200 图3 串行终端及其配置  3. 在其中一个板子的终端输入“ thr create ” ,该板子将成为领导者。 图 4 带有命令“thr create”的板 1 图 5 执行“thr create”命令后的 Board 1   4. 网络创建完成后, 在第二块板的终端中 输入“thr join” 。 图 6 使用命令“thr join”的板 2 图 7 执行“thr join”命令后的板 2 5. 在两个串行终端中输入命令“ifconfig” 。此命令将显示板的所有地址。 图 8 使用“ifconfig”命令后,板 1 图 9 执行“ifconfig”命令后的板 2   6. 为了测试创建的回调,必须发送 CoAP 消息。必须输入以下命令; coap                                                                                      coap CON POST fe80::5df0:2bf0:d69b:1b3c  /resource1 hello                                                                                      图10 CoAP命令发送 7. 发送的结果必须是这样的: —董事会 1 董事会 1 将向董事会 2 请求资源 1 图 11 发送 CoAP 命令之前的 Board 1 由于它已被编码,另一块板将发送 ACK 并打印消息。 图 12 发送 CoAP 命令后的 Board 1 —董事会 2 图13 收到CoAP命令后的Board 2 如果使用CON消息,请求板将收到响应,而如果消息是NON类型,则不会收到响应。 当使用这种类型的消息时,无论包类型如何,发送消息时都会打开一个新会话,并且它将发送非类型的消息。
View full article
Kinetis W: [スレッド] CoAPの基本と実践 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Threadは、UDPを介したユニキャストおよびマルチキャスト伝送を使用して、アプリケーションフレームワークの実装に必要な基本サービスを提供します。 スレッドの仕様は、ネットワーク層にのみ焦点を当てています。多くのアプリケーション層は、アプリケーション層に依存しないため、問題なく実行するように設計できます。 このラボでは、Threadスタックがマルチホップネットワーク管理およびコミッショニングメッセージのほとんどにCoAPを使用するため、ユーザーはこのアプリケーション層のConstrain Application Protocol(CoAP)を使用します。 制約付きアプリケーションプロトコル(CoAP)は、モノのインターネット(Internet of Thing)の制約付きノードと制約付きネットワークで使用する専用のWeb転送プロトコルです。これは、4つのメソッドを持つバイナリRESTfulプロトコルを使用します 投稿 取得 置く 削除 CoAP は ACK 応答も使用します。CONfirmable (ACK が要求されました) メッセージと NONconfirmable メッセージ。 Thread スタックは、マルチホップ ネットワーク管理およびコミッショニング メッセージの大部分に CoAP を使用します   目標 このラボを通じて、ユーザーはファームウェアを変更して次のリストを実現します。 2 つの新しい COAP URI リソース "/resource1" と "/resource2" を追加します。 CoAP 標準で指定されているように CON 要求を受信した場合に備えて、"/resource1" で ACK メッセージを送信します。ACK メッセージにデフォルトのペイロードを含めます。 "/resource1" 宛てのすべてのパケットは、デフォルトのペイロードを持つ "/resource2" URI パス宛ての NON POST パケット応答 (予想される ACK パケットとは無関係) をトリガーします。 すべてのCoAPトランザクションをシェルに出力して、リクエストが送信され、レスポンスがいつ受信されたかを完全に理解し、メソッドとリソースを示します。 CON POST を受信した場合は、シェルに「'NON' packet received, 'POST'」とペイロード ' ' を印刷します。 NON POSTが送信された場合は、シェルに「'NON'パケットが送信されました。ペイロード' 'とともに'POST'を印刷 します ラボが望ましい行動をとるプロセスを図1に示します。 図1 実験室の望ましい行動を示す図   設定 次のリストでは、ダッシュ (—) の付いたコンポーネントが、このラボの作成に使用されるコンポーネントです。   2 FRDM-KW41Z — 牧師 ある 最新のNXPリリースの 接続ソフトウェア 。 — Thread Router Eligible Device プロジェクト シリアルターミナル — テラターム   図2 FRDM-KW41Z   ファームウェアの変更       router_eligible_device_app.c ファイル では、次の変更が加えられます 。 1. シェルでリソースにアクセスするために使用する URI パス名を定義します。 #define APP_RESOURCE1_URI_PATH "/resource1" #define APP_RESOURCE2_URI_PATH "/resource2" 2. URI リソースを coapUriPath_t で宣言します。この構造体を使用する場合、ユーザーは URI パスの長さと、最後の手順で作成したパスを入力する必要があります。 定数 coapUriPath_t gAPP_RESOURCE1_URI_PATH = {SizeOfString(APP_RESOURCE1_URI_PATH), APP_RESOURCE1_URI_PATH}; 定数 coapUriPath_t gAPP_RESOURCE2_URI_PATH = {SizeOfString(APP_RESOURCE2_URI_PATH), APP_RESOURCE2_URI_PATH}; 3. リソースのコールバックを作成します。このコールバックは、受信したパケットを処理し、受信したCOAPメソッドのタイプに応じて必要なアクションを実行します。 static void APP_CoapResource1Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); static void APP_CoapResource2Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); 4.受信したパケットのコールバックハンドラを追加すると、この関数では、受信したCOAPメソッドのタイプに応じて実行されるアクションが定義されます。 APP_CoapResource1Cb static void APP_CoapResource1Cb(coapSessionStatus_t sessionStatus,void *pData,coapSession_t *pSession,uint32_t dataLen){ static uint8_t pMySessionPayload[3]={0x31,0x32,0x33}; 静的uint32_t pMyPayloadSize=3; coapSession_t *pMySession = NULL; pMySession = COAP_OpenSession(mAppCoapInstId); COAP_AddOptionToList(pMySession,COAP_URI_PATH_OPTION, APP_RESOURCE2_URI_PATH,SizeOfString(APP_RESOURCE2_URI_PATH)); if (gCoapConfirmable_c == pSession->msgType) { if (gCoapGET_c == pSession->code) { shell_write("'CON' パケットはペイロードと共に 'GET' を受け取りました: "); } if (gCoapPOST_c == pSession->code) { shell_write("'CON' パケットはペイロードと共に 'POST' を受信しました: "); } if (gCoapPUT_c == pSession->コード) { shell_write("'CON'パケットはペイロードを含む'PUT'を受信しました:"); } if (gCoapFailure_c!=sessionStatus) { COAP_Send(pSession, gCoapMsgTypeAckSuccessChanged_c, pMySessionPayload, pMyPayloadSize); } } else if(gCoapNonConfirmable_c == pSession->msgType) { if (gCoapGET_c == pSession->code) { shell_write("'NON' パケットはペイロードと共に 'GET' を受け取りました: "); } if (gCoapPOST_c == pSession->code) { shell_write("'NON' パケットはペイロードと共に 'POST' を受信しました: "); } if (gCoapPUT_c == pSession->code) { shell_write("'NON' パケットはペイロードと共に 'PUT' を受信しました: "); } } shell_writeN (pData, dataLen); shell_write("\r\n"); pMySession -> msgType=gCoapNonConfirmable_c; pMySession -> コード = gCoapPOST_c; pMySession -> pCallback =NULL; FLib_MemCpy(&pMySession->remoteAddr,&gCoapDestAddress,sizeof(ipAddr_t)); COAP_SendMsg(pMySession, pMySessionPayload, pMyPayloadSize); shell_write("'NON'パケットはペイロード付きで'POST'を送信しました: "); shell_writeN((char*) pMySessionPayload, pMyPayloadSize); shell_write("\r\n"); } アプリケーションが 1 つのポートのみを使用する場合は、UDP ポートごとに 1 つの COAP インスタンスが存在する可能性があります。 インスタンスごとに複数の COAP セッションが存在する可能性があり、COAP セッションはパケット/トランザクションごとです。この場合、ACK の応答が異なることが望ましい結果であったため、新しいリソースを使用して新しいセッションを作成する必要があります。 APP_CoapResource2Cb   static void APP_CoapResource2Cb(coapSessionStatus_t sessionStatus,void *pData,coapSession_t *pSession,uint32_t dataLen){ if (gCoapNonConfirmable_c == pSession->msgType) { shell_write("'NON' パケットは 'POST' をペイロードと共に受信しました: "); shell_writeN(pData, dataLen); shell_write("\r\n"); } } 5. コールバックを作成した後 、コールバックは関数 APP_InitCoapDemo(void) の CoAP コールバック配列に登録する必要があります {APP_CoapResource1Cb, (coapUriPath_t*)&gAPP_RESOURCE1_URI_PATH}, {APP_CoapResource2Cb, (coapUriPath_t*)&gAPP_RESOURCE2_URI_PATH},   CoAPライブラリの使用については、このラボでは使用されなかったが、他のタイプのアプリケーションに役立つ可能性のある点がいくつかあります。 COAP_SendMsg() を使用すると 、 pSession->autoClose の使用方法で示されない限り、セッションはデフォルトで自動的に閉じ ます。 メッセージの送信には、次の 2 つのオプションがあります。 確認可能(CON):ACKの応答を待ち、メッセージを受け取るまでセッションを閉じるか、再送信が使い果たされたときにセッションを閉じます。 確認不可 (NON😞 NO の場合、メッセージを送信した直後。 メッセージが送信され、応答がなかった場合、再送信はCOAP_ACK_TIMEOUTごとに(ミリ秒単位)送信され、再送信は指数関数的に送信されます:最初はランダム(2、3)秒後、次にタイムアウトを2倍にするなど、COAP_MAX_RETRANSMITに達するまで続きます。 再送信が停止すると、セッションは自動的に閉じられ、アプリケーションにエラーが通知され、ステータス gCoapFailure_c でアプリケーションコールバックが呼び出されます。 コールバックが呼び出されても、現在のセッションはまだ有効ですが、CoAP セッションは関数の終了後にコールバックを閉じます。これには2つの異なる作業があります。 新しいセッションを作成する必要があります auto>Close が FALSE に設定されている場合は、アプリケーションからセッションを閉じることを忘れないでください。COAP_CloseSession() を使用して、アプリケーションからセッションを閉じることを忘れないでください 。     デモの実行    1. 変更したファームウェアをボードにダウンロードします 2. 各ボードのシリアル端子をボーレート 115200 で開きます 図3 シリアル端末とその構成  3. ボードの端末タイプ「thr create」の1つでは、このボードがリーダーになります。 図 4 ボード 1 とコマンド "thr create" 図 5 ボード 1 のコマンド「thr create」の後   4.ネットワークが作成されたら 、2番目のボードの端末に 「thrjoin」 と入力します。 図 6 「thr join」コマンドが設定されたボード 2 図 7 ボード 2 のコマンド "thr join" の後 5. 両方のシリアル端末で、コマンド「ifconfig」を入力します。このコマンドは、ボードのすべてのアドレスを表示します。 図 8 ボード 1 のコマンド "ifconfig" の後 図 9 ボード 2 のコマンド "ifconfig" の後   6. 作成されたコールバックをテストするには、CoAP メッセージを送信する必要があります。次のコマンドを入力する必要があります。 coap                                                                                      coap CON POST fe80::5df0:2bf0:d69b:1b3c  /resource1 hello                                                                                      図 10 送信する CoAP コマンド 7. 送信の結果は、次のようになる必要があります。 ― ボード1 ボード 1 は、ボード 2 にリソース1を要求します 図 11 CoAP コマンドを送信する前のボード 1 コード化されたとおりに、他のボードはACKを送信し、メッセージを印刷します。 図 12 CoAP コマンドを送信した後のボード 1 — ボード2 図 13 CoAP コマンドを受信した後のボード 2 CON メッセージを使用する場合、リクエスターボードは応答を受け取りますが、メッセージが NON T ype の場合、応答はありません。  このタイプのメッセージをパッケージタイプとは無関係に使用すると、メッセージの送信時に新しいセッションがオープンされ、NON タイプのメッセージが送信されます。
View full article
Kinetis W: [Thread] CoAP basics and hands on   Thread provides basic services required for application frameworks implementation with the usage of Unicast and Multicast transmissions over UDP. Thread specification is only focused on the network layer; many application layers can be designed to run without any problem as it is application layer agnostic.  In this laboratory the user will work with the Constrain Application Protocol (CoAP) for this application layer as the Thread stack uses CoAP for most of the multi-hop network management and commissioning messages. The Constrained Application Protocol (CoAP) is a specialized web transfer protocol to use with constrained nodes and constrained networks in the Internet of Thing.  It uses a binary RESTful protocol with four methods POST GET PUT DELETE   CoAP also uses ACK responses; CONfirmable (ACK requested) and NONconfirmable messages. The Thread stack uses CoAP for the majority of multi-hop network management and commissioning messages   Objectives Through this laboratory the user will modify the firmware to achieve the following list: Add 2 new COAP URI resources “/resource1” and “/resource2”. Send an ACK message in “/resource1” in case a CON request was received as specified by the CoAP standard. Include a default payload in the ACK message. All packets destined to “/resource1” will trigger a NON POST packet reply (independent from the expected ACK packet) destined to “/resource2” URI path with a default payload. Print in shell all CoAP transactions to fully understand when a request was sent and when a response was received, indicating the method and the resource, e.g. If a CON POST was received, print on shell “‘NON’ packet received, ‘POST’ with payload of ‘ ’ If a NON POST was sent, print on shell “‘NON’ packet sent, ‘POST’ with payload ‘ ’   The process desired behavior by the laboratory is shown in figure 1.   Figure 1 Diagram showing the desired behavior of the laboratory     Setup In the following list, the components with a dash (—) will be the ones used to create this laboratory.   2 FRDM-KW41Z       — Rev.  A Connectivity Software from the latest NXP release.       — Thread Router Eligible Device project Serial Terminal       — TeraTerm   Figure 2 FRDM-KW41Z      Modifying Firmware         The following changes will be made in the router_eligible_device_app.c file.  1. Define the URI path names that will be used in the shell to access the resources. #define APP_RESOURCE1_URI_PATH                       "/resource1" #define APP_RESOURCE2_URI_PATH                       "/resource2"     2. Declare the URI resources with coapUriPath_t. When using this struct the user must enter the length of the URI path and the path created in the last step. const coapUriPath_t gAPP_RESOURCE1_URI_PATH = {SizeOfString(APP_RESOURCE1_URI_PATH), (uint8_t *)APP_RESOURCE1_URI_PATH}; const coapUriPath_t gAPP_RESOURCE2_URI_PATH = {SizeOfString(APP_RESOURCE2_URI_PATH), (uint8_t *)APP_RESOURCE2_URI_PATH};     3. Create the callbacks for the resources. This callbacks will handle the packet received and perform the desired action depending on the type of COAP method received. static void APP_CoapResource1Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); static void APP_CoapResource2Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen);       4. Add the callback handler for the packet received, in this function it will be defined which action will be performed depending on the type of COAP method received. APP_CoapResource1Cb static void APP_CoapResource1Cb ( coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen ) {   static uint8_t pMySessionPayload[3]={0x31,0x32,0x33};   static uint32_t pMyPayloadSize=3;   coapSession_t *pMySession = NULL;   pMySession = COAP_OpenSession(mAppCoapInstId);   //COAP_AddOptionToList(pMySession,COAP_URI_PATH_OPTION, APP_RESOURCE2_URI_PATH,SizeOfString(APP_RESOURCE2_URI_PATH)); pMySession->pUriPath = (coapUriPath_t *)&gAPP_RESOURCE2_URI_PATH;     if (gCoapConfirmable_c == pSession->msgType)   {     if (gCoapGET_c == pSession->code)     {       shell_write("'CON' packet received 'GET' with payload: ");     }     if (gCoapPOST_c == pSession->code)     {       shell_write("'CON' packet received 'POST' with payload: ");     }     if (gCoapPUT_c == pSession->code)     {       shell_write("'CON' packet received 'PUT' with payload: ");     }         if (gCoapFailure_c!=sessionStatus)     {       COAP_Send(pSession, gCoapMsgTypeAckSuccessChanged_c, pMySessionPayload, pMyPayloadSize);     }   }   else if(gCoapNonConfirmable_c == pSession->msgType)   {     if (gCoapGET_c == pSession->code)     {       shell_write("'NON' packet received 'GET' with payload: ");     }     if (gCoapPOST_c == pSession->code)     {       shell_write("'NON' packet received 'POST' with payload: ");     }     if (gCoapPUT_c == pSession->code)     {       shell_write("'NON' packet received 'PUT' with payload: ");     }      }   shell_writeN(pData, dataLen);   shell_write("\r\n");   pMySession -> msgType=gCoapNonConfirmable_c;   pMySession -> code= gCoapPOST_c;   pMySession -> pCallback =NULL;   //FLib_MemCpy(&pMySession->remoteAddr,&gCoapDestAddress,sizeof(ipAddr_t)); FLib_MemCpy(&pMySession->remoteAddrStorage.ss_addr, &gCoapDestAddress, sizeof(ipAddr_t));   //COAP_SendMsg(pMySession,  pMySessionPayload, pMyPayloadSize); COAP_Send(pMySession, gCoapMsgTypeNonPost_c, pMySessionPayload, pMyPayloadSize);   shell_write("'NON' packet sent 'POST' with payload: ");   shell_writeN((char*) pMySessionPayload, pMyPayloadSize);   shell_write("\r\n"); }   There can be one COAP instance per UDP port, in case the application only uses one port, one instance will be enough. There can be multiple COAP sessions per instance, a COAP session is per packet/transaction. In this case as the desired result was to have a different response of the ACK, it will be necessary to create a new session with the new resource. APP_CoapResource2Cb   static void APP_CoapResource2Cb ( coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen ) {   if (gCoapNonConfirmable_c == pSession->msgType)   {       shell_write("'NON' packet received 'POST' with payload: ");        shell_writeN(pData, dataLen);       shell_write("\r\n");   }  }   5. After creating the callbacks, those must be registered in the CoAP callback array in the function APP_InitCoapDemo(void)     {APP_CoapResource1Cb, (coapUriPath_t*)&gAPP_RESOURCE1_URI_PATH}, {APP_CoapResource2Cb, (coapUriPath_t*)&gAPP_RESOURCE2_URI_PATH},   There are some things to mention of the usage of the CoAP library that were not used for this laboratory but might be useful for other types of applications. When using COAP_Send() the session will close automatically by default unless it is indicated with the usage of pSession->autoClose. There are two options while sending the message: Confirmable (CON): It waits for an ACK reply and until it gets the message it will close the session or it will close the session when retransmissions are exhausted. Non-confirmable (NON): For NON, immediately after sending the message. In case a message was sent and there was no response a retransmission will be sent each COAP_ACK_TIMEOUT (in miliseconds), the retransmissions are sent exponentially: first after random (2, 3) seconds, next doubles the timeout and so on, until COAP_MAX_RETRANSMIT is reached. After retransmissions stop, the session is automatically closed and informs the application of failure the application callback will be called with status gCoapFailure_c. When the callback is called the current session is still valid, but CoAP session will close it after exiting the function. There are two different work this out: A new session must be created Set pSession->autoClose = FALSE. If autoClose is set to FALSE, without forgetting to close the session from application, using COAP_CloseSession().     Running the demo    1. Download the modified firmware in the boards 2. Open a serial terminal for each board with a baud rate of 115200 Figure 3 Serial terminal and its configuration  3. In one of the board’s terminal type “thr create”, this board will be the leader. Figure 4 Board 1 with command "thr create" Figure 5 Board 1 after the command "thr create"   4. Once the network has been created type “thr join” in the second board’s terminal.   Figure 6 Board 2 with command "thr join" Figure 7 Board 2 after command "thr join" 5. In both serial terminals type the command “ifconfig”. This command will display all the addresses of the board.   Figure 8 Board 1 after command "ifconfig" Figure 9 Board 2 after command "ifconfig"   6. To test the callbacks created, a CoAP message must be sent. The following command must be typed;   coap                                                                                      coap CON POST fe80::5df0:2bf0:d69b:1b3c  /resource1 hello                                                                                      Figure 10 CoAP command to send 7. The result of sending must look like :   — Board 1 The board 1 will request the board 2 the resource1 Figure 11 Board 1 before sending the CoAP command As it was coded the other board will send an ACK and print the message. Figure 12 Board 1 after sending the CoAP command — Board 2 Figure 13 Board 2 after receiving the CoAP command If using the CON message the requester board will receive a response, while if the message is a NON type it will not have the response.   When using this types of messages independently of the package type when sending a message a new session will be open and it will send a NON type of message.
View full article
FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear All In the download page https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER There is the package pberna67_1-1790030347425.png However if you click the Download button, no download stats.  I need to support LPC1766, but it seams it is not supported by version 3 (strange because the Driver is indicated), but still I don't see any driver in version V2 for LPC1766 Thanks Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael Thanks for your fast replay! I'm already using Jlink/MCU Link and MCU Link2 without any driver, to read/write variables, however I would like to add also the Application Command management (nothing more than that). I don't need any support of USB/UART/CAN ect... interface support. " The "dreg" directory then contains drivers which do not depend on the SDK at all. The "dreg" drivers use a direct register access instead - this is basically what you need, but unfortunately again, the legacy LPC is not in the list." With this additional limitations, do you think that  dreg directory contents  is enough  for me ? I read  that V2 version the driver should support also LPC1766. Is it true ? Can you send me this driver? Thanks Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Paolo, the link you used to get the FreeMASTER driver is correct.  Unfortunately, this driver only supports the newer devices supported by NXP MCUXpresso SDK. The LPC1766 is not supported by the SDK. There are two options for you when using LPC1766: - Use FreeMASTER over JTAG (Segger J-Link or LPCLink2/CMSIS-DAP) - This will enable you to inspect and control variables. No communication driver is needed, FreeMASTER accesses the memory while the MCU is running. - Get the driver for a different part and port it to LPC1766. See more details below: The reason for the SDK dependency is that the FreeMASTER driver layers its communication drivers on top of SDK low-level drivers. You can still get the full FreeMASTER "middleware" driver from the SDK builder link when you select one of supported MCUs, such as (e.g. MCXN947). After downloading you will find the FreeMASTER code in the middleware/freemaster directory. Note that there are also other drivers in the FreeMASTER package (in the src/drivers), that might be partially useful to you. The mcuxsdk directory contains the primary drivers based on SDK low-level - you can still look at them to understand how the FreeMASTER driver code is structured. The "dreg" directory then contains drivers which do not depend on the SDK at all. The "dreg" drivers use a direct register access instead - this is basically what you need, but unfortunately again, the legacy LPC is not in the list. We have this kind of drivers for NXP DSC, Kinetis, Power Architecture, S12Z and S32 platforms. Porting this concept to LPC shall be quite straightforward task. Regards, Michal Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael, You convinced me to use the direct JLink SWD connection without the support of your Application Command (so there is no need to port the driver to the LPC1766). However, I just discovered that I also need to support the TSA table. In fact, I want to build a configurator for my product (parameter read/write), but it can happen that the firmware in it changes version. I don't have any display to know that version number, so it is not possible to know in advance which firmware image version is loaded, which means it is not possible to load the right .AXF file in FreeMaster in advance. I need to read the address of the variables from the host processor, so unfortunately I need to port the target driver :(, unless there are other ways to work around this problem. The only doubt I have is that you wrote: "You can see that this simple function operates directly on UART peripheral registers. Porting this to LPC means creating similar functions which operate on the LPC UART module (which is different from the Kinetis one)." I shouldn't need to port any peripheral communication driver (UART, CAN, USB), because I only need to support SWD. Is that correct? Can you elaborate more the porting "path trace" for only this option? Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Hello Paolo, no, the V2 driver does not support the LPC. It supports some legacy platforms such as HCS08, HCS12, ColdFire or PowerPC, but not the LPC. If your motivation is just to enable Application Commands, I would suggest that it would be much easier and generally a better solution to change the way how your application is controlled. Application Commands can be easily replaced by picking a few variables into which FreeMASTER writes the control request parameters and use another variable as a "request to process". Once the target application discovers this request variable set, it can process the control command and acknowledge it by resetting the request variable back to zero. This behavior is functionally equal to Application Commands, and it enables to operate over JTAG without any communication driver. To answer your other question: The "dreg" drivers are not directly usable for you. As I wrote, the LPC is not supported, but you can create the port quite easily yourself. If you look at one of UART files such as freemaster_kxx_uart.c, you can find driver functions making atomic UART operations. For example enabling interrupts: You can see, that this simple function operates directly on UART peripheral registers. Porting this to LPC means creating similar functions which operate on LPC UART module (which is different from Kinetis one). Regards, Michal Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael I made the porting of the freemaster_examples/fmstr_example_pdbdm of the lpcxpresso54114 SDK in  the LPC1768 platform using the Keil MCB1700 board . Everything work well. NXP did a very good job, no change in code during the porting activity, it is a very simple task Unfortunately is not possible to attach it the to this forum as .zip file Regards Paolo Thanks and regards
View full article
FreeMASTER 通信驱动程序 3.0,适用于 i.MX、LPC、Kinetis 和 DSC 各位 在下载页面 https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER 包裹在这里。 pberna67_1-1790030347425.png 但是,如果您点击“下载”按钮,则不会显示下载统计数据。我需要支持 LPC1766,但版本 3 似乎不支持(很奇怪,因为驱动程序明明已经标明了),而且我在版本 2 中仍然找不到 LPC1766 的驱动程序。 谢谢 Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔 感谢您的快速回复! 我目前已经在使用 Jlink/MCU Link 和 MCU Link2,无需任何驱动程序即可读取/写入变量,但我还想添加应用程序命令管理功能(仅此而已)。我不需要任何USB/UART/CAN等接口支持。 “dreg”目录则包含完全不依赖于SDK的驱动程序。“dreg”驱动程序改用直接寄存器访问——这基本上就是你需要的,但不幸的是,传统的LPC不在列表中。 考虑到这些额外的限制,您认为 dreg 目录的内容对我来说足够了吗? 我看到有资料说V2版本的驱动程序也应该支持LPC1766。这是真的吗?你能把这个驱动程序发给我吗? 谢谢保罗 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的保罗, 您用来获取FreeMASTER驱动程序的链接是正确的。遗憾的是,该驱动程序仅支持 NXP MCUXpresso SDK 支持的较新设备。SDK 不支持 LPC1766。 使用 LPC1766 时,您有两种选择: - 通过 JTAG(Segger J-Link 或 LPCLink2/CMSIS-DAP)使用 FreeMASTER - 这将使您能够检查和控制变量。无需通信驱动程序,FreeMASTER 可在 MCU 运行时访问内存。 - 获取其他部件的驱动程序并将其移植到 LPC1766。更多详情请见下文: 之所以存在 SDK 依赖关系,是因为 FreeMASTER 驱动程序将其通信驱动程序构建在 SDK 底层驱动程序之上。当您选择支持的 MCU 之一时,例如(例如),您仍然可以从 SDK 构建器链接获取完整的 FreeMASTER“中间件”驱动程序。MCXN947)。下载完成后,您将在 中间件/freemaster 目录中找到 FreeMASTER 代码。 请注意,FreeMASTER 软件包(位于 src/drivers 中)中还有其他驱动程序,这些驱动程序可能对您部分有用。mcuxsdk 目录包含基于 SDK 底层的主要驱动程序 - 您仍然可以查看它们以了解 FreeMASTER 驱动程序代码的结构。“dreg”目录则包含完全不依赖于SDK的驱动程序。“dreg”驱动程序使用直接寄存器访问——这基本上就是你需要的,但不幸的是,传统的LPC不在列表中。我们有适用于 NXP DSC、Kinetis、Power Architecture、S12Z 和 S32 平台的此类驱动程序。将这个概念移植到LPC应该是一项相当简单的任务。 问候, 米哈尔 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔: 你说服我使用直接的 JLink SWD 连接,而不需要你的应用程序命令的支持(因此无需将驱动程序移植到 LPC1766)。然而,我刚刚发现我还需要支持 TSA 表格。事实上,我想为我的产品构建一个配置器(参数读取/写入),但其中的固件版本可能会发生变化。我没有显示版本号,因此无法预先知道加载的是哪个固件映像版本,这意味着无法预先在 FreeMaster 中加载正确的 .AXF 文件。我需要从主机处理器读取变量的地址,所以很遗憾,我需要移植目标驱动程序 :(,除非有其他方法可以解决这个问题。 我唯一的疑问是,你写道: “可以看到,这个简单的函数直接操作 UART 外设寄存器。将此移植到 LPC 意味着创建类似的功能,这些功能在 LPC UART 模块上运行(该模块与 Kinetis 的 UART 模块不同)。 我不需要移植任何外围通信驱动程序(UART、CAN、USB),因为我只需要支持 SWD。是这样吗?能否详细说明一下仅针对此选项的移植“路径跟踪”? 保罗 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 你好,保罗, 不,V2驱动程序不支持LPC。它支持一些旧平台,如 HCS08、HCS12、ColdFire 或 PowerPC,但不支持 LPC。 如果你的动机仅仅是启用应用程序命令,我建议改变应用程序的控制方式会更容易,通常也是更好的解决方案。可以通过选择几个变量来轻松替换应用程序命令,FreeMASTER 会将控制请求参数写入这些变量,并使用另一个变量作为“要处理的请求”。一旦目标应用程序发现此请求变量集,它就可以处理控制命令,并通过将请求变量重置为零来确认该命令。这种行为在功能上等同于应用程序命令,它允许在没有任何通信驱动程序的情况下通过 JTAG 进行操作。 关于你的另一个问题:你无法直接使用“dreg”驱动程序。正如我之前所说,LPC 不受支持,但您可以很轻松地自己创建端口。如果你查看像 freemaster_kxx_uart.c 这样的 UART 文件,你会发现驱动程序函数可以执行原子 UART 操作。例如,启用中断: 您可以看到,这个简单的函数直接操作 UART 外设寄存器。将其移植到 LPC 意味着创建在 LPC UART 模块(与 Kinetis UART 模块不同)上运行的类似功能。 问候, 米哈尔 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔 我使用 Keil MCB1700 板将 lpcxpresso54114 SDK 的 freemaster_examples/fmstr_example_pdbdm 移植到了 LPC1768 平台上。一切运转良好。NXP做得非常好,移植过程中代码没有做任何改动,这是一项非常简单的任务。 很遗憾,无法将其以 .zip 格式附加到此论坛。文件 问候 保罗 谢谢,此致敬礼。
View full article