Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32 Design Studio for ARM v2.2のライセンス期限延長申請 Arm用のS32 Design Studio アクティベーションID: 2FBC-9F2F-AF20-37D9 評価日数:27日 機能バージョン: 2.2 機能ステータス:評価中(27日間) Re: Request to extend expiring license for S32 Design Studio for ARM v2.2 こんにちは、 お客様のS32DSライセンスが延長されました。 Re: Request to extend expiring license for S32 Design Studio for ARM v2.2 はい、今確認したところ、ライセンスが延長されていました。ご協力いただき、誠にありがとうございました!
記事全体を表示
Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive Objective: I am attempting to power my FRDM-MCXN947 development board from an external 1.8V supply. bypassing the default USB 3.3V LDO (U2). My attempts have been unsuccessful, and the microcontroller remains unresponsive until I revert to the default USB power configuration. Hardware Modifications Made: Referencing to FRDM-MCXN947 schematic I have disabled the DCDC core and enabled the LDO core by completing the following changes Populated (Enabled): R17. R194. R20. Removed / DNP (Disabled): R14, R18, R19: These resistors are DNP (Do Not Populate) to disable the DCDC_CORE. 2. Power Supply Setup: External Supply: 1.8V, connected to J25 (P3V3_MCU), pin 1. Jumper Configuration: The J24 (VDD_USB) jumper has been removed to isolate the board from the USB 5V input and the U2 LDO. 3. Observed Behavior: With External 1.8V: The board is completely unresponsive. A pre-flashed "blinky" program does not run. An external debugger detects target voltage but cannot establish communication with the MCU. With Default USB Power (J24 jumper on): Everything functions perfectly. Probing J25 shows 3.3V (from the U2 LDO), and the program runs correctly. 4. Troubleshooting Steps Already Taken: Verified the external power supply is stable and providing a clean 1.8V. Confirmed the power is present on the J25 header. Tried supplying 3.3V to J25 (with J24 off) as a test, but the MCU was still unresponsive. 5. Core Question / Suspected Issue: My understanding from the schematics is that the MCU's primary power rail (VDD_CORE) is fed only through the J24/J25 network. Therefore, disconnecting J24 and applying voltage to J25 should power the MCU directly. The fact that it does not, and that even 3.3V fails to work, suggests I may be missing a critical step or a secondary power requirement. What am I missing? Could there be another voltage rail  that must also be powered for the MCU to boot from an external supply on J25? Any insight would be greatly appreciated. Power Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive Hi Habib,  Thanks for the reply but we switch To MCX-N9XX Eval board Since it has the jumper settings we want and with that we were able to run the board successfully with 1.8v  Thanks again  Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive Hello @ashwinanil, To better assist you, could you please share a picture showing how you are supplying 3.3V to J25, along with any reworks involving resistors that have been made? BR Habib Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive Hi Wimansha, I am trying to make the I3C communication work at 1.8V using the same MCX-N9XX evaluation board. However, I am not able to flash the core and get an error  “Core not discovered” and “target not discovered”. I did some jumper settings which I will highlight them below - 1. For MCU_POWER (1.8V) - JP38 (2-3) to enable rail supply of 1.8V at MCU_PWR. This enables power for the core and the LDO to operate at 1.8V as well as port 1 where I3C is connected. The above jumper setting for 1.8V stops the communication with the MCU, whereas the target MCU is discovered when the rail supply is switched to 3.3V. I would request to please help me with the correct jumper settings or anything else which I am missing during the process.  Your help will be highly appreciated in this regard!  Thanks
記事全体を表示
FRDM-MCXN947ボードの外部1.8V電源の問題 - MCUが応答しない 目的: FRDM-MCXN947 開発ボードに外部 1.8V 電源から電力を供給しようとしています。デフォルトの USB 3.3V LDO (U2) をバイパスします。私の試みは失敗し、デフォルトの USB 電源構成に戻すまでマイクロコントローラは応答しないままです。 行われたハードウェアの変更: FRDM-MCXN947回路図を参考に、以下の変更を行ってDCDCコアを無効にし、LDOコアを有効にしました。 入力済み(有効): R17 。 R194 。 R20。 削除済み/DNP(無効): R14、R18、R19:これらの抵抗器は、 DCDC_CORE を無効にするためにDNP (Do Not Populate)です。 2. 電源の設定: 外部電源: 1.8V、 J25 (P3V3_MCU)、ピン 1にコネクテッド。 ジャンパー構成:ボードを USB 5V 入力と U2 LDO から分離するために、 J24 (VDD_USB)ジャンパーが削除されています。 3. 観察された行動: 外部1.8Vの場合:ボードはまったく反応しません。事前にフラッシュされた「点滅」プログラムは実行されません。外部デバッガーはターゲット電圧を検出しましたが、MCU との通信を確立できません。 デフォルトの USB 電源 (J24 ジャンパーがオン) の場合:すべてが完璧に機能します。J25 をプローブすると 3.3V (U2 LDO から) が表示され、プログラムは正常に実行されます。 4. すでに実行したトラブルシューティング手順: 外部電源が安定しており、クリーンな 1.8 V を供給していることを確認しました。 J25 ヘッダーに電力が供給されていることを確認しました。 テストとして J25 (J24 はオフ) に3.3Vを供給してみましたが、MCU はまだ応答しませんでした。 5. 核心的な質問/疑わしい問題: 回路図から私が理解しているのは、MCU のプライマリ電源レール (VDD_CORE) は J24/J25 ネットワークを通じてのみ供給されるということです。したがって、J24 を切断し、J25 に電圧を印加すると、MCU に直接電力が供給されるはずです。それが機能せず、3.3V でも機能しないという事実は、重要な手順または二次電源要件が不足している可能性があることを示唆しています。 何が足りないのでしょうか?MCU が J25 の外部電源から起動するために、別の電圧レールにも電力を供給する必要があるのでしょうか?どのような洞察でも大いに歓迎します。 パワー Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive こんにちは、ハビブさん。 返信ありがとうございます。しかし、必要なジャンパー設定が備わっているため、MCX-N9XX評価ボードにスイッチしました。これにより、1.8Vでボードを正常に動作させることができました。 再度、感謝します Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive こんにちは@ashwinanil 、 より適切にサポートするために、J25 に 3.3V を供給する方法と、抵抗器に関連する再作業を示す写真を共有していただけますか? BR ハビブ Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive こんにちは、ウィマンシャさん。 同じMCX-N9XX評価ボードを使ってI3C通信を1.8Vで動作させようとしています。しかし、コアをフラッシュすることができず、「コアが検出されません」および「ターゲットが検出されません」というエラーが発生します。ジャンパー設定をいくつか行ったので、以下にその内容を説明します。 1.MCU_POWER (1.8V) の場合 - JP38 (2-3) で MCU_PWR に 1.8V のレール電源を有効にします。これにより、コアとLDOの電力は1.8Vで動作し、I3Cがコネクテッドポート1でも動作します。 上記のジャンパー設定の1.8VはMCUとの通信を停止しますが、レール電源が3.3Vに切り替わるとターゲットMCUが発見されます。 正しいジャンパー設定、またはその他手順で私が見落としている点について、ご教示いただければ幸いです。 この件に関して、皆様のご協力は大変ありがたく存じます! よろしくお願いします。
記事全体を表示
MCX-N947 Motor Control example code is not available in SDK. Hi Team, I am unable to find the motor control SDK example for the MCX-N947. I am using the latest SDK downloaded through the NXP SDK Builder. Could you please let me know where I can find the example code for motor control on the MCX-N947? Thank you. MCXN Motor Control Re: MCX-N947 Motor Control example code is not available in SDK. Hello @embedabu , Thanks for your post. Regarding the Motor Control demo, it is not necessarily included in every SDK release. If the demo has not changed compared to the previous SDK version, it is typically not repackaged in subsequent SDK releases. You can refer to the MCUXpresso SDK for Motor Control | NXP Semiconductors webpage to identify which SDK version contains the latest available release of a specific demo. For example, for FRDM-MCXN947, the demo can be found in SDK v26.03. for MCXN9XX EVK board, the demo can be found in SDK v2.14. Celeste_Liu_0-1787886386939.png Hope it helps. BR Celeste Re: MCX-N947 Motor Control example code is not available in SDK. Hi, Thank you for your reply. The example was available in SDK V25.09 
記事全体を表示
SDK 中不提供 MCX-N947 电机控制示例代码。 大家好, 我找不到 MCX-N947 的电机控制 SDK 示例。 我使用的是通过 NXP SDK Builder 下载的最新 SDK。请问哪里可以找到 MCX-N947 电机控制的示例代码? 谢谢! MCX N 电机控制 Re: MCX-N947 Motor Control example code is not available in SDK. 你好@embedabu , 感谢你的帖子。 关于电机控制演示,它并非一定包含在每个 SDK 版本中。如果演示程序与之前的 SDK 版本相比没有变化,则通常不会在后续的 SDK 版本中重新打包。 您可以参考MCUXpresso SDK for Motor Control | NXP 半导体网页,以确定哪个 SDK 版本包含特定演示的最新可用版本。 例如,对于FRDM-MCXN947 ,可以在SDK v26.03中找到演示。 对于MCXN9XX EVK 板,演示可以在SDK v2.14中找到。 Celeste_Liu_0-1787886386939.png 希望对您有所帮助。 BR 塞莱斯特 Re: MCX-N947 Motor Control example code is not available in SDK. 你好, 感谢你的回复。 该示例在 SDK V25.09 中提供。
記事全体を表示
MCX-N947 モーター制御の例コードはSDKには含まれていません。 チームの皆さん、こんにちは。 MCX-N947のモーター制御SDKの例が見つかりません。 NXP SDK Builderからダウンロードした最新のSDKを使っています。MCX-N947のモーター制御の例コードがどこにあるか教えていただけますか? よろしくお願いします。 MCX N モータ制御 Re: MCX-N947 Motor Control example code is not available in SDK. こんにちは、 @embedabu さん、 投稿ありがとうございます。 モータ制御のデモについては、必ずしもすべてのSDKリリースに含まれているわけではありません。デモが以前のSDKバージョンと変わっていなければ、通常はその後のSDKリリースで再パッケージされません。 モータ制御のためのMCUXpresso SDK |NXPセミコンダクターズのウェブページを参照して、特定のデモの最新リリースを含むSDKバージョンを特定してください。 例えば 、FRDM-MCXN947のデモは SDK v26.03で見ることができます。 EVKボードMCXN9XXデモはSDK v2.14で見ることができます。 Celeste_Liu_0-1787886386939.png お役に立てば幸いです。 BR セレステ Re: MCX-N947 Motor Control example code is not available in SDK. こんにちは、 お返事ありがとうございます。 この例はSDK V25.09で利用可能でした
記事全体を表示
FRDM-MCXN947 主板的外部 1.8V 电源出现问题-MCU 无响应 目标:我正在尝试使用外部 1.8V 电源为我的 FRDM-MCXN947 开发板供电。绕过默认的 USB 3.3V LDO (U2)。我的尝试没有成功,微控制器仍然没有反应,直到我恢复到默认 USB 电源配置。 硬件修改: 参考 FRDM-MCXN947 原理图我禁用了 DCDC 内核并通过完成以下更改启用了低压差线性稳压器(LDO) 内核 已填充(启用): R17. R194. R20. 已删除 / DNP(已禁用): R14、R18、R19:这些电阻为DNP(不填充),用于禁用DCDC_CORE。 2.电源设置: 外部电源:1.8V,连接至J25(P3V3_MCU)第 1 针。 跳线配置:已移除 J24 (VDD_USB) 跳线,以将板与 USB 5V 输入和 U2 低压差线性稳压器隔离开来。 3.观察到的行为: 带外置 1.8V 电压: 董事会完全没有反应。"blinky" 程序无法运行。外部调试器检测到目标电压,但无法与 MCU建立通信。 使用默认 USB 电源(J24 跳线处于打开状态):一切正常。探测 J25 显示 3.3V(来自 U2 LDO),程序可以正常运行。 4.已采取的故障排除步骤: 验证外部电源是否稳定,并提供干净的 1.8V 电压。 确认 J25 接头有电。 试着向 J25 供电3.3V(J24 关断)进行测试,但 MCU 仍无反应。 5.核心问题/疑似问题: 根据原理图,我的理解是 MCU 的主电源轨(VDD_CORE)仅通过 J24/J25 网络供电。因此,断开 J24 连接并向 J25 施加电压应能直接为 MCU 供电。但事实并非如此,甚至 3.3V 也无法工作,这表明我可能缺少了一个关键步骤或一个辅助电源要求。 我错过了什么? 是否还必须有另一个电压轨才能让 MCU 从 J25 的外部电源启动?如有任何见解,我们将不胜感激。 电源 Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive 嗨,哈比卜 感谢您的回复但我们切换到 MCX-N9XX 评估板由于它有我们想要的跳线设置,有了这个我们就能在 1.8v 下成功运行该评估板 再次感谢 Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive 你好@ashwinanil, 为了更好地帮助您,能否请您提供一张图片,说明您是如何向 J25 提供 3.3V 电压的,以及涉及电阻器的任何返工? BR Habib Re: Issue with External 1.8V Power on FRDM-MCXN947 Board - MCU Unresponsive 你好,维曼莎, 我正在尝试使用相同的 MCX-N9XX 评估板,使 I3C 通信在 1.8V 电压下工作。但是,我无法刷写核心,并收到“未发现核心”和“未发现目标”的错误提示。我做了一些跳线设置,下面我会重点介绍一下—— 1.对于 MCU_POWER (1.8V) - JP38 (2-3),可在 MCU_PWR 处启用 1.8V 电源轨供电。这样一来,核心和 低压差线性稳压器(LDO) 以及连接 I3C 的端口 1 都可以在 1.8V 电压下工作。 上述跳线设置为 1.8V 时会停止与 MCU 的通信,而当电源轨切换到 3.3V 时,即可发现目标 MCU。 我想请您帮忙确认一下正确的跳线设置,或者指出我在这个过程中遗漏的任何其他步骤。 在这方面,您的帮助将不胜感激! 谢谢!
記事全体を表示
S32DSライセンスの有効期限が切れました こんにちは、NXPサポートチームの皆さん、 私のS32DS v2.2ライセンスは2026年8月24日に期限切れとなりました。ライセンスの延長を手伝ってもらえますか? アクティベーションコード:563B-6314-7B07-7945 ご支援ありがとうございます。 Re: S32DS License Expired こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。 Re: S32DS License Expired こんにちは: 私のARM 2018R1 IDE用のS32DSライセンスが期限切れです。確認して延長してもらえますか? 私のソフトウェアアクティベーションコードは09D2-DE37-6529-87FBです ありがとうございます。
記事全体を表示
Accessing Micro Safety Manual Hi, On date 12/06/2026 i should have been enable to view secure resources for S32K3. I'm looking for the Safety Manual of S32K358 and i still can't find it at all. I tried in secure documentation here: https://www.nxp.com/products/S32K3#myDocument and in My NXP Account -> Secure Resources but i couldn't find it. Could someone help me? Thanks, Simon Re: Accessing Micro Safety Manual Hi @simon98  We have reviewed your account and our internal records and were unable to locate any previous request for the S32K3 Safety Manual. Could you please help us by requesting higher access permissions to obtain this document? BR, VaneB Re: Accessing Micro Safety Manual Hi @simon98  Please take a look at the NXP SECURE ACCESS RIGHTS FIRST-TIME USER REGISTRATION GUIDE, as you may find it useful.  Re: Accessing Micro Safety Manual hi @VaneB , Could you please tell me how could i request the access of S32K358 safety manual?  I thought having access to secure resourses (which was campleted in 12/06) i'd been able to acces it... BR, Simon Re: Accessing Micro Safety Manual Hi @VaneB  I've already got access to secure resources but i couldn't find the safety manual in secure resources section. I tried to apply a higher rights request specifying my needs. Is it correct? Thanks, Simon Re: Accessing Micro Safety Manual Hi @VaneB , I've checked the guide you mentioned above. I tried to request more higher rights for S32 Automotive Processing Platform but the page riminds me that it's still pending for all the items. I'd ask you if this is the right way to gain access to s32k358 safety manual or if there is other ways slipping off from me, missing something and wath else. Do i need to proivide something in order to gain access to it? Thanks, Simon
記事全体を表示
What Makes a Denver Mobile App Development Company a Good Choice for Businesses? A Mobile App Development Company in Denver can help businesses turn digital ideas into scalable iOS and Android applications with custom features, intuitive interfaces, secure integrations, and reliable backend systems. These services can support customer engagement, business automation, payments, real-time functionality, and other digital requirements. JPLOFT develops customized mobile applications aligned with business goals and user needs.
記事全体を表示
S32DS License Expired Hello NXP Support Team,   My S32DS v2.2 license expired on August 24, 2026. Could you please help extend the license? Activation Code: 563B-6314-7B07-7945   Thank you for your support. Re: S32DS License Expired Hi, your S32DS license has been extended. Please activate S32DS again with your old code.  Re: S32DS License Expired Hi: My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me?  My Software Activation Code is 09D2-DE37-6529-87FB Thanks.
記事全体を表示
マイクロセーフティマニュアルへのアクセス こんにちは、 2026年12月6日時点で、私はS32K3のセキュアなリソースを閲覧できる状態になっているはずです。 S32K358のセーフティマニュアルを探しているのですが、まだ全く見つかりません。 ここ https://www.nxp.com/products/S32K3#myDocument の安全なドキュメントやMy NXPアカウントの「Secure Resources」>で試しましたが、見つかりませんでした。 どなたか助けていただけますか? ありがとう、 サイモン Re: Accessing Micro Safety Manual こんにちは、 @simon98さん お客様のアカウントおよび内部記録を確認しましたが、S32K3セーフティマニュアルの過去のリクエストは見つかりませんでした。この文書を取得するために、より高いアクセス権限を申請する手助けをいただけますか? BR、VaneB Re: Accessing Micro Safety Manual こんにちは、 @VaneB さん。 セーフティマニュアルのアクセスをどう申請すればよいか教えていただけますかS32K358? 安全な資源(2006年12月にキャンプされたもの)にアクセスできると思っていましたが... BR、 サイモン Re: Accessing Micro Safety Manual こんにちは、 @simon98さん 役立つかもしれない「 NXPのセキュアアクセス権初回ユーザー登録ガイド」をご覧ください。 Re: Accessing Micro Safety Manual こんにちは、 @VaneBさん すでに安全なリソースへのアクセスはできていますが、セーフティマニュアルは安全なリソースのセクションで見つかりませんでした。 私は自分のニーズを具体的に明記した、より上位の権限要求を申請しようと試みました。それは正しいですか? ありがとうございます サイモン Re: Accessing Micro Safety Manual こんにちは、 @VaneB さん。 上記で言及されていたガイドを確認しました。 S32自動車処理プラットフォームの権利をさらに高めて申請しようとしましたが、ページがすべてのアイテムについてまだ保留中であることを思い出させてくれました。 これがs32k358セーフティマニュアルにアクセスする正しい方法なのか、それとも他に見落としや見落としがあるのかをお聞きしたいです。アクセスするには何かをプロビッドする必要がありますか? ありがとうございます サイモン
記事全体を表示
访问微型功能安全手册 您好, 截至 2026 年 12 月 6 日,我应该能够查看 S32K3 的安全资源。 我正在寻找S32K358的功能安全手册,但我仍然找不到。 我尝试在以下安全文档中查找: https://www.nxp.com/products/S32K3#myDocument以及“我的 NXP 帐户”->“安全资源”,但都找不到。 请问有人能帮帮我吗? 谢谢, 西蒙 Re: Accessing Micro Safety Manual 嗨@simon98 我们已查阅您的账户和我们的内部记录,但未能找到任何之前对 S32K3 功能安全手册的请求。请您帮忙申请更高的访问权限,以便我们获取这份文件? BR,VaneB Re: Accessing Micro Safety Manual 嗨@simon98 请查阅《NXP 安全访问权限首次用户注册指南》 ,您可能会觉得它很有用。 Re: Accessing Micro Safety Manual 嗨@VaneB , 请问如何申请获取S32K358功能安全手册? 我以为有了安全资源访问权限(这项权限已于 12 月 6 日完成),我就能访问它了…… BR, 西蒙 Re: Accessing Micro Safety Manual 嗨@VaneB 我已经获得了访问安全资源的权限,但我在安全资源部分找不到功能安全手册。 我尝试申请更高的权限,并详细说明了我的需求。这样说对吗? 谢谢! 西蒙 Re: Accessing Micro Safety Manual 嗨@VaneB , 我已查阅过您上面提到的指南。 我尝试申请更高的S32 汽车处理平台权限,但页面提示我所有项目的申请仍在审核中。 我想问一下,这是获取 s32k358 功能安全手册的正确方法吗?还是我遗漏了其他方法,或者还有其他什么原因?我需要提供什么才能获得访问权限? 谢谢! 西蒙
記事全体を表示
SC16IS740:需要帮助配置自动RTS SC16IS740_750_760 我目前正在编写一个MicroPython库,以支持通过SPI接口使用SC16IS740。 我正在使用分线板测试与 MAX3237 连接的 SC16IS740。 所有基本功能均有效(包括 RX & TX FiFo),并通过物理 TX > RX 环回(以及我的示波器)进行了测试。 现在,我想测试/实现自动RTS功能。 为了验证这一点:我放置了一个示波器,通道 1 接 RX,通道 2 接 RTS。 我向接收缓冲区发送大量数据,期望示波器上的RTS信号变为高电平……但这种情况并没有发生。 以下是 Halt_trigger 和 resume_trigger 的值(以字符为单位)的 MicroPython 代码。代码主要读取和写入给定通道(“ch”参数)的寄存器。 数据手册里好像漏掉了什么,但我找不到原因。 备注:最后一条指令强制 RTS 为高电平,以便在瞄准镜上检查手动激活。然后它的值会降到很低,并且永远不会被自动RTS激活……可以肯定的是,RX FIFO已满。 def enable_rts( self, halt_trigger, resume_trigger ): assert 4<=halt_trigger<=60, "RTS trigger must be within 4-60 range" assert 4<=resume_trigger<=60, "RTS trigger must be within 4-60 range" assert (halt_trigger%4) + (resume_trigger%4) == 0, "Trigger level are step by 4!" assert halt_trigger > resume_trigger, "halt_trigger must be greater than resume_trigger!" _halt = halt_trigger//4 _resume = resume_trigger//4 # Set LCR=0xBF to access EFR register _old_lcr = self.owner.bus_wrapper.read_reg( REG_LCR, ch=self.ch ) # store transmission config (eg: 8n1) self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # activate enhanced feature _efr = self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch) _efr = _efr | 0b00010000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enhanced function activation') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Enable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr | 0b00000100 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Enable TCR & TLR register') # Set TCR trigger values _tcr = self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch) _tcr = _tcr | (_resume<<4) _tcr = _tcr | _halt self.owner.bus_wrapper.write_reg(REG_TCR, _tcr, ch=self.ch) print( "TCR:", bin(self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch)), "Transmission Control register (resume & halt levels)") # TLR must be cleared (to use TCR) self.owner.bus_wrapper.write_reg(REG_TLR, 0x00, ch=self.ch) print( "TLR:", bin(self.owner.bus_wrapper.read_reg(REG_TLR, ch=self.ch)), "Disable TLR values (so use TCR)") # Disable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr & 0b11111011 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Disable TCR & TLR register') self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # Enable auto RTS flow control _efr = _efr | 0b01000000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enable auto RTS') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Initial State of RTS bit in Modem (MCR) _mcr = self.owner.bus_wrapper.read_reg( REG_MCR, ch=self.ch ) _mcr = _mcr | 0x02 self.owner.bus_wrapper.write_reg( REG_MCR, _mcr, ch=self.ch ) 非常欢迎提出建议和意见。 干杯, 多米尼克 Re: SC16IS740 : Need help to configure Auto-RTS 你好, 根据数据表,我建议检查以下几点: 请确认 EFCR[4] = 0。EFCR[4] 启用自动 RS-485 RTS 控制。当此位被设置时,发射器将控制 RTS 引脚,并且此功能优先于手动 RTS 控制和硬件流控制电路。因此,在使用 Auto-RTS 硬件流控制时,应清除 EFCR[4]。 TLR 未定义 Auto-RTS 停止/恢复阈值。对于 Auto-RTS,接收器 FIFO 触发电平取自 TCR,如果 TCR 位被清除,则取自 FCR。TLR 用于与中断生成相关的可编程发送和接收 FIFO 触发电平。因此,自动RTS操作不应要求清除TLR。 Re: SC16IS740 : Need help to configure Auto-RTS 嗨@ErikaC , 谢谢你的留言。 虽然我检查了 EFCR[4],但我注意到一切都按预期进行。 总之,感谢 EFCR[4],这在未来会非常有用。 问:发生了什么变化? 响应:完全重启电源。 推测:测试和尝试次数过多可能导致 SC16IS7xxx 配置损坏。 感谢您的帮助。 多米尼克
記事全体を表示
SC16IS740:Auto-RTSの設定について助けが必要です SC16IS740_750_760 現在、SPIを使ったこのSC16IS740をサポートするMicroPythonライブラリを書いています。 私はブレークアウトボードを使って、MAX3237に接続されたSC16IS740のテストを行っています。 すべての基本機能(RX & TX FiFoを含む)は正常に動作し、物理的なTX->RXループバック(および私のオシロスコープ)でテスト済みです。 今、Auto-RTS機能をテスト・実装したいと思っています。 確認するために、ch1をRXに、ch2をRTSに接続してオシロスコープを設置しました。 RXバッファをフラッディングして、RTS信号がスコープでHighに切り替わると思っていますが、実際には起こりません。 以下に、halt_trigger と resume_trigger の値 (文字単位) を含む MicroPython コードを示します。コードは主に特定のチャネル(「ch」パラメータ)に対してレジスタの読み書きを行います。 データシートに何か見落としがあるのですが、それが何なのか分かりません。 注記:最後の命令は、オシロスコープでの手動アクティベーションを確認するために、RTSをハイレベルに強制します。その後、その数値が低くなり、オートRTSで一度も起動されません......確かに、RXのFIFOは満タンになります。 def enable_rts( self, halt_trigger, resume_trigger ): assert 4<=halt_trigger<=60, "RTS trigger must be within 4-60 range" assert 4<=resume_trigger<=60, "RTS trigger must be within 4-60 range" assert (halt_trigger%4) + (resume_trigger%4) == 0, "Trigger level are step by 4!" assert halt_trigger > resume_trigger, "halt_trigger must be greater than resume_trigger!" _halt = halt_trigger//4 _resume = resume_trigger//4 # Set LCR=0xBF to access EFR register _old_lcr = self.owner.bus_wrapper.read_reg( REG_LCR, ch=self.ch ) # store transmission config (eg: 8n1) self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # activate enhanced feature _efr = self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch) _efr = _efr | 0b00010000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enhanced function activation') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Enable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr | 0b00000100 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Enable TCR & TLR register') # Set TCR trigger values _tcr = self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch) _tcr = _tcr | (_resume<<4) _tcr = _tcr | _halt self.owner.bus_wrapper.write_reg(REG_TCR, _tcr, ch=self.ch) print( "TCR:", bin(self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch)), "Transmission Control register (resume & halt levels)") # TLR must be cleared (to use TCR) self.owner.bus_wrapper.write_reg(REG_TLR, 0x00, ch=self.ch) print( "TLR:", bin(self.owner.bus_wrapper.read_reg(REG_TLR, ch=self.ch)), "Disable TLR values (so use TCR)") # Disable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr & 0b11111011 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Disable TCR & TLR register') self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # Enable auto RTS flow control _efr = _efr | 0b01000000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enable auto RTS') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Initial State of RTS bit in Modem (MCR) _mcr = self.owner.bus_wrapper.read_reg( REG_MCR, ch=self.ch ) _mcr = _mcr | 0x02 self.owner.bus_wrapper.write_reg( REG_MCR, _mcr, ch=self.ch ) ご意見やご提案を心よりお待ちしております。 乾杯、 ドミニク Re: SC16IS740 : Need help to configure Auto-RTS こんにちは、 データシートに基づき、以下の点を確認することをお勧めします。 EFCR[4] = 0 であることを必ず確認してください。EFCR[4] は Auto RS-485 RTS コントロールを有効にします。このビットが設定されると、**トランスミッタ**はRTSピンの制御を行い、この機能は手動RTS制御およびハードウェアフロー制御回路の両方よりも優先されます。したがって、Auto-RTSハードウェアフロー制御を使用する場合はEFCR[4]をクリアする必要があります。 TLRはAuto-RTSの停止/再開閾値を定義していません。Auto-RTSでは、**レシーバ**のFIFOトリガーレベルはTCRから、またはTCRビットがクリアされている場合はFCRから取られます。TLRは、割り込み生成に関連する、プログラム可能な送信および受信FIFOトリガーレベルに使用されます。したがって、オートRTS動作にTLRのクリアリングは必須ではありません。 Re: SC16IS740 : Need help to configure Auto-RTS こんにちは、 @ErikaC さん。 ご連絡ありがとうございます。 EFCR[4]を確認したところ、すべてが予想通りに進んでいることがわかりました。 ともあれ、EFCR[4]ありがとうございます。FUTURE的に役立つでしょう。 質問:何が変わったのですか? 応答:完全な電源サイクル。 推測:テストと試行錯誤が多すぎたために、SC16IS7xxxの設定が壊れてしまった可能性が高い。 ご協力いただきありがとうございます。 ドミニク
記事全体を表示
为什么丹佛移动应用开发公司是企业的理想选择? 丹佛的一家移动应用开发公司可以帮助企业将数字创意转化为可扩展的 iOS 和 Android 应用,这些应用具有自定义功能、直观的界面、安全的集成和可靠的后端系统。这些服务可以支持客户互动、业务自动化、支付、实时功能和其他数字化需求。JPLOFT开发符合业务目标和用户需求的定制化移动应用程序。
記事全体を表示
SC16IS740 : Need help to configure Auto-RTS SC16IS740_750_760  I'm currently writing a MicroPython library to support the SC16IS740 over SPI. I'm using a breakout for testing the SC16IS740 coupled to a MAX3237. Every basic features works (including RX & TX FiFo) and tested with physical  TX->RX Loopback (and my scope). Now, I want to test/implement the Auto-RTS feature. To check it: I placed a scope with ch1 on RX and ch2 on RTS. I flood the RX buffer and expect the RTS signal to switch High on the scope.... but it doesn't happens. Here follows the MicroPython code with value of halt_trigger & resume_trigger (in chars). Code mainly read & write register for a given channel (the 'ch' parameter). I'm missing something with the datasheet but I'm not able to identify it. Remark: the last instructions force the RTS high for checking manual activation at the scope. It then goes low and never gets activated by auto-RTS.... for sure, the RX FIFO get full. def enable_rts( self, halt_trigger, resume_trigger ): assert 4<=halt_trigger<=60, "RTS trigger must be within 4-60 range" assert 4<=resume_trigger<=60, "RTS trigger must be within 4-60 range" assert (halt_trigger%4) + (resume_trigger%4) == 0, "Trigger level are step by 4!" assert halt_trigger > resume_trigger, "halt_trigger must be greater than resume_trigger!" _halt = halt_trigger//4 _resume = resume_trigger//4 # Set LCR=0xBF to access EFR register _old_lcr = self.owner.bus_wrapper.read_reg( REG_LCR, ch=self.ch ) # store transmission config (eg: 8n1) self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # activate enhanced feature _efr = self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch) _efr = _efr | 0b00010000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enhanced function activation') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Enable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr | 0b00000100 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Enable TCR & TLR register') # Set TCR trigger values _tcr = self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch) _tcr = _tcr | (_resume<<4) _tcr = _tcr | _halt self.owner.bus_wrapper.write_reg(REG_TCR, _tcr, ch=self.ch) print( "TCR:", bin(self.owner.bus_wrapper.read_reg(REG_TCR, ch=self.ch)), "Transmission Control register (resume & halt levels)") # TLR must be cleared (to use TCR) self.owner.bus_wrapper.write_reg(REG_TLR, 0x00, ch=self.ch) print( "TLR:", bin(self.owner.bus_wrapper.read_reg(REG_TLR, ch=self.ch)), "Disable TLR values (so use TCR)") # Disable TCR & TLR register access _mcr = self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch) _mcr = _mcr & 0b11111011 self.owner.bus_wrapper.write_reg(REG_MCR, _mcr, ch=self.ch) print( "MCR:" , bin(self.owner.bus_wrapper.read_reg(REG_MCR, ch=self.ch)), 'Disable TCR & TLR register') self.owner.bus_wrapper.write_reg( REG_LCR, 0xBF, ch=self.ch ) # Enable auto RTS flow control _efr = _efr | 0b01000000 self.owner.bus_wrapper.write_reg(REG_EFR, _efr, ch=self.ch) print( "EFR:" , bin(self.owner.bus_wrapper.read_reg(REG_EFR, ch=self.ch)) , 'Enable auto RTS') # Close access to EFR & restore transmission config (eg:8n1) self.owner.bus_wrapper.write_reg( REG_LCR, _old_lcr, ch=self.ch ) # Initial State of RTS bit in Modem (MCR) _mcr = self.owner.bus_wrapper.read_reg( REG_MCR, ch=self.ch ) _mcr = _mcr | 0x02 self.owner.bus_wrapper.write_reg( REG_MCR, _mcr, ch=self.ch )   Hint and suggestions would be warmly welcome. Cheers, Dominique Re: SC16IS740 : Need help to configure Auto-RTS Hello, Based on the data sheet, I would suggest checking the following points: Please verify that EFCR[4] = 0. EFCR[4] enables the Auto RS-485 RTS control. When this bit is set, the transmitter takes control of the RTS pin, and this function has precedence over both manual RTS control and the hardware flow-control circuitry. Therefore, EFCR[4] should be cleared when using Auto-RTS hardware flow control. TLR does not define the Auto-RTS halt/resume thresholds. For Auto-RTS, the receiver FIFO trigger levels are taken from TCR, or from FCR if the TCR bits are cleared. TLR is used for the programmable transmit and receive FIFO trigger levels associated with interrupt generation. Therefore, clearing TLR should not be required for Auto-RTS operation. Re: SC16IS740 : Need help to configure Auto-RTS Hi @ErikaC , Thank for the note. While I did check the EFCR[4], I noticed that everything went as expected. Anyway, thank for the EFCR[4], this will be very useful in the future. Question: What changed? Response: a complete power cycle. Supposition: too many test and tries did probably brick the SC16IS7xxx configuration. Thanks for your help. Dominique
記事全体を表示
S32DS许可证已过期 您好,NXP支持团队, 我的S32DS v2.2许可证已于2026年8月24日到期。请问您能否帮忙延长许可证期限? 激活码:563B-6314-7B07-7945 感谢您的支持。 Re: S32DS License Expired 您好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。 Re: S32DS License Expired 您好: 我的 S32DS for ARM 2018R1 IDE 许可证已过期。您能帮我检查并延长一下吗? 我的软件激活码是 09D2-DE37-6529-87FB 谢谢。
記事全体を表示
デンバーのモバイルアプリ開発会社が企業にとって良い選択肢である理由は何ですか? デンバーのモバイルアプリ開発NXPについては、デジタルアイデアをカスタム機能、直感的なインターフェース、安全な統合、信頼性の高いバックエンドシステムを備えたスケーラブルなiOSやAndroidアプリケーションへと変換するお手伝いをします。これらのサービスはお客様エンゲージメント、ビジネスオートメーション、ペイメント、リアルタイム機能、その他のデジタル要件をサポートできます。JPLOFT は、ビジネス目標やユーザーニーズに沿ったカスタマイズされたモバイルアプリケーションを開発しています。
記事全体を表示
i.MX93 SAI1 TX FIFO errors Platform Board: i.MX93 EVK; /sys/devices/soc0/soc_id=i.MX93, /sys/devices/soc0/revision=1.1. Package marking/mask not yet recorded. Linux: 6.12.20-lts-next-gdfaf2136deb2, PREEMPT, A55. SAI1 at 0x443b0000, TX via 44000000.dma-controller-CH21. SAI1 serial root: 40 MHz from VIDEO_PLL; 40 MHz BCLK, 1.25 MHz frame rate. SAI3/WM8962 is Linux-owned and was idle for the reproductions below. LMX2571 I2S FSK sink: signed 16-bit code in active slot, zero in other slot. Constant code +8500 produces the expected +17 kHz RF offset. Minimal Linux reproduction (M33 remoteproc offline) Custom DTB exposes SAI1 as an ALSA playback device; SAI1 PCM card 0. Static ALSA PCM: hw:0,0, S16_LE, 2 channels, 1,250,000 frames/s; period 2,400 frames, buffer 19,200 frames. No Gaussian filter or other real-time waveform generation. TX FIFO depth 32 words, TX DMA burst 8 words, FIFO watermark 24. Static data: slot 0=8500, slot 1=0. Command: python3 /root/cp7g_static_playback.py --device hw:0,0 --seconds 600 Latest result: 750,000,000 frames written in 599.958 s, ALSA xruns=0. SAI1 FEF IRQ diagnostic: 1 episode, 9 IRQ entries over 2.685 ms. First observed at monotonic uptime about 675.892537 s, approximately 7.16 s before playback stopped; not an end-of-stream drain event. First-IRQ instrumentation (timings are after the hardware FEF assertion) TCSR=0x90150c01; consecutive time reads=41 ns; handler work before first TCSR read=209 ns; first TCSR regmap read=120,607 ns (return 0). FEF W1C regmap write=241,007 ns (return 0), before detailed snapshot. Post-ACK TFR0=0x00020001, read=242,799 ns. Post-ACK eDMA CH21 first raw register read=241,423 ns; total CH21 snapshot time=487,722 ns. CH_CSR=0x80000005, CH_ES=0x00000000, CH_INT=0x00000000, CH_SBR=0x00208003, CH_PRI=0x00000000. The TFR0 and CH21 values were sampled after the acknowledgment, not at initial FEF assertion. The long reads/writes cannot establish that they caused the initial FIFO error; CH_ES=0 only says no channel error was latched when sampled. The FEF is a hardware event despite ALSA xruns=0. Independent simplified firmware reproduction With Linux booted and ALSA capture idle, M33 code drove the same SAI1 TX using a single self-linked eDMA CH21 TCD, constant +8500 / zero slots, no major-loop callbacks, no foreground buffer refill, no Gaussian filter. At 40 MHz BCLK, FIFO depth 32, watermark 24, DMA minor loop 16 bytes, it stopped on SAI1 FEF after 216 s (Rev R). In the post-FEF fault snapshot, CH21_ES=0 and DMA global ES=0; the TCD was still self-linked. Similar faults occurred in later priority and internal-BCLK trials. A half-rate trial also failed. Thus neither Python nor M33 waveform computation/refill is necessary to reproduce the intermittent SAI1 FEF. Linux playback also fails with the M33 offline. Probe loading and external wire length changes did not remove the problem. Additional observation A burst-4 / watermark-28 Linux run had one FEF episode at uptime about 676.889 s on a separate boot; the latest burst-8 fault was at 675.893 s. A system journal search around 670–682 s in the latest boot found no logged activity. Similar uptime is suggestive only, not proof of a timer. Questions for NXP 1. Is there a known i.MX93 rev 1.1 mask erratum or low-power/interconnect condition that can delay SAI1 and eDMA CH21 register access and/or DMA service by 100–250 us while SAI1 TX and its clocks are enabled? 2. What hardware status, clock-gating, interconnect, or eDMA traces can identify the first missed SAI1 FIFO service request before FEF? 3. Does SAI1 TX FEF indicate any condition other than an actual FIFO underrun in this asynchronous master configuration? 4. Are there documented SAI1/eDMA burst, watermark, or clock constraints for continuous 40 MHz BCLK / 1.25 MHz stereo frame output on i.MX93? Can provide custom DTB, Linux fsl_sai.c/h changes and static playback script, M33 self-linked TCD source, full boot clock tree, and scope/RF data. Audio(PDM | I2S | SAI) Re: i.MX93 SAI1 TX FIFO errors Hello, I apologize for the delay, please note that due to limited bandwidth during the holidays in China, the response may be delayed. Thank you for your understanding. 1. No, there are no erratum describing the behavior you are seeing in your design. 2. TCSR[FEF] means that an enabled transmit FIFO has an underrun error, it does not identify whether the cause was a lost DMA request. 3. No, just FIFO underrun. 4. This configuration is within the SAI switching specifications. Please share the modifications you made so we can review them for any noticeable issue that could be contributing to this behavior. Please note that driver modifications are not validated on our side. Best regards.
記事全体を表示