Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi Team, We are using S32 Design Studio 3.6.10 for the development of a Non-AUTOSAR application on the NXP S32K312 Mini Board. The project is currently based on FreeRTOS, using SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zip, which in turn uses SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip as the RTD version. We have successfully implemented the following UDS services: Service 0x10 – Diagnostic Session Control Service 0x22 – Read Data By Identifier Service 0x27 – Security Access Service 0x3E – Tester Present As part of the next development phase, we plan to implement UDS Service 0x29 (Authentication) and would like to leverage HSE/Crypto support for the implementation. To enable this, we installed: SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip The installation completed successfully, and we can see Crypto-related folders (e.g., Crypto_43_HSE, CryIf, Csm, etc.) under the RTD installation directory. However, we are unable to find any HSE/Crypto components in: S32 Configuration Tools (.mex) Peripherals/Drivers view Sample Applications/Examples To verify the setup, we also created a new S32K312 sample project. However, the HSE/Crypto components are still not available for selection. Could you please help clarify the following: How can HSE/Crypto support be enabled for an S32K312 project in S32 Design Studio? Are any additional packages, plugins, SDKs, or HSE firmware required? Is there a specific RTD version or project configuration recommended for using HSE/Crypto together with FreeRTOS on the S32K312? Are the Crypto_43_HSE modules provided by the package intended only for AUTOSAR/EB Tresos-based projects, or can they also be used in Non-AUTOSAR S32 Design Studio projects? Are there any example projects or reference documents available for integrating HSE/Crypto in a Non-AUTOSAR S32K312 application? Any guidance or reference documentation related to HSE/Crypto integration would be greatly appreciated. Thanks & Regards, Pramod Jadhav Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2
In the thread S32DS 3.6.7 RTD 7.0.1 P02 HSE code generation error, I shared a step-by-step guide describing how I installed S32K3 Real-Time Drivers ASR R23-11 Version 7.0.1 P02. You may find it helpful to compare those steps with your current installation process.
Also, when working with HSE, it is necessary to include the HSE Interface files in your project. These files can be obtained from the HSE Firmware package, specifically from the interface folder (C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface).
Finally, although there are no RTD examples specifically developed for the S32K312, the examples available for other S32K3 devices can be used as a good reference, as the implementation is very similar across the family.
You may also find the examples included in the HSE Demo App and the S32K3 MCUs for General Purpose HSE Demo Examples helpful. While these examples do not directly use the Crypto/Hse_Ip drivers, they demonstrate how to work with HSE services.
BR, VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2
The HSE-B Reference Manual, training presentations, and application notes are under NDA and are therefore not publicly available. Access to these materials is provided only through Secure Files.
If you do not currently have access to Secure Files, you can request it by following the procedure described in the NXP Secure Access Rights First-Time User Registration Guide.
Additionally, the HSE Service API Reference Manual, which contains detailed information on how to install, configure, and use HSE, is included in the SE Interface files. It can be found, for example, at the following location: C:\NXP\HSE_FW_S32K344_0_2_55_0\docs
If you plan to use the Hse_Ip/Crypto drivers, we also recommend referring to the Driver User Manual and Integration Manual. These documents provide detailed information about hardware and software requirements, supported configurations, usage guidelines, integration steps, and known limitations. These documents can be found, for example, at: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Thank you for the quick support. I was able to successfully add the HSE driver by following the steps provided in the shared link. Could you please share any reference user manuals, application notes, or documentation that we can use to configure the HSE in the application and validate its functionality on the target board? Thank you for your assistance.
View full article