Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application Hello NXP Support, We are using an S32K311 with HSE_B. Our primary bootloader uses Advanced Secure Boot (ASB) with an AES-CMAC-authenticated Secure Memory Region and a Core Reset entry. UID-diversified ADKPm has already been programmed, and Secure Recovery is enabled. We need to regenerate the authentication data for a replacement Secure Recovery Application after a firmware update, without changing the existing ADKP or retaining its derived signing key in host-accessible memory. The recovery application begins with the Cortex-M7 vector table. Its layout is: Region Address Recovery IVT 0x00480000 Recovery application vector table and code Starts at 0x00482000 Recovery IV, 12 bytes 0x0049FFE4–0x0049FFEF Recovery GMAC, 16 bytes 0x0049FFF0–0x0049FFFF Signing the IVT separately succeeds. However, submitting the raw recovery application's vector-table address to HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN returns HSE_SRV_RSP_INVALID_PARAM. The request uses inTagLength = 28 and an output buffer in system SRAM. On S32K311 HSE_B, with UID-diversified ADKPm already programmed and Secure Recovery enabled, how can the host generate the 12-byte IV and 16-byte GMAC for a raw Secure Recovery Application? HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN returns HSE_SRV_RSP_INVALID_PARAM when pInImage points to the Cortex-M7 vector table. Is there an HSE service that generates the Secure Recovery GMAC using the internally derived ADKP without exposing that key? If not, must the GMAC be generated externally? Additionally, does the IVT Secure Recovery length include the 12-byte IV, and what exact bytes are authenticated? Thank you. Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application Hi @sameer_chawla  Some time ago, the secure recovery process was incorrectly described in the manual (in some old revision, probably 2.3, it is already updated). From that time, I have these additional notes, which summarize how it should be implemented:              Don’t add AppBL header format to Secure Recovery Image              The "First executable byte" of the Secure Recovery Image means its Vector Table start address. Boot header / IVT is not needed in the image.              Don't use HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN service for Secure Recovery Image GMAC generation              The IV should be specified by customer and the GMAC should be generated by customer also (by some general tool like OpenSSL or in separate application project by HSE)              Before customer calculating the GMAC, the 12-byte IV should be added into the image end, and its length(12-byte) also should be added in the image size              Don’t use AES-128 (ADKP) for GMAC calculation. Instead of that, use AES-256 (ADKP-Hash256) to calculate the GMAC as shown in Figure 11 in HSE Firmware reference manual rev. 2.8. The manual now explicitly says in “2.6.1.3.1  Secure Recovery Mode”: Regards, Lukas Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application Hi @lukaszadrapa,  Thank you for the quick reply.  We have since tested an alternative using Advanced Secure Boot, as we wanted to avoid retaining or separately provisioning ADKP-Hash256 for recovery-image GMAC generation. Our configuration is: CB (our primary bootloader) is authenticated through SMR0. SRB (our recovery bootloader) is authenticated through SMR1 using AES-CMAC and an HSE-resident key, following the same authentication approach as CB. The Core Reset entry selects CB as the primary destination and SRB as the alternate destination. If CB authentication fails, HSE authenticates SRB before starting it. Our understanding is that this uses ASB’s authenticated alternate boot path rather than the dedicated ADKP-based Secure Recovery mechanism. ADKP remains provisioned for its existing IVT authentication and secure-debug purposes. Is this a supported and recommended approach on S32K311 HSE_B? Is using a separate SMR and CR alternate boot destination a usual design for an authenticated recovery bootloader, or are there limitations compared with the dedicated Secure Recovery mechanism that we should consider? Thank you,  Sameer Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application Hi @sameer_chawla  Yes, this is also a valid approach. You can use the alternate boot destination instead of the dedicated Secure Recovery mechanism. The choice mainly depends on the level of fallback protection required. If one fallback level is sufficient, using a separate SMR for SRB and configuring it as the alternate boot destination is an appropriate solution. If an additional fallback level is required, for example if authentication of the alternate boot image also fails, the Secure Recovery mechanism can still be used as another recovery level. So, it ultimately depends on the application requirements. There is no inherent limitation in using the alternate boot path for this purpose. In fact, it provides more configuration flexibility than the relatively simple dedicated Secure Recovery image mechanism. Regards, Lukas
View full article
lpx43xx usb0 主机 HID 键盘 你好 我正在使用LPX4357,并且已经成功完成了通过USB HID的键盘接口连接。但是当我连接条码扫描器时,扫描后出现硬故障……只读取/检测到一个字节,然后就出现硬故障……请问这是什么原因造成的?或者有什么建议吗? 请大家帮忙! LPC43xx 外设 USB Re: lpx43xx usb0 host HID keyboard 你好, 我正在尝试连接USB条形码扫描器。我正在使用 LPCOpen 键盘主机示例。连接USB键盘时,系统能够正确接收到输入的任何数据。但是使用条形码扫描器时,扫描的条形码数据仅在开机时接收一次。这种情况有时也会发生,但并非总是如此。每次我从条码扫描器接收到数据后,下次扫描时总是收到HID_Host_IsReportReceived 标志为 false 的情况,导致之后无法从条码扫描器接收到数据。这是管道问题吗?我该如何解决? 控制器 LPC4337 条形码制作 Zebronics。 型号 BS2H1000 此致问候 Re: lpx43xx usb0 host HID keyboard 您好, 我正在尝试连接USB条形码扫描器。我正在使用 LPCOpen 键盘主机示例,我已经获取到键盘按键了。但是当我连接条形码扫描器时,它显示设备已枚举,但无法读取条形码数据。请问需要对键盘代码示例进行哪些修改才能读取条形码数据? 控制器 LPC4337 条形码制造新大陆。 型号 NLS-HR11 温暖的问候。 Re: lpx43xx usb0 host HID keyboard 问题已解决,谢谢。 Re: lpx43xx usb0 host HID keyboard 您的项目是基于lpcopen示例吗?如果是,是哪一个?需要修改吗? 请追踪出错的运行环节?是吗? 列举清楚了吗? Re: lpx43xx usb0 host HID keyboard 我正在使用 LPCUSBLIB 库将 USB 条码扫描器与 LPC4337 控制器连接起来。我想知道清除管道缓冲器的条件是什么。有时候我能正确收到完整的条形码。有时扫描第一个字符后就收不到任何数据,而且USB线还会卡住,导致之后多次扫描条形码都收不到任何数据。 Re: lpx43xx usb0 host HID keyboard 您好@RDGC_member 这个帖子是5年前创建的。我建议你在LPC论坛创建一个新帖子。NXP技术支持会为您提供帮助。 https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc 谢谢! 张军
View full article
EB tresos Studio 32.1.4 Where could I download EB tresos Studio 32.1.4?  S32K3 Standard Software -> Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool , on the path can only find EB tresos Studio 30.0.0 the highest. Re: EB tresos Studio 32.1.4 Hello Peter, I have followed your advice and checked how to apply for secure access, but the process is quite complicated. I don't intend to access highly classified documents; I only wish to download EB Tresos Studio 32.x.x. Is there a way to add EB Tresos Studio 32.x.x to my Product List? Thanks! Re: EB tresos Studio 32.1.4 Hello, Looking at the available versions: So the issue is most probably tied to your NXP SW account. Please follow the FAQ to gain further access: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS Best regards, Peter Re: EB tresos Studio 32.1.4 Hello, My account email: [email protected] Thanks! Re: EB tresos Studio 32.1.4 Hello, Yes, there is a direct way if admin add it to your account. Please share with me account email you are using for it. Best regards, Peter Re: EB tresos Studio 32.1.4 Hello, It should be available at your SW account now. Best regards, Peter
View full article
FRDM-MCXN947 Ethernet port set up - PHY LAN8741A I am struggling to get the ethernet port to connect.  On debug, I keep getting the following below on frdm board.  [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) Link already configured [00:00:00.015,000] eth_nxp_enet_qos_mac: Can't clear SWR [00:00:00.021,000] eth_nxp_enet_qos_mac: Link is down *** Booting Zephyr OS build v4.4.2 *** Starting application and checking MDIO bus... PHY Reg 0x01 (BMSR): 0x7809 PHY Reg 0x05 (Partner Ability): 0xCDE1 PHY Reg 0x1A (Symbol Errors): 51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate timeout [00:00:14.042,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:00:14.062,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:00:14.069,000] eth_nxp_enet_qos_mac: Link is up [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher It seems like MDIO comms is working fine but link keeps resetting every 30ms.  Any clue as to what configuration needs to be to get LAN8741A to work properly on the FRDM-MCXN947 board?  Development Board 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi @thisisdarlensonl  Thanks for the detailed information. To help us further investigate this issue, could you please provide the following information? Which Zephyr sample are you using? Your prj.conf, application overlay file, and build command. Have you made any changes to the FRDM-MCXN947 board DTS? Could you provide the complete log showing the link resetting every 30 ms? I want to reproduce this issue. BR Harry 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi Harry,  Thanks for getting back to me. I have attached the prj.cong and app.overlay file. I started with a hello world sample and build on that. The current version of Zephyr is 4.4.2  As for full console messages. See below  [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) Link already configured [00:00:00.015,000] eth_nxp_enet_qos_mac: Can't clear SWR [00:00:00.021,000] eth_nxp_enet_qos_mac: Link is down *** Booting Zephyr OS build v4.4.2 *** === FRDM-MCXN947 PM-Optimized Heartbeat Demo === Starting application and checking MDIO bus... PHY Reg 0x01 (BMSR): 0x7809 PHY Reg 0x05 (Partner Ability): 0xCDE1 PHY Reg 0x1A (Symbol Errors): 51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate timeout [00:00:14.042,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:00:14.062,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:00:14.069,000] eth_nxp_enet_qos_mac: Link is up [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:00:14.085,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:00:15.094,000] phy_mii: PHY (0) is down [00:00:15.098,000] eth_nxp_enet_qos_mac: Link is down [00:01:08.626,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:01:08.636,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:01:08.646,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:01:08.653,000] eth_nxp_enet_qos_mac: Link is up [00:01:08.659,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:01:08.668,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:01:09.177,000] phy_mii: PHY (0) is down [00:01:09.182,000] eth_nxp_enet_qos_mac: Link is down [00:01:22.193,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:01:22.203,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:01:22.213,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:01:22.220,000] eth_nxp_enet_qos_mac: Link is up [00:01:22.226,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:01:22.235,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:01:22.744,000] phy_mii: PHY (0) is down [00:01:22.749,000] eth_nxp_enet_qos_mac: Link is down [00:03:57.817,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:03:57.827,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:03:57.837,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:03:57.844,000] eth_nxp_enet_qos_mac: Link is up [00:03:57.850,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:03:57.859,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:03:58.368,000] phy_mii: PHY (0) is down [00:03:58.373,000] eth_nxp_enet_qos_mac: Link is down [00:05:08.907,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:05:08.917,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:05:08.927,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:05:08.934,000] eth_nxp_enet_qos_mac: Link is up [00:05:08.940,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:05:08.949,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:05:09.958,000] phy_mii: PHY (0) is down [00:05:09.963,000] eth_nxp_enet_qos_mac: Link is down [00:05:36.980,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:05:36.990,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:05:37.000,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:05:37.007,000] eth_nxp_enet_qos_mac: Link is up [00:05:37.013,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:05:37.022,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:05:38.031,000] phy_mii: PHY (0) is down [00:05:38.036,000] eth_nxp_enet_qos_mac: Link is down [00:12:00.195,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:12:00.205,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:12:00.215,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:12:00.222,000] eth_nxp_enet_qos_mac: Link is up [00:12:00.228,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:12:00.237,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:12:00.746,000] phy_mii: PHY (0) is down [00:12:00.751,000] eth_nxp_enet_qos_mac: Link is down [00:13:41.297,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:13:41.307,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:13:41.317,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:13:41.324,000] eth_nxp_enet_qos_mac: Link is up [00:13:41.330,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:13:41.340,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:13:41.848,000] phy_mii: PHY (0) is down [00:13:41.853,000] eth_nxp_enet_qos_mac: Link is down [00:14:02.868,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:14:02.877,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:14:02.888,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:14:02.894,000] eth_nxp_enet_qos_mac: Link is up [00:14:02.900,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:14:02.910,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:14:03.418,000] phy_mii: PHY (0) is down [00:14:03.423,000] eth_nxp_enet_qos_mac: Link is down [00:14:26.439,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:14:26.448,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:14:26.459,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:14:26.466,000] eth_nxp_enet_qos_mac: Link is up [00:14:26.471,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:14:26.481,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:14:27.490,000] phy_mii: PHY (0) is down [00:14:27.495,000] eth_nxp_enet_qos_mac: Link is down [00:19:14.115,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:19:14.125,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:19:14.135,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:19:14.142,000] eth_nxp_enet_qos_mac: Link is up [00:19:14.148,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:19:14.158,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:19:14.666,000] phy_mii: PHY (0) is down [00:19:14.671,000] eth_nxp_enet_qos_mac: Link is down [00:20:45.214,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:20:45.223,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:20:45.234,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:20:45.240,000] eth_nxp_enet_qos_mac: Link is up [00:20:45.246,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:20:45.256,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:20:45.764,000] phy_mii: PHY (0) is down [00:20:45.769,000] eth_nxp_enet_qos_mac: Link is down [00:25:14.383,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [ 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi @thisisdarlensonl  Thank you for the additional information. For a quick verification, I tested the Zephyr DHCPv4 client sample using the following command: west build -b frdm_mcxn947/mcxn947/cpu0 zephyr/samples/net/dhcpv4_client -p always Initially, I observed a similar issue on my FRDM-MCXN947 board. After checking the board hardware, I found that SJ27 had been reworked. After restoring SJ27 to its default position, I ran the same DHCPv4 client example again and the issue no longer occurred. The PHY was detected correctly and the Ethernet link came up at 100 Mbps full duplex: [00:00:00.050,000] phy_mii: PHY (0) ID 7C121 *** Booting Zephyr OS build v4.4.0-17350-g1ee3b93134be *** [00:00:00.051,000] net_dhcpv4_client_sample: Run dhcpv4 client [00:00:00.051,000] net_dhcpv4_client_sample: Start on ethernet@40100000: index=1 [00:00:03.758,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex Could you please check whether SJ27 or any other Ethernet-related solder jumpers on your FRDM-MCXN947 board have been reworked? If so, please restore them to the default Ethernet configuration and test again. BR Harry 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Thanks @Harry_Zhang, massive help legend. I didn't realize that it was configured for display by default. Now I can move on. Thanks a lot for your help.  It is probably worthwhile noting this somewhere else. Also, the solder jumpers are painful 😉 Again massive thanks
View full article
HTRC11001T 的 EVM 您好, HTRC11001T是否有可用的EVM(评估模块)? Re: EVM of HTRC11001T NXP 没有为 HTRC110 提供专用的官方评估板。 不过,我们可以提供一些参考资料来帮助您进行设计和开发工作。 硬件设计参考:我们建议参考应用笔记AN98080_基于 HITAG 读写 IC 的读写设备。本文档详细介绍了基于HTRC110的读写器设计,包括: 125 kHz 天线设计 谐振和匹配网络设计 外围耦合电路 解调电路原理 时钟和电源相关设计 其他外部元器件选择建议 软件开发参考:NXP 可提供 HTRC110 的相关示例代码和参考文档,作为客户进行底层驱动程序和应用程序开发的起点。但是,申请这两项都需要签署保密协议。 对于评估硬件或现成的读卡器解决方案,我建议查看 NXP ®合作伙伴市场: https://www.nxp.com/design/design-center/partner-marketplace:PARTNER-MARKETPLACE Re: EVM of HTRC11001T 您好, 感谢您的快速回复。 其中一个查询,如 HTRC110 应用笔记中所述,仅针对 HITAG 系列标签进行了优化。那么,这是否意味着它不能与其他标签(例如 EM 系列 (EM4305) 标签)一起使用? Re: EVM of HTRC11001T 你好@Shanmukh 很抱歉,HTRC11001T 没有可用的 EVM(评估模块)! BR 凯莉
View full article
About CW 3.1 Who can provide a download link for CodeWarrior 3.1 that runs on Windows XP? The file  name may be Codewarrior-HC(S)08-v3.1.iso.  Thanks a lot. Re: About CW 3.1 I'm really sorry for the inconvenience this might cause you, but the information and files of this software version is no longer available for download, I need to clarify that CodeWarrior 3.1 is a legacy product. The search results indicate that some CodeWarrior versions for specific devices have not been supported in years, and NXP has transitioned away from maintaining certain legacy CodeWarrior implementations.   You could move to a more recent version, The software tool to use 8 bits devices is CodeWarrior for MCUs (Eclipse IDE) v11.1 available for windows 10/11; in this tool you can test with various 8-bit devices if you are interested. Best Regards
View full article
NXP S32K388マイクロコントローラでサポートされるキースロットの最大数について明確化が必要 こんにちは、チームの皆さん、 S32K388デバイスでサポートされる最大キースロット数について、いくつか確認が必要でした。 以下のRTD 701 QLP04_D2608を統合したところ、5つのSHEグループ(1グループが10キーにマッピング)まで、つまり合計50個のキースロットが制限されていることがわかりました。これはHSE(英国安全衛生庁)による制限ですか? 100個のキースロットを有効にする必要があるため、今回はさらに多くのキースロットを設定できるかどうか知りたいです。 よろしくお願いします! ニムシャ Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro こんにちは、 @Nimshaさん これはRTDの実装による制限ではなく、HSEファームウェア自体によって規定された制限です。 HSE-BファームウェアリファレンスマニュアルRev. 2.8の6.3.2および6.3.3節に記載されているように、NVMキーカタログ内のSHEキーは、10個のキースロットを含むグループ0にマッピングできます。さらに、HSEはSEEキー更新プロトコル(拡張SEEキーと呼ばれる)を用いて追加のAES-128 SHE鍵をプロビジョニング可能にし、グループ1から4までにマッピングでき、各グループに10スロットがあります。ご指摘のとおり、これにより合計50個のSHEキースロットが提供されます。 リファレンス・マニュアルによると、NVM SHEキーカタログの設定は以下の通りです。 行0:MASTER_ECU_KEY、BOOT_MAC_KEY、KEY_1~KEY_10 1行目:KEY_11~KEY_20 2行目:KEY_21~KEY_30 3行目:KEY_31~KEY_40 4行目:KEY_41~KEY_50 hseKeyGroupCfgEntry_t NVM_key_catalog[] = { /* SHE keys */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, HSE_KEY128_BITS}, /* MASTER_ECU_KEY, BOOT_MAC_KEY, KEY_1 to KEY_10 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_11 to KEY_20 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_21 to KEY_30 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_31 to KEY_40 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_41 to KEY_50 */ { 0U, 0U, 0U, 0U, 0U } }; リファレンスマニュアルには、SHEキーをグループ5以上にマッピングしようとすると、キーカタログのフォーマット操作中にエラーが発生すると記載されています。 BR、VaneB Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro こんにちは、 @Nimshaさん これらの仕様は、標準のHSEファームウェアに適用されます。しかし、プレミアムなHSEファームウェア(有料ライセンス製品として提供)は、特定のお客様要件やユースケースに合わせてカスタマイズ可能です。 詳しい内容を記載したプライベートメッセージをお送りしました。 Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro こんにちは、 @VaneBさん ご返信ありがとうございます。 GM OEMは100個のキースロットを有効にするという特定の要件を持っていることがわかりました。この制限事項はGMに認識されているのでしょうか? HSE FWが現在50キースロットのみをサポートしているとおっしゃっていましたが、FUTURE 100キースロットをサポートするファームウェアバージョンがあれば教えていただけませんか? よろしくお願いします! ニムシャ
View full article
Request for "AES_ACCEL Subsystem Reference Manual" Hi NXP  I am currently analyzing the AES_ACCEL (AES Accelerator) module for my project. The documentation mentions referring to the "AES_ACCEL Subsystem Reference Manual", but I am unable to locate or download it from the product page. Could you please let me know where I can obtain this manual, or how I can gain access to download it? Best regards Re: Request for "AES_ACCEL Subsystem Reference Manual" The document is a secure file. Please follow the secure access registration procedure described here, unless you have already completed it: NXP Secure Access Rights Registration For additional information, please refer to: NXP Secure Access Rights Because this particular file has a higher confidentiality level, access is subject to manual approval. If you have already completed the registration but the file is still not available, please contact your NXP representative or distributor and ask them to request the required access for you.
View full article
HTRC11001TのEVM こんにちは、 HTRC11001T用のEVM(評価モジュール)はありますか? Re: EVM of HTRC11001T NXPはHTRC110専用の公式評価ボードを設置していません。 ただし、デザインや開発作業を支援するための参考資料をご提供することは可能です。 ハードウェアデザイン参考文献: HITAG読み書きICに基づくアプリケーションノート AN98080_Read書き込みデバイスを参照することをお勧めします。この文書は、HTRC110に基づくリーダー/ライター デザインの詳細を述べています。 125 kHzアンテナデザイン 共振およびマッチングネットワークデザイン 周辺結合回路 デモジュレーション回路の原理 クロックおよび電源関連デザイン その他の外部部品選択の推奨事項 ソフトウェア開発リファレンス:NXPは、お客様が低レベルのドライバおよびアプリケーション開発を行うための出発点として、HTRC110に関連するサンプルコードや参照ドキュメントを提供できます。しかし、どちらの場合も申請には秘密保持契約(NDA)が必要です。 評価用ハードウェアや既製のリーダーソリューションについては、NXP®パートナー市場をご確認ください。 https://www.nxp.com/design/design-center/partner-marketplace:PARTNER-MARKETPLACE Re: EVM of HTRC11001T こんにちは、 迅速なご返信をありがとうございます。 HTRC110のアプリケーションノートに記載されているように、HITAGシリーズタグ専用に最適化されたクエリの一つです。ということは、EMシリーズ(EM4305)タグなど他のタグでは動作しないということですか? Re: EVM of HTRC11001T こんにちは、 @Shanmukh さん。 HTRC11001T用のEVM(評価モジュール)は現在提供されておりません。申し訳ございません。 BR ケリー
View full article
S32K311 HSE_B ASB:生のセキュアリカバリーアプリケーション用のADKP由来GMAC生成 こんにちは、NXPサポートの皆さん、 私たちはHSE_Bを搭載したS32K311を使用しています。プライマリブートローダーはAES-CMAC認証のSecure Memory RegionとCore Reset エントリを持つAdvanced Secure Boot(ASB)を使用しています。UIDを多様化したADKPmは既にプログラムされており、セキュアリカバリが有効になっています。 既存のADKPを変更したり、ホストがアクセス可能なメモリに派生署名キーを保持したりせずに、ファームウェアアップデート後に交換用のSecure Recovery Applicationの認証データを再生成する必要があります。 リカバリーアプリケーションはCortex-M7ベクターテーブルから始まります。その配置は以下の通りです: 地域住所 回復IVT 0x00480000 リカバリーアプリケーションベクターテーブルとコードは0x00482000から始まります リカバリーIV、12バイト0x0049FFE4–0x0049FFEF リカバリーGMAC、16バイト 0x0049FFF0–0x0049FFFF IVTに別途署名することは成功します。しかし、生のリカバリーアプリケーションのベクターテーブルアドレスをHSE_SRV_ID_BOOT_DATA_IMAGE_SIGNに送信するとHSE_SRV_RSP_INVALID_PARAM返されます。このリクエストはinTagLength = 28とシステムSRAM内の出力バッファを使用します。 S32K311 HSE_Bでは、UIDに多様化されたADKPmがすでにプログラムされ、Secure Recoveryが有効になっている場合、ホストは生のSecure Recovery アプリケーションのためにどのようにして12バイトのIVおよび16バイトのGMACを生成できるのでしょうか?HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN pInImage が Cortex-M7 ベクトルテーブルを指すと HSE_SRV_RSP_INVALID_PARAM を返します。 内部で生成されたADKPを使用してセキュアリカバリGMACを生成し、その鍵を公開しないHSEサービスはありますか?そうでない場合、GMACは外部で生成する必要があるのでしょうか? さらに、IVTセキュアリカバリの長さには12バイトのIVが含まれますか?また、具体的にどのバイトが認証されるのでしょうか? ありがとう。 Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application こんにちは、 @sameer_chawla さん 以前、マニュアルに安全な復旧プロセスに関する誤った記述がありました(おそらく2.3という古いバージョンで、現在は更新されています)。それ以降、私は以下の追加メモを作成しました。これらは、どのように実施すべきかをまとめたものです。 セキュアリカバリイメージにAppBLヘッダー形式を追加しないでください セキュアリカバリイメージの「最初の実行可能バイト」とは、そのベクターテーブルの開始アドレスを意味します。イメージにはブートヘッダー/IVTは不要です。 セキュアリカバリイメージのGMAC生成にはHSE_SRV_ID_BOOT_DATA_IMAGE_SIGNサービスを使用しないでください IVはお客様が指定し、GMACもお客様が生成すべきです(OpenSSLのような一般的なツールやHSEの別のアプリケーションプロジェクトで)。 お客様がGMACを計算する前に、12バイトのIVを画像側に追加し、その長さ(12バイト)も画像サイズに加算する必要があります GMAC計算にはAES-128(ADKP)は使わないでください。それではなく、HSE Firmwareのリファレンスマニュアルの図11に示されているように、AES-256(ADKP-Hash256)を使ってGMACを計算してください。2.8. マニュアルには「2.6.1.3.1」と明記されています。「セキュアリカバリーモード」: よろしくお願いいたします。 ルーカス Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application こんにちは、 @lukaszadrapa さん。 迅速なご返信ありがとうございます。 その後、リカバリイメージのGMAC生成のためにADKP-Hash256を保持したり、別途プロビジョニングしたりすることを避けたかったため、Advanced Secure Bootを使用した代替案をテストしました。 当社の構成は以下のとおりです。 CB(当社の主要ブートローダー)はSMR0を介して認証されます。 SRB(リカバリーブートローダー)は、AES-CMACとHSE常駐キーを用いてSMR1を通じて認証され、CBと同じ認証方式に従っています。 コアリセットのエントリでは、プライマリ宛先としてCB、代替宛先としてSRBが選択されます。CB認証が失敗した場合、HSEはSRBを起動前に認証します。 我々の理解では、これは専用のADKPベースのセキュアリカバリメカニズムではなく、ASBの認証済み代替ブートパスを使用している。ADKPは既存のIVT認証およびセキュアデバッグ目的のために引き続きプロビジョニングされています。 これはS32K311 HSE_Bにおいてサポートされ、推奨されているアプローチですか?認証済みリカバリーブートローダーでは、SMRとCRの別々の代替ブート先を使うのが一般的な設計なのでしょうか?それとも専用のセキュアリカバリー機構と比べて考慮すべき制限があるのでしょうか? ありがとう、 サミール Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application こんにちは、 @sameer_chawla さん はい、これも有効なアプローチです。専用のSecure Recovery機構の代わりに、代替の起動先を使うことができます。 選択は主に、必要とされるフォールバック保護のレベルによって決まります。フォールバックレベルが1つで十分な場合は、SRB用に別のSMRを使用し、それを代替ブート先として構成するのが適切な解決策です。追加のフォールバックレベルが必要な場合、例えば代替ブートイメージの認証も失敗した場合など、Secure Recovery機構は別の回復レベルとして使用できます。 結局のところ、アプリケーション要件によります。この目的で代替ブートパスを使用することに、本質的な制限はありません。実際、これは比較的単純な専用のセキュアリカバリイメージ機構よりも、構成の柔軟性が高い。 よろしくお願いいたします。 ルーカス
View full article
「AES_ACCELサブシステムリファレンス・マニュアル」の要請 こんにちは、NXPさん 現在、プロジェクトのためにAES_ACCEL(AESアクセラレータ)モジュールを分析しています。 ドキュメントには 「AES_ACCELサブシステムリファレンス・マニュアル」を参照していると書かれていますが、製品ページから見つけたりダウンロードしたりできません。 このマニュアルをどこで入手できるのか、またはダウンロードのアクセス方法を教えていただけますか? よろしくお願いいたします。 Re: Request for "AES_ACCEL Subsystem Reference Manual" この文書は安全なファイルです。すでに手続きを完了している場合は、ここに記載された安全なアクセス登録手順に従ってください。 NXPセキュアアクセス権登録 詳細については、以下を参照してください。 NXPセキュアアクセス権 この特定のファイルはより高い機密性レベルであるため、アクセスは手動承認の対象となります。すでに登録を完了しているのにファイルがまだ利用できない場合は、NXPの担当者または代理店にお問い合わせのうえ、必要なアクセス権の申請をお願いしてください。
View full article
FRDM-MCXN947イーサネットポート設定 - PHY LAN8741A イーサネットポートに接続するのに苦労しています。デバッグ中に、FRDMボードで以下のエラーが繰り返し発生します。 [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) リンクは既に設定済みです [00:00:00.015,000] eth_nxp_enet_qos_mac:SWRをクリアできません[00:00:00.021,000] eth_nxp_enet_qos_mac: リンクがダウン Zephyr OSビルドv4.4.2の起動 *** アプリケーションを開始し、MDIOバスをチェックしています... PHYレグ0x01(BMSR):0x7809 PHYレギュラー 0x05(パートナー能力):0xCDE1 PHY登録番号0x1A(記号エラー):51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉タイムアウト [00:00:14.042,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:00:14.062,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:00:14.069,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 MDIO通信自体は正常に動作しているようですが、リンクが30msごとにリセットされてしまいます。 FRDM-MCXN947ボード上でLAN8741Aを正しく動作させるには、どのような設定が必要か、何か手がかりはありますか? 開発ボード 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A こんにちは、 @thisisdarlensonl 詳細な情報ありがとうございます。この問題をさらに調査するために、以下の情報を教えていただけますか? どのZephyrサンプルを使っていますか? prj.conf、アプリケーションオーバーレイファイル、ビルドコマンドです。 FRDM-MCXN947ボードのDTSに変更を加えましたか? リンクが30msごとにリセットされる完全なログを教えてもらえますか? この問題を再現したいと思います。 BR ハリー 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A こんにちは、ハリーさん。 ご連絡いただきありがとうございます。prj.congファイルとapp.overlayファイルを添付しました。 私は「ハローワールド」のサンプルから始めて、それを発展させていきました。現在のZephyrのバージョンは4.4.2です コンソールメッセージ全文については、以下をご覧ください。以下を参照してください [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) リンクは既に設定済みです [00:00:00.015,000] eth_nxp_enet_qos_mac:SWRをクリアできません[00:00:00.021,000] eth_nxp_enet_qos_mac: リンクがダウン Zephyr OSビルドv4.4.2の起動 *** === FRDM-MCXN947 PM-最適化心拍デモ === アプリケーションを開始し、MDIOバスをチェックしています... PHYレグ0x01(BMSR):0x7809 PHYレギュラー 0x05(パートナー能力):0xCDE1 PHY登録番号0x1A(記号エラー):51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉タイムアウト [00:00:14.042,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:00:14.062,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:00:14.069,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:00:14.085,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:00:15.094,000] phy_mii: PHY (0) がダウンしています [00:00:15.098,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:01:08.626,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:01:08.636,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:01:08.646,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:01:08.653,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:01:08.659,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:01:08.668,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:01:09.177,000] phy_mii: PHY (0) がダウンしています [00:01:09.182,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:01:22.193,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:01:22.203,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:01:22.213,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:01:22.220,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:01:22.226,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:01:22.235,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:01:22.744,000] phy_mii: PHY (0) がダウンしています [00:01:22.749,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:03:57.817,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:03:57.827,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:03:57.837,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:03:57.844,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:03:57.850,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:03:57.859,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:03:58.368,000] phy_mii: PHY (0) がダウンしています [00:03:58.373,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:05:08.907,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:05:08.917,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:05:08.927,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:05:08.934,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:05:08.940,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:05:08.949,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:05:09.958,000] phy_mii: PHY (0) がダウンしています [00:05:09.963,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:05:36.980,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:05:36.990,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:05:37.000,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:05:37.007,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:05:37.013,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:05:37.022,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:05:38.031,000] phy_mii: PHY (0) がダウンしています [00:05:38.036,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:12:00.195,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:12:00.205,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:12:00.215,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:12:00.222,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:12:00.228,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:12:00.237,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:12:00.746,000] phy_mii: PHY (0) がダウンしています [00:12:00.751,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:13:41.297,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:13:41.307,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:13:41.317,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:13:41.324,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:13:41.330,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:13:41.340,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:13:41.848,000] phy_mii: PHY (0) がダウンしています [00:13:41.853,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:14:02.868,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:14:02.877,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:14:02.888,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:14:02.894,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:14:02.900,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:14:02.910,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:14:03.418,000] phy_mii: PHY (0) がダウンしています [00:14:03.423,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:14:26.439,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:14:26.448,000] phy_mii: check_車載negotiation_completion: PHY (0) 車載交渉シーケンス完了 [00:14:26.459,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:14:26.466,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:14:26.471,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:14:26.481,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:14:27.490,000] phy_mii: PHY (0) がダウンしています [00:14:27.495,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:19:14.115,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:19:14.125,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:19:14.135,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:19:14.142,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:19:14.148,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:19:14.158,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:19:14.666,000] phy_mii: PHY (0) がダウンしています [00:19:14.671,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:20:45.214,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [00:20:45.223,000] phy_mii: check_autonegotiation_completion: PHY (0) 自動交渉シーケンス完了 [00:20:45.234,000] phy_mii: PHY (0) リンク速度 100 Mb、全二重 [00:20:45.240,000] eth_nxp_enet_qos_mac: リンクが確立されました [00:20:45.246,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク速度100Mbit以上 [00:20:45.256,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: リンク全二重 [00:20:45.764,000] phy_mii: PHY (0) がダウンしています [00:20:45.769,000] eth_nxp_enet_qos_mac: リンクがダウンしています [00:25:14.383,000] phy_mii: update_link_state: PHY (0) MII PHY自動交渉シーケンス開始 [ 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A こんにちは、 @thisisdarlensonl 追加情報ありがとうございます。 迅速な検証のために、Zephyr DHCPv4クライアントサンプルを以下のコマンドでテストしました: west build -b frdm_mcxn947/mcxn947/cpu0 zephyr/samples/net/dhcpv4_client -p always 当初、私は自分のFRDM-MCXN947ボードで同様の問題を確認しました。基板のハードウェアを確認したところ、SJ27が改造されていることが判明しました。 SJ27をデフォルトの位置に戻した後、同じDHCPv4クライアントの例を再度実行したところ、問題は起きなくなりました。PHYは正しく検出され、イーサネットリンクは100 Mbpsの全二重接続で接続されました: [00:00:00.050,000] phy_mii: PHY (0) ID 7C121 *** Booting Zephyr OS build v4.4.0-17350-g1ee3b93134be *** [00:00:00.051,000] net_dhcpv4_client_sample: Run dhcpv4 client [00:00:00.051,000] net_dhcpv4_client_sample: Start on ethernet@40100000: index=1 [00:00:03.758,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex FRDM-MCXN947ボードのSJ27や他のイーサネット関連のはんだジャンパーが再加工されていないか確認してもらえますか?もしそうなら、デフォルトのイーサネット設定に戻して再度テストしてください。 BR ハリー 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A @Harry_Zhang さん、本当にありがとうございました。大変助かりました、レジェンドです。 デフォルトで表示設定になっているとは気づきませんでした。これで前に進めます。ご協力ありがとうございました。 この点については、別の場所にも記載しておくと良いだろう。また、はんだジャンパーは厄介です 😉 改めて本当にありがとうございました。
View full article
AN4908SW 下载 您好, 我的谷歌搜索技巧好像出了问题,因为我到处都找不到“AN4908SW 发动机控制 eTPU 演示应用程序”。 请问有人能提供链接或压缩文件吗? 谢谢您! 回复: AN4908SW download 嗨,Peter,我也在寻找用于 MPC5674F 开发的 AN4908SW 软件包。能否也发到我的邮箱里?谢谢你! Re: AN4908SW download 你好, 非常感谢! 干杯, 何塞 Re: AN4908SW download 你好, 我已经发送到你的邮箱了。 顺祝商祺! Peter
View full article
データベースファイルを共有メモリにアップロードする方法 こんにちは。現在S32G VNP RDB2ボードを使用しています。クライアントからデータベースファイルを共有メモリに配置するように依頼されましたが、データベースファイルを共有メモリにアップロードすることは可能でしょうか? どんなアドバイスでも本当にありがたいです Re: How to upload Database file to share memory こんにちは@Poji9900 S32Gプラットフォーム内でデータベース導入に関する文書やガイドは提供していません。この特定の状況については当社が技術サポートのチャネルでない場合があるため、データベース導入に関しては関連する技術サポートチームにお問い合わせください。 ご不便をおかけして申し訳ありません。 敬具、ミゲル
View full article
How to upload Database file to share memory Hey there, Im currently working with S32G VNP RDB2 board, My client ask me to put one of his database file to shared memory, is it possible to upload database file in to shared memory,  any guidence im really appreciate  Re: How to upload Database file to share memory Hi @Poji9900  We do not provide any documents or guides within the S32G platform for database implementation. We may not be the channel to provide technical support on this specific situation, we recommend contacting the related technical support team on regards of your database implementation. We do apologize for the inconvenience. Best Regards, Miguel
View full article
LINUX环境 下开发S32K324咨询   在UBUNT24版本下,使用S32DS进行底层软件配置。此方案是否可行 ?主要疑虑点是linux 下关于S32DS 3.6.11版本 使用config tools 工具生成配置后,RTE是否已经可以生成代码 ? Re: LINUX环境 下开发S32K324咨询 希望能上报此需求并建立更新计划 Re: LINUX环境 下开发S32K324咨询 Hi@han00 这不是bug,只是RTD不适配LINUX系统,我没看到RTD有适配LINUX系统的计划。 Re: LINUX环境 下开发S32K324咨询 @ Senlent 我看到参考链接日期是2024.1.18的,我想确认这个问题是否仍未被修复 Re: LINUX环境 下开发S32K324咨询 Hi@han00 建议使用windows开发,LINUX环境下的RTD生成存在问题。 参考回答: https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/td-p/1791431
View full article
Consulting on S32K324 development in a Linux environment Is it feasible to use S32DS for low-level software configuration under Ubuntu 24? The main concern is with S32DS version 3.6.11 under Linux.After generating the configuration using the config tools, can the RTE generate code ? Re: LINUX环境 下开发S32K324咨询 We hope to report this request and establish an update plan. Re: LINUX环境 下开发S32K324咨询 Hi@ han00 This is not a bug; it's just that RTD is not compatible with Linux systems, and I haven't seen any plans to adapt RTD to Linux systems. Re: LINUX环境 下开发S32K324咨询 @Senlent I see the reference link is dated January 18, 2024. I want to confirm if this issue has still not been fixed. Re: LINUX环境 下开发S32K324咨询 Hi@ han00 It is recommended to use Windows for development, as there are issues with RTD generation under the Linux environment. Suggested answer: https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/td-p/1791431
View full article
AN4908SWのダウンロード こんにちは、 私のGoogle検索がうまくいかず、「AN4908SW Engine Control eTPU Demo Application」がどこにも見つからないようです。 どなたかリンクかzipファイルを教えてもらえますか? よろしくお願いします! 回复: AN4908SW download こんにちは、ピーター。私もMPC5674F開発のためのAN4908SWパッケージを探しています。メールにも送ってもらえますか?ありがとう! Re: AN4908SW download こんにちは、 どうもありがとうございます! 乾杯、 ホセ Re: AN4908SW download こんにちは、 あなたのメールアドレスに送信しました。 よろしくお願いいたします。 ピーター
View full article
如何上传数据库文件到共享内存 您好,我目前正在使用S32G VNP RDB2板,我的客户要求我将他的一个数据库文件放到共享内存中,请问是否可以将数据库文件上传到共享内存中? 任何指导我都非常感激。 Re: How to upload Database file to share memory 嗨@Poji9900 S32G平台内不提供任何数据库部署相关的文档或指南。我们可能无法针对此特定情况提供技术支持,建议您就数据库部署事宜联系相关技术支持团队。由此给您带来的不便,我们深表歉意。 此致敬礼,米格尔
View full article
Linux環境におけるS32K324開発に関するコンサルティング Ubuntu 24環境でS32DSを使用して低レベルのソフトウェア設定を行うことは可能でしょうか?特に、Linux環境におけるS32DSバージョン3.6.11について懸念しています。設定ツールを使用して設定を生成した後、 RTEはコードを生成できますか? Re: LINUX环境 下开发S32K324咨询 この要望を報告し、更新計画を策定したいと考えています。 Re: LINUX环境 下开发S32K324咨询 こんにちは@ han00 これはバグではありません。単にRTDがLinuxシステムと互換性がないだけで、RTDをLinuxシステムに対応させる計画も今のところ見当たりません。 Re: LINUX环境 下开发S32K324咨询 @Senlent 参照リンクの日付が2024年1月18日になっているのを確認しました。この問題がまだ解決されていないかどうか確認したいのですが。 Re: LINUX环境 下开发S32K324咨询 こんにちは@ han00 Linux環境ではRTD生成に問題が発生する可能性があるため、開発にはWindowsを使用することをお勧めします。 提案された回答: https://community.nxp.com/t5/S32-Design-Studio/S32K3-Linux-development-with-gcc-without-S32DS/td-p/1791431
View full article