Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
克隆 Mifare Classic 1K 数据和序列号 您好,希望我问这个问题的论坛没错…… 我计划推出一款基于 Mifare 1k Classic 卡的支付产品,我想知道是否有一种方法可以将一张卡的所有信息(包括序列号)克隆到另一张卡上。 即使不知道行业的密钥 A/密钥 B,是否可以使用特殊工具复制数据? 卡的序列号(4字节)可以被克隆/复制吗?因为如果能够做到这一点,那么将卡的序列号与数据库进行比对就毫无意义了。 此致 Re: Cloning Mifare Classic 1K Data and Serial Number 你好, 实际上可以使用特殊的卡片(“魔法”)来克隆 UID,这些卡片可以覆盖第一个扇区。 https://www.youtube.com/watch?v=RMoX_fyFZ60 马可 Re: Cloning Mifare Classic 1K Data and Serial Number 是的@Daniel_Gutierrez !我指的是卡的 4 字节 UID,例如 07:6E:3D:3C(命令 FF CA OO OO 00)。 如果无法复制到另一张卡上,我可以构建一个机制,以便在尝试访问数据以满足客户需求之前,验证该卡是否由正确的应用程序发行。 我必须使用这种卡片类型,因为我认为客户已经订购了一大批。不过,我还是会把你的回复转发给他们,以便他们考虑还有其他方案可供选择。 非常感谢您的回复。 顺祝商祺! 卡洛斯·阿尔马格尔 Re: Cloning Mifare Classic 1K Data and Serial Number 你好@calmaguer ,祝你今天愉快! 非常感谢您对我们产品的关注。 请问,您指的是卡的UID吗?如果情况属实,请注意,这是一个在生产测试中已编程并进行写保护的唯一标识符,因此无法更改。 有关 UID 处理的更多详细信息,请参阅MIFARE Classic EV1 1K 数据表第 10 节和以下应用笔记AN10927 。 请注意,不建议将此产品用于新设计。相反,您可以考虑查看我们推荐的安全型MIFARE DESFire Light和MIFARE DESFire EV3 。 我最诚挚的问候, 丹尼尔。
View full article
S32DS for ARM 2018R1 许可证 您好: 我的 S32DS for ARM 2018R1 IDE 许可证已过期。您能帮我检查并延长一下吗? 谢谢。 Re: S32DS for ARM 2018R1 license 你好, 您的S32DS许可证已延期,请使用您之前的激活码重新激活S32DS。 Re: S32DS for ARM 2018R1 license 谢谢!!
View full article
MC33PF8200A0ES 我看MC33PF8200A0ES的升级版是MC33PF8200A0TS,这两者的区别是什么啊? 如果买的MC33PF8200A0TS是没烧录的,用什么工具烧录啊? 除了用KITPF8200FRDMPGM烧录,还能有什么方式烧录啊? KITPF5200FRDMEVM能烧录MC33PF8200A0TS吗? 帮忙给看看,谢谢。 Re: MC33PF8200A0ES 1:MC33PF8200A0ES 不推荐新设计中了已经,MC33PF8200A0ES的升级版是MC33PF8200A0TS,他俩封装厚度不一样,但是不影响PCB 封装。 2:可以选择下面的板子烧录 PF8200/PF8100 Programming Board | NXP Semiconductors 也可以选择: SBC and PMIC Product OTP Programming Board | NXP Semiconductors + PF8200-OTP-DB Product Information | NXP Semiconductors 这种组合烧录 3:不推荐用KITPF5200FRDMEVM烧录
View full article
MC33PF8200A0ES I see that the upgraded version of MC33PF8200A0ES is MC33PF8200A0TS. What are the differences between the two? If the MC33PF8200A0TS I bought doesn't have any files burned in it, what tool should I use to burn it? Besides using the KITPF8200FRDMPGM for burning, what other methods are there for burning? Can the KITPF5200FRDMEVM burn an MC33PF8200A0TS? Could you please take a look? Thank you. Re: MC33PF8200A0ES 1: The MC33PF8200A0ES is no longer recommended for new designs. The upgraded version of the MC33PF8200A0ES is the MC33PF8200A0TS. The two packages have different thicknesses, but this does not affect the PCB packaging. 2: You can choose the following board for programming. PF8200/PF8100 Programming Board | NXP Semiconductors Alternatively, you can choose: SBC and PMIC Product OTP Programming Board | NXP Semiconductors + PF8200-OTP-DB Product Information | NXP Semiconductors This combination burning 3: It is not recommended to use KITPF5200FRDMEVM for burning.
View full article
Analog IC Design Progression Hey, Just want opinions on how to adjust my learning. I'm very interested in Analog IC design (just a little worried seeing all these digital people takeover - Yes I know "the real world is always analog", anyways that's not the point). I've taken one module based on Razavi's Design of Analog CMOS ICs in which we covered the earlier more basic chapters such as CS, CG, CD stages Differential Amplifiers Feedback, Stability Poles, etc A bit of op-amps I2C Re: Analog IC Design Progression Hi, The NXP Community support channel is intended for questions related to NXP products and their applications. Your question is about general Analog IC design education, which falls outside the scope of NXP technical support. For learning progression advice, the r/chipdesign and r/ECE communities on Reddit are well-suited for this type of discussion and Razavi's own lecture series on YouTube is an excellent next step after completing the introductory chapters you mentioned. Feel free to explore NXP's training resources at nxp.com/training for additional learning materials. If you have a question related to a specific NXP product, we are happy to help. BRs, Tomas
View full article
EVM of HTRC11001T Hi, Is there any EVM (Evaluation module) available for HTRC11001T? Re: EVM of HTRC11001T NXP does not provide a dedicated official evaluation board for the HTRC110. However, we can provide some reference materials to assist you in your design and development work. Hardware Design Reference: We recommend referring to the application note AN98080_Read write devices based on the HITAG read write IC. This document details the reader/writer design based on the HTRC110, including: 125 kHz antenna design Resonance and matching network design Peripheral coupling circuitry Demodulation circuit principle Clock and power supply related design Other external component selection recommendations Software Development Reference: NXP can provide relevant sample code and reference documentation for the HTRC110 as a starting point for customers to conduct low-level driver and application development. However, both require an NDA to apply for them. For evaluation hardware or a ready-made reader solution, I would recommend checking the NXP® Partner Marketplace: https://www.nxp.com/design/design-center/partner-marketplace:PARTNER-MARKETPLACE Re: EVM of HTRC11001T Hello @Shanmukh  There is not any EVM (Evaluation module) available for HTRC11001T, sorry for that! BR kelly Re: EVM of HTRC11001T Hi, Thanks for the quick response. one query, as mentioned in the application note of HTRC110, it is optimized for HITAG series tag only. So, does that mean it will not work with other tags like EM series (EM4305) tags?
View full article
FRDM-MCXN947 以太网端口设置 - PHY LAN8741A 我一直无法连接以太网端口。调试时,我在frdm板上一直遇到以下错误。 [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) 链路已配置 [00:00:00.015,000] eth_nxp_enet_qos_mac:无法清除驻波比 [00:00:00.021,000] eth_nxp_enet_qos_mac:链路已断开 *** 正在启动 Zephyr OS 版本 v4.4.2 *** 启动应用程序并检查MDIO总线... PHY寄存器0x01(BMSR):0x7809 PHY 寄存器 0x05(合作伙伴能力):0xCDE1 PHY寄存器0x1A(符号错误):51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商超时 [00:00:14.042,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:00:14.062,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:00:14.069,000] eth_nxp_enet_qos_mac:链路已连接 [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 MDIO通信似乎工作正常,但链路每隔30毫秒就会 RESET 一次。 请问如何配置 LAN8741A 才能使其在 FRDM-MCXN947 板上正常工作? 开发板 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A 嗨@thisisdarlensonl 感谢您提供如此详细的信息。为了帮助我们进一步调查此问题,请您提供以下信息? 你使用的是哪个 Zephyr 采样? 您的 prj.conf 文件、应用程序覆盖文件和版本命令。 您是否对 FRDM-MCXN947 板的 DTS 进行过任何更改? 能否提供完整的日志,显示链路每 30 毫秒 RESET 一次的情况? 我想重现这个问题。 BR 哈里 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A 嗨,哈里, 谢谢您的回复。我已附上 prj.cong 和 app.overlay 文件。 我从一个“Hello World”示例开始,并在此基础上进行扩展。Zephyr 的当前版本是 4.4.2。 至于完整的控制台消息。见下文 [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) 链路已配置 [00:00:00.015,000] eth_nxp_enet_qos_mac:无法清除驻波比 [00:00:00.021,000] eth_nxp_enet_qos_mac:链路已断开 *** 正在启动 Zephyr OS 版本 v4.4.2 *** === FRDM-MCXN947 PM 优化心跳演示 === 启动应用程序并检查MDIO总线... PHY寄存器0x01(BMSR):0x7809 PHY 寄存器 0x05(合作伙伴能力):0xCDE1 PHY寄存器0x1A(符号错误):51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商超时 [00:00:14.042,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:00:14.062,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:00:14.069,000] eth_nxp_enet_qos_mac:链路已连接 [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:00:14.085,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:00:15.094,000] phy_mii:PHY (0) 已关闭 [00:00:15.098,000] eth_nxp_enet_qos_mac:链路已断开 [00:01:08.626,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:01:08.636,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:01:08.646,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:01:08.653,000] eth_nxp_enet_qos_mac:链路已连接 [00:01:08.659,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:01:08.668,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:01:09.177,000] phy_mii:PHY (0) 已关闭 [00:01:09.182,000] eth_nxp_enet_qos_mac:链路已断开 [00:01:22.193,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:01:22.203,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:01:22.213,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:01:22.220,000] eth_nxp_enet_qos_mac:链路已连接 [00:01:22.226,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:01:22.235,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:01:22.744,000] phy_mii:PHY (0) 已关闭 [00:01:22.749,000] eth_nxp_enet_qos_mac:链路已断开 [00:03:57.817,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:03:57.827,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:03:57.837,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:03:57.844,000] eth_nxp_enet_qos_mac:链路已连接 [00:03:57.850,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:03:57.859,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:03:58.368,000] phy_mii:PHY (0) 已关闭 [00:03:58.373,000] eth_nxp_enet_qos_mac:链路已断开 [00:05:08.907,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:05:08.917,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:05:08.927,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:05:08.934,000] eth_nxp_enet_qos_mac:链路已连接 [00:05:08.940,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:05:08.949,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:05:09.958,000] phy_mii:PHY (0) 已关闭 [00:05:09.963,000] eth_nxp_enet_qos_mac:链路已断开 [00:05:36.980,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:05:36.990,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:05:37.000,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:05:37.007,000] eth_nxp_enet_qos_mac:链路已连接 [00:05:37.013,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:05:37.022,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:05:38.031,000] phy_mii:PHY (0) 已关闭 [00:05:38.036,000] eth_nxp_enet_qos_mac:链路已断开 [00:12:00.195,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:12:00.205,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:12:00.215,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:12:00.222,000] eth_nxp_enet_qos_mac:链路已连接 [00:12:00.228,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:12:00.237,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:12:00.746,000] phy_mii:PHY (0) 已关闭 [00:12:00.751,000] eth_nxp_enet_qos_mac:链路已断开 [00:13:41.297,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:13:41.307,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:13:41.317,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:13:41.324,000] eth_nxp_enet_qos_mac:链路已连接 [00:13:41.330,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:13:41.340,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:13:41.848,000] phy_mii:PHY (0) 已关闭 [00:13:41.853,000] eth_nxp_enet_qos_mac:链路已断开 [00:14:02.868,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:14:02.877,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:14:02.888,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:14:02.894,000] eth_nxp_enet_qos_mac:链路已连接 [00:14:02.900,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:14:02.910,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:14:03.418,000] phy_mii:PHY (0) 已关闭 [00:14:03.423,000] eth_nxp_enet_qos_mac:链路已断开 [00:14:26.439,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:14:26.448,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:14:26.459,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:14:26.466,000] eth_nxp_enet_qos_mac:链路已连接 [00:14:26.471,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:14:26.481,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:14:27.490,000] phy_mii:PHY (0) 已关闭 [00:14:27.495,000] eth_nxp_enet_qos_mac:链路已断开 [00:19:14.115,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:19:14.125,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:19:14.135,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:19:14.142,000] eth_nxp_enet_qos_mac:链路已连接 [00:19:14.148,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:19:14.158,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:19:14.666,000] phy_mii:PHY (0) 已关闭 [00:19:14.671,000] eth_nxp_enet_qos_mac:链路已断开 [00:20:45.214,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [00:20:45.223,000] phy_mii: check_autonegotiation_completion: PHY (0) 自动协商序列已完成 [00:20:45.234,000] phy_mii: PHY (0) 链路速度 100 Mb,全双工 [00:20:45.240,000] eth_nxp_enet_qos_mac:链路已连接 [00:20:45.246,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路速度 100Mbit 或更高 [00:20:45.256,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: 链路全双工 [00:20:45.764,000] phy_mii:PHY (0) 已关闭 [00:20:45.769,000] eth_nxp_enet_qos_mac:链路已断开 [00:25:14.383,000] phy_mii: update_link_state: PHY (0) 启动 MII PHY 自动协商序列 [ 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A 嗨@thisisdarlensonl 感谢您提供的补充信息。 为了快速验证,我使用以下命令测试了 Zephyr DHCPv4 客户端示例: west build -b frdm_mcxn947/mcxn947/cpu0 zephyr/samples/net/dhcpv4_client -p always 最初,我在我的 FRDM-MCXN947 板上观察到了类似的问题。检查板上的硬件后,我发现 SJ27 被重新加工过。 将 SJ27 恢复到默认位置后,我再次运行了相同的 DHCPv4 客户端示例,问题不再出现。PHY芯片检测正确,以太网链路以100 Mbps全双工模式建立连接: [00:00:00.050,000] phy_mii: PHY (0) ID 7C121 *** Booting Zephyr OS build v4.4.0-17350-g1ee3b93134be *** [00:00:00.051,000] net_dhcpv4_client_sample: Run dhcpv4 client [00:00:00.051,000] net_dhcpv4_client_sample: Start on ethernet@40100000: index=1 [00:00:03.758,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex 请您检查一下FRDM-MCXN947板上的SJ27或其他任何与以太网相关的焊接跳线是否被重新焊接过?如果问题仍然存在,请将它们恢复为默认以太网配置并再次测试。 BR 哈里 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A 感谢@Harry_Zhang ,你真是帮了大忙,太棒了! 我之前没注意到它默认是设置为显示的。现在我可以继续前进了。非常感谢您的帮助。 或许应该在其他地方也提到这一点。此外,焊接跳线也很痛苦。 😉 再次万分感谢
View full article
S32K311 HSE_B ASB:为原始安全恢复应用程序生成 ADKP 派生的 GMAC 您好,NXP技术支持, 我们正在使用带有 HSE_B 的 S32K311。我们的主要启动引导加载程序使用高级安全启动 (ASB),具有 AES-CMAC 认证的安全内存区域和核心 RESET 条目。UID多样化的ADKPm已经完成编程,并且安全恢复功能已启用。 固件更新后,我们需要为替换的安全恢复应用程序重新生成身份验证数据,而无需更改现有的 ADKP 或将其派生的签名密钥保留在主机可访问的内存中。 恢复应用程序从 Cortex-M7 向量表开始。其布局如下: 区域地址 恢复 IVT 0x00480000 恢复应用程序向量表和代码起始于 0x00482000 恢复 IV,12 字节 0x0049FFE4–0x0049FFEF 恢复 GMAC,16 字节 0x0049FFF0–0x0049FFFF 单独签署IVT成功。然而,将原始恢复应用程序的向量表地址提交给 HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN 会返回 HSE_SRV_RSP_INVALID_PARAM 错误。该请求使用 inTagLength = 28 和系统 SRAM 中的输出缓冲区。 在 S32K311 HSE_B 上,UID 多样化的 ADKPm 已编程并启用了安全恢复,主机如何为原始安全恢复应用程序生成 12 字节 IV 和 16 字节 GMAC?当 pInImage 指向 Cortex-M7 向量表时,HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN 返回 HSE_SRV_RSP_INVALID_PARAM。 是否存在 HSE 服务,可以在不暴露该密钥的情况下,使用内部派生的 ADKP 生成安全恢复 GMAC?否则,GMAC 是否必须从外部生成? 此外,IVT 安全恢复长度是否包含 12 字节的 IV,以及具体验证哪些字节? 谢谢。 Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application 嗨@sameer_chawla 之前手册中对安全恢复过程的描述有误(可能是在某个旧版本中,比如 2.3 版本,现在已经更新了)。从那时起,我还有以下补充笔记,总结了它的实施方式: 不要向安全恢复映像添加 AppBL 标头格式。 安全恢复映像的“第一个可执行字节”是指其向量表起始地址。镜像中不需要启动头/IVT。 不要使用 HSE_SRV_ID_BOOT_DATA_IMAGE_SIGN 服务生成安全恢复映像 GMAC IV 应由客户指定,GMAC 也应由客户生成(可通过 OpenSSL 等通用工具生成,或由 HSE 在单独的应用程序项目中生成)。 在客户计算 GMAC 之前,应将 12 字节的 IV 添加到镜像末尾,并且其长度(12 字节)也应计入镜像大小。 不要使用 AES-128 (ADKP) 进行 GMAC 计算。相反,使用 AES-256 (ADKP-Hash256) 计算 GMAC,如图 11 所示,参见 HSE 固件参考手册修订版。2.8. 手册现在在“2.6.1.3.1”中明确指出安全恢复模式”: 此致, Lukas Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application 嗨@lukaszadrapa , 感谢您的快速回复。 此后,我们测试了一种使用高级安全启动的替代方案,因为我们想避免保留或单独配置 ADKP-Hash256 以生成恢复映像 GMAC。 我们的配置如下: CB(我们的主要引导加载程序)通过 SMR0 进行身份验证。 SRB(我们的恢复引导加载程序)通过 SMR1 使用 AES-CMAC 和 HSE 驻留密钥进行身份验证,遵循与 CB 相同的身份验证方法。 核心 RESET 条目选择 CB 作为主要目的地,SRB 作为备用目的地。如果 CB 认证失败,HSE 会在启动 SRB 之前对其进行认证。 据我们了解,这使用的是 ASB 的已验证备用启动路径,而不是专用的基于 ADKP 的安全恢复机制。ADKP 仍为其现有的 IVT 身份验证和安全调试目的配置。 在 S32K311 HSE_B 上,这是受支持和推荐的方法吗?对于经过身份验证的恢复引导加载程序来说,使用单独的 SMR 和 CR 备用启动目标是否是一种常见的设计?或者与专用的安全恢复机制相比,是否存在我们应该考虑的限制? 谢谢你, 萨米尔 Re: S32K311 HSE_B ASB: Generating ADKP-derived GMAC for a raw Secure Recovery Application 嗨@sameer_chawla 是的,这也是一种有效的方法。您可以使用备用启动目标,而不是专用的安全恢复机制。 选择主要取决于所需的备用保护级别。如果一个备用级别就足够了,那么使用单独的 SMR 作为 SRB 并将其配置为备用启动目标是一个合适的解决方案。如果需要额外的回退级别,例如备用启动映像的身份验证也失败,则安全恢复机制仍然可以用作另一个恢复级别。 所以,最终取决于应用需求。使用备用启动路径来实现此目的并没有什么固有的限制。事实上,它比相对简单的专用的安全恢复映像机制提供了更大的配置灵活性。 此致, Lukas
View full article
EB tresos Studio 32.1.4 哪里可以下载 EB tresos Studio 32.1.4?  S32K3 标准软件-> 汽车软件 - EB tresos Studio / AUTOSAR 配置工具,在该路径下只能找到 EB tresos Studio 30.0.0 最高版本。 Re: EB tresos Studio 32.1.4 你好,彼得, 我按照您的建议查看了如何申请安全访问权限,但这个过程相当复杂。 我无意访问高度机密的文件;我只想下载 EB Tresos Studio 32.x.x。有什么方法可以将 EB Tresos Studio 32.xx 添加到我的产品列表中吗? 谢谢! Re: EB tresos Studio 32.1.4 你好, 查看可用版本: 所以问题很可能与您的NXP软件帐户有关。 请参考常见问题解答以获取更多信息: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS 顺祝商祺! Peter Re: EB tresos Studio 32.1.4 你好, 我的账户邮箱:[email protected] 谢谢! Re: EB tresos Studio 32.1.4 你好, 是的,如果管理员将其添加到您的帐户中,则有直接的方法。 请告诉我您用于此账户的邮箱地址。 顺祝商祺! Peter Re: EB tresos Studio 32.1.4 你好, 现在应该可以在您的SW账户中看到了。 顺祝商祺! Peter
View full article
lpx43xx usd0 ホスト HID キーボード こんにちは 私はLPX4357を使っていて、USB HIDを使ってキーボードインターフェースを無事に完了しましたが、バーコードスキャナーを接続するとスキャン後にハードフォールが発生します...読み取り・検出されたバイトは1バイトだけで、その後はハードフォールに入ります...なぜこうなるのか、何かアイデアを教えてもらえますか?何かアドバイスはありますか? ご協力ください! LPC43xx ペリフェラル USB Re: lpx43xx usb0 host HID keyboard こんにちは、 USBバーコードスキャナーとのインターフェースを試みています。私はLPCOpen Keyboard Hostのサンプルを使用しています。USBキーボードを接続すると、システムは入力されたデータを正しく受信します。しかし、バーコードスキャナの場合、スキャンされたバーコードデータは電源投入時に一度だけ受信されます。それは必ずしも起こるわけではなく、時々起こることだ。バーコードスキャナーからデータを受け取ったとき、次のスキャンでは必ず HID_Host_IsReportReceived falseフラグが表示されます。そのため、その後はバーコードからのデータが受信できません。ピピリンの問題はありますか?どうすれば解決できますか?  コントローラ LPC4337 バーコードメーカー、ゼブロニクス。 モデルBS2H1000 よろしくお願いします。 Re: lpx43xx usb0 host HID keyboard こんにちは、 USBバーコードスキャナーのインターフェースを試みています。LPCOpen Keyboard Host のサンプルを使用して、キーボードのキーを取得しています。しかし、バーコードスキャナーを接続すると、デバイスは認識されるものの、バーコードデータを読み取ることができません。バーコードデータを読み取るためにキーボードコードの例でどんな修正が必要か教えていただけませんか? コントローラ LPC4337 バーコードメーカー、ニューランド。 モデルNLS-HR11 敬具。 Re: lpx43xx usb0 host HID keyboard 問題は解決しました。ありがとうございました。 Re: lpx43xx usb0 host HID keyboard あなたのプロジェクトはlpcopenのデモをベースにしていますか?はいの場合、どれですか?修正はありますか? 実行時にエラーが発生する箇所を特定してください。そうですか きちんと列挙する? Re: lpx43xx usb0 host HID keyboard こんにちは、 @RDGC_member さん。 このThreadは5年前に作られました。LPCフォーラムに新しいThreadを作ることをお勧めします。NXPのサポートが助けてくれます。 https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc ありがとうございます ジャン・ジュン Re: lpx43xx usb0 host HID keyboard 私はLPCUSBLIBライブラリを使って、USBバーコードスキャナーとコントローラをインターフェースしていますLPC4337。パイプバッファをクリアする条件を知りたいです。時々、バーコード全体が正しく表示されることがあります。最初の文字の後に何も受信しないこともあり、USB回線も詰まってしまい、その後何度もバーコードスキャンを繰り返しても何も受信されません。
View full article
请求提供“AES_ACCEL子系统参考手册” 您好,恩智浦 我目前正在分析项目中的 AES_ACCEL(AES 加速器)模块。 文档中提到可以参考“AES_ACCEL 子系统参考手册” ,但我无法从产品页面找到或下载该手册。 请问您能否告知我在哪里可以获取这份手册,或者如何才能下载它? 顺祝商祺! Re: Request for "AES_ACCEL Subsystem Reference Manual" 该文件为安全文件。请按照此处所述的安全访问注册流程进行操作,除非您已完成该流程: NXP 安全访问权限注册 更多信息,请参阅: NXP 安全访问权限 由于该文件具有较高的保密级别,因此需要人工批准才能访问。如果您已经完成了注册,但文件仍然不可用,请联系您的 恩智浦代表或代理商,并要求他们为您申请所需的访问权限。
View full article
TAA3033AT – 400 V DCリンクプリチャージ適用の適性 こんにちは、NXPコミュニティの皆さん、 現在、DCリンクのプリチャージ用途向けにTAA3033ATアクティブプリチャージコントローラーを評価しています。 当システムの仕様は以下のとおりです。 直流入力電圧:24 Vから400 V 直流リンクの静電容量:1.5 mF 定格動作電流:25A プリチャージ後にDCリンクを接続するために使用されるメインコンタクタ このTAA3033ATがこのアプリケーションに適しているか、特に広い入力電圧範囲と電流制限に関して確認したいと思います。 いくつか質問があります。 TAA3033ATは24〜400Vの入力範囲全体で動作できますか? TAA3033DB1649評価ボードは、大幅な修正なしにこれらの条件を試験するのに適しているのでしょうか? コントローラは低電圧制御システムと高電圧電源回路の間に追加のガルバニック絶縁を必要としますか? ご協力ありがとうございました。 よろしくお願いいたします。 Re: TAA3033AT – Suitability for 400 V DC-Link Precharge Application こんにちは、 @sayf さん。 1.原則的には、そうです。TAA3033ATは調整電流コントローラとして動作し、サポートされる高電圧入力範囲は主に外部MOSFET、ダイオード、インダクタ、センス抵抗、そして設定可能なタイミングおよび電流センスパラメータによって決まります。しかし、24Vまでの動作については公開されたドキュメントでは明確に記述されていません。 2. TAA3033DB1649は出発点として使用できますが、400Vおよび800Vの動作に特化しています。したがって、24Vでのテストは構成や部品の変更が必要になることがあり、別途検証されるべきです。 3. TAA3033ATにはガルバニック絶縁が含まれていません。ローサイドトポロジーでは、その制御インターフェースはHVバッテリーの負極子を参照されます。低電圧コントローラがこの領域からガルバティックアイソレータを保つ必要がある場合、外部アイソレータが必要です。ハイサイドトポロジーでは、フローティング電源とレベルシフトが必要となる。 よろしくお願いいたします。 パベル
View full article
Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro Hello Team, We needed some clarification on the maximum supported keyslot number for S32K388 device. We integrated the following RTD 701 QLP04_D2608 and find that is limit of 5 SHE group( 1 group map to 10key) i.e. a total of 50 Key slots. Is this a limitation from HSE ? We have a requirement to enable 100 key slots, so in this case would like to understand if there a possibility to configure more key slots. Thanks! Nimsha Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro Hi @Nimsha  This is a limitation defined by the HSE firmware itself, rather than by the RTD implementation. As stated in Sections 6.3.2 and 6.3.3 of the HSE-B Firmware Reference Manual, Rev. 2.8, SHE keys in the NVM key catalog can be mapped to Group 0, which contains 10 key slots. In addition, HSE allows the application to provision extra AES-128 SHE keys using the SHE key update protocol (referred to as extended SHE keys), which can be mapped to Groups 1 through 4, with 10 slots available in each group. This provides a total of 50 SHE key slots, as you noted. According to the reference manual, the NVM SHE Key Catalog configuration is as follows: Row 0: MASTER_ECU_KEY, BOOT_MAC_KEY, KEY_1 to KEY_10 Row 1: KEY_11 to KEY_20 Row 2: KEY_21 to KEY_30 Row 3: KEY_31 to KEY_40 Row 4: KEY_41 to KEY_50 hseKeyGroupCfgEntry_t NVM_key_catalog[] = { /* SHE keys */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, HSE_KEY128_BITS}, /* MASTER_ECU_KEY, BOOT_MAC_KEY, KEY_1 to KEY_10 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_11 to KEY_20 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_21 to KEY_30 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_31 to KEY_40 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_41 to KEY_50 */ { 0U, 0U, 0U, 0U, 0U } }; The reference manual also states that attempting to map SHE keys to Group 5 or higher will result in an error during the key catalog formatting operation.  BR, VaneB Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro Hi @Nimsha  These specifications apply to the standard HSE Firmware. However, premium HSE Firmware variants (available as a paid licensed product) can be tailored to address specific customer requirements and use cases. I have sent you a private message with further details. Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro Hi @VaneB  Thank you for the reply. We find that GM OEM has specific requirement to enable the 100 Keyslots. Is this limitation known to GM. Since you have mentioned that HSE FW is currently supporting only 50Key slots, could you please let me know any future Firmware version the 100 keyslots are supported. Thanks! Nimsha
View full article
EB tresos Studio 32.1.4 EB Tresos Studio 32.1.4はどこでダウンロードできますか?  S32K3標準ソフトウェア - > 自動車ソフトウェア - EB tresos Studio / AUTOSAR 設定ツールでは、ルート上で EB tresos Studio 30.0.0 しか最高位を見つけられません。 Re: EB tresos Studio 32.1.4 こんにちは、ピーター。 あなたのアドバイスに従い、セキュアアクセスの申請方法も確認しましたが、手続きはかなり複雑です。 私は極秘文書にアクセスするつもりはありません。私はEB Tresos Studio 32.x.xをダウンロードしたいだけです。EB Tresos Studio 32.x.xを製品リストに追加する方法はありますか? ありがとうございます! Re: EB tresos Studio 32.1.4 こんにちは、 利用可能なバージョンを見てみましょう。 つまり、問題はおそらくNXPのソフトウェアアカウントに関係しているのでしょう。 さらなるアクセスを得るにはFAQをご確認ください: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS よろしくお願いいたします。 ピーター Re: EB tresos Studio 32.1.4 こんにちは、 はい、管理者があなたのアカウントに追加すれば、直接的な方法があります。 そのアカウントで使用しているメールアドレスを教えてください。 よろしくお願いいたします。 ピーター Re: EB tresos Studio 32.1.4 こんにちは、 私のアカウントのメールアドレス:[email protected] ありがとう! Re: EB tresos Studio 32.1.4 こんにちは、 現在、お客様のSWアカウントでご利用いただけるはずです。 よろしくお願いいたします。 ピーター
View full article
关于 CW 3.1 谁能提供可在 Windows XP 系统上运行的 CodeWarrior 3.1 的下载链接?文件名可能是Codewarrior-HC(S)08-v3.1.iso。非常感谢。 Re: About CW 3.1 对此给您带来的不便,我深感抱歉,但此软件版本的资料和文件已不再提供下载,我需要澄清一下,CodeWarrior 3.1 是一个过时的产品。搜索结果显示,某些特定设备的 CodeWarrior 版本已经多年未得到支持,NXP 也已停止维护某些旧版 CodeWarrior 实现。   您可以升级到更新的版本。用于操作 8 位设备的软件工具是CodeWarrior for MCUs (Eclipse IDE) v11.1,适用于 Windows 10/11;如果您感兴趣,可以使用此工具测试各种 8 位设备。 顺祝商祺!
View full article
lpx43xx usb0 host HID keyboard HI  i'm using lpx4357 and successfully completed keyboard interfacing using USB HID but when i connect a barcode scanner hard fault occurs after scanning .. only one byte read / detected and then it goes to hard fault.. can i get some ideas why this could be happen?? or any suggestions ? please help! LPC43xx Peripherals USB Re: lpx43xx usb0 host HID keyboard Hello, I am trying to interface the USB barcode scanner . I am using the LPCOpen Keyboard Host example. while connecting Usb key board ,system receives proper data what ever entered. but with barcode scanner, the barcode data scanned, is received only once at power on time . that is also happens sometimes not always. When ever i received data from barcode scanner , for the next scanning i  always receive HID_Host_IsReportReceived flag false. which causes no data receive from barcode after that.  Is there any pipiline issue? how can i resolve it?   Controller LPC4337 Barcode Make Zebronics. Model BS2H1000 Regards. Re: lpx43xx usb0 host HID keyboard Hi, I am trying to interface the USB barcode scanner. I am using the LPCOpen Keyboard Host example, I am getting the keyboard keys. But when I connect the barcode scanner, it shows device is enumerated, but now able to read the barcode data. Can you please let me know, what modification need to be done in the keyboard code example to read the barcode data.  Controller LPC4337 Barcode Make Newland. Model NLS-HR11 Warm regards. Re: lpx43xx usb0 host HID keyboard issue solved .. thank you.. Re: lpx43xx usb0 host HID keyboard Is your project based on lpcopen demo ? if yes which one? any revise ? Please track where runs to error? Does it enumerate well? Re: lpx43xx usb0 host HID keyboard Hi @RDGC_member  This thread was created 5 years ago. I suggest you to create a new thread in LPC forum. The NXP support will help you. https://community.nxp.com/t5/LPC-Microcontrollers/bd-p/lpc Thanks, Jun Zhang Re: lpx43xx usb0 host HID keyboard I am using LPCUSBLIB library for interfacing USB barcode scanner with LPC4337 controller. i wanted to know that which are the conditions cause to clear the  pipe buffer. some times i receive full barcode properly. some times after first character nothing is received also the usb line gets stuck so that after that nothing is received for several times barcode scanning. 
View full article
CW 3.1について Windows XPで動作するCodeWarrior 3.1のダウンロードリンクを提供できる人はいますか?ファイル名はCodewarrior-HC(S)08-v3.1.isoかもしれません。どうもありがとうございました。 Re: About CW 3.1 ご不便をおかけして申し訳ありませんが、このソフトウェアバージョンの情報やファイルはもはやダウンロードできません。CodeWarrior 3.1はレガシー製品であることを明確にしておきます。検索結果によると、特定のデバイス向けの一部のCodeWarriorバージョンは長年サポートされておらず、NXPは一部のレガシーCodeWarrior実装の維持から移行しています。   より新しいバージョンに移行することもできます。8ビットデバイスを使用するソフトウェアツールは、Windows 10/11向けに利用可能な CodeWarrior for MCUS (Eclipse IDE) v11.1 です。このツールで様々な8ビットデバイスでテストできます。 よろしくお願いいたします。
View full article
需要澄清NXP S32K388微型芯片支持的最大键槽数量。 各位团队成员,大家好! 我们需要了解一下 S32K388 设备支持的最大键槽数量。 我们集成了以下 RTD 701 QLP04_D2608,发现其限制为 5 个 SHE 组(1 组映射到 10 个密钥),即总共 50 个密钥槽。这是英国健康与安全执行局 (HSE) 的限制吗? 我们需要启用 100 个钥匙槽,因此想了解是否有可能配置更多钥匙槽。 谢谢您! 尼姆莎 Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro 嗨@Nimsha 这是 HSE 固件本身的限制,而不是 RTD 实现的限制。 如 HSE-B 固件参考手册第 2.8 版第 6.3.2 节和第 6.3.3 节所述,NVM 密钥目录中的 SHE 密钥可以映射到第 0 组,该组包含 10 个密钥槽。此外,HSE 允许应用程序使用 SHE 密钥更新协议(称为扩展 SHE 密钥)配置额外的 AES-128 SHE 密钥,这些密钥可以映射到第 1 组到第 4 组,每组有 10 个可用槽位。正如您所指出的,这总共提供了 50 个 SHE 钥匙槽。 根据参考手册,NVM SHE 密钥目录配置如下: 第 0 行:MASTER_ECU_KEY、BOOT_MAC_KEY、KEY_1 至 KEY_10 第 1 行:KEY_11 至 KEY_20 第 2 行:KEY_21 至 KEY_30 第 3 行:KEY_31 至 KEY_40 第 4 行:KEY_41 至 KEY_50 hseKeyGroupCfgEntry_t NVM_key_catalog[] = { /* SHE keys */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, HSE_KEY128_BITS}, /* MASTER_ECU_KEY, BOOT_MAC_KEY, KEY_1 to KEY_10 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_11 to KEY_20 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_21 to KEY_30 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_31 to KEY_40 */ { HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 10U, HSE_KEY128_BITS}, /* KEY_41 to KEY_50 */ { 0U, 0U, 0U, 0U, 0U } }; 参考手册还指出,尝试将 SHE 密钥映射到第 5 组或更高组会导致密钥目录格式化操作期间出错。 BR,VaneB Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro 嗨@VaneB 感谢您的回复。 我们发现通用汽车OEM对启用100个钥匙槽有具体要求。通用汽车公司是否了解这一限制? 既然您提到 HSE 固件目前仅支持 50 个键槽,请问未来哪个固件版本会支持 100 个键槽? 谢谢您! 尼姆莎 Re: Clarification needed on Maximum number of Keyslots supported in NXP S32K388 micro 嗨@Nimsha 这些规范适用于标准 HSE 固件。然而,高级 HSE 固件版本(作为付费许可产品提供)可以根据客户的具体需求和使用案例进行定制。 我已私信您更多详情。
View full article
TAA3033AT – 适用于 400 V 直流链路预充电应用 NXP社区的各位朋友,大家好! 我目前正在评估 TAA3033AT 有源预充电控制器在直流链路预充电应用中的性能。 我们的系统具有以下规格: 直流输入电压:24V 至 400V 直流母线电容:1.5 mF 额定工作电流:25 A 主接触器用于预充电后连接直流链路。 我想确认一下 TAA3033AT 是否适合此应用,特别是关于其宽输入电压范围和电流限制方面。 我还有几个问题: TAA3033AT 能否在 24–400 V 的整个输入范围内工作? TAA3033DB1649 评估板是否适合在不进行重大修改的情况下测试这些条件? 控制器是否需要在低压控制系统和高压电源电路之间增加额外的电气隔离? 谢谢你的帮助。 顺祝商祺! Re: TAA3033AT – Suitability for 400 V DC-Link Precharge Application 你好@sayf , 1.原则上,是的。TAA3033AT 用作稳压电流控制器,其支持的高压输入范围主要由外部 MOSFET、二极管、电感器、检测电阻以及可配置的定时和电流检测参数决定。然而,已发布的文档中并未明确描述低至 24 V 的工作电压。 2. TAA3033DB1649 可用作起点,但其特性适用于 400 V 和 800 V 的工作电压。因此,在 24 V 电压下进行测试可能需要更改配置或元器件,并且应该单独进行验证。 3. TAA3033AT 不包含电气隔离。在低侧拓扑结构中,其控制接口以高压电池负极为参考。如果低压控制器必须与该功能域保持电气隔离,则需要外部隔离。在高侧拓扑结构中,需要浮空电源和电平转换。 顺祝商祺! 帕维尔
View full article
TAA3033AT – Suitability for 400 V DC-Link Precharge Application Hello NXP COMMUNITY , I am currently evaluating the TAA3033AT active precharge controller for a DC-link precharge application. Our system has the following specifications: DC input voltage: 24 V to 400 V DC-link capacitance: 1.5 mF Nominal operating current: 25 A Main contactors used to connect the DC link after precharge I would like to confirm whether the TAA3033AT is suitable for this application, particularly regarding the wide input voltage range and current limitation. I also have a few questions: Can the TAA3033AT operate across the full 24–400 V input range? Is the TAA3033DB1649 evaluation board suitable for testing these conditions without significant modifications? Does the controller require additional galvanic isolation between the low-voltage control system and the high-voltage power circuit? Thank you for your assistance. Best regards, Re: TAA3033AT – Suitability for 400 V DC-Link Precharge Application Hello @sayf , 1. In principle, yes. The TAA3033AT operates as a regulated current controller, while the supported HV input range is primarily determined by the external MOSFET, diode, inductor, sense resistor, and the configurable timing and current-sense parameters. However, operation down to 24 V is not explicitly characterized in the published documentation. 2. The TAA3033DB1649 can be used as a starting point, but it is characterized for 400 V and 800 V operation. Testing at 24 V may therefore require configuration or component changes and should be validated separately. 3. The TAA3033AT does not include galvanic isolation. In the low-side topology, its control interface is referenced to the HV battery negative terminal. If the low-voltage controller must remain galvanically isolated from this domain, external isolation is required. In the high-side topology, a floating supply and level shifting are required. Best regards, Pavel
View full article