Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Number of supported endpoints on the iMX8 The iMX8 uses the DWC3 for USB, which is an xHCI controller. When I read out the register from iMX8 i can figure out, that it may support up to 64 devices. But when I attach a few devices I much earlier on run in xHCI resource error. It seems there is some kind of a limitation on the number of endpoints, and it also seems that it depends on the type of transfer type (Bulk, Control, ...). On the type of devices I use (includsing the hubs) it seem I run after 80 endpoints into the problem. Could you please provide some exact numbers/formula how many endpoints are supported. Re: Number of supported endpoints on the iMX8 Hello,  The i.MX8 xHCI MaxSlots = 64 value specifies the maximum number of enabled USB device slots, not the total endpoint capacity. xHCI is up to 31 endpoint contexts per device, but the controller does not guarantee that all 64 slots can simultaneously use the maximum number of endpoints. The usable total depends mainly on periodic bandwidth, device speed, endpoint interval and packet size, hub topology, Transaction Translator allocation and DWC3 implementation resources.   Please refer xHCI specification for detailed information. Re: Number of supported endpoints on the iMX8 I checked the xHCI specification and could not find any indication. The only thing xHCI specifies that a controller can return resource error (the one I already mentioned above) E.g. Intel describes for one of their xHCI controller that they support up to 2048 Bulk/Control EPs or up to 128 Interrupt/Isochronous EPs. https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... We have test setup (USB 2.0 only) which works well on Intel chips (several hundred EPs), but fails on a fraction on devices on the iMX8MP (the mentioned 80 EPs). But to know how many and what type of devices we can support we need to know what the limitation of the iMX8MP/DWC3 are. It would be very helpful if you can provide us some kind of formula or limitations, the same way Intel does.
View full article
Mbd Career Advice needed I started my career on Model Based Design of Automotive software 5 years ago and now I feel that its very monotonous and not much learning on the tools side, how have you tackled this situation? The quantum of work that I might be involved in a monthly basis might be 10% on simulink modelling , 50% on testing these models and reporting and the rest on manual compliance docs.
View full article
RTT189 SDK 版本(不含 FDCB) 我正在使用 i.MX RT1180 和 MCUXpresso for VS Code,SDK 版本为 26.03。导入 rledblinky 示例后,我尝试了独立组网 \(SA\)应用程序和存储库应用程序两种应用程序类型。然而,编译后的 .bin 文件该文件不包含 FDCB 数据,导致编程后示例无法正确启动。 相比之下,当我在 MCUXpresso IDE 中导入相同的示例时,生成的二进制文件默认包含 FDCB 内容。 请问在将 MCUXpresso for VS Code 中的示例导入时,有哪些需要特别注意的地方可能会导致这种差异? Re: RTT189 SDK Build without FDCB 嗨@ChandlerY , 非常感谢您对我们产品的关注和提问。 RT1180 RAW/POR 图像切换的详细说明如下: 文档指出,XIP_BOOT_HEADER_ENABLE=1 选择 POR 镜像,而 0 选择 RAW 镜像。 https://docs.mcuxpresso.nxp.com/mcuxsdk/latest/boards/RT/evkmimxrt1180/gettingStarted/topics/RAW_POR_image_switch.html 祝你今天过得愉快。 顺祝商祺! 刘梅 Re: RTT189 SDK Build without FDCB 亲爱的梅, 感谢您的回复。文档中的详细设置只有 KEIL/IAR/MCUXpresso 的示例,我不知道如何在 VS Code 中修改 MCUXpresso 的 XIP_BOOT_HEADER_ENABLE 设置?为什么不直接使用 SDK 示例的默认设置编译 XIP 镜像呢? 祝你今天过得愉快。 顺祝商祺! 钱德勒  Re: RTT189 SDK Build without FDCB 嗨@ChandlerY , 感谢您提供的最新信息。 请您尝试从MCUXpresso SDK Builder下载 SDK,然后在 Toolchain / IDE / Layout 下选择 ARM GCC / MCUXpresso for VS Code,如下图所示? https://mcuxpresso.nxp.com/ 顺祝商祺! 5月 Re: RTT189 SDK Build without FDCB 首先,我选择了为 ARM GCC / MCUXpresso for VS Code 构建的 SDK 包。我重新下载了三个 SDK 版本——25.09、26.04 和 26.09——并为每个版本导入了 hello_world 示例。测试结果如下。 我怀疑这个问题是由 SDK 版本或 MCUXpresso for VS Code 扩展引起的。请您尝试在本地重现这个问题。您有什么建议的解决方案或变通方法吗? 顺祝商祺! 钱德勒 Re: RTT189 SDK Build without FDCB 嗨@ChandlerY , 感谢您的回复。 我这边测试了 SDK 版本 26.09,未能重现该问题;预期的构建配置是存在的。 我注意到在您的截图中,受影响的项目显示为“CMake”。请先查看导入流程和生成的项目配置。请尝试将 hello_world 示例再次导入到新的项目目录中,并确保在导入过程中选择了合适的工具链。 顺祝商祺! 5月 Re: RTT189 SDK Build without FDCB 你好,May 非常感谢。我使用默认设置导入的 SDK 示例不包含 flexspi_nor_debug 版本配置,这让我觉得很不寻常。我使用的是 SDK 版本 26.03,并且也安装了最新版本的 MCUXpresso for VS Code。 顺祝商祺! 钱德勒 Re: RTT189 SDK Build without FDCB 嗨@ChandlerY , 感谢您提供的最新信息。 我建议您在“版本配置”下选择 flexspi_nor_debug 或 flexspi_nor_release,然后重新构建项目。 构建完成后,您应该能够在生成的 .bin 文件中找到 FDCB。文件。 祝你今天过得愉快。 顺祝商祺! 刘梅 Re: RTT189 SDK Build without FDCB 你好,May 谢谢你的提醒。我重新对比了导入步骤,确认这个问题只发生在独立组网 \(SA\)应用程序类型中。为什么 CMake 选项卡下没有其他版本配置可用?能否帮忙解释一下原因? 顺祝商祺! 钱德勒
View full article
iMX8でサポートされるエンドポイントの数 iMX8はUSB用のDWC3を使っており、これはxHCIコントローラです。iMX8のレジスタを読み上げると、最大64台のデバイスをサポートしている可能性があることがわかりました。しかし、いくつかのデバイスを接続すると、かなり早い段階でxHCIリソースエラーが発生します。エンドポイントの数には何らかの制限があるようで、転送タイプ(バルク、コントロールなど)によっても異なるようです。私が使用しているタイプのデバイス(ハブを含む)では、エンドポイントが80個を超えると問題が発生するようです。サポートされているエンドポイントの数について、正確な数字や計算式を教えていただけますか? Re: Number of supported endpoints on the iMX8 こんにちは、 i.MX8 xHCI MaxSlots = 64という値は、有効にできるUSBデバイススロットの最大数を指定するものであり、エンドポイントの総容量を指定するものではありません。xHCIは1デバイスあたり最大31のエンドポイントコンテキストを利用できますが、コントローラは64スロットすべてが同時に最大数のエンドポイントを使用できる保証はありません。使用可能な合計値は、主に周期的な帯域幅、デバイスの速度、エンドポイントの間隔とパケットサイズ、ハブのトポロジー、トランザクショントランスレータの割り当て、およびDWC3の実装リソースに依存します。   詳細については、xHCI仕様書を参照してください。 Re: Number of supported endpoints on the iMX8 xHCI仕様を確認しましたが、特に表示はありませんでした。xHCIがコントローラがリソースエラーを返すと指定しているのは(先に述べたものです) 例えば。Intelは、xHCIコントローラの一つで最大2048のバルク/コントロールEPまたは最大128の割り込み/アイソクロナスEPをサポートすると説明しています。 https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... 当社にはテスト環境(USB 2.0のみ)があり、Intelチップ(数百個のEP)では正常に動作しますが、iMX8MP搭載デバイスの一部(前述の80個のEP)では動作しません。 しかし、どれくらいのデバイス、どのタイプのデバイスがサポートできるかを知るには、iMX8MP/DWC3の制限を知る必要があります。インテルのように、何らかの公式や制限を教えていただけるととても助かります。
View full article
RTT189 SDK Build without FDCB I am using the i.MX RT1180 with MCUXpresso for VS Code,and SDK version 26.03. After importing the rledblinky example, I have tried both Standalone Application and Repository Application as the App type. However, the compiled .bin file does not contain FDCB data, which make the example from booting incorrectly after programing. In contrast, when I import the same example in the MCUXpresso IDE, the generated binary includes FDCB content by default. Could you please help if there are any special points to note when importing examples in MCUXpresso for VS Code that could cause this difference? Re: RTT189 SDK Build without FDCB Hi @ChandlerY , Thank you so much for your interest in our products and foryour question. The RT1180 RAW/POR image switch is described here: The documentation states that  XIP_BOOT_HEADER_ENABLE=1 selects a POR image, while 0 selects a RAW image.   https://docs.mcuxpresso.nxp.com/mcuxsdk/latest/boards/RT/evkmimxrt1180/gettingStarted/topics/RAW_POR_image_switch.html Have a nice day. Best Regards May Liu Re: RTT189 SDK Build without FDCB Hi @ChandlerY , Thanks  for your updated information. Could you please try downloading the SDK from the MCUXpresso SDK Builder and select ARM GCC / MCUXpresso for VS Code under Toolchain / IDE / Layout, as shown in the screenshot below? https://mcuxpresso.nxp.com/ Best Regards May Re: RTT189 SDK Build without FDCB Hi, May     Thanks a lot.The SDK example I imported with default settings does not include the flexspi_nor_debug build configuration, which I find quite unusual. I am using SDK version 26.03, and I have also installed the latest version of MCUXpresso for VS Code. Best Regards ChandlerY Re: RTT189 SDK Build without FDCB I selected the SDK package built for ARM GCC / MCUXpresso for VS Code,firstly. I have re-downloaded three SDK versions — 25.09, 26.04 and 26.09 — and imported the hello_world example for each version. The test results are as follows. I suspect this issue is caused either by the SDK releases versions, or by the MCUXpresso for VS Code extension. Could you please try to reproduce this issue on your side? Do you have any suggested solutions or workarounds? Best Regards ChandlerY Re: RTT189 SDK Build without FDCB Hi @ChandlerY , Thanks for your reply. I tested SDK version 26.09 on my side and could not reproduce the issue; the expected build configurations were available. I noticed that the affected projects are displayed as “CMake” in your screenshot. Please first review the import procedure and the generated project configuration. Try importing the hello_world example again into a new project directory, ensuring that the appropriate toolchain is selected during import. Best Regards May Re: RTT189 SDK Build without FDCB Hi @ChandlerY , Thanks for your updated information. I suggest you can select flexspi_nor_debug or flexspi_nor_release under Build Configurations, and then rebuilding the project. After the build is complete, you should be able to find the FDCB in the generated .bin file. Have a nice day. Best Regards May Liu Re: RTT189 SDK Build without FDCB Dear May,         Thanks for your reply.The documentation detailed settings just have KEIL\IAR\MCUXpresso example, I have no idea how change XIP_BOOT_HEADER_ENABLE at MCUXpresso  for vscode? And why not compile a XIP image by SDK example default settings?  Have a nice day. Best Regards ChandlerY  Re: RTT189 SDK Build without FDCB Hi, May   Thank you for the reminder. I re-compared the import steps and confirmed that this issue only occurs with the standalone application type. Why no other build configurations available under the CMake tab? Could you please help clarify the reason behind this? Best Regards ChandlerY
View full article
关于使用77–81 GHz FMCW雷达进行人和宠物分类的技术咨询 你好, 我的名字是权恩珍,我是韩国GS工程建设公司环保建筑研究团队的研究员。 我们目前正在探索毫米波雷达技术在住宅环境中的非接触式跌倒检测和活动监测方面的应用。 我们的关键技术要求之一是区分人和宠物(如狗和猫),以防止宠物移动引起的误报,同时确保对居住者进行可靠的跌倒检测。 我们对恩智浦半导体的77–81 GHz FMCW雷达解决方案特别感兴趣,希望您能就以下问题提供技术指导: 1. NXP 是否有利用毫米波雷达进行人与宠物(人/非人)分类的现有技术、研究成果或应用实例? 2. 通过基于人工智能的分类算法,利用雷达数据(如点云和多普勒信息)区分人类和宠物在技术上是否可行? 3. 是否有与此应用相关的参考设计、技术文档或开发资源? 我们也希望有机会与恩智浦半导体(NXP)韩国的雷达技术专家或现场应用工程师(FAE)讨论这个话题。 感谢您抽出时间提供帮助。期待您的回复。 顺祝商祺! 恩真 Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar 你好, 让我仔细看看我们是否做过类似的事情,因为我们的雷达是汽车雷达。 顺祝商祺! Peter Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar 你好, 1. NXP 是否有利用毫米波雷达进行人与宠物(人/非人)分类的现有技术、研究成果或应用实例? NXP 目前没有提供专门用于住宅跌倒检测和人与宠物分类的即用型 77–81 GHz 参考解决方案。NXP 的 77–81 GHz 雷达产品组合主要面向汽车雷达应用。 2. 通过基于人工智能的分类算法,利用雷达数据(如点云和多普勒信息)区分人类和宠物在技术上是否可行? 利用雷达进行人/宠物分类在技术上是可行的。机器学习模型可以使用距离、速度、多普勒或微多普勒特性、空间分布和随时间变化的运动等特征。然而,这需要针对特定客户收集数据,并在具有代表性的居住条件下进行模型训练和验证。仅凭点云数据无法保证稳健的性能;较低级别的距离多普勒或距离角度数据可能有所帮助。 3. 是否有与此应用相关的参考设计、技术文档或开发资源? NXP 可提供基于 SAF85xx 平台的雷达评估硬件和信号处理资源,以支持可行性评估和定制开发。这些资源不包含完整的跌倒检测或宠物分类算法。 我们也希望有机会与恩智浦半导体(NXP)韩国的雷达技术专家或现场应用工程师(FAE)讨论这个话题。 请联系分配给贵公司的恩智浦代表销售/现场应用工程师或贵公司的分销商,以便建立单独的支持渠道。 此致, 彼得
View full article
77〜81GHz FMCWレーダーを用いた人間およびペットの分類に関する技術的調査 こんにちは、 私の名前はクォン・ウンジンで、韓国のGSエンジニアリング&建設の環境に優しいビルディング研究チームの研究者です。 現在、住宅環境における非接触落下検知および活動モニタリングにmmWaveレーダー技術の応用を模索しています。 当社の重要な技術要件の一つは、ペット(犬や猫など)の動きによる誤報を防ぎつつ、人間の転倒を確実に検知するために、人間とペットを区別することです。 特にNXPの77–81 GHz FMCWレーダーソリューションに関心があり、以下の質問について技術的なご指導をいただけるとありがたいです。 1. NXPには、mmWaveレーダーを用いた人間とペット(人間/非人間)の分類に関する既存のテクノロジ、研究成果、またはアプリケーション例はありますか? 2. 点群やドップラー情報などのレーダーデータを使って、AIベースの分類アルゴリズムを使って人間とペットを技術的に区別することは可能でしょうか? 3. このアプリケーションに関連するリファレンスデザイン、技術文書、または開発リソースはありますか? また、韓国のNXPレーダー技術専門家やフィールドアプリケーションエンジニア(FAE)とこのテーマについて議論する機会があればありがたいです。 お時間とご協力に感謝いたします。ご回答をお待ちしております。 よろしくお願いいたします。 ウンジン Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar こんにちは、 もし私たちも同じようなことをしたことがあるなら、もっと詳しく見てみます。私たちのレーダーはオートモーティブです。 よろしくお願いいたします。 ピーター Re: Technical Inquiry Regarding Human and Pet Classification Using 77–81 GHz FMCW Radar こんにちは、 1. NXPには、mmWaveレーダーを用いた人間とペット(人間/非人間)の分類に関する既存のテクノロジ、研究成果、またはアプリケーション例はありますか? NXPは現在、住宅における転倒検知および人間とペットの識別を目的とした、すぐに使用できる77~81GHz帯のリファレンスソリューションを提供していません。NXPの77〜81 GHzレーダーポートフォリオは主に自動車用レーダー用途を想定しています。 2. 点群やドップラー情報などのレーダーデータを使って、AIベースの分類アルゴリズムを使って人間とペットを技術的に区別することは可能でしょうか? レーダーを使った人間とペットの分類は理論的には可能です。機械学習モデルは、距離、速度、ドップラーやマイクロドップラーの特性、空間分布、時間経過の動きなどの特徴を利用できます。しかしながら、これにはお客様専用のデータ収集、モデルのトレーニング、代表的な居住条件下での検証が必要です。点雲データだけでは堅牢な性能を保証できません。低レベルの距離ドップラーや距離角データが有益である場合があります。 3. このアプリケーションに関連するリファレンスデザイン、技術文書、または開発リソースはありますか? NXPはSAF85xxプラットフォームに基づくレーダー評価ハードウェアおよび信号プロセッシングリソースを提供し、実現可能性評価やカスタム開発をサポートします。これらのリソースには、完成した転倒検知アルゴリズムやペット分類アルゴリズムは含まれていません。 また、韓国のNXPレーダー技術専門家やフィールドアプリケーションエンジニア(FAE)とこのテーマについて議論する機会があればありがたいです。 ご自社に配属されているNXPの営業担当者/FAE、または代理店にご連絡いただき、別のサポートチャネルを確立してください。 よろしくお願いします、 ピーター
View full article
BCC MC33771Cの測定タイミング こんにちは、チームの皆さん、   私たちはMC33771Cバッテリー・セルコントローラ(BCC)を使って作業しており、異なる読み取り間隔を使うと電圧/温度測定の読み取りタイミングに違いがあることが観察されました。   テスト結果:   構成:スレーブ4台を備えた、BCCと同じ構成。 読み取り間隔:10 ms:4 つのスレーブすべてから温度データを読み取るのに約 40 ms かかります。 読み取り間隔: 100 ms: 4 つのスレーブすべてから同じ温度データを読み取るのに約 7.7 ms かかります。 設定は変更されていないにもかかわらず、読み取り間隔を10msに設定すると、測定全体の読み取り時間が著しく長くなることが観察された。   以下の点についてご理解いただけますか?   10ミリ秒と100ミリ秒の読み取り間隔で、測定値の読み取り時間が大きく異なるのはなぜですか? 読み取り間隔とADC変換、測定値更新、またはBCC通信タイミングの間には、何らかの依存関係がありますか? 4台のBCCスレーブを使用する場合、電圧/温度の読み取りタイミングを安定かつ最適化するための推奨構成や手順はありますか? 複数のMC33771Cデバイスから測定データを読み取る際に考慮すべき、特定のタイミング制約や同期要件はありますか? さらなる分析のために、追加の設定情報や測定ログが必要な場合はお知らせください。 Re: BCC MC33771C measurement timing こんにちは、ニルマルさん。 ADCの設定をご確認いただきありがとうございます。これは重要な補足事項です。ADC_CFG[AVG] = 0、16ビット分解能の場合、ハードウェアtEOCはわずか約520µsです。10ms間隔で40msの読み出し時間が見られるのはADC変換自体によるものではなく、ほぼ間違いなくファームウェアの測定シーケンスによるものです。 tEOCが約520µsの場合、データはどちらの間隔が満了するよりもかなり前に準備完了となる。したがって、観測される読み出し時間の差は、ファームウェアがSOCをトリガーし、間隔に対して結果を読み取る方法とタイミングに起因する。この特定の症状の最も一般的な原因は以下のとおりです。 1. SYS_CFG1[CYCLIC_TIMER]は10msでアクティブになります 周期タイマーが10msに設定されている場合、デバイスは10msごとに自動的に周期変換をトリガーします。ただし、周期的な変換ではMEAS_xxxx測定レジスタは更新されず、OV/UV/OT/UT障害フラグのみが更新されます。MCUファームウェアがオンデマンドSOCを発行する前にサイクリックトリガーを待つと、実効測定サイクルはサイクル周期と連動し、各読み取りまでに最大10msのレイテンシが加算されます。100msの周期周期でこのレイテンシは消えます。なぜならMCUは独立してオンデマンドSOCを発行するためです。SYS_CFG1[CYCLIC_TIMER]の値を確認し、もし有効であれば無効化するか、MCUのリードシーケンスを完全に切り離すことを検討してください。 2. 読み取り前に固定間隔の遅延を挿入(EOCを待たない) ファームウェアがSOCを発行し、EOCフラグをポーリングするのではなく、読み取り間隔全体(10msまたは100ms)待ってから読み取る場合、動作は次のようになります。 100 ms: SOC → 100 ms待機 → 読み取り (7.7 ms 通信) → 測定値 ≈ 7.7 ms ✓ 10 ms: SOC → 10 ms 待機 → 読み取り (7.7 ms 通信) → しかし、サイクルが繰り返され、タイミングが複合すると、実効測定期間が長くなります。 3. SOCはブロードキャストではなく、スレーブごとに発行される ファームウェアが各スレーブに対して個別にSOCをトリガーし、各スレーブ間の読み取り間隔を強制する場合、4つのスレーブの合計は間隔の倍数になります。 4体の奴隷の正しい順序は次のとおりです。 - 4つのスレーブすべてに同時に単一のブロードキャストSOCを発行します。 - EOCフラグをポーリングする(または16ビットで最低520µs待機する、AVG=0)—読み取り間隔と同じ固定遅延は使用しない。 - EOCが確認された後、4つのスレーブすべてを順番に読み込む。 BRs、トーマス お好みの間隔で繰り返してください。 Re: BCC MC33771C measurement timing こんにちは、 @TomasVaverka さん。 詳しい説明をありがとうございました。 私たちの構成では、以下の設定を使用しています。 ADC_CFG[AVG] = 0 ADC分解能 = 16ビット BCCスレーブの数 = 4 両方のテストCASE(10msと100msの読み取り間隔)で同じ構成を使用しています。 しかしながら、以下のようなタイミングのずれが観察された。 10 ms 読み取り間隔: 4 つのスレーブすべてから温度データを読み取るのに約 40 ms かかります。 100 ms 読み取り間隔: 4 つのスレーブすべてから温度データを読み取るのに約 7.7 ms かかります。 ADCの平均化と解像度の設定は両者で同じですが、なぜ変換と測定表示のタイミングが大きく異なるのか、説明していただけますか? この動作を説明するために、SOCトリガー間隔、ADC変換状況、EOCフラグ処理に何か依存関係があるのでしょうか? また、10msの測定間隔で一貫した測定表示タイミングを実現する方法についても提案していただけますか? Re: BCC MC33771C measurement timing こんにちは、ニルマルさん。 タイミングのずれは、おそらくADC_CFG[AVG]の平均化設定が原因です。 平均化が有効になっている場合、tEOC(SOCからデータ準備完了までの時間)はサンプル数に比例して変化します。例えば、16ビット解像度でAVG=64の場合、tEOCは約32.5msとなり、10msの読み取り間隔をはるかに超えます。これは、観察された挙動を説明するものです。 100 ms間隔で:MCUが読み取り→通信時間のみ(~7.7 ms)を測定した時点で変換は完了しています。 10 ms間隔で:MCUは変換完了を待つ必要があります →測定時間=残りのtEOC待ち時間+通信≈40ms。 ご質問に関連する追加事項をいくつかご紹介します。 1. サイクルモード (SYS_CFG1[CYCLIC_TIMER]) は MEAS_xxxx レジスタを更新しません。障害フラグ (OV/UV/OT/UT) のみを更新します。実際の電圧/温度測定値を取得するには、オンデマンドSOCが必要です。平均化機能は、周期モードでは利用できません。 2. 結果を読む前に、必ずEOCフラグが表示されるまで待ってください。読み取り間隔と同じ固定遅延時間は、tEOCを超えることが保証されている場合を除き、使用しないでください。 3. 4台のスレーブの場合:1つのSOCをすべてのスレーブに同時にブロードキャストし(すべてが並列で変換し、tEOCで完了)、その後、順次読み取ります。16ビット、AVG=0の場合、最小合計時間は約0.52ms(tEOC)+ 4×0.7ms(TPL通信)≈3.3msです。 4. フルタイム最適化フレームワークについては、AN12637 MC33771CおよびMC33772Cベースのシステムタイミング最適化(nxp.com で利用可能、ログインが必要)を参照してください。 BRs、トーマス Re: BCC MC33771C measurement timing こんにちは、 @TomasVaverka さん、 SOCにブロードキャストメッセージを使用していますが、それでもタイミングのずれが発生しています。
View full article
eTPU A/Bクロック停止中のMPC5777C Nexusトレース こんにちは、 eTPU A/B クロックがSIU_HLT1 ETPUAビットで停止されると、Nexus Port コントローラ(NPC)からのMDOおよびMSEO Nexus出力が0V(死)に固定されることが判明しました。他の Nexus クライアント (例:e200) は Nexus トレースデータを生成しています。 SIU_HLT1.ETPUA が後で「0」で書き込まれると(クロックが停止しなくなる)、e200 Nexus クライアントからの Nexus トレース ストリームが NPC と外部の世界に到達します。 いくつかのテストを行った結果、HLT1レジスタ内の他のクロック停止要求では、MSEO/MDOピンで同様の動作は発生しないようです。 つまり、eTPUのA/Bクロック停止がNexusのトレース動作全般に影響を与えるように見えるのが核心問題です。 これは、NPCのクロック分周器やポート幅に関係なく発生します。 試行錯誤で見つけた回避策は、まず各 (A と B) eTPU エンジンをそれぞれの ECR.MDIS ビットで無効にし、次に HLT1.ETPUA でモジュール クロック全体を無効にすると、トレースが他の Nexus クライアント (例:e200コア)。   しかし、この回避策はユーザーのアプリケーションを変更する必要があるため最適ではありません。この挙動をデバッガで軽減できるかどうか気になっています。   Re: MPC5777C Nexus trace while eTPU A/B clock halted こんにちは、 私はこれまでそのような問題に遭遇したことがありません。私たちはいつもAshware of the CodewarriorのeTPUシミュレータを使っているからです。 詳しく調べて、できるだけ早くご連絡いたします。 よろしくお願いいたします。 ピーター Re: MPC5777C Nexus trace while eTPU A/B clock halted こんにちは、 この動作は、MPC5777Cのクロックゲーティングの実装に関連しているようです。eTPU A/B停止要求がNexusの出力に影響を与えないようにするNPC構成は、我々の知る限り存在しません。 デバッガーの回避策として、SIU_HLT1[ETPUA] = 1 を設定する前に、以下の手順を実行してください。 eTPUエンジンのECR[MDIS]ビットを両方とも1に設定します。 エンジンが現在の作業を完了するまでお待ちください。 SIU_HLT1[ETPUA]を1に設定します。 このシーケンスはデバッガの停止スクリプトで自動化可能です。ただし、両方のeTPUエンジンを停止させるため、アプリケーション側には透過性がありません。この問題はシリコンデザインチームによっても、デバイスのエラタムの可能性として検討されるべきです。 よろしくお願いいたします。 ピーター Re: MPC5777C Nexus trace while eTPU A/B clock halted こんにちは、 調べていただきありがとうございます。問題は、デバッガとしてSoC周辺レジスタの変更を避けようとすることです。なぜなら、それがユーザーのアプリケーションに影響を与えるからです。 この場合の問題は、SIU_HLT1[ETPUA] = 1がデバッガである私たちではなく、ユーザーアプリケーションによって書かれていることです。したがって、デバッガはユーザーアプリケーションがいつそれを実行するかを知ることができず、デバッガがアプリケーションが書く前にECR[MDIS]を書くことができます SIU_HLT1[ETPUA] = 1; ユーザーには、ECR[MDIS]がSIU_HLT1[ETPUA] = 1の前に書かれた方法でアプリケーションを更新することを推奨します。
View full article
クロックと電源の関係:MIMXRT685 - EVK こんにちは、 アプリケーションでは、コアクロック周波数を可能な限り最大、つまりデフォルトの250MHzから297MHzまで上げています。権力という観点から見て、それがどのような影響をもたらすのかを知りたかった。今は何も壊れていませんが、データシートの静的な特性から判断すると、FUTUREのハードフォールトを避けるためにいくつか変更が必要だと思います。ぜひアドバイスをいただけるとありがたいです。 よろしくお願いいたします! シュリ Re: Clock - power relationship : MIMXRT685 - EVK こんにちは、 @shri00 さん。 私たちの製品にご関心を寄せ、コミュニティをご利用いただき、本当にありがとうございます。 MIMXRT685-EVKで297MHz動作を行う場合は、VDDCORE電圧とクロック構成を確認してください。基板が現在故障なく動作しているという事実は、必ずしもVDDCOREが目標とする周波数および温度範囲の動作要件を満たしていることを意味するものではありません。   クロック周波数を上げる際は、まずVDDCOREを目標周波数に必要なレベルに設定し、その後より高い周波数に切り替えます。   VDDCOREとクロック周波数の関係については、RT600データシートの表20および表21を参照してください。 32ビットCortex-M33®およびXtensa HiFi4オーディオDSP CPUを搭載したデュアルコアマイクロコントローラ 良い1日を。 よろしくお願いいたします。 メイ・リウ
View full article
Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi, I am currently working on porting the NXP Matter stack to the MIMXRT700-EVK (MIMXRT798S) using the MCUXpresso SDK and VS Code. The board uses an external Murata Type 2EL wireless module based on the IW612 chipset. Development Setup and Changes I downloaded and set up the Matter MCUXpresso SDK workspace through VS Code. The workspace is located at matter_mcuxpresso/mcuxsdk. I have made RT700-specific changes in the following areas: Matter: Modified files under middleware/matter for RT700 platform integration. Wireless framework: Added RT700-specific platform support and integration for the external Murata Type 2EL (IW612) wireless module. Linker script: Used the RT700 SDK-provided MIMXRT798Sxxxx_cm33_core0_flash.ld as the reference and modified it for the Matter application's memory layout and NVS storage configuration. Issue Description The Matter application builds successfully and can be programmed using LinkServer. However, runtime initialization fails with CHIP_ERROR_PERSISTED_STORAGE_FAILED at the following call in src/platform/nxp/common/NXPConfigNVS.cpp: flash_init(fa->fa_dev) CHIP_ERROR_PERSISTED_STORAGE_FAILED Linker Script Attachment I will attach the modified MIMXRT798Sxxxx_cm33_core0_flash.ld linker script for reference. It is based on the RT700 SDK-provided linker script and includes changes for the Matter application's memory layout and NVS storage configuration. Support Required Could you please help clarify: How should the flash device and driver be configured for Matter persistent storage on the RT700-EVK? Are any additional RT700-specific flash driver or NVS integration steps required? Could the modified linker script or NVS memory layout contribute to the flash_init() failure? I would appreciate your guidance on resolving this issue. Thank you. Evaluation Board Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi @Aparna1 , Thanks for your questions! I reviewed the provided linker script. It currently references the following FlexSPI-related objects: *(EXCLUDE_FILE( ... *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o* ) .text*) However, the MIMXRT700 uses the XSPI controller. Please confirm that the application is linked with the correct RT700 XSPI flash backend and that fa->fa_dev refers to this device, rather than to a FlexSPI backend used by other i.MX RT platforms. Please also check the map file for flash_init() , the flash erase/program functions, and the related XSPI_* functions. These functions and their required configuration data should be located in RAM rather than in the XIP flash region. We suggest checking the port in this order: Verify the official RT700 XSPI NOR flash example from the SDK; Confirm that fa->fa_dev uses the correct XSPI backend; Verify that the flash-operation code actually executes from RAM; Then check the NVS address, sector alignment, and whether the driver expects an absolute address or a device-relative offset. Best regards, Gavin Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure hi @Gavin_Jia  I have modified the linker (MIMXRT798Sxxxx_cm33_core0_flash.ld) file based on the suggested changes and updated the XSPI-related configuration. However, the issue still persists, and the flash_init() function continues to fail. I am sharing the modified MIMXRT798Sxxxx_cm33_core0_flash.ld file for your review. Could you please check the linker configuration and guide me on what additional changes are required to resolve the XSPI flash initialization issue? Thank you. Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hi @Aparna1 , Thanks for your update. I still recommend using the `mimxrt700evk_flash_component_octal_xspi_cm33_core0` project—along with its associated linker script (LD file)—as a baseline. Please ensure that the code related to flash operations is successfully ported before moving on to Matter. It is not possible to fully diagnose your porting project based solely on the linker script, so I can only offer a few suggestions. Thank you for your understanding. Below are some issues I identified after reviewing your script: 1. The XSPI code may still be linked into the XIP region In the .text section, the script first excludes the XSPI and NVS-related object files: *(EXCLUDE_FILE( ... *fsl_xspi_nor_flash.c* *mflash_drv.c.o* *fsl_xspi.c.o* ) .text*) However, the script later contains unconditional rules:   *(.text) *(.text*) *(.rodata) *(.rodata*) These later rules can collect the previously excluded input sections again and place them back into m_text , which is located in the external XSPI Flash region. Therefore, the current EXCLUDE_FILE rules do not guarantee that the XSPI/NVS execution path is running from RAM. 2. The RAM section still contains FlexSPI objects instead of the RT700 XSPI objects The .data section currently places the following code into RAM: *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o*   However, RT700 uses the XSPI controller.  3. fsl_xspi_nor_flash constants are not consistently moved to RAM fsl_xspi_nor_flash is included in the .text* exclusion list, but it is not included in the .rodata* exclusion list. If you are uncertain about a modified linker script or the final image, extracting key information from the map file is a debugging approach worth trying. Best regards, Gavin Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure Hello @Gavin_Jia  The previously reported flash_init  issue (CHIP_ERROR_PERSISTED_STORAGE_FAILED) has been resolved. The application now successfully completes the flash initialization process. However, I am currently facing a new issue during IW612 Wi-Fi initialization on the RT700-EVK with the external Murata Type 2EL (IW612) M.2 module. The following error messages appear during startup: [wifi_io] Error: SDIO - FW Ready Registers not set [wifi] Error: sd_wifi_init failed. status code -1 [wlcm] Error: wifi init/reinit failed. status code -1 ASSERT ERROR " WM_SUCCESS == ret "  Could you please help us investigate this issue and suggest the required SDIO configuration, firmware download sequence, or any RT700-specific changes needed for IW612 initialization? Thank You 
View full article
请求提供基于霍尔传感器的电机控制参考固件和培训资料 尊敬的恩智浦团队: 我们正在与一位客户合作开发一种使用 24V、3.47A 电机的空气冷却系统。 我们已经成功完成了基于无传感器FOC电机控制的演示。客户现在希望使用 FRDM-MCXA156 EVK(控制卡)和 FRDM-MC-LVPMSM(电源卡)集成霍尔传感器进行转子位置检测。 能否推荐一个合适的参考固件或应用示例,用于在该硬件组合上实现基于霍尔传感器的电机控制? 我查看了GitHub上提供的LPC55S36霍尔传感器BLDC示例。 但是,我找不到此示例对应的 FreeMASTER 配置文件(.pmpx)。 请问您能否帮我们解决以下问题? FRDM-MC-LVPMSM 上霍尔传感器集成的 FRDM-MCXA156 参考固件。 相应的 FreeMASTER 项目/配置文件(.pmpx)(如有)。 基于 FRDM-MCXA156 EVK,将霍尔传感器反馈集成到现有无传感器 FOC 项目中的相关应用笔记、培训材料或实施指南。 非常感谢您的技术指导和建议。 此致 达尔尚·J·L WPG印度 电路板设计 开发板 FRDM 培训 动手实践培训 MCXA 电机控制 Re: Request for Hall Sensor-Based Motor Control Reference Firmware and Training Material 你好@Darshan_J_L , 感谢您的帖子。 MCUXpresso SDK 包含多个电机控制示例项目。您可以在下一页找到有关 FRDM-MCXA156 的更多信息。 MCUXpresso 电机控制 SDK | NXP 半导体。   FRDM-MCXA156 + FRDM-MC-LVPMSM 组合的 pmsm_enc 示例位于 SDK v25.06 中。它支持无传感器和有传感器的 FOC,并包含 pmsm_float_enc.pmpx FreeMASTER 项目。您可以参考UG10247.pdf 文件。更多详情请见下文。   关于 LPC55S36 演示对应的 FreeMASTER 配置文件 (.pmpx),您可以在这里找到: an-lpc55s36_mc_bldc_whall/LPC5536_mc_bldc_wHall.pmpx at main · nxp-appcodehub/an-lpc55s36_mc_bldc_whall · GitHub   希望对您有所帮助。如果您还有其他问题,请告诉我。   BR 塞莱斯特    
View full article
S32 Design Studio for Power Architecture 2017.R1 在许可证过期后显示“缺少许可证” 我正在 Windows 系统上使用S32 Design Studio for Power Architecture 2017.R1 版本。现在 IDE 显示“缺少许可证” ,而且许可证似乎已经过期。 激活 | 安装 | 许可 | 安装程序下载
View full article
BCC MC33771C measurement timing Hello Team,   We are working with the MC33771C Battery Cell Controller (BCC) and have observed a difference in voltage/temperature measurement readout timing when using different read intervals.   Test observations:   Configuration: Same BCC configuration with 4 slaves. Read interval: 10 ms: Reading temperature data from all 4 slaves takes approximately 40 ms. Read interval: 100 ms: Reading the same temperature data from all 4 slaves takes approximately 7.7 ms. We observe that the total measurement readout time is significantly higher when the read interval is set to 10 ms, even though the configuration remains unchanged.   Could you please help us understand the following?   Why does the measurement readout time differ significantly between the 10 ms and 100 ms read intervals? Is there any dependency between the read interval and the ADC conversion, measurement update, or BCC communication timing? Is there any recommended configuration or procedure to achieve consistent and optimized voltage/temperature readout timing when using 4 BCC slaves? Are there any specific timing constraints or synchronization requirements that we should consider when reading measurement data from multiple MC33771C devices? Please let us know if any additional configuration details or measurement logs are required for further analysis. Re: BCC MC33771C measurement timing Hello Nirmal, Thank you for confirming the ADC configuration. This is a critical clarification: with ADC_CFG[AVG] = 0 and 16-bit resolution, the hardware tEOC is only ~520 µs. The 40 ms readout time you observe at 10 ms intervals cannot be caused by the ADC conversion itself, it is almost certainly caused by the firmware measurement sequence. With tEOC ≈ 520 µs, data is ready well before either interval expires. The difference in observed readout time therefore comes from how and when the firmware triggers SOC and reads results relative to the interval. The most common causes of this specific symptom are: 1. SYS_CFG1[CYCLIC_TIMER] is active at 10 ms If the cyclic timer is set to 10 ms, the device autonomously triggers a cyclic conversion every 10 ms. However, cyclic conversions do not update the MEAS_xxxx measurement registers — they only update OV/UV/OT/UT fault flags. If the MCU firmware waits for a cyclic trigger before issuing an on-demand SOC, the effective measurement cycle gets coupled to the cyclic period, adding up to 10 ms of latency before each read. At 100 ms cyclic period, this latency disappears because the MCU issues on-demand SOC independently. Please verify the value of SYS_CFG1[CYCLIC_TIMER] and, if active, consider disabling it or decoupling your MCU read sequence from it entirely. 2. Fixed interval delay inserted before reading (not waiting for EOC) If the firmware issues SOC, then waits the full read interval (10 ms or 100 ms) before reading — rather than polling the EOC flag — the behavior would be: 100 ms: SOC → wait 100 ms → read (7.7 ms comm) → measured ≈ 7.7 ms ✓ 10 ms: SOC → wait 10 ms → read (7.7 ms comm) → but then if the cycle repeats and timings compound, the effective measured duration grows. 3. SOC issued per slave rather than as a broadcast If the firmware triggers SOC individually to each slave and enforces the read interval between each, the total for 4 slaves compounds to a multiple of the interval. The correct sequence for 4 slaves is: - Issue a single broadcast SOC to all 4 slaves simultaneously. - Poll the EOC flag (or wait a minimum of 520 µs at 16-bit, AVG=0) — do not use a fixed delay equal to the read interval. - Read all 4 slaves sequentially after EOC is confirmed. BRs, Tomas Repeat at your desired interval. Re: BCC MC33771C measurement timing Hello @TomasVaverka  Thank you for the detailed explanation. In our configuration, we are using the following settings: ADC_CFG[AVG] = 0 ADC Resolution = 16-bit Number of BCC slaves = 4 We are using the same configuration for both test cases (10 ms and 100 ms read intervals). However, we observe the following timing difference: 10 ms read interval: Approximately 40 ms to read temperature data from all 4 slaves. 100 ms read interval: Approximately 7.7 ms to read temperature data from all 4 slaves. Since the ADC averaging and resolution settings are identical in both cases, could you please clarify why the conversion and measurement readout timing differs significantly? Is there any dependency on the SOC trigger interval, ADC conversion status, or EOC flag handling that could explain this behavior? Could you also suggest how we can achieve consistent measurement readout timing with a 10 ms measurement interval? Re: BCC MC33771C measurement timing Hello Nirmal, The timing difference is most likely caused by your ADC_CFG[AVG] averaging setting. When averaging is enabled, tEOC (time from SOC to data ready) scales proportionally with the sample count. For example, at 16-bit resolution with AVG=64, tEOC ≈ 32.5 ms — far exceeding your 10 ms read interval. This explains the observed behavior: At 100 ms interval: Conversion is already complete when the MCU reads → only communication time is measured (~7.7 ms). At 10 ms interval: The MCU must wait for conversion to finish → measured time = remaining tEOC wait + communication ≈ 40 ms. A few additional points relevant to your questions: 1. Cyclic mode (SYS_CFG1[CYCLIC_TIMER]) does NOT update MEAS_xxxx registers — it only updates fault flags (OV/UV/OT/UT). For actual voltage/temperature readings, on-demand SOC is required. Averaging is also not available in cyclic mode. 2. Always wait for the EOC flag before reading results. Do not use a fixed delay equal to the read interval unless it is guaranteed to exceed tEOC. 3. For 4 slaves: broadcast a single SOC to all slaves simultaneously (all convert in parallel, completing at tEOC), then read sequentially. At 16-bit, AVG=0, the minimum total time is approximately 0.52 ms (tEOC) + 4 × 0.7 ms (TPL comm) ≈ 3.3 ms. 4. For a full timing optimization framework, refer to AN12637: MC33771C and MC33772C Based System Timing Optimization (available on nxp.com, login required). BRs, Tomas Re: BCC MC33771C measurement timing Hello @TomasVaverka , I am using broadcast message for SOC, still i am facing timing difference.
View full article
S32 设计工作室 v.3.5 版本许可 您好,NXP支持团队, 我的 S32 Design Studio v.3.5 版本许可证已于 2026 年 10 月 19 日到期。请问您能否帮忙延长许可证期限? 激活码:30E0-0F7D-F883-9AFB 感谢您的支持。 Eclipse IDE 使用和设置
View full article
FDCBなしのRTT189 SDKビルド 私は i.MX RT1180とMCUXpresso for VS Code、SDKバージョン26.03を使っています。rledblinkyの例をインポートした後、アプリタイプとして Standalone Application と Repository Application の両方を試しました。しかし、コンパイルされた.binファイルはファイルにはFDCBデータが含まれていないため、プログラミング後にサンプルが正しく起動しない。 対照的に、同じ例をMCUXpresso IDEにインポートすると、生成されたバイナリにはデフォルトでFDCBコンテンツが含まれています。 MCUXpresso for VS Codeでサンプルをインポートする際に、この違いの原因となる特別なポイントがあれば教えていただけませんか? Re: RTT189 SDK Build without FDCB こんにちは、 @ChandlerY さん。 私たちの製品にご関心をお寄せいただき、ご質問をいただき、本当にありがとうございます。 RT1180 RAW/PORイメージスイッチについては以下に説明しています: ドキュメントによると、XIP_BOOT_HEADER_ENABLE=1はPOR画像を選択し、0はRAW画像を選択します。 https://docs.mcuxpresso.nxp.com/mcuxsdk/latest/boards/RT/evkmimxrt1180/gettingStarted/topics/RAW_POR_image_switch.html 良い1日を。 よろしくお願いいたします。 メイ・リウ Re: RTT189 SDK Build without FDCB こんにちは、 @ChandlerY さん。 最新情報をありがとうございます。 ビルド構成のflexspi_nor_debugかflexspi_nor_releaseを選択してからプロジェクトを再構築することをお勧めします。 ビルドが完了すると、生成された.binファイルの中にFDCBが見つかるはずです。ファイル。 良い1日を。 よろしくお願いいたします。 メイ・リウ Re: RTT189 SDK Build without FDCB メイ様、 ご返信ありがとうございます。ドキュメントの詳細設定にはKEIL\IAR\MCUXpressoの例しかなく、MCUXpressoでVScodeでXIP_BOOT_HEADER_ENABLEを変更する方法が全く分かりません。それに、なぜSDK例でXIPイメージをコンパイルしないのですか? 良い1日を。 よろしくお願いいたします。 チャンドリー  Re: RTT189 SDK Build without FDCB まずはARM GCC / MCUXpresso for VS Code用にビルドされたSDKパッケージを選びました。私は3つのSDKsバージョン(25.09、26.04、26.09)を再ダウンロードし、それぞれのバージョンのhello_world例をインポートしました。試験結果は以下のとおりです。 この問題はSDKsのリリースバージョンか、MCUXpresso for VS Code拡張機能が原因だと思います。この問題をあなたの側でも再現していただけますか?何か解決策や回避策をご提案いただけますか? よろしくお願いいたします。 チャンドリー Re: RTT189 SDK Build without FDCB こんにちは、 @ChandlerY さん。 ご返信ありがとうございます。 SDKバージョン26.09を自分でテストしましたが、問題を再現できませんでした。期待されるビルド構成は利用可能でした。 スクリーンショットを見ると、影響を受けているプロジェクトが「CMake」と表示されていることに気づきました。まず、インポート手順と生成されたプロジェクト構成を確認してください。新しいプロジェクトディレクトリにhello_worldのサンプルを再度インポートしてみてください。その際、インポート時に適切なツールチェーンが選択されていることを確認してください。 よろしくお願いいたします。 5月 Re: RTT189 SDK Build without FDCB こんにちは、メイ ありがとうございます。デフォルト設定でインポートしたSDKの例にはflexspi_nor_debugビルド構成が含まれておらず、これはかなり珍しいと感じます。私はSDKバージョン26.03を使っており、最新バージョンのMCUXpresso for VS Codeもインストールしています。 よろしくお願いいたします。 チャンドリー Re: RTT189 SDK Build without FDCB こんにちは、 @ChandlerY さん。 最新情報をありがとうございます。 MCUXpresso SDK BuilderからSDKをダウンロードし、下のスクリーンショットのようにToolchain / IDE / Layoutの「ARM GCC / MCUXpresso for VS Code」を選択してください。 https://mcuxpresso.nxp.com/ よろしくお願いいたします。 5月 Re: RTT189 SDK Build without FDCB こんにちは、メイ ご指摘ありがとうございます。インポート手順を再比較したところ、この問題はスタンドアロンのアプリケーションタイプでのみ発生することが確認されました。なぜCMakeタブで他のビルド構成が使えないのでしょうか?その理由を教えていただけますか? よろしくお願いいたします。 チャンドリー
View full article
MatterスタックのMIMXRT700-EVK(MIMXRT798S)への移植 — 永続的なストレージ初期化の失敗 こんにちは、 現在、MCUXpresso SDKとVS Codeを使ってNXP MatterスタックをMIMXRT700-EVK(MIMXRT798S)に移植する作業を進めています 。このボードはIW612チップセットをベースにした外付けのMurata Type 2EL無線モジュールを使用しています。 開発環境のセットアップと変更 VS Codeを通じてマター MCUXpresso SDKワークスペースをダウンロードし、セットアップしました。ワークスペースはmatter_mcuxpresso/mcuxsdkにあります。 以下の点において、RT700専用の変更を加えました。 マター:RT700プラットフォーム統合のためにミドルウェア/マター上でファイルを修正しました。 ワイヤレスフレームワーク: 外部村田タイプ2EL(IW612)無線モジュールのRT700専用プラットフォームサポートと統合を追加。 リンカースクリプト:RT700 SDKが提供するMIMXRT798Sxxxx_cm33_core0_flash.ldを参照として使用し、MatterアプリケーションのメモリレイアウトおよびNVSストレージ構成に合わせて修正しました。 問題の説明 Matterアプリケーションは正常にビルドでき、LinkServerを使ってプログラム可能です。しかし、src/platform/nxp/common/NXPConfigNVS.cppの以下の呼び出しでCHIP_ERROR_PERSISTED_STORAGE_FAILEDが実行されると実行時の初期化が失敗します。 flash_init(fa->fa_dev) CHIP_ERROR_PERSISTED_STORAGE_FAILED リンカースクリプトの添付ファイル 参照のために修正されたMIMXRT798Sxxxx_cm33_core0_flash.ldリンカースクリプトを添付します 。これはRT700 SDKが提供するリンカースクリプトを基にしており、MatterアプリケーションのメモリレイアウトおよびNVSストレージ構成の変更を含んでいます。 サポートが必要です もう少し詳しく教えていただけますか: RT700-EVKのマター永続保存ストレージ用にフラッシュデバイスとドライバーはどのように設定すべきでしょうか? RT700専用のフラッシュドライバーやNVS統合の追加ステップは必要ですか? 修正されたリンカースクリプトやNVSメモリレイアウトがflash_init()の失敗に影響している可能性はありますか? この問題の解決について、ご指導いただければ幸いです。 よろしくお願いします。 評価ボード Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure こんにちは、@Aparna1 さん。 ご質問ありがとうございます! 提供されたリンカースクリプトを確認しました。現在、以下のFlexSPI関連オブジェクトを参照しています。 *(EXCLUDE_FILE( ... *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o* ) .text*) ただし、MIMXRT700はXSPIコントローラを使用しています。アプリケーションが正しいRT700 XSPIフラッシュバックエンドとリンクされており、他のRTプラットフォームで使われるFlexSPIバックエンドではなく、このデバイスを指している i.MX fa->fa_dev 確認してください。 また、マップファイルで flash_init() 、フラッシュ消去/プログラム機能、および関連する XSPI_* 機能を確認してください。これらの機能およびそれらに必要な設定データは、XIPフラッシュ領域ではなく、RAMに配置する必要があります。 ポートの確認は以下の順序で行うことをお勧めします。 SDKの公式RT700 XSPI NORフラッシュ例を確認してください。 fa->fa_dev 正しいXSPIバックエンドを使用していることを確認してください。 フラッシュ操作コードが実際にRAMから実行されることを確認する。 次にNVSアドレス、セクターアライメント、ドライバが絶対アドレスかデバイス相対オフセットを期待しているかを確認します。 よろしくお願いします、 ギャビン Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure こんにちは、 @Gavin_Jia ご提案いただいた変更に基づいてリンカーファイル( MIMXRT798Sxxxx_cm33_core0_flash.ld )を修正し、XSPI関連の設定を更新しました。しかし、問題は依然として解決せず、 flash_init()関数が引き続き失敗します。 修正済みのMIMXRT798Sxxxx_cm33_core0_flash.ldファイルを共有してご覧いただきます。リンク設定を確認し、XSPIフラッシュの初期化問題を解決するために追加で何の変更が必要か教えていただけませんか? よろしくお願いします。 Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure こんにちは、@Aparna1 さん。 最新情報のご提供ありがとうございます。 ベースラインとして、`mimxrt700evk_flash_component_octal_xspi_cm33_core0` プロジェクトと、それに関連するリンカースクリプト (LD ファイル) を使用することをお勧めします。マターに移行する前に、フラッシュ操作に関連するコードが正常に移植されていることを確認してください。 リンカースクリプトだけで移植プロジェクトを完全に診断することはできないため、いくつかの提案しかできません。ご理解いただきありがとうございます。 あなたのスクリプトをレビューした結果、いくつか問題点が見つかりました。以下にその点を記載します。 1.XSPIコードはXIP領域にリンクされている可能性がある .text セクションでは、スクリプトはまず XSPI および NVS 関連のオブジェクトファイルを除外します。 *(EXCLUDE_FILE( ...​​ *fsl_xspi_nor_flash.c* *mflash_drv.c.o* *fsl_xspi.c.o* ) 。文章*) しかし、スクリプトには後ほど無条件のルールが含まれる。   *(。文章) *(。文章*) *(.rodata) *(.rodata*) これらの後のルールは、以前に除外された入力セクションを再び収集し、外部XSPI Flash領域にある m_text に戻すことができます。 したがって、現在の EXCLUDE_FILE ルールでは、XSPI/NVS実行パスがRAMから実行されることが保証されません。 2. RAMセクションには、RT700のXSPIオブジェクトではなく、FlexSPIオブジェクトが依然として含まれています。 .data セクションは現在、以下のコードを RAM に配置します。 *fsl_adapter_flexspi_nor_flash.c.o* *mflash_drv.c.o* *fsl_flexspi.c.o*   しかし、RT700はXSPIコントローラを使用しています。 3. fsl_xspi_nor_flash 定数は一貫してRAMに移動されません fsl_xspi_nor_flash .text* 除外リストには含まれていますが、 .rodata* 除外リストには含まれていません。 変更したリンカースクリプトや最終イメージについて不明な点がある場合は、マップファイルから重要な情報を抽出するというデバッグ手法を試してみる価値があります。 よろしくお願いします、 ギャビン Re: Matter Stack Porting to MIMXRT700-EVK (MIMXRT798S) — Persistent Storage Initialization Failure こんにちは、 @Gavin_Jia さん。 以前報告されたflash_initの問題(CHIP_ERROR_PERSISTED_STORAGE_FAILED)は解決されました。アプリケーションはフラッシュ初期化プロセスを正常に完了しました。 しかしながら、現在、RT700-EVK上で外部のMurata Type 2EL (IW612) M.2モジュールを使用してIW612 Wi-Fiを初期化する際に、新たな問題に直面しています。 起動時に以下のエラーメッセージが表示されます。 [wifi_io] Error: SDIO - FW Ready Registers not set [wifi] Error: sd_wifi_init failed. status code -1 [wlcm] Error: wifi init/reinit failed. status code -1 ASSERT ERROR " WM_SUCCESS == ret "  この問題の調査に協力していただき、必要なSDIO設定、ファームウェアダウンロードシーケンス、またはIW612初期化に必要なRT700固有の変更をご提案いただけますか? ありがとうございます
View full article
时钟-电源关系:MIMXRT685-EVK 你好, 对于某个应用,我将核心时钟频率提升到最大可能值,即从默认的 250 MHz 提升到 297 MHz。我想知道从权力角度来看,这会造成哪些影响。虽然目前还没有出现任何问题,但根据数据手册中的静态特性,我认为我需要做一些更改,以避免将来出现硬故障。我非常希望得到一些指导。 提前感谢! 什里 Re: Clock - power relationship : MIMXRT685 - EVK 嗨@shri00 , 非常感谢您对我们产品的关注以及对我们社区的使用。 对于 MIMXRT685-EVK 的 297 MHz 运行,请检查 VDDCORE 电压以及时钟配置。板目前运行无故障这一事实并不一定意味着 VDDCORE 满足您目标频率和温度范围的运行要求。   提高时钟频率时,首先将 VDDCORE 设置为目标频率所需的电平,然后再切换到更高的频率。   有关 VDDCORE 与时钟频率的关系,请参阅 RT600 数据手册的表 20 和表 21。 采用 32 位 Cortex®-M33 和 Xtensa HiFi4 音频 DSP CPU 的双核微控制器 祝你今天过得愉快。 顺祝商祺! 刘梅
View full article
HSE [等待中断(WFI)] 状态理解 目前,我正在进行 MCU 时钟初始化,并等待 HSE 进入 WFI 状态(CLOCK_IP_WFI_EXECUTED == 0x80000000U),然后再进行时钟配置。 目前的实现方式如下所示。但是,我担心如果 HSE 始终无法转换到 WFI 状态,ECU 将无限期地陷入等待循环。请问能否建议一种合适的保护措施或超时机制来安全地处理这种情况? 做 { WfiStatus = (IP_MC_ME->PRTN0_CORE2_STAT & MC_ME_PRTN0_CORE2_STAT_WFI_MASK); } while (CLOCK_IP_WFI_EXECUTED != WfiStatus); Re: HSE [Wait for Interrupt(WFI)] status understanding 你好@ManuSharma1 最糟糕的情况是 HSE 固件的安装、更新或恢复,正如 HSE-B 固件参考手册中所述,这可能需要大约 1 秒钟。因此,我建议超时时间设置为大约 1.3 秒,以便留出一些余地,避免在未达到预期 WFI 状态时出现无限等待。 此致, Lukas Re: HSE [Wait for Interrupt(WFI)] status understanding 亲爱的@lukaszadrapa 谢谢你提供的详细信息。 根据建议,我计划使用大约1.3 秒的基于定时器的超时时间,等待 HSE 进入 WFI 状态。如果在此超时时间内未达到 WFI 状态,我打算执行故障保护措施。 故障保护操作方面,我正在考虑执行MCU RESET,因为 HSE 将无法处于处理进一步请求的适当状态。在继续之前,我希望您能就以下几点提供指导: 对于 HSE WFI 超时情况,执行 MCU RESET 是否是正确的处理方法? 如果建议RESET,应该使用哪种RESET方式: 功能 RESET(FES),或 破坏性RESET(DES)? 在 S32K312 架构中,HSE 作为独立的引擎运行,负责网络安全相关的功能。如果发出 MCU RESET 指令,HSE 引擎也会 RESET 吗,还是会继续独立运行? 您的意见将有助于确保超时处理机制得到正确、稳健的实现。 谢谢,此致敬礼! 马努·夏尔马 Re: HSE [Wait for Interrupt(WFI)] status understanding 你好@ManuSharma1 通常,第一步是检查 0x4039_C028 处的 HSE GPR是否设置了位 0。如果RESET后第 0 位为“0”,则 HSE 固件根本不存在,由于某些致命错误而被完全擦除。 如果 HSE GPR 中的第 0 位为“1”(HSE 固件存在),但 RESET 后 HSE_STATUS_INIT_OK 仍为“0”,则表示需要启动握手过程。参见“14.6.7有关详细信息,请参阅 HSE FW RM 中的“HSE 固件握手”。如该部分所述,您应该触发几次功能重置。 不能使用外部复位,因为它会触发信号破坏性复位。另一种方法是通过软件触发功能重置。您可以看看这篇文章: https://community.nxp.com/t5/S32K/S32K344-How-to-manually-trigger-one-Function-Reset/m-p/1506101/highlight/true#M17079 简而言之: RESET 后,检查 0x4039_C028 处的 HSE GPR 寄存器中的第 0 位。如果值为 0,则表示固件已被擦除,您可以尝试重新安装。如果结果是 1,则进行下一步。 等待 FSR 寄存器中的 HSE_STATUS_INIT_OK 位置位。如果已设置,则 HSE 固件已启动并运行。如果在复位后约 1 秒内未设置(使用约 1.3 秒或更长的超时时间),则触发功能复位。 重复此步骤,直到固件恢复或擦除为止。如果固件被擦除,则需要重新安装固件。 另请注意,如果您使用 AB_SWAP 版本,并且由于某些致命错误导致固件被 SBAF 擦除,则重新安装固件的唯一选项是“通过 MU 接口安装”方法。在这种情况下,通过 IVT 进行安装或通过默认位置进行安装的方法均无效。 更多详情请参阅 HSE 固件参考手册中的“10 错误和警告管理”部分。 此致, Lukas
View full article
iMX8 支持的端点数量 iMX8 使用 DWC3 作为 USB 控制器,DWC3 是一款 xHCI 控制器。从 iMX8 的寄存器中读取数据后,我发现它最多可以支持 64 个设备。但是当我连接几个设备时,之前就出现了 xHCI 资源错误。似乎端点数量存在某种限制,而且似乎还取决于传输类型(批量、控制等)。在我使用的这类设备(包括集线器)中,似乎在连接 80 个终端后就会出现问题。请问能否提供一些确切的数字/公式,说明支持多少个端点? Re: Number of supported endpoints on the iMX8 你好, i.MX8 xHCI MaxSlots = 64 值指定了可启用 USB 设备插槽的最大数量,而不是端点总容量。xHCI 每个设备最多支持 31 个端点上下文,但控制器不保证所有 64 个插槽都能同时使用最大数量的端点。可用总量主要取决于周期带宽、设备速度、端点间隔和数据包大小、集线器拓扑结构、事务转换器分配和 DWC3 实现资源。   详细信息请参考xHCI规范。 Re: Number of supported endpoints on the iMX8 我查阅了xHCI规范,但没有找到任何相关说明。xHCI 唯一明确规定控制器可以返回资源错误(就是我上面提到的那个错误)的地方是…… 例如。英特尔表示,他们的一款 xHCI 控制器支持多达 2048 个批量/控制 EP 或多达 128 个中断/同步 EP。 https://edc.intel.com/content/www/us/en/design/ipla/software-development-platforms/servers/platforms... 我们有一个测试装置(仅限 USB 2.0),它在 Intel 芯片上运行良好(数百个 EP),但在 iMX8MP 上的部分设备(前面提到的 80 个 EP)上失败。 但是,要了解我们可以支持多少种以及哪些类型的设备,我们需要知道 iMX8MP/DWC3 的限制是什么。如果您能像英特尔那样,为我们提供一些公式或限制条件,那将非常有帮助。
View full article