Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
s32k2018.R1 は延期できません。 このアクティベーションコードの有効期限を次回の期間まで延長していただけますでしょうか?よろしくお願いいたします。 アクティベーションコード D870-0066-E5E6-ACC7 Re: s32k2018.R1没办法延期 こんにちは、 お客様のS322DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
過熱 hi S32K32には内蔵温度センサが付いていて、自己チップの温度を監視できるのか知りたいです。 S32K32には内部温度センサが搭載されていて、ソフトウェアの設定や処理方法ができると仮定します。 戦車。 Re: overtemperature こんにちは@qiaoqin_wang はい。 例S32K344温度センサーS32DS36 RTD600/500/400_p24を参照してください。 よろしくお願いいたします ロビン
View full article
The S32K344 cannot connect to the debugger. I'm debugging an AUTOSAR project on an S32K344 chip development board. After successfully flashing the program to the board once, my debugger (J-Link ARM V9) can no longer connect to the board. My integrated development environment (IDE) is IAR 9.5. This is my first time using the S32K344 to run an AUTSAR project, so I encountered some problems during integration. I tried to fix the issues using AI, and initially I was able to connect to the chip and debug the program using J-link, but it kept getting stuck in the memory-related initialization phase. Later, after another modification and burning, it could no longer connect to the chip. This might be caused by modifications to the memory layout settings in the linked file. (This is just my guess.) I tested the signal of the Reset pin using a logic analyzer and found that the Reset pin was pulled low with a period of 3.8ms and a duration of 80us. I tried using Jlink.exe to connect via command and then erase the entire chip, but the connection failed (although it could recognize the S32K344 chip); I also tried connecting "in reset state", but that also failed. I also tried using Jflash to connect and then erase the entire area, but it also failed to connect. I don't know how to erase or reconnect the chip, and I would appreciate guidance. Thanks. S32K344-WB #J-Link #IAR #S32K3xx 回复: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) You can try connecting and erasing using the following methods. I've encountered similar issues on other platforms. Shortly after powering on, the firmware immediately configures SWDIO/SWCLK/RESET to GPIO push-pull output low, causing J-Link to fail to connect. For your reference: For the situation you encountered where the chip cannot connect due to periodic resets and possible reuse of the debug port, I recommend trying a combination of "hardware forced reset + low-level command line forced wipe" to recover the bricked chip. In terms of specific operation, it is recommended that you abandon simply pressing buttons or relying on the IDE graphical interface, and instead use tweezers or DuPont wires to physically short the chip's RESET pin to GND (keeping it continuously pulled low) . This can completely block the periodic reset cycle of the chip's internal watchdog, preventing the kernel from executing your firmware code at all, creating an absolutely safe handshake window for the debugger. With this pin shorted to ground, power on the board, open the J-Link Commander command-line tool, reduce the SWD rate to 100kHz, and manually enter the connection command. Once the kernel is successfully recognized and successfully halved, immediately enter `unlock Kinetis` in the command line or directly execute the `erase` command to erase the entire chip, thereby completely removing this problematic firmware. Re: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) Hi@ 813270556 You can try the reply method above. What version of RTD are you using? Did you overlook crucial configuration details related to the SWD port during the setup process? Older versions might default to configuring the SWD port. Configure it as a port pin.
View full article
i.MX8M Mini H.264 意図しないクロップ 正直に言うと、(明らかに)これはAIツールが書いたものです。しかし、この問題は確かに存在するようで、記事の内容もその問題点を的確に説明していると思います。 vpuenc_h264 は i.MX8M Mini の SPS に偽の左側切り抜き (14 px) を書き込んでいるようです。 まとめ NXPリリースimx-6.18.37-2.1.0を実行しているi.MX8M Miniにおいて(Yocto wrynose)は、1920x1080入力を正しくエンコードしますがvpuenc_h264、書き込みはします frame_crop_left_offset = SPSに7。そのため、プレイヤーは 1920x1080ではなく、1906x1080。同じハードウェアでL4.14.98 BSPを使った (Yocto相撲)は左刈りなしのSPSヘッダーを生産しました。 環境 SoC i.MX8M Mini(Hantro H1エンコーダー) NXPリリース imx-6.18.37-2.1.0(IMX-Linux-Wrynoseマニフェスト) カーネル linux-imx 6.18.37 IMX-GST1.0-プラグイン4.11.1、ブランチ MM_04.11.01_2608_L6.18.37 imx-vpuwrap 4.11.1、ブランチ MM_04.11.01_2608_L6.18.37 imx-vpu-hantro 1.40 GStreamer 1.28.1 作業参照 L4.14.98 BSP、imx-gst1.0-plugin4.4.5 (MM_04.04.05_1902_L4.14.98_GA)、同じボード 再生 カメラは一切使用していません。 gst-launch-1.0-e videotestsrc num-buffers=10 \ !video/x-raw,format=NV12,width=1920,height=1080,framerate=60/1 \ !vpuenc_h264 !video/x-h264,stream-format=byte-stream \ !filesink location=/tmp/raw.h264 SPSを検査する(FFmpegがインストールされているホスト上で): ffmpeg -i raw.h264 -c copy -bsf:v trace_headers -frames:v 1 \ -f null - 2>&1 | grep -E "pic_width|pic_height|frame_crop" 観察された pic_width_in_mbs_minus1 = 119 (1920 px) pic_height_in_map_units_minus1 = 67 (1088 px) frame_cropping_flag = 1 frame_crop_left_offset = 7 (14 px) <-- 予期しない値 frame_crop_right_offset = 0 frame_crop_top_offset = 0 frame_crop_bottom_offset = 4 (8 px) (予想値:1088~1080) デコード後のサイズは1906x1080です。録画されたクリップで、作物畑を取り除く SPSからの完全な1920x1088画像は連続画像で表示されます 左端の内容を横切るため、画像データは幅と 間違っているのはヘッダーのクロップだけです。 期待される frame_crop_left_offset = 0 となり、1920x1080 (8 の下半分のみ、 パディングを削除して1088にする。作物オフセットは通常左側でゼロです そして、幅がすでに16の倍数になっているとき。 除外したもの - 入力データ: GST_DEBUG=vpuenc:6 は、プラグインが VPU を渡していることを示しています。 1920x1080フレーム("VPU enc 幅: 1920、高さ: 1080、fps: 60")および 出力上限は幅1920、高さ1080です。 - カメラおよびキャプチャドライバー:videotestsrcで再現します 出典(NV12)。同じクロップは実際のカメラでも表示されます。 キャプチャ形式がUYVYかYUY2か、ピクセル形式は マターではありません。 - h264parse / mp4mux: 要素を含まない生のエンコーダー出力 既に収穫済みで、計画段階にある。 - ビットレートと GOP: デフォルト設定と ビットレート=14000、GOPサイズ=30。 ソースレビュー imx-gst1.0-plugin の plugins/vpu/gstvpuenc.c を比較しました4.4.5 および 4.11.1.Hantro パスの違い: 4.11.1 バッファ プールは 平面ごとのストライドアライメントなしの16ピクセル水平アライメント、 そして、nOrigWidth/nOrigHeight をラッパーに渡します。imx-vpuwrapでは 4.11.1、VPU_EncSetPreProcessorDefaults は、左 0 の切り抜きから始まります。 top 0、および VPU_EncSetCommonConfig は origWidth = (Width + 15) & ~15 を設定します。 プラグインやラッパーで、 の左オフセットを設定するものは見つかりませんでした 14のため、H1エンコーダライブラリかカーネルVPUドライバが原因と推測されています。 これはHantro H1 H.264エンコーダーのLF6.18.xにおける既知の問題ですか? それを回避するための解決策や設定はありますか?現在、私たちは以下の方法で対処しています エンコード後にSPSを書き換える。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8M Mini H.264 Unintended Crop こんにちは@dave00dave  この問題は再現可能であることを確認しました。これが既知の問題かどうか、社内チームに確認する必要があります。 よろしくお願いします、 志明
View full article
S32K344はデバッガに接続できません。 S32K344チップ開発ボード上でAUTOSARプロジェクトのデバッグを行っています。プログラムをボードに一度正常に書き込んだ後、デバッガ(J-Link ARM V9)がボードに接続できなくなりました。使用している統合開発環境(IDE)はIAR 9.5です。 S32K344を使ってAUTSARプロジェクトを実行するのは今回が初めてだったので、統合中にいくつか問題が発生しました。AIを使って問題を解決しようと試み、最初はJ-linkを使ってチップに接続し、プログラムをデバッグすることができましたが、メモリ関連の初期化フェーズで処理が停止してしまいました。 その後、さらなる改造と書き込みを行った結果、チップに接続できなくなってしまった。 これは、リンクされたファイルのメモリレイアウト設定の変更が原因である可能性があります。(これはあくまで私の推測です。) ロジックアナライザを使用してリセットピンの信号をテストしたところ、リセットピンは3.8msの周期と80μsの持続時間でローレベルにプルダウンされていることが分かりました。 Jlink.exeを使ってコマンド経由で接続し、チップ全体を消去しようとしましたが、接続に失敗しました(S32K344チップは認識できたのですが)。また、「リセット状態」で接続しようとしましたが、それも失敗しました。 Jflashを使って接続してから領域全体を消去しようとも試みましたが、接続に失敗しました。 チップの消去方法や再接続方法がわからないので、ご教示いただけると幸いです。 ありがとう。 S32K344-WB #J-Link #IAR #S32K3xx 回复: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) 以下の方法で接続と消去を試してみてください。他のプラットフォームでも同様の問題が発生したことがあります。電源投入直後、ファームウェアがSWDIO/SWCLK/RESETをGPIOプッシュプル出力ローに設定してしまうため、J-Linkが接続に失敗します。参考までに: 定期的なリセットやデバッグポートの再利用が原因でチップが接続できなくなるという状況が発生した場合、故障したチップを復旧するために「ハードウェア強制リセット+低レベルコマンドライン強制ワイプ」の組み合わせを試してみることをお勧めします。 具体的な操作方法としては、単にボタンを押したり、IDEのグラフィカルインターフェースに頼ったりするのではなく、ピンセットやデュポンワイヤを使ってチップのRESETピンをGNDに物理的に短絡させる(常にローレベルにプルダウンする)ことをお勧めします。これにより、チップ内部のウォッチドッグの周期的なリセットサイクルを完全にブロックし、カーネルがファームウェアコードを実行するのを防ぎ、デバッガにとって完全に安全なハンドシェイクウィンドウを作成できます。このピンをグランドに短絡させた状態で、ボードの電源をオンにし、J-Link Commanderコマンドラインツールを開き、SWDレートを100kHzに下げて、接続コマンドを手動で入力します。カーネルが正常に認識され、正常にハーフされたら、すぐにコマンドラインで`unlock Kinetis`と入力するか、`erase`コマンドを直接実行してチップ全体を消去し、問題のあるファームウェアを完全に削除します。 Re: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) こんにちは@ 813270556 上記の返信方法を試してみてください。 お使いのRTDのバージョンは何ですか?セットアッププロセス中に、SWDポートに関する重要な設定を見落としていませんか?古いバージョンでは、SWDポートの設定がデフォルトで行われる場合があります。 ポートピンとして設定してください。
View full article
i.MX8M Mini H.264 Unintended Crop Full disclose: (clearly) an AI tool wrote this. The issue appears to be a real one, though, and I think the writeup describes the issues well. vpuenc_h264 appears to write a bogus left crop (14 px) into the SPS on i.MX8M Mini SUMMARY On an i.MX8M Mini running NXP release imx-6.18.37-2.1.0 (Yocto wrynose), vpuenc_h264 encodes 1920x1080 input correctly but writes frame_crop_left_offset = 7 into the SPS. Players therefore show 1906x1080 instead of 1920x1080. The same hardware with the L4.14.98 BSP (Yocto sumo) produced SPS headers with no left crop. ENVIRONMENT SoC i.MX8M Mini (Hantro H1 encoder) NXP release imx-6.18.37-2.1.0 (imx-linux-wrynose manifest) Kernel linux-imx 6.18.37 imx-gst1.0-plugin 4.11.1, branch MM_04.11.01_2608_L6.18.37 imx-vpuwrap 4.11.1, branch MM_04.11.01_2608_L6.18.37 imx-vpu-hantro 1.40 GStreamer 1.28.1 Working reference L4.14.98 BSP, imx-gst1.0-plugin 4.4.5 (MM_04.04.05_1902_L4.14.98_GA), same board REPRODUCTION No camera is involved: gst-launch-1.0 -e videotestsrc num-buffers=10 \ ! video/x-raw,format=NV12,width=1920,height=1080,framerate=60/1 \ ! vpuenc_h264 ! video/x-h264,stream-format=byte-stream \ ! filesink location=/tmp/raw.h264 Inspect the SPS (on a host with FFmpeg): ffmpeg -i raw.h264 -c copy -bsf:v trace_headers -frames:v 1 \ -f null - 2>&1 | grep -E "pic_width|pic_height|frame_crop" OBSERVED pic_width_in_mbs_minus1 = 119 (1920 px) pic_height_in_map_units_minus1 = 67 (1088 px) frame_cropping_flag = 1 frame_crop_left_offset = 7 (14 px) <-- unexpected frame_crop_right_offset = 0 frame_crop_top_offset = 0 frame_crop_bottom_offset = 4 (8 px) (expected: 1088 - 1080) Decoded size is 1906x1080. On a recorded clip, removing the crop fields from the SPS shows a complete 1920x1088 picture with continuous image content across the left edge, so the picture data is full width and only the header's crop is wrong. EXPECTED frame_crop_left_offset = 0, giving 1920x1080 (bottom crop of 8 only, to remove the padding to 1088). Crop offsets are normally zero on the left and right when the width is already a multiple of 16. WHAT WE RULED OUT - Input data: GST_DEBUG=vpuenc:6 shows the plugin passing the VPU a 1920x1080 frame ("VPU enc width: 1920, height: 1080, fps: 60") and its output caps are width=1920,height=1080. - Camera and capture driver: reproduces with videotestsrc as the source (NV12). The same crop also appears with the real camera, whether the capture format is UYVY or YUY2, so the pixel format doesn't matter. - h264parse / mp4mux: the raw encoder output, with neither element in the pipeline, already has the crop. - Bitrate and GOP: present with the default settings and with bitrate=14000 gop-size=30. SOURCE REVIEW We compared plugins/vpu/gstvpuenc.c in imx-gst1.0-plugin 4.4.5 and 4.11.1. Differences in the Hantro path: the 4.11.1 buffer pool uses a 16 pixel horizontal alignment without the per-plane stride alignment, and it passes nOrigWidth/nOrigHeight to the wrapper. In imx-vpuwrap 4.11.1, VPU_EncSetPreProcessorDefaults starts with a crop of left 0, top 0, and VPU_EncSetCommonConfig sets origWidth = (Width + 15) & ~15. We found nothing in the plugin or wrapper that sets a left offset of 14, so we suspect the H1 encoder library or the kernel VPU driver. Is this a known issue in LF6.18.x for the Hantro H1 H.264 encoder, and is there a fix or a setting to avoid it? We currently work around it by rewriting the SPS after encoding. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8M Mini H.264 Unintended Crop Hi @dave00dave  I've confirmed that this issue can be reproduced. I need to check with our internal team to see if this is a known issue. Best Regards, Zhiming
View full article
S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) 我正在基于 S32K344 芯片开发板调试 Autosar 项目。当我成功向开发板烧录进去一次程序之后,我的调试器(J-Link ARM V9)再也无法连接到开发板。我使用的集成开发工具是 IAR 9.5。 我是第一次使用 S32K344 运行 Autosar 项目,所以在集成时遇到了一些问题。我尝试通过 AI 去修改问题,刚开始可以连接到芯片并通过 J-link 去调试程序,但一直卡死在内存相关的初始化阶段。 后来,再一次修改之后烧录完就再也无法连接到芯片了。 可能是修改了链接文件中内存分布相关的内容引起的。(这只是我的猜测) 我通过逻辑分析仪测试了 Reset 引脚的信号:发现 Reset 引脚在以 3.8ms 的周期在拉低,拉低持续时间 80us。 我尝试使用 Jlink.exe 通过命令去连接然后整片擦除,提示连接失败。(但它可以识别到 S32K344芯片);尝试通过 “在复位状态下” 去连接,也连接失败了。 我也尝试使用  Jflash 去连接然后整片擦除,也提示连接失败。 我不知道应该如何操作才能擦除芯片或者连接上芯片,希望得到指导。 谢谢。 S32K344-WB   #J-Link  #IAR  #S32K3xx 回复: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) 可以试一下如下方式尝试连接和擦除,我在其他平台上遇到过类似问题,产品上电短时间内固件立即将 SWDIO/SWCLK/RESET 配置为 GPIO 推挽输出低,导致 J-Link 无法连接,供参考: 针对你遇到的这种芯片因周期性复位且可能复用调试口导致无法连接的情况,我推荐尝试“硬件强制拉死复位 + 底层命令行强擦”的组合方案来救砖。 具体操作上,建议你放弃单纯按键或依赖IDE图形界面的操作,改为用镊子或杜邦线直接将芯片的 RESET 引脚物理短接到 GND(保持持续拉低)。这样可以彻底阻断芯片内部看门狗的周期性复位循环,让内核完全不执行你的固件代码,为调试器创造一个绝对安全的握手窗口。在保持该引脚短接地的状态下,给板子上电,打开 J-Link Commander 命令行工具,将 SWD 速率降至 100kHz,手动输入连接命令。一旦成功识别到内核并成功 Halt,立刻在命令行输入 unlock Kinetis 或直接执行 erase 指令进行整片擦除,从而彻底清除这版有问题的固件。 Re: S32K344 无法连接到调试器(The S32K344 cannot connect to the debugger) Hi@813270556 你可以尝试一下上面回复的方法。 你所使用的RTD版本是多少,是不是配置的时候没考虑到配置SWD口相关的关键,旧版本会将SWD口默认 配置为port管脚。
View full article
i.MX8M Mini H.264 意外裁剪 坦白说:(很明显)这是人工智能工具编写的。这个问题似乎确实存在,而且我认为这篇文章对这些问题描述得很好。 vpuenc_h264 似乎在 i.MX8M Mini 的 SPS 中写入了一个错误的左侧裁剪区域(14 像素)。 概括 在运行 NXP 版本 imx-6.18.37-2.1.0 的 i.MX8M Mini 上(Yocto wrynose),vpuenc_h264 可以正确编码 1920x1080 输入,但写入 frame_crop_left_offset = 7 进入 SPS。因此,球员们表现出 分辨率为 1906x1080 而不是 1920x1080。使用相同的硬件和 L4.14.98 电路板支持包。 (Yocto sumo)生产出没有左侧作物的SPS收割台。 环境 SoC i.MX8M Mini(Hantro H1编码器) NXP 版本 imx-6.18.37-2.1.0(imx-linux-wrynose 清单) 内核 linux-imx 6.18.37 imx-gst1.0 插件4.11.1,分支 MM_04.11.01_2608_L6.18.37 imx-vpuwrap 4.11.1,分支 MM_04.11.01_2608_L6.18.37 imx-vpu-hantro 1.40 GStreamer 1.28.1 工作参考 L4.14.98 BSP,imx-gst1.0-plugin4.4.5 (MM_04.04.05_1902_L4.14.98_GA),同一块板 生殖 过程中没有使用摄像头: gst-launch-1.0-e videotestsrc num-buffers=10 \ !video/x-raw,format=NV12,width=1920,height=1080,framerate=60/1 \ !vpuenc_h264!video/x-h264,stream-format=byte-stream \ !文件接收器位置=/tmp/raw.h264 检查 SPS(在安装了 FFmpeg 的主机上): ffmpeg -i raw.h264 -c copy -bsf:v trace_headers -frames:v 1 \ -f null - 2>&1 | grep -E "pic_width|pic_height|frame_crop" 观察到 pic_width_in_mbs_minus1 = 119 (1920 像素) pic_height_in_map_units_minus1 = 67 (1088 像素) frame_cropping_flag = 1 frame_crop_left_offset = 7 (14 px) <-- 意外情况 frame_crop_right_offset = 0 frame_crop_top_offset = 0 frame_crop_bottom_offset = 4 (8 像素) (预期值:1088 - 1080) 解码后的尺寸为 1906x1080。一段录像显示,农田被移除。 SPS 显示的是一张完整的 1920x1088 像素的连续图像。 左侧边缘的内容,因此图片数据占据了整个宽度,并且 只有标题的裁剪有问题。 预期的 frame_crop_left_offset = 0,得到 1920x1080(仅裁剪底部 8 个部分)。 移除填充至 1088)。左侧的裁剪偏移量通常为零。 恰好在宽度已经是 16 的倍数的时候。 我们排除了哪些选项 - 输入数据:GST_DEBUG=vpuenc:6 显示插件正在传递 VPU a 1920x1080帧(“VPU编码宽度:1920,高度:1080,帧率:60”) 它的输出尺寸为宽度=1920,高度=1080。 - 摄像头和捕获驱动程序:使用 videotestsrc 作为测试源时会重现此问题 来源(NV12)。同样的裁剪方式在实际相机拍摄中也会出现。 无论捕获格式是 UYVY 还是 YUY2,也就是像素格式 没关系。 - h264parse / mp4mux:原始编码器输出,不包含任何元素 正在筹备中,作物已经成熟。 - 比特率和 GOP:默认设置下存在,并且 比特率=14000 gop-size=30。 资料审查 我们比较了 imx-gst1.0-plugin 中的 plugins/vpu/gstvpuenc.c 文件。4.4.5 和 4.11.1.Hantro 路径的差异:4.11.1 缓冲池使用 16像素水平对齐,不进行逐平面步长对齐, 并将 nOrigWidth/nOrigHeight 传递给包装器。在 imx-vpuwrap 中 4.11.1,VPU_EncSetPreProcessorDefaults 以左侧 0 的裁剪开始, top 0,并且 VPU_EncSetCommonConfig 设置 origWidth = (Width + 15) & ~15。 我们在插件或封装器中没有找到任何设置左偏移量的地方。 14,因此我们怀疑是 H1 编码器库或内核 VPU 驱动程序的问题。 这是LF6.18.x版本中Hantro H1 H.264编码器的已知问题吗? 是否有解决方法或设置可以避免这种情况?我们目前通过以下方式来解决这个问题: 编码后重写SPS。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8M Mini H.264 Unintended Crop 嗨@dave00dave 我已经确认这个问题可以重现。我需要向我们内部团队确认一下这是否是已知问题。 此致, 志明
View full article
ZSDK BLE主机资质参考似乎已过时 nxp-zsdk 版本说明中提到的 BLE 主机资格认证参考的是一个非常古老的资格认证。 例如nxp-zsdk 4.4状态; BLE主机,DN#: Q305748,链路*:主机资质 BLE 控制器, DN#: Q380314,链接*:控制器资质 *:需要 BLE SIG 帐户。 此主机资质要求支持 BLE 5.4。 控制器明确支持 BLE 6.1。 为了支持控制器的所有功能,主机需要相同或更高的 BLE 级别。 所以我认为版本说明中的参考有误,您能提供正确的参考吗? 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀, 感谢你的回复。我还有一个关于蓝牙主机认证的后续问题。 版本说明链接至https://qualification.bluetooth.com/ListingDetails/227830 ,这表明: Bluetooth Host Solution Zephyr,2024-09-16 ( www.nxp.com ) 核心规格:主机 5.4,活动 这是两年前针对 BLE 5.4 的主机认证,而控制器则针对 BLE 6.1 进行了认证。如果我们按照这些标准来评判我们的产品,我们就不能声称其性能高于 BLE 5.4。 您提到了 BLE 6.3 的新主机认证,但版本说明中没有引用它。这就引出了两个问题: 我们的控制器符合 6.1 版本标准,主机符合 6.3 版本标准,那么我们的产品可以声明为哪个 BLE 版本? 版本说明能否引用 Zephyr 项目/Linux 基金会主机认证信息(例如https://qualification.bluetooth.com/ListingDetails/332380 )?只有当我们能在自己的资质认证中使用它时,提供主办方参考信息才对我们有帮助。 提前谢谢您。 此致, 托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 感谢您的回复。 我查看了您提到的标签 ,NXP Zephyr 项目 v4.4.0将于2026 年 5 月 11 日版本。 我们还有另一个更新的 NXP 低功耗蓝牙 Host Stack Zephyr DN: Q393055,于2026-7-30获取。这意味着,我们在版本说明中没有列出错误的 BLE 主机 QDID: nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub 。 实际上应该是旧的 QDID 号码:DN#: Q305748。 但我想要纠正你的理解,主机和控制器不需要具有相同的蓝牙核心规范版本。主机和控制器被认定为独立的蓝牙子系统,符合 Core 5.4 标准的主机可以与符合 Core 6.1 标准的控制器一起使用。 如果您对此帖还有其他疑问,请告诉我。 否则,请随时将我的回答标记为此问题的解决方案,谢谢! BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 请问您使用的是哪款BLE产品? 我查看了您提供的链接,上面是RW610和RW612,所以我想和您确认一下您使用的是RW610还是RW612? 这样我就可以帮你查一下了。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 它的NXP RW612。 谢谢托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀, 我们与 NXP RW612 一起使用的 BLE 主机是 Zephyr 项目中的主机,以源代码形式提供。这不是恩智浦半导体(NXP)的软件。 Zephyr 大约每 6 个月发布一个新版本,而 BLE 主机通常每个版本都会发生变化。如果我们只能使用 NXP 认证的 BLE 主机,那么我们就只能使用一个 Zephyr 版本。发行说明中提到的版本现在已经超过两年了(可能是 Zephyr 3.7.0)。从那时到目前的 4.5.0 版本,每个版本都包含了许多网络安全和功能性错误修复。自 3.7.0 版本以来,Zephyr 项目已发布了 61 份蓝牙网络安全公告,其中 43 份针对 BLE。 如果我们只依赖 NXP 的认证,那么 NXP 需要对每个 Zephyr 版本中的主机进行认证。 能否提供一份概述,说明每个 Zephyr 版本应该使用哪个 QDID?例如,Nordic 发布了一份类似这样的矩阵: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (在 Nordic 的矩阵中,他们的 SDK 版本号与 Zephyr 版本号不同。) 此致, 托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 我查看了此链接中的所有分支: nxp-zsdk/doc/wireless/版本-notes/topics/rw610rw612_release_notes.md,位于 nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub 我们已经在每个版本说明中列出了 QDID。即使 QDID 相同,也意味着它们都基于我们 NXP 的相同认证。 我们只有 2 个基于 Zephyr 的 QDID,一个在 2024 年,另一个在 2026 年。 继 2026 年发布这个新的 QDID 之后,我们的 GitHub 上将不再发布任何其他新版本: nxp-zsdk/doc/wireless/版本-notes/topics/rw610rw612_release_notes.md 位于 nxp-v4.4-branch· nxp-zephyr/nxp-zsdk · GitHub 所以我认为在未来的 nxp-zephyr 版本中,我们可能会修改版本说明,以提及新的 QDID。 如果您还有其他疑问,请告诉我。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀 NXP 更新了 BLE 4.4.0 的认证信息,这很好。即使版本说明中没有提到这一点。 如果是这样,Zephyr BLE 主机在 Zephyr 3.7 和 4.4.0 之间发生了变化,但 nxp-zsdk 并未对中间的任何版本进行认证。 从 4.5.0 版本开始,你们有什么计划?我们需要每次发布 nxp-zsdk 版本时都包含一个合格的 BLE 主机,无论主机何时发生更改。 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 我们的控制器符合 6.1 版本标准,主机符合 6.3 版本标准,那么我们的产品可以声明为哪个 BLE 版本? ==>[克里斯汀]:是的,你说得对。我认为你们的产品只能用于 6.1 这个较低版本。但需要指出的是,当您申请产品认证时,蓝牙技术联盟还会检查主机和控制器的 ICS 详细信息以及您在申请表中输入的我的类型。 版本说明能否引用 Zephyr 项目/Linux 基金会主机认证信息(例如https://qualification.bluetooth.com/ListingDetails/332380 )?只有当我们能在自己的资质认证中使用它时,提供主办方参考信息才对我们有帮助。 ==>[Christine]:具体可以参考哪个主机 QDID 取决于您使用的 Zephyr 主机协议栈。此链接仅适用于Linux 基金会提供的 Zephyr RTOS LE 主机。如果您指的是 NXP 的低功耗蓝牙主机协议栈 Zephyr,那么我不建议您参考此链接,而是参考我们 NXP 的 QDID。 BR, Christine。 Re: ZSDK BLE host qualification references seems obsolete 嗨,克里斯汀 NXP 针对 4.4.0 版本更新了 BLE 认证,这很好,但是发行说明中没有提到这一点。 Zephyr BLE主机在Zephyr 3.7和4.4.0之间发生了变化,但在 nxp-zsdk 中,他没有资格参与中间的任何版本发布。 从 4.5.0 版本开始,你们有什么计划?我们需要每次发布 nxp-zsdk 版本时都包含一个合格的 BLE 主机,无论主机何时发生更改。 此致,托尼 Re: ZSDK BLE host qualification references seems obsolete 嗨, @tobg 感谢您的回复。 是的,我们当然有针对未来 Zephyr SDK 的规划。但具体的日程安排,请允许我花些时间向我们的内部团队核实。 一旦得到确认信息,我会通知你。 BR, Christine。
View full article
ZSDK BLE host qualification references seems obsolete The BLE host qualification references in nxp-zsdk release notes refers to a very old qualification. E.g. nxp-zsdk  4.4 states; BLE Host, DN#: Q305748, Link *: Host qualification BLE Controller, DN#: Q380314, Link *: Controller qualification *: Requires BLE SIG account. This host qualification specifies BLE 5.4 support. The controller specifies BLE 6.1 support. To support all the features of the controller, the host would need the same BLE level or higher. So I think that the reference in the release notes are wrong, can you provide the correct references? Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Thanks for your reply. I checked the tag you mentioned NXP Zephyr project v4.4.0  is release on May 11 2026. And we have another newer NXP Bluetooth Low Energy Host Stack Zephyr DN: Q393055 is gotten on 2026-7-30. It means, we did not list the wrong BLE host QDID in the release note:nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub. It actually should be the old QDID number: DN#: Q305748. But I want to correct your understandings, Host and Controller does not need to have matched Bluetooth Core Spec version. The Host and Controller are qualified as separate Bluetooth subsystems, and a Host qualified against Core 5.4 can be used with a Controller qualified against Core 6.1. Please let me know whether still have any other concerns on this thread. Otherwise, please do not hesitate to mark my answer as a solution for this case, Thanks! BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine, Thank you for your reply. I have a follow-up question about the Bluetooth host qualification. The release note links to https://qualification.bluetooth.com/ListingDetails/227830, which shows: Bluetooth Host Solution Zephyr, 2024-09-16 (www.nxp.com) Core Specification: Host 5.4, Active This is a two-year-old host qualification at BLE 5.4, while the controller is qualified for BLE 6.1. If we qualify our product against these listings, we can’t claim anything higher than BLE 5.4. You mentioned a newer host qualification for BLE 6.3, but the release note doesn’t reference it. That raises two questions: With a controller qualified for 6.1 and a host qualified for 6.3, which BLE version can we claim for our product? Could the release notes refer to the Zephyr Project / Linux Foundation host qualification instead (for example https://qualification.bluetooth.com/ListingDetails/332380)? Including a host reference only helps us if we can use it in our own qualification. Thank you in advance. Best regards, Tonny Re: ZSDK BLE host qualification references seems obsolete Its NXP RW612. Thanks Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Can you please let me know which BLE product are you using? I checked in the link you provided, it is RW610 and RW612, so I prefer to confirm with you that you are using RW610 or RW612? So that I can check for you. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine, The BLE host we use with the NXP RW612 is the one in the Zephyr project, delivered as source code. It is not NXP software. Zephyr has a new release every 6 months or so, and the BLE host usually changes with each release. If we may only use BLE hosts that NXP has qualified, we are tied to one Zephyr version. The release notes refer to a version that is now more than two years old (probably Zephyr 3.7.0). Every release since then, up to the current 4.5.0, has included many security and functional bug fixes. Since 3.7.0, the Zephyr project has published 61 Bluetooth security advisories, 43 of them for BLE. If we are to rely only on NXP’s qualification, NXP would need to qualify the host for each Zephyr release. Could you send us an overview of which QDID to use for each Zephyr release? Nordic publishes a matrix like this, for example: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (In Nordic’s matrix, their SDK version numbers are different from the Zephyr version numbers.) Best regards, Tonny Re: ZSDK BLE host qualification references seems obsolete Hi Christine It is nice that NXP has an updated BLE qualification for 4.4.0, even though the release notes don’t mention it. If so, the Zephyr BLE host changed between Zephyr 3.7 and 4.4.0 but wasn’t qualified in nxp-zsdk for any of the releases in between. What are your plans from 4.5.0 onward? We need each nxp-zsdk release to include a qualified BLE host whenever the host has changed. Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  I checked all of the branches in this link, nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub we already listed the QDID in each Release note. Even it is the same QDID, it means all of them are based on our NXP's same certification. We only have 2 Zephyr based QDID, one is in 2024, another is in 2026. And after this new QDID in 2026, there is still no other new release on our github: nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk · GitHub So I think in the future nxp-zephyr release, we might modify the release note to refer to the new QDID. If you have any other concerns, please let me know. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  With a controller qualified for 6.1 and a host qualified for 6.3, which BLE version can we claim for our product? ==>[Christine]:Yes, you are right. I think your product can only be claimed  for 6.1 as the lower version. But need to point out that when you apply for the certification for your product, the Bluetooth Sig will also check the details of host and Controller's ICS and what kind of profiles you input in the application form. Could the release notes refer to the Zephyr Project / Linux Foundation host qualification instead (for example https://qualification.bluetooth.com/ListingDetails/332380)? Including a host reference only helps us if we can use it in our own qualification. ==>[Christine]:Which host QDID can be referred to depends on which Zephyr Host Stack you are using.  This link is only applicable to Zephyr RTOS LE host from the Linux Foundation. If you are referring to NXP Bluetooth Low Energy Host Stack Zephyr, then I do not recommend you to refer this link, but our NXP's QDID. BR, Christine. Re: ZSDK BLE host qualification references seems obsolete Hi Christine Its fine that NXP has an updated BLE qualification for 4.4.0, but the release note don’t mention it. The Zephyr BLE host changed between Zephyr 3.7 and 4.4.0, but wasn’t qualified in nxp-zsdk for any of the releases in between. What are your plans from 4.5.0 onward? We need each nxp-zsdk release to include a qualified BLE host whenever the host has changed. Regards Tonny Re: ZSDK BLE host qualification references seems obsolete Hi, @tobg  Thanks for your reply. Yes, for sure, we have plan for the future Zephyr SDK.  But for the detailed schedule, please allow me some time to check with our internal team. Once have confirmed info, I will let you know. BR, Christine.
View full article
ZSDK BLEホスト認定に関するリファレンスは古くなっているようです nxp-zsdkのリリースノートに記載されているBLEホストの認定情報は、非常に古い認定情報に基づいています。 例:nxp-zsdk 4.4の状態; BLE ホスト、DN#: Q305748、リンク *: ホスト資格 BLEコントローラ、DN#:Q380314、リンク*:コントローラ資格 *: BLE SIGアカウントが必要です。 このホスト資格はBLE 5.4のサポートを指定しています。 コントローラはBLE 6.1サポートを指定しています。 コントローラのすべての機能をサポートするには、ホストは同じBLEレベルまたはそれ以上のレベルが必要です。 SO、リリースノートの参照が間違っていると思いますが、正しい参考文献を教えてもらえますか? 敬具 トニー Re: ZSDK BLE host qualification references seems obsolete これはNXP RW612です。 ありがとう、トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg どのBLE製品を使っているのか教えてもらえますか? ご提供いただいたリンクを確認しましたが、RW610とRW612のどちらかです。なので、RW610を使っているのか、それともRW612なのか確認したいです。 SO、CAN調べられるように。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg ご返信ありがとうございます。 あなたが言及したタグを確認しました。NXP Zephyrプロジェクトv4.4.0は 2026年5月11日にリリースされます。 そして、もう一つ新しいNXP Bluetooth Low EnergyホストスタックのZephyr DNが登場します。Q393055は 2026年7月30日に入手可能です。つまり、リリースノートで間違ったBLEホストQDIDを記載していないということです:nxp-zsdk/doc/wireless/release-notes/topics/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk ·GitHub。 実際には、古い QDID 番号であるべきです: DN#: Q305748。 しかし、誤解を訂正したいのですが、ホストとコントローラは必ずしもBluetooth Core Specのバージョンが一致する必要はありません。ホストとコントローラは別々のBluetoothサブシステムとして認定されており、Core 5.4に適合したホストとCore 6.1に適合したコントローラを使用可能です。 このThreadで他に何か懸念があれば教えてください。 それ以外の場合は、このCASEの解決策として私の回答をマークしてください。ありがとうございます! BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティンさん。 お返事ありがとうございます。Bluetoothホストの認証について、追加の質問があります。 リリースノートはhttps://qualification.bluetooth.com/ListingDetails/227830にリンクしています。これは以下を示しています。 Bluetooth ホストソリューション Zephyr、2024-09-16(www.nxp.com) コア仕様:ホスト5.4、アクティブ これはBLE 5.4の2年前のホスト資格であり、コントローラはBLE 6.1の資格を持っています。これらのリスティングに対して製品を基準にすると、BLE 5.4を超えるものは請求できません。 BLE 6.3の新しいホスト認定について言及されていましたが、リリースノートにはそれに関する記述がありません。これによって2つの疑問が生じる。 コントローラが6.1に対応し、ホストが6.3に対応している場合、私たちの製品でどのBLEバージョンを主張できますか? リリースノートは代わりにZephyr Project / Linux Foundationのホスト資格(例えば https://qualification.bluetooth.com/ListingDetails/332380)を指すことはあり得ますか?ホストの推薦を含めるのは、自分の資格審査で使える場合に限ります。 事前に感謝いたします。 よろしくお願いします、 トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg コントローラが6.1に対応し、ホストが6.3に対応している場合、私たちの製品でどのBLEバージョンを主張できますか? ==>[クリスティン]:はい、おっしゃる通りです。あなたの製品は6.1の下位バージョンしか主張できないと思います。ただし、製品の認証を申請する際には、Bluetooth SigがホストやコントローラのICSの詳細やアプリケーションフォームに入力したプロファイルもチェックします。 リリースノートは代わりにZephyr Project / Linux Foundationのホスト資格(例えば https://qualification.bluetooth.com/ListingDetails/332380)を指すことはあり得ますか?ホストの推薦を含めるのは、自分の資格審査で使える場合に限ります。 ==>[Christine]:どのホストQDIDを参照できるかは、使用するZephyrホストスタックによって異なります。このリンクはLinux FoundationのZephyr RTOS LEホストにのみ適用可能です。もしあなたが言及しているのであれば、このリンクBluetooth Low Energy Host Stack Zephyrを指すのではなく、私たちのNXPのQDIDを参照することをお勧めします。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg このリンクのすべてのブランチを確認しました。nxp-zsdk/doc/wireless/release-notes/トピック/rw610rw612_release_notes.md at nxp-v4.4-branch · nxp-zephyr/nxp-zsdk ·GitHub QDIDは既に各リリースノートに記載済みです。同じQDIDであっても、それは全てNXPの同じ認証に基づいていることを意味します。 ZephyrベースのQDIDは2つしかなく、1つは2024年、もう1つは2026年です。 そして、2026年のこの新しいQDID以降、私たちのGitHubには新たなリリースはありません。 NXP-ZSDK/DOC/Wireless/release-Notes/トピック/rw610rw612_release_notes.MD at NXP-V4.4-branch·nxp-zephyr/nxp-zsdk ·GitHub SO、FUTUREのnxp-Zephyrリリースでは、リリースノートを新しいQDIDに付けて修正するかもしれません。 他に何かご心配な点がありましたら、お知らせください。 BR、 Christine。 Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティン NXPが4.4.0向けのBLE認証を更新したことは素晴らしい。リリースノートには記載されていないが。 もしそうなら、Zephyr BLEホストはZephyr 3.7と4.4.0の間で 変更 されましたが、nxp-zsdkのリリースには適用されていませんでした。 バージョン4.5.0以降の計画について教えてください。ホストが変更された場合は、各nxp-zsdkリリースに必ず認定済みのBLEホストを含める必要があります。 トニーより Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティンさん。 NXP RW612で使っているBLEホストはZephyrプロジェクトに搭載されているもので、ソースコードとして提供されています。NXPのソフトウェアではありません。 Zephyrはだいたい6ヶ月ごとに新作がリリースされ、BLEホストはリリースごとに通常変わります。NXPが認定したBLEホストのみを使える場合、Zephyrのバージョンは1つに縛られます。リリースノートには、現在2年以上前のバージョン(おそらくZephyr 3.7.0)について言及されています。それ以降のすべてのリリース、現在の4.5.0まで、多くのセキュリティおよび機能上のバグ修正が含まれています。3.7.0以降、Zephyrプロジェクトは61件のBluetoothセキュリティアドバイザリーを発表しており、そのうち43件はBLE向けです。 もしNXPの資格だけに頼るなら、NXPはZephyrの各リリースごとにホストを資格付けする必要があります。 各ZephyrリリースでどのQDIDを使うべきかの概要を教えていただけますか?Nordicは次のようなマトリックスを公開しています。例えば: https://docs.nordicsemi.com/r/bundle/comp_matrix_nrf52840/page/comp/nrf52840/nrf52840_ble_qdid_qual_matrix.html?section=nrf52840_ble_qdid_qual_matrix__sd-fn (Nordicのマトリックスでは、彼らのSDKsバージョン番号はZephyrのバージョン番号とは異なります。) よろしくお願いします、 トニー Re: ZSDK BLE host qualification references seems obsolete こんにちは、クリスティン NXPが4.4.0向けのBLE認証を更新したことは良いのですが、リリースノートにはそのことが記載されていません。 Zephyr BLEホストはZephyr 3.7と4.4.0の間で 変更 されました。しかし、その間のどのリリースにおいても、nxp-zsdk の認定は受けていませんでした。 バージョン4.5.0以降の計画について教えてください。ホストが変更された場合は、各nxp-zsdkリリースに必ず認定済みのBLEホストを含める必要があります。 トニーより Re: ZSDK BLE host qualification references seems obsolete こんにちは、 @tobg ご返信ありがとうございます。 はい、間違いなく、FUTUREのZephyr SDKの計画があります。詳細なスケジュールについては、社内チームに確認するため、少々お時間をいただきます。 情報が確認でき次第、お知らせします。 BR、 Christine。
View full article
TRIGMUX+eMIOSを用いたBLDCモータの方向測定 説明:私はNXPが推奨する6ステップ整流方式を使用してBLDCモーターを駆動しています。 アプリノート「 https://community.nxp.com/t5/S32M-Knowledge-Base/S32M276-Hall-sensor-based-6-step-BLDC-motor-control/ta-p/2035021#jump_PwmAndTriggers 」によると ホールセンサーの出力はTRIGMUXに送られ、その後LCUに送られ、整流や速度信号の計算にも使われます。この記事では運動方向の測定方法については触れていません。 NXP社製のモーター回転方向測定ソリューションはありますか?私の理解では、方向を測るには入力キャプチャユニットを使って3つのホールセンサー出力すべてをキャプチャする必要があるようです。 eMIOSチャネルを以下のように設定することは可能でしょうか? CH0 - TRIGMUXを介してLCUから速度信号を受信する入力キャプチャモード。 CH1 - Hall1を受信するための入力キャプチャモード。 CH2 - Hall2を受信するための入力キャプチャモード。 CH3 - Hall3を受信するための入力キャプチャモード。 もう少し詳しく説明してください。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS eMIOS 0 CH0 - 入力キャプチャモードを、TRIGMUXを介してLCUから速度信号(3つのホール入力のXOR値)を受信するように構成します。 XOR信号の変化に応じてeMIOSから割り込みを発生させることは可能ですか?(ここでは、セクターが変化するたびにXOR信号に遷移が生じることを前提としています。)もし可能なら、ホールセンサー入力を受けるGPIOピンを読み取り、ホールパターンやセクターを確認できます。また、各セクター変更間のタイムスタンプを使って速度を測定することもできます。SO、同じISRでも速度と方向を測定できます。 それが実現可能か、あるいは推奨されるかどうか教えてください。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS こんにちは、@ RIJILKP モーターの回転方向は、ホールセンサーからの信号の順序によって決定できます。 しかし、「S32M276 - ホールセンサーベースの6ステップBLDCモーター制御」では、モーターの回転方向がユーザーソフトウェアから入力として提供されます。 現在のセクターは、Hall_A、Hall_B、Hall_Cの3つの信号の状態に基づいて決定できます。 あらかじめ設定された回転方向に基づき、次の整流位置を計算できます。 このリファレンス・デザインでは、セクター番号が変化する順序に基づいてモーターの回転方向を決定できます。 ご質問に戻ります。 回転方向を特定することだけが目的であれば、 GPIOを使って3つのホール信号の状態を単純に読み取ることができます。連続した2つの読み取り間でこれらの信号の変化を分析することで、現在の回転方向を特定できます。 ご質問について: 「eMIOSチャネルを以下のように設定することは可能でしょうか。 CH0 - TRIGMUXを介してLCUから速度信号を受信する入力キャプチャモード。 CH1 - Hall1を受信するための入力キャプチャモード。 CH2 - Hall2を受信するための入力キャプチャモード。 CH3 - Hall3を受信するための入力キャプチャモード。 私はこの方法をお勧めしません。eMIOSを使って信号をキャプチャすることは確かに可能ですが、この方法は周辺リソースを消費するだけでなく、プロセッシング(SW)にはCPUに依存し続けます。 推奨事項: 例えば、 MCSPTE1AK116 解で示されている方法: あるいは、前述の通り、回転方向はセクター番号の変化に基づいて決定することもできます。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 私のハードウェア設計によると、ホールセンサー信号は下記のようにTRIGMUXチャネルにマッピングされています。 M1_Hall1_Sig_PWM 1 PTA18 入力 TRGMUX_IN12 M1_Hall2_Sig_PWM 2 PTA19 入力 TRGMUX_IN13 M1_Hall3_Sig_PWM 3 PTA20 入力 TRGMUX_IN14 これらのTRIGMUXチャネルをLCUに送り込み、整流と速度信号の計算をしたいと考えています。また、モーターの回転方向も測定したいです。ホールセンサーの入力がTRIGMUXにマッピングされているので、ポートピンの状態を読み取ることは可能でしょうか? Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 1. この関数「Lcu_Ip_GetSyncLogicInput」は、LCUに入力される3つのホールピンすべてのピンの状態を一度に読み取ることができますか。UMのドキュメントを確認しても、関数がポインタを返すのは見当たりません。では、ピン状態はどうやって取得すればいいのでしょうか? M1_Hall1_Sig_PWM 1 PTA18 M1_Hall2_Sig_PWM 2 PTA19 M1_Hall3_Sig_PWM 3 PTA20 2. アプリケーションノートの例では、「関数eMIOS1IcuNotifyは、7つのエッジがキャプチャされた後に呼び出されます」と記載されています。7番目のエッジごとにではなく、すべてのエッジで通知やISRを取得して、そのISR内のホールピン状態を読み取る方法はありますか?そうすれば、速度とモーターの方向を計算するISRは1つだけで済みます。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS こんにちは、@ RIJILKP ホールセンサー入力がTRIGMUXにマッピングされているので、ポートピンの状態を読み取ることは可能 1.Is のでしょうか? それは可能だが、全く必要ない。 LCUモジュール自体はすでに入力の現在の状態を取得できます。 /* @brief [LC_INPUTS] This function Indicates states of LC inputs /* @details This service is a reentrant function that shall Indicates states of LC inputs Lcu_Ip_ReturnType Lcu_Ip_GetSyncLogicInput(Lcu_Ip_SyncInputValueType List[], const uint8 Dimension); 2. XOR信号の変化に応じてeMIOSから割り込みを発生させることは可能ですか?(ここでは、セクターが変化するたびにXOR信号に遷移が生じることを前提としています。) はい、こちらがサンプルコードの設定画面のスクリーンショットです。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS ICU測定モードの設定をEDGE DETECTに変更した場合、以下のAPIを使用してタイムスタンプを取得できますか? 「Emios_Icu_Ip_StartTimestamp」 「Emios_Icu_Ip_GetTimestampIndex」 前提条件には「チャネルはタイムスタンプ測定のために設定されている必要があります」と書かれています。 また、スクリーンショットに表示されているコードを入手することは可能でしょうか?私はドキュメントしかアクセスできませんでした。サンプル実装が手に入れば大いに助かります。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS こんにちは、@ RIJILKP このソリューションのデモコードでは、次のようになります。 1.Lcu Lcu_Ip_GetSyncLogicInput(InputSector, 3); SensorHall.InA = InputSector[0].Value; SensorHall.InB = InputSector[1].Value; SensorHall.InC = InputSector[2].Value; SensorHall.Sector = (SensorHall.InC << 2) + (SensorHall.InB << 1) + SensorHall.InA - 1; 2. 「関数 eMIOS1IcuNotify は7つのエッジがキャプチャされた後に呼び出される」、その関数は修正可能です。 1に変えられます。 あるいは、eMIOSの測定モードを以下のように変更することをお勧めします。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS こんにちは@RIJILKP あなたがこのデモを入手できなかったのは意外です。実は、あなたが提供したリンクに含まれているんですよ。 また、S32K344の場合: https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344 質問に戻りますが、ICUチャネルをEDGE DETECTに設定すると、通常そのチャネルに対してEmios_Icu_Ip_StartTimestamp()やEmios_Icu_Ip_GetTimestampIndex()は使えません。 しかし、先ほども言ったように、「関数 eMIOS1IcuNotify は7つのエッジがキャプチャされた後に呼び出される」というものは、修正可能です。
View full article
IMX8QXP OTA 更新:通过 OTA 更新创建和调整分区大小的可行性 大家好, IMX8QXP - 斯卡思间隙 - L 6.6.52   当当前软件目标的分区布局与 OTA 包的分区布局略有不同时,是否可以在软件更新 (OTA) 过程中创建新分区和调整现有分区的大小? 我们想了解 OTA 更新机制是否可以动态处理分区布局变更,包括分区创建、调整大小和更新相应的分区信息,而无需人工干预。 请分享您对可行性、局限性和推荐方案的看法。 谢谢,此致敬礼! VKS i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Linux Yocto Project Re: IMX8QXP OTA update: Feasibility of Partition Creation and Resizing Through OTA Update 嗨@WinR 请参考此知识库。 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416 此致, 志明 Re: IMX8QXP OTA update: Feasibility of Partition Creation and Resizing Through OTA Update 嗨@Zhiming_Liu , 感谢您的反馈, 我有一个具体的问题。目标设备上已存在该分区。 是否可以通过OTA更新重新创建或调整现有分区的大小?   谢谢,此致敬礼! VKS Re: IMX8QXP OTA update: Feasibility of Partition Creation and Resizing Through OTA Update 嗨@WinR 以下列出了目前可用的OTA文档。请参考该资料。 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416 此致, 志明
View full article
S32K328 HyperRAM read write errors at low temperatures Hello NXP Community, we are using an NXP S32K328 with an Infineon S27KL0642DPBHB023 64-Mbit HyperRAM connected through the QuadSPI interface. The interface operates with the following basic configuration:   HyperRAM voltage = 3.3 V   QuadSPI clock = 120 MHz   Interface mode = Octal DDR   Clock mode = Single-ended CK   Read-data strobe = External RWDS   Latency mode = Fixed latency   Normal memory access = Memory-mapped AHB At room temperature, the HyperRAM interface appears to work correctly. At low temperatures, down to −40 °C, we observe read/write comparison errors. The problem appears to be related mainly to the temperature of the S32K328. Cooling the S32K328 can reproduce the errors, while cooling the HyperRAM alone has a much smaller effect. The relevant S32K328 QuadSPI settings are: DDR_EN = 1   DQS_EN = 1   External DQS/RWDS = selected   DQS_OUT_EN = 1   VAR_LAT_EN = 0   FLSHCR.TCSS = 4   FLSHCR.TCSH = 7   FLSHCR.TDH = 1 The current DLL configuration is:   SLV_DLL_BYPASS = 0   SLAVE_AUTO_UPDT = 1   SLV_EN = 1   SLV_DLY_COARSE = 0   FREQEN = 1   DLL_CDL8 = 0   DLLRES = 8   DLL_REFCNTR = 2   SMPR.FSPHS = 0   SMPR.FSDLY = 0   SMPR.DLLFSMPFA = 0 We tested all available combinations of:   SLV_DLY_OFFSET = 0 to 7   SLV_FINE_OFFSET = 0 to 15 At low temperatures, failures occur across all tested DLL configurations. The sweep shows differences between the configurations, but it does not provide a completely error-free operating range or a clearly optimal DLL parameter set. Therefore, we are currently not sure whether the problem is caused by the DLL configuration itself or by another temperature-dependent part of the S32K328 QuadSPI interface. Could you please help us with the following questions? Is the S32K328 QuadSPI configuration shown above suitable for HyperRAM operation at 120 MHz? Are the selected DLL parameters correct for this frequency and the full temperature range? Which values should be used for FREQEN, DLL_CDL8, DLLRES and DLL_REFCNTR at 120 MHz? Which DLL status flags should be monitored to verify correct operation? Should both DLLA_LOCK and SLVA_LOCK be checked before accessing the HyperRAM? How should DLLA_RANGE_ERR or FINE_UNDERFLOW be handled? Could the QuadSPI DLL or external-DQS path operate outside its valid range at low temperatures? Does the DLL configuration affect only read-data sampling, or can it also affect write timing? Are FLSHCR.TCSS = 4, FLSHCR.TCSH = 7 and FLSHCR.TDH = 1 suitable for 120 MHz HyperRAM operation? Which pad settings are recommended for CK, CS#, DQ[7:0] and RWDS at 120 MHz Octal DDR? Are there any known S32K328 errata or RTD issues related to QuadSPI, external DQS or operation at low temperatures? Is there a validated S32K328 HyperRAM initialization example or register configuration for 120 MHz operation? Any guidance on additional S32K328 registers or status information that should be checked would be very helpful. Thank you. Re: S32K328 HyperRAM read write errors at low temperatures 1) The operating mode is supported, but the current configuration does not fully match the required 120 MHz DDR external-DQS settings in Table 66. FREQEN should be 0, SMPR.DLLFSMPFA should be 4, FLSHCR.TCSS should be 2, FLSHCR.TCSH should be 5, and both delay offsets should initially be 0. The remaining listed settings match Table 66. The configuration should be corrected before further low-temperature testing. 2) The operating mode is supported, but the current configuration does not fully match the required 120 MHz DDR external-DQS settings in Table 66. FREQEN should be 0, SMPR.DLLFSMPFA should be 4, FLSHCR.TCSS should be 2, FLSHCR.TCSH should be 5, and both delay offsets should initially be 0. The remaining listed settings match Table 66. The configuration should be corrected before further low-temperature testing. 3) According to Table 66: FREQEN = 0 DLL_CDL8 = 0 DLLRES = 8 DLL_REFCNTR = 2 The DLL programming sequence described in the “DLL and delay chain usage” chapter must also be followed. 4) Monitor these DLLSR flags: DLLA_LOCK = 1: DLL reference chain is locked. SLVA_LOCK = 1: Slave delay chain is locked. DLLA_RANGE_ERR = 0: DLL master delay chain is within its valid range. DLLA_FINE_UNDERFLOW = 0: No fine-delay-chain underflow occurred. 5) Yes. When the DLL and slave delay line are enabled, both DLLA_LOCK and SLVA_LOCK should indicate lock before starting HyperRAM accesses. 6) These flags indicate that the configured delay cannot be generated correctly. HyperRAM operation should not be considered reliable while either error is present. Recheck the Table 66 configuration and the required DLL initialization sequence. If the error remains, reduce the QuadSPI frequency for further testing. 7) Please retest with the documented settings first. 😎 The external DQS and slave-DLL settings primarily control read-data sampling. Write timing is mainly determined by CK, CS#, data-output timing, pad configuration and the FLSHCR timing fields. Separate read-only and write/read-back tests can help identify which path is failing. 9) They do not match Table 66. For the characterized 120 MHz DDR configuration, use: FLSHCR.TCSS = 2 FLSHCR.TCSH = 5 FLSHCR.TDH = 1 10) The data-sheet characteristics use DSE = 1 and SRE = 0. They assume a maximum output load of 25 pF, an input transition time of 1 ns and QuadSPI traces no longer than 2 inches. These conditions and the actual CK/RWDS signal quality should be verified on the board. 11) I have not identified a published S32K328 erratum specifically describing external-DQS failures at low temperature. The applicable errata and the release notes for the exact RTD version should nevertheless be checked. 12) No validated HyperRAM initialization example is currently available. Please use the configuration specified in Table 66 of the S32K3xx Data Sheet as the reference for the QuadSPI settings. Re: S32K328 HyperRAM read write errors at low temperatures Hello NXP Community, we are continuing our investigation of temperature-dependent HyperRAM errors on an S32K328 connected to an Infineon S27KL0642DPBHB023, 8 MiB, 3.3 V. The interface operates at 120 MHz in Octal DDR mode using external edge-aligned RWDS/DQS. Normal memory access uses the QuadSPI AHB memory-mapped window:     0x68000000 to 0x687FFFFF Current relevant configuration ------------------------------     QuadSPI SCK             = 120 MHz     DDR_EN                  = 1     DQS_EN                  = 1     DQS_FA_SEL              = 3     DQS_OUT_EN              = 1     FLSHCR.TCSS             = 2     FLSHCR.TCSH             = 5     FLSHCR.TDH              = 1     SMPR.DLLFSMPFA          = 4     SMPR.FSDLY              = 0     SMPR.FSPHS              = 0     DLL FREQEN              = 0     DLL_CDL8                = 0     DLL_REFCNTR             = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 8     SLAVE_AUTO_UPDT         = 1     SLV_EN                  = 1     SLV_DLL_BYPASS          = 0 The fine offset of 8 was selected empirically from temperature tests. It is not taken from the zero-offset reference configuration in Data Sheet Rev. 14.  Our current initialization contains this sequence:     Configure QuadSPI and LUT     Configure DLL using auto-update     Perform one dummy AHB read     Perform QuadSPI software reset     Configure DLL again     Read HyperRAM registers using IP commands     Start normal AHB accesses The dummy read currently performs a volatile 32-bit read first and invalidates the corresponding Cortex-M7 cache line afterwards. Difference from Data Sheet Rev. 14 ---------------------------------- In S32K3xx Data Sheet Rev. 14, Table 66 appears to specify the following for the S32K328 120 MHz DDR, External DQS, Edge Aligned configuration:     FLSHCR.TCSS             = 3     FLSHCR.TCSH             = 3     FREQEN                  = 0     DLL_REFCNTR             = 2     DLLRES                  = 8     SLV_DLY_OFFSET          = 0     SLV_FINE_OFFSET         = 0     SLAVE_AUTO_UPDT         = 0     SLV_UPD                 = 1, according to the RM programming sequence     DLLFSMPFA               = 4     FSDLY                   = 0 This differs from our current TCSS/TCSH = 2/5, fine offset 8 and auto-update mode. Failure signature ----------------- Temperature testing still shows occasional memory-test failures even with settings near the center of the measured sampling window. The reported failures have a repeatable signature: - A complete 32-byte block is affected. - When reading address A, the returned block appears to match the expected pattern for address A + 0xFFE0. - The same signature was reported with several DLL offset/fine settings. The initialization-time DLL status indicated:     DLLA_LOCK              = 1     SLVA_LOCK              = 1     DLLA_RANGE_ERR         = 0     FINE_UNDERFLOW         = 0 We have not yet confirmed that these status values remain unchanged at the exact instant of every memory failure. The 0xFFE0 displacement is notable because it equals 0x10000 - 0x20, but we do not assume that this proves a 64-KiB wrap or AHB addressing issue. Questions --------- 1. For the S32K328 at 120 MHz DDR with external edge-aligned DQS, should we use the complete configuration from Data Sheet Rev. 14 Table 66, including:        TCSS/TCSH             = 3/3        SLAVE_AUTO_UPDT       = 0        SLV_DLY_OFFSET        = 0        SLV_FINE_OFFSET       = 0 2. Could you confirm the correct FLSHCR.TDH value for this exact Table 66 column? 3. If SLAVE_AUTO_UPDT = 0 is required, what is the exact sequence for:        SLV_EN        SLV_UPD        DLLEN        DLLA_LOCK        SLVA_LOCK        SLV_UPD clear 4. Is the following initialization sequence valid?        DLL configuration        dummy AHB read        QuadSPI software reset        second DLL configuration        first IP access        first AHB memory-mapped access    Or should software reset occur before the only DLL initialization? 5. After clearing SLV_UPD, which DLL lock indications remain valid and should be checked before the first HyperRAM access? 6. Which QuadSPI AHB buffers, FIFOs and sequence pointers must be cleared after software reset, DLL reconfiguration or IP-command access? 7. For the dummy AHB read, should the CPU cache line be invalidated and a DSB executed before the volatile read? 8. Is there any known S32K328 QuadSPI behavior that could return a complete 32-byte block associated with another address, particularly with an apparent displacement of 0xFFE0? 9. Which measurements or register traces would NXP recommend to distinguish between:        read-address generation error        write-address error        stale AHB buffer data        CPU cache coherency        HyperBus address wrapping        external-DQS sampling error We can provide the complete LUT contents, initialization source and register dumps as attachments. Thank you.
View full article
MCAL 需要源代码以进行代码生成。 您好,NXP技术支持, MCAL 版本:SW32K3_S32M27x_RTD_4.4_4.0.0_P24 当我重命名以下 .h 文件时如果文件格式为 .hh,ADC 生成将会失败。 为什么在代码生成过程中需要生成的源代码? 我问这个问题是因为我的工作场所没有本地源代码策略,我只能在本地电脑上安装 ARXML 等非源代码配置。 BR/熊本熊 Re: MCAL expects source code for code generation 嗨@kumamon 配置生成不一定仅基于 ARXML。在生成过程中,MCAL 配置工具还需要作为已安装的 RTD/MCAL 软件包的一部分提供的文件,包括包含生成器所需的定义或信息的头文件。 因此,如果其中一个预期的 .h 文件存在,则如果文件重命名为 .hh,生成器可能无法再找到或处理该依赖项,这可能会导致代码生成失败。 BR,VaneB Re: MCAL expects source code for code generation 你好@VaneB , 谢谢你的回答。 现在很清楚了。 BR/熊本熊
View full article
S32K328 HyperRAM 在低温下出现读写错误 NXP社区的各位朋友,大家好! 我们使用NXP S32K328 ,并通过 QuadSPI 接口连接Infineon S27KL0642DPBHB023 64-Mbit HyperRAM 。 该接口采用以下基本配置运行:   HyperRAM 电压 = 3.3 V   QuadSPI 时钟频率 = 120 MHz   接口模式 = 八进制 DDR   时钟模式 = 单端 CK   读取数据选通 = 外部 RWDS   延迟模式 = 固定延迟   普通内存访问 = 内存映射 AHB 在室温下,HyperRAM 接口似乎工作正常。 在低至-40 °C 的温度下,我们观察到读/写比较错误。问题似乎主要与 S32K328 的温度有关。冷却 S32K328 可以重现这些错误,而单独冷却 HyperRAM 的效果则小得多。 S32K328 QuadSPI 的相关设置如下: DDR_EN = 1   DQS_EN = 1   外部 DQS/RWDS = 已选择   DQS_OUT_EN = 1   VAR_LAT_EN = 0   FLSHCR.TCSS = 4   FLSHCR.TCSH = 7   FLSHCR.TDH = 1 当前 DLL 配置为:   SLV_DLL_BYPASS = 0   SLAVE_AUTO_UPDT = 1   SLV_EN = 1   SLV_DLY_COARSE = 0   频率 = 1   DLL_CDL8 = 0   DLLRES = 8   DLL_REFCNTR = 2   SMPR.FSPHS = 0   SMPR.FSDLY = 0   SMPR.DLLFSMPFA = 0 我们测试了所有可能的组合:   SLV_DLY_OFFSET = 0 到 7   SLV_FINE_OFFSET = 0 到 15 在低温下,所有测试的 DLL 配置都会出现故障。扫描结果显示了不同配置之间的差异,但并未提供完全无错误的运行范围或明显最优的 DLL 参数集。 因此,我们目前还不确定该问题是由 DLL 配置本身引起的,还是由 S32K328 QuadSPI 接口中其他与温度相关的部分引起的。 请问您能否协助我们解答以下问题? 上述 S32K328 QuadSPI 配置是否适合 120 MHz 的 HyperRAM 运行? 所选的 DLL 参数是否适用于此频率和整个温度范围? 在 120 MHz 时,FREQEN、DLL_CDL8、DLLRES 和 DLL_REFCNTR 应该使用哪些值? 应该监测哪些 DLL 状态标志来验证其运行是否正确? 访问 HyperRAM 之前是否应该同时检查 DLLA_LOCK 和 SLVA_LOCK? 应该如何处理 DLLA_RANGE_ERR 或 FINE_UNDERFLOW 错误? QuadSPI DLL 或外部 DQS 路径在低温下是否会在其有效范围之外运行? DLL 配置是否仅影响读取数据采样,还是也会影响写入时序? FLSHCR.TCSS = 4、FLSHCR.TCSH = 7 和 FLSHCR.TDH = 1 是否适用于 120 MHz HyperRAM 运行? 对于 120 MHz 八进制 DDR,CK、CS#、DQ[7:0] 和 RWDS 的推荐焊盘设置是什么? 是否存在与 QuadSPI、外部 DQS 或低温运行相关的已知 S32K328 勘误或 RTD 问题? 是否有经过验证的适用于 120 MHz 运行的 S32K328 HyperRAM 初始化示例或寄存器配置? 任何关于需要检查的其他 S32K328 寄存器或状态信息的指导都将非常有帮助。 谢谢! Re: S32K328 HyperRAM read write errors at low temperatures 1) 支持该操作模式,但当前配置与表 66 中要求的 120 MHz DDR 外部 DQS 设置不完全匹配。FREQEN 应为 0,SMPR.DLLFSMPFA 应为 4,FLSHCR.TCSS 应为 2,FLSHCR.TCSH 应为 5,两个延迟偏移量最初应为 0。其余列出的设置与表 66 相符。在进行进一步的低温测试之前,应先修正配置。 2) 支持该操作模式,但当前配置与表 66 中要求的 120 MHz DDR 外部 DQS 设置不完全匹配。FREQEN 应为 0,SMPR.DLLFSMPFA 应为 4,FLSHCR.TCSS 应为 2,FLSHCR.TCSH 应为 5,两个延迟偏移量最初应为 0。其余列出的设置与表 66 相符。在进行进一步的低温测试之前,应先修正配置。 3)根据表66: 频率 = 0 DLL_CDL8 = 0 DLLRES = 8 DLL_REFCNTR = 2 还必须遵循“DLL 和延迟链使用”章节中描述的 DLL 编程顺序。 4) 监测以下 DLLSR 标志: DLLA_LOCK = 1:DLL 引用链已锁定。SLVA_LOCK = 1:从设备延迟链已锁定。DLLA_RANGE_ERR = 0: DLL 主延迟链在其有效范围内。DLLA_FINE_UNDERFLOW = 0:未发生精细延迟链下溢。 5)是的。当 DLL 和从属延迟线启用时,DLLA_LOCK 和 SLVA_LOCK 都应在开始 HyperRAM 访问之前指示锁定。 6) 这些标志表明无法正确生成配置的延迟。当出现上述任一错误时,HyperRAM 的运行都不能被视为可靠。重新检查表 66 配置和所需的 DLL 初始化顺序。如果错误仍然存在,请降低 QuadSPI 频率进行进一步测试。 7)请先按照文档中记录的设置重新测试。 😎 外部 DQS 和从属 DLL 设置主要控制读取数据采样。写入时序主要由 CK、CS#、数据输出时序、焊盘配置和 FLSHCR 时序字段决定。分别进行只读测试和写/读回测试可以帮助确定哪条路径出现故障。 9)它们与表 66 不符。对于典型的 120 MHz DDR 配置,请使用: FLSHCR.TCSS = 2 FLSHCR.TCSH = 5 FLSHCR.TDH = 1 10) 数据表特性采用 DSE = 1 和 SRE = 0。他们假设最大输出负载为 25 pF,输入转换时间为 1 ns,QuadSPI 走线长度不超过 2 英寸。这些条件和实际的CK/RWDS信号质量需要在板上进行验证。 11) 我尚未找到已发布的 S32K328 勘误表,专门描述低温下的外部 DQS 故障。不过,仍应查看适用的勘误表和确切 RTD 版本的发行说明。 12) 目前没有经过验证的 HyperRAM 初始化示例。请以 S32K3xx 数据手册表 66 中指定的配置作为 QuadSPI 设置的参考。 Re: S32K328 HyperRAM read write errors at low temperatures NXP社区的各位朋友,大家好! 我们正在继续研究连接到英飞凌 S27KL0642DPBHB023、8 MiB、3.3 V 的 S32K328 上与温度相关的 HyperRAM 错误。 该接口在八进制 DDR 模式下以 120 MHz 的频率运行,采用外部边缘对齐的 RWDS/DQS。正常的内存访问使用 QuadSPI AHB 内存映射窗口:     0x68000000 至 0x687FFFFF 当前相关配置 ------------------------------     QuadSPI SCK = 120 MHz     DDR_EN = 1     DQS_EN = 1     DQS_FA_SEL = 3     DQS_OUT_EN = 1 FLSHCR.TCSS = 2 FLSHCR.TCSH = 5     FLSHCR.TDH = 1     SMPR.DLLFSMPFA = 4 SMPR.FSDLY = 0     SMPR.FSPHS = 0     DLL 频率 = 0     DLL_CDL8 = 0     DLL_REFCNTR = 2 DLLRES = 8 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 8     SLAVE_AUTO_UPDT = 1     SLV_EN = 1 SLV_DLL_BYPASS = 0 精细偏移量 8 是通过温度测试经验性地选定的。它并非取自数据手册第14版中的零偏移参考配置。 我们当前的初始化包含以下序列: 配置 QuadSPI 和 LUT 使用自动更新配置 DLL 执行一次虚拟 AHB 读取 执行 QuadSPI 软件 RESET 再次配置 DLL 使用 IP 命令读取 HyperRAM 寄存器 开始正常AHB访问 目前,虚拟读取操作首先执行易失性 32 位读取,然后使相应的 Cortex-M7 缓存行失效。 与数据手册第 14 版的差异 ---------------------------------- 在 S32K3xx 数据手册 Rev. 14 中,表 66 似乎对 S32K328 120 MHz DDR、外部 DQS、边缘对齐配置规定了以下内容: FLSHCR.TCSS = 3 FLSHCR.TCSH = 3     频率 = 0     DLL_REFCNTR = 2 DLLRES = 8 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 0     SLAVE_AUTO_UPDT = 0 根据 RM 编程序列,SLV_UPD = 1 DLLFSMPFA = 4 FSDLY = 0 这与我们目前的 TCSS/TCSH = 2/5、精细偏移 8 和自动更新模式不同。 故障特征 ----------------- 即使将设置调整到接近测量采样窗口中心的位置,温度测试仍然偶尔会出现内存测试失败的情况。 所报告的故障具有可重复的特征: 一个完整的 32 字节块受到影响。 -读取地址 A 时,返回的块似乎与地址 A + 0xFFE0 的预期模式相匹配。 -报告称,在多个 DLL 偏移/精细设置下,都出现了相同的签名。 初始化时 DLL 状态指示如下: DLLA_LOCK = 1     SLVA_LOCK = 1 DLLA_RANGE_ERR = 0     FINE_UNDERFLOW         = 0 我们尚未确认这些状态值在每次内存故障发生的瞬间是否保持不变。 0xFFE0 位移值得注意,因为它等于 0x10000 - 0x20,但我们并不认为这证明了 64-KiB 的循环或 AHB 地址问题。 问题 --------- 1.对于采用外部边沿对齐 DQS 的 120 MHz DDR 内存的 S32K328,我们是否应该使用数据手册 Rev. 14 表 66 中的完整配置,包括: TCSS/TCSH = 3/3        SLAVE_AUTO_UPDT = 0 SLV_DLY_OFFSET = 0 SLV_FINE_OFFSET = 0 2.您能否确认一下表 66 列中 FLSHCR.TDH 的正确值? 3.如果需要将 SLAVE_AUTO_UPDT 设置为 0,那么具体的操作顺序是什么? SLV_EN        SLV_UPD        DLLEN DLLA_LOCK SLVA_LOCK        SLV_UPD 清除 4.以下初始化序列是否有效? DLL 配置 虚拟 AHB 读取 QuadSPI 软件RESET 第二个 DLL 配置 首次 IP 访问 首次 AHB 内存映射访问 或者,软件 RESET 应该在唯一的 DLL 初始化之前进行吗? 5.清除 SLV_UPD 后,哪些 DLL 锁定指示仍然有效,在首次访问 HyperRAM 之前应该检查哪些? 6.软件 RESET、DLL 重新配置或 IP 命令访问后,必须清除哪些 QuadSPI AHB 缓冲区、FIFO 和序列指针? 7.对于虚拟 AHB 读取,是否应该在易失性读取之前使 CPU 缓存行失效并执行 DSB? 8.是否有已知的 S32K328 QuadSPI 行为可以返回与另一个地址关联的完整 32 字节块,特别是当位移明显为 0xFFE0 时? 9. NXP建议使用哪些测量值或寄存器轨迹来区分: 读取地址生成错误 写入地址错误        过时的 AHB 缓冲区数据 CPU缓存一致性 HyperBus地址包装 外部DQS采样误差 我们可以提供完整的 LUT 内容、初始化源代码和寄存器转储作为附件。 谢谢!
View full article
MCALはコード生成のためにソースコードを必要とします。 こんにちは、NXPサポートの皆さん、 MCALバージョン: SW32K3_S32M27x_RTD_4.4_4.0.0_P24 以下の.hファイルの名前を変更するとファイルを.hhに変換すると、ADC生成が失敗します。 コード生成時に生成されたソースコードが必要なのはなぜですか? 私の職場にはローカルソースポリシーがなく、ARXMLのような非ソースコードの設定しかローカルPCに入れられないので質問しました。 BR/くまモン Re: MCAL expects source code for code generation こんにちは、 @kumamon さん。 構成生成は必ずしもARXMLのみに基づいて行われるわけではない。生成プロセス中、MCAL設定ツールはインストールされたRTD/MCALパッケージの一部として、定義やジェネレーターに必要な情報を含むヘッダーファイルも提供する必要があります。 したがって、期待される .h のいずれかがファイル名が.hhに変更されると、ジェネレーターがその依存関係を特定・処理できなくなる可能性があり、コード生成が失敗することがあります。 BR、VaneB Re: MCAL expects source code for code generation こんにちは、 @VaneB さん。 ご回答ありがとうございます。 今や明らかになった。 BR/くまモン
View full article
使用 TRIGMUX+eMIOS 进行 BLDC 电机方向测量 描述:我正在使用 NXP 推荐的 6 步换向解决方案来驱动我的 BLDC 电机。 根据应用笔记“ https://community.nxp.com/t5/S32M-Knowledge-Base/S32M276-Hall-sensor-based-6-step-BLDC-motor-control/ta-p/2035021#jump_PwmAndTriggers ” 霍尔传感器的输出信号送至 TRIGMUX,然后送至 LCU 进行换向,并用于计算速度信号。本文并未提及如何测量电机旋转方向。 NXP是否有测量电机方向的解决方案?我的理解是,要测量方向,我们需要使用输入采集单元捕获所有 3 个霍尔传感器的输出。 我的 eMIOS 通道是否可以按如下方式配置? CH0 - 输入捕获模式,通过 TRIGMUX 从 LCU 接收速度信号。 CH1 - 输入捕获模式,用于接收 Hall1。 CH2 - 输入捕获模式,用于接收 Hall2。 CH3 - 输入捕获模式,用于接收 Hall3。 请提供一些说明。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 您好@RIJILKP 电机旋转方向可以通过霍尔传感器发出的信号序列来确定。 然而,在“S32M276 - 基于霍尔传感器的 6 步 BLDC 电机控制”解决方案中,电机的旋转方向由用户软件作为输入提供。 当前扇区可根据三个信号的状态确定:Hall_A、Hall_B 和 Hall_C。 根据预设的旋转方向,可以计算出下一个换向位置。 在这个参考设计中,您可以根据扇区编号变化的顺序来确定电机的当前旋转方向(如果您愿意的话)。 回到你的问题: 如果你的目标仅仅是确定旋转方向,你可以简单地通过GPIO读取三个霍尔信号的状态;通过分析两次连续读取之间这些信号的变化,你就可以确定当前的旋转方向。 关于您的问题: “我的 eMIOS 通道是否可以按如下方式配置? CH0 - 输入捕获模式,通过 TRIGMUX 从 LCU 接收速度信号。 CH1 - 输入捕获模式,用于接收 Hall1。 CH2 - 输入捕获模式,用于接收 Hall2。 CH3 - 输入捕获模式,用于接收 Hall3。 我不推荐这种做法。虽然使用 eMIOS 进行信号捕获是完全可行的,但你的方法不仅消耗外围资源,而且还依赖于 CPU 进行处理(软件)。 推荐 : 例如, MCSPTE1AK116解决方案中提供的方法: 或者,正如我上面提到的,旋转方向可以根据扇区编号的变化来确定。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 如果我将 eMIOS 0 CH0 - 输入捕获模式配置为通过 TRIGMUX 从 LCU 接收速度信号(3 个霍尔输入的 XOR 值)。 是否可以通过对异或信号的任何变化,从 eMIOS 触发中断?(这里我假设每次扇区变化时,异或信号都会发生转换。)如果可行,我可以读取接收霍尔传感器输入的 GPIO 引脚来检查霍尔模式或扇区,还可以使用每个扇区变化之间的时间戳来测量速度。因此,速度和方向可以在同一个ISR中测量。 请告诉我这是否可行/推荐。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 根据我的硬件设计,霍尔传感器信号被映射到如下所示的 TRIGMUX 通道。 M1_Hall1_Sig_PWM 1 PTA18 输入 TRGMUX_IN12 M1_Hall2_Sig_PWM 2 PTA19 输入 TRGMUX_IN13 M1_Hall3_Sig_PWM 3 PTA20 输入 TRGMUX_IN14 我想将这些 TRIGMUX 通道馈送到 LCU 进行换向以及速度信号计算。另外,我还想测量电机的旋转方向。由于霍尔传感器输入映射到 TRIGMUX,是否可以读取端口引脚状态? Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 1. “Lcu_Ip_GetSyncLogicInput” 函数是否能够一次性读取 LCU 的所有 3 个霍尔引脚的引脚状态?我查看了 UM 文档,没有看到该函数返回任何指针,那么我该如何获取引脚状态呢? M1_Hall1_Sig_PWM 1 PTA18 M1_Hall2_Sig_PWM 2 PTA19 M1_Hall3_Sig_PWM 3 PTA20 2. 应用说明示例中提到,“ 在捕获 7 个边沿后调用 函数 eMIOS1IcuNotify ”。有没有办法在每个边沿捕获到通知/中断服务例程 (ISR) 时而不是每 7 个边沿捕获到一次,以便我可以在 ISR 中读取霍尔引脚状态?这样我就只需要一个中断服务例程(ISR)来计算速度和电机方向。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 您好@RIJILKP 1.由于霍尔传感器输入映射到TRIGMUX,是否可以读取端口引脚状态? 这虽然可行,但完全没有必要; LCU 模块本身已经可以获取输入的当前状态。 /* @brief [LC_INPUTS] This function Indicates states of LC inputs /* @details This service is a reentrant function that shall Indicates states of LC inputs Lcu_Ip_ReturnType Lcu_Ip_GetSyncLogicInput(Lcu_Ip_SyncInputValueType List[], const uint8 Dimension); 2.是否可以通过异或信号的任何变化从 eMIOS 触发中断?(这里我假设每次扇区变化都会伴随一个异或信号转换。) 是的,这是示例代码中的配置截图。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 如果我将 ICU 测量模式配置更改为 EDGE DETECT,我是否可以使用以下 API 获取时间戳? "Emios_Icu_Ip_StartTimestamp" "Emios_Icu_Ip_GetTimestampIndex" 前提条件是“通道必须配置为时间戳测量”。 另外,能否提供您在截图中展示的代码?我只能访问文档。如果能拿到示例实现,将对我帮助很大。 Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 您好@RIJILKP 本解决方案演示代码如下: 1.Lcu Lcu_Ip_GetSyncLogicInput(InputSector, 3); SensorHall.InA = InputSector[0].Value; SensorHall.InB = InputSector[1].Value; SensorHall.InC = InputSector[2].Value; SensorHall.Sector = (SensorHall.InC << 2) + (SensorHall.InB << 1) + SensorHall.InA - 1; 2. “函数eMIOS1IcuNotify在捕获 7 个边后调用”,这可以修改。 你可以把它改成1, 或者,我建议对 eMIOS 测量模式进行如下修改: Re: BLDC Motor Direction measurement using TRIGMUX+eMIOS 您好@RIJILKP 我很惊讶你竟然没收到这个演示;它实际上包含在你提供的链接中。 另外,对于 S32K344: https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344 回到你的问题,如果你将 ICU 通道配置为 EDGE DETECT,通常不能对该通道使用 Emios_Icu_Ip_StartTimestamp() 和 Emios_Icu_Ip_GetTimestampIndex()。 但就像我之前说的, “函数eMIOS1IcuNotify在捕获 7 个边后调用”,这是可以修改的。
View full article
S32 Design Studioのライセンスが切れました こんにちは、NXPサポートの皆さん。このメッセージがあなたの元に無事届くことを願っています。私のS32DSライセンスが期限切れになり、現在の開発作業が妨げられています。延長を手伝ってもらえますか? 私の認証ID: 406C-B408-57DB-0C62 製品:ARM v2.2用のS32 Design Studio。 ご返信よろしくお願いします。 SDK Re: S32 Design Studio License Expired こんにちは、 お客様のS32DSライセンスが延長されました。
View full article
S32 Design Studio License Expired Hello NXP Support, I hope this message finds you well. My S32DS license has expired, and it’s blocking my current development work. Could you kindly help extend it? My Activation ID : 406C-B408-57DB-0C62.  Product : S32 Design Studio for ARM v2.2. Thank you very much. SDKs Re: S32 Design Studio License Expired Hi,  your S32DS license has been extended. 
View full article