Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX95:推奨BSP / Neutron SDKsのバージョン管理戦略(LF_6.18.20_2.0.0) こんにちは、 私たちはi.MX95をプラットフォームとして用いる自動車アプリケーション向けのPoCを開発しており、推奨されるBSPおよびNeutron SDKのバージョン管理戦略を明確にしたいと考えています。 NeutronSDKUserGuide.md 年の「Neutron SDK Version Compatibility with Yocto BSP」の表を読み、コンパイラとランタイムは同じSDKから来なければならないと理解しています。しかし、ガイドにはどのバージョンが推奨されているかは明記されていない。 以下の点について教えていただけますか: 1.現在のBSPでは常に最新のNeutron SDKバージョン(ランタイムがアップグレードされたもの)を使うべきでしょうか、それともそのBSPのデフォルトバージョンを使うべきでしょうか? 2. 新しいBSPリリースが利用可能になった場合、現在のBSPからアップグレードするのが推奨されますか?それともアップグレードが必要でない限り現行バージョンを維持すべきでしょうか? 環境 - ボード:IMX95LPD5EVK-19 - BSP:LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so、libneutron_delegate.soはNeutron SDK 3.2.3のバージョンに更新されています。 ご回答をお待ちしています。
View full article
i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? I am using a custom i.mx93 board but mostly follows evk's design and PMIC.  On software, I am using NXP BSP-based Yocto (walnascar-6.12.34-2.1.0 branch). I want a watchdog timeout to reset only the Cortex-A55 and leave the Cortex-M33 (Zephyr) running, so the M33 can supervise the A55 and buffer data during the outage. I found in the reference manual that - Section 32.2.10 lists wdog4_ca55_rst_b and wdog5_ca55_rst_b as cold reset sources. - Section 32.2.12.2 says the CA55 cannot be warm reset and describes a power down, CPUWAIT, power up, release sequence. - The WDOG chapter 69 does not say what a timeout resets. I have dump the registers of SRC base 0x44460000 by using devmem2  +0x18 (reset mask): 0x00000FBF. Bit 6 (CSU) is clear, and the WDOG bits, including WDOG5 (bit 4), are set, so those sources are masked. Is it supported to unmask WDOG4 or WDOG5 and set its reset mode to the CA55 slices only, so the A55 resets while the M33 keeps running? If so, is there anything else required for the A55 to restart?  Is there an application note or example for it? Thank you for any pointers in advance. Best Regards Linux Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? The SRC can route a WDOG4/5 reset to A55 domains without selecting the M33 domain, but that alone does not establish that the A55 will power-cycle, restart, and boot Linux while the M33 keeps running. The A55 restart sequence and any watchdog-triggered PMIC reset must also be accounted for. I could not find an NXP example implementing that complete flow for your BSP. Also, your mask-bit reading appears off: in SRMASK , WDOG4 and WDOG5 are bits 19 and 20 , not bits 3 and 4. Recheck the register fields before changing them. Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? Thanks you for the quick reply. My SRMASK diagram (screenshot attached) has WDOG4 and WDOG5 at bits 3 and 4, and WDOG1 to WDOG3 at bits 0 to 2, with reset value 0xFBF. That matches what I read at boot. I am reading IMX93RM.pdf Rev. 7, 2026-02-10. Could you confirm which document and revision you are reading? My open question is the restart: after this reset, with CPUWAIT held and the reset vector set, what is the supported sequence to get the A55 running again? The RM says the CA55 cannot be warm reset and needs a power cycle. Is there a supported way to power-cycle it from the M33? Thank you. Best Regards Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? You are right about SRMASK . I misread the diagram’s bit-position labels. For the restart, an A55 reset alone is not the documented sequence. Section 32.2.12.2 says the CA55 cannot be warm reset and specifies: power down the CA55; set its CA55_CPUWAIT[CPUn_WAIT] bit to 1; power the CA55 up; then release WAIT so the core can run. Setting the reset vector and holding CPUWAIT therefore do not, by themselves, perform the required power cycle. There is a documented software mechanism to power-cycle SRC slices , potentially usable by M33 firmware: §32.2.8 describes enabling MEM_CTRL[MEM_LP_EN] , setting the slice’s SLICE_SW_CTRL[PDN_SOFT] to 1 for power-down, and clearing it to 0 for power-up. It permits software slice control only with AUTHEN_CTRL[LPM_MODE] = 0 ; the slice’s AUTHEN_CTRL[WHITE_LIST] also determines which TRDC domains may write its registers. The RM identifies separate A55 core and platform slices, so this must be applied to the appropriate CA55 power domains—not assumed to happen when a WDOG reset is routed to them. Use the RM’s CA55 power-down → CPUWAIT → power-up → WAIT-release sequence; watchdog reset routing alone does not establish a complete A55 restart.
View full article
S32DS 3.5 激活失败——剩余激活次数已用完,请请求 RESET 你好, 我尝试在我的新 Windows PC 上激活 S32 Design Studio for S32 Platform v3.5,但激活失败,并出现错误提示说没有剩余的激活次数。 我之前在虚拟机(Mac 上的 Parallels)上激活了它,但我已经删除了该虚拟机,所以我无法从中恢复许可证。 请问能否重置我的激活码的激活次数,或者发放一个新的激活码? 产品:S32平台S32设计工作室 v3.5 Windows 11 如有需要,我可以通过私信发送完整的激活码。 谢谢! Re: S32DS 3.5 activation failed – no remaining activations, request reset 你好, 请立即尝试。应该可以正常运行了。 顺祝商祺! Peter
View full article
i.MX93:看门狗能否只重置 Cortex-A55 而让 Cortex-M33 继续运行? 我使用的是定制的i.MX93主板,但大部分设计和电源管理芯片(PMIC)都参考了evk的方案。软件方面,我使用的是基于 NXP 电路板支持包。 的 Yocto(walnascar-6.12.34-2.1.0)。分支)。 我希望看门狗超时功能只重置 Cortex-A55,而让 Cortex-M33 (Zephyr) 继续运行,以便 M33 可以在断电期间监控 A55 并缓冲数据。 我在参考手册中发现: - 第 32.2.10 节将 wdog4_ca55_rst_b 和 wdog5_ca55_rst_b 列为冷 RESET 源。 - 第 32.2.12.2 节指出 CA55 不能进行热 RESET,并描述了掉电、CPUWAIT、上电、版本序列。 - WDOG 第 69 章没有说明超时 RESET 什么。 我使用 devmem2 转储了 SRC 基址 0x44460000 的寄存器。 +0x18(RESET掩码):0x00000FBF。第 6 位(CSU)为 0,WDOG 位(包括 WDOG5(第 4 位))已设置,因此这些源被屏蔽。 是否支持取消屏蔽 WDOG4 或 WDOG5 并将其复位模式设置为仅 CA55 切片,以便 A55 复位而 M33 继续运行?如果是这样,A55重启还需要其他什么步骤吗?是否有相关的应用笔记或示例? 提前感谢您的任何建议。 此致 Linux Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? SRC 可以将 WDOG4/5 RESET 路由到 A55 功能域而不选择 M33 功能域,但这本身并不能证明 A55 会在 M33 继续运行时进行电源循环、重新启动和启动 Linux。还必须考虑 A55 重启序列和任何看门狗触发的 PMIC RESET。我找不到 NXP 提供的能够实现您电路板支持包。完整流程的示例。 另外,您的掩码位读取似乎有误:在 SRMASK 中,WDOG4 和 WDOG5 是第 19 位和第 20 位,而不是第 3 位和第 4 位。更改寄存器字段之前,请重新检查它们。 Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? 感谢您的快速回复。 我的 SRMASK 图(附截图)中,WDOG4 和 WDOG5 位于第 3 位和第 4 位,WDOG1 到 WDOG3 位于第 0 位到第 2 位,复位值为 0xFBF。这与我启动时读取到的信息一致。 我正在阅读 IMX93RM.pdf 文件。牧师7、2026-02-10。 请问您正在阅读的是哪份文件以及哪个版本? 我目前的问题是关于重启:在这次 RESET 之后,保持 CPUWAIT 并设置 RESET 向量,要让 A55 再次运行,支持的顺序是什么?RM 表示 CA55 无法进行热 RESET,需要断电重启。是否有官方支持的方法通过 M33 对其进行断电重启? 谢谢。 此致 Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? 您对 SRMASK 的看法是对的。我误读了图表中的位位置标签。 对于重启,单独使用 A55 RESET 并不是官方记录的步骤。第 32.2.12.2 节指出 CA55 不能进行热复位,并规定:关闭 CA55 的电源;将其 CA55_CPUWAIT[CPUn_WAIT] 位设置为 1;打开 CA55 的电源;然后释放 WAIT,以便内核可以运行。因此,单独设置复位向量和保持 CPUWAIT 状态并不能执行所需的电源循环。 有一个已记录的软件机制可以对 SRC 切片进行断电重启,M33 固件可能可以使用该机制:§32.2.8 描述了启用 MEM_CTRL[MEM_LP_EN],将切片的 SLICE_SW_CTRL[PDN_SOFT] 设置为 1 以掉电,并将其清除为 0 以上电。它仅允许通过 AUTHEN_CTRL[LPM_MODE] = 0 进行软件切片控制;切片的 AUTHEN_CTRL[WHITE_LIST] 还决定哪些 TRDC 功能域可以写入其寄存器。RM 识别出单独的 A55 内核和平台切片,因此必须将其应用于相应的 CA55 功率域——不能假定当 WDOG 复位路由到它们时就会发生这种情况。 使用 RM 的 CA55 掉电 → CPUWAIT → 上电 → WAIT 释放序列;仅看门狗 RESET 路由无法建立完整的 A55 重启。
View full article
S32DS 3.5 activation failed – no remaining activations, request reset Hello, I am trying to activate S32 Design Studio for S32 Platform v3.5 on my new Windows PC, but activation fails with an error saying there are no remaining activations. I previously activated it on a virtual machine (Parallels on Mac), but I have already deleted that VM, so I cannot return the license from it. Could you please reset the activation count for my activation code or issue a new activation code? Product: S32 Design Studio for S32 Platform v3.5 Windows 11 I can send the full activation code via private message if needed. Thank you. Re: S32DS 3.5 activation failed – no remaining activations, request reset Hello, Please try now. It should be working. Best regards, Peter
View full article
i.MX95:推荐的 电路板支持包 / Neutron SDK 版本控制策略 (LF_6.18.20_2.0.0) 你好, 我们正在使用 i.MX95 作为平台开发汽车应用的 PoC,并希望明确推荐的 电路板支持包 和 Neutron SDK 版本策略。 我们已经阅读了 NeutronSDKUserGuide.md 中的“Neutron SDK 版本与 Yocto 电路板支持包的兼容性”表格,并了解到编译器和运行时必须来自同一个 SDK。但是,该指南并未说明推荐哪个版本。 您能帮我们理解一下吗? 1.我们应该始终在当前的 电路板支持包。 上使用最新的 Neutron SDK 版本(运行时已升级),还是应该使用该 电路板支持包。 的默认 SDK 版本? 2. 当有新的 电路板支持包。 版本发布时,建议从我们当前的 电路板支持包。 版本升级,还是应该保留当前版本,除非有必要升级? 环境 - 板:IMX95LPD5EVK-19 - 电路板支持包:LF_6.18.20_2.0.0 - Neutron SDK:eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so 和 libneutron_delegate.so 已更新至 Neutron SDK 3.2.3 的版本。 谢谢!
View full article
i.MX95: Recommended BSP / Neutron SDK versioning strategy (LF_6.18.20_2.0.0) Hello, We are developing a PoC for an automotive application using the i.MX95 as our platform and would like to clarify the recommended BSP and Neutron SDK versioning strategy. We have read the "Neutron SDK Version Compatibility with Yocto BSP" table in NeutronSDKUserGuide.md and understand that the compiler and runtime must come from the same SDK. However, the guide does not say which version is recommended. Could you help us understand: 1. Should we always use the latest Neutron SDK version (with the runtime upgraded) on our current BSP, or should we use the SDK version that is Default for that BSP? 2. When a new BSP release becomes available, is it recommended to upgrade from our current BSP, or should we keep the current version unless an upgrade is necessary? Environment - Board: IMX95LPD5EVK-19 - BSP: LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf, libNeutronDriver.so, and libneutron_delegate.so have been updated to the versions from Neutron SDK 3.2.3. Thank you!
View full article
PT2001ソフトウェア診断 こんにちは、 PT2001ソフトウェアの診断コードについて質問させてください。どなたか助けていただけませんか? 私はマイクロコードにおけるSTG検出と、HSおよびLS障害の区別に取り組んでいます。 これまでにやったのは、HSのVBATを短時間ONにして、HSのVdsが故障しているか確認し、それがLSの故障かHSの故障かを判断することです。 しかし、これはうまくいかないようだ。LSドレンにSTHを適用しても、常にHS故障として検出されるためです。 STG故障をHS(ソース)とLS(ドレイン)の故障から区別するには、どのように解決すればよいでしょうか? 本当にありがとうございます。 アティカ Re: PT2001 SW diagnostic こんにちは、アティカさん 良い一日! あなたが観察している挙動は想定内のものです。ローサイドドレインにアースショートをかけると、VBATハイサイドがオンになった際にハイサイドVDS診断が作動します。これは、VBATからハイサイドMOSFETと負荷を通って接地されたローサイドドレインに電流が流れ、ハイサイドVDSのしきい値を超えるために発生します。 したがって、ハイサイドを一時的に有効化しても、物理的なショートがハイサイドソースにあるのかローサイドドレインにあるのかを確実に特定することはできません。このトポロジーでは、両方の故障がPT2001のセンス入力で同じ電気的条件を生じさせることができます。 推奨される方法は、HS および LS MOSFET の両方をオフにしたアイドル診断フェーズ中に、HS VSRC および LS VDS フィードバックを使用して、接地短絡を特定することです。両方のフィードバックが低い場合、結果は「負荷経路の接地短絡」と分類されるべきである。PT2001は故障を検出できますが、追加の外部検出またはアイソレータ回路がなければ、HSソース側やLSドレイン側で故障を特定することはできません。 この情報がお役に立てば幸いです。他に何かご不明な点がありましたら、お気軽にお問い合わせください。 良い一日をお過ごしください。幸運を祈ります。 Re: PT2001 SW diagnostic こんにちは、RafaRさん。 アイドル状態中に、負荷経路が接地短絡していることが特定され、接地短絡故障がHS電源にあるのかLSドレインにあるのかを区別する必要がありました。 今回の診断では、外部HS MOSFETを短時間オンにし、Vdsしきい値を下げることで、故障箇所を正しく特定できるようになりました。 ありがとうございます。良い一日をお過ごしください!
View full article
S32DS3.4安装iar插件失败 报错如下: 收集要安装的项目时发生错误,会话上下文为:(profile=DefaultProfile,phase=org.eclipse.equinox.internal.p2.engine.phases.Collect,operand=,action=)。下载工件时出现问题:osgi.bundle,com.iar.dmgr,1.1.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar 的签名时出错 下载工件时出现问题:org.eclipse.update.feature,com.iar.dmgr.feature,1.1.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar 的签名时出错 下载工件时出现问题:osgi.bundle,com.iar.dmgr.jna,3.4.0.202505161156。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar 的签名时出错 下载工件 osgi.bundle,com.iar.dmgr.ui,1.1.0.202505161156 时出现问题。读取签名内容时出错:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 处理文件 C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 的签名时出错 回复: S32DS3.4 安装iar插件失败 HI,CHRIS 目前遇到这个问题:S32DS3.5安装IAR插件;路径是官网下的https://eclipse-update.iar.com/plugin-manager/1.0 安装重启之后在HELP下看不到IAR EMBEDED workbench plugin manager这一个选项 IAR 版本为9.32.2 回复: S32DS3.4 安装iar插件失败 s32ds v3.5可以用 插件eclipse-iar-arm-8.0 有的版本s32ds(对应不同版本eclipse),可以试试离线安装iar插件的 https://eclipse-update.iar.com/updatesites.html 回复: S32DS3.4 安装iar插件失败 3.5以上就可以了 回复: S32DS3.4 安装iar插件失败 好的 ,请教下 现在什么版本可以安装IAR插件? 回复: S32DS3.4 安装iar插件失败 前段时间我问过,iar插件升级不支持老版本的eclipse
View full article
PT2001 软件诊断 您好, 我想咨询一下关于PT2001软件诊断代码的问题。我想知道有没有人能帮帮我。 我正在研究微代码中的 STG 检测,并区分 HS 和 LS 故障。 我目前所做的就是将 HS vbat 打开一小段时间,然后检查 HS Vds,并判断是 LS 故障还是 HS 故障。 但这似乎行不通。即使我对 LS 漏极施加 STH,它仍然总是检测为 HS 故障。 如何区分 STG 故障与 HS(源)故障和 LS(漏)故障? 太感谢了, 阿提卡 Re: PT2001 SW diagnostic 你好,阿蒂卡 再会! 你观察到的这种行为是预期之内的。当 VBAT 高侧开启时,低侧漏极接地短路也会触发信号高侧 VDS 诊断。这是因为电流从 VBAT 流经高侧 MOSFET 和负载进入接地的低侧漏极,导致高侧 VDS 阈值被超过。 因此,短暂启用高侧无法可靠地确定物理短路位于高侧源极还是低侧漏极。对于这种拓扑结构,两种故障都可以在 PT2001 感知输入端产生相同的电气状态。 建议的方法是,在空闲诊断阶段,让 HS 和 LS MOSFET 都关闭,利用 HS VSRC 和 LS VDS 反馈来识别对地短路。如果两个反馈都很低,则结果应归类为“负载路径对地短路”。PT2001 可以检测到故障,但如果没有额外的外部传感或隔离电路,它无法唯一地将故障定位在高源极侧或低漏极侧。 希望这些信息对您有所帮助,如果您还需要其他帮助,请告诉我。 祝你今天过得愉快,一切顺利。 Re: PT2001 SW diagnostic 你好 RafaR, 在空闲阶段,发现负载路径对地短路,我需要区分对地短路故障是发生在HS源极还是LS漏极。 现在,通过短暂地打开外部 HS MOSFET 并降低 Vds 阈值,可以正确识别故障。 谢谢,祝您今天过得愉快!
View full article
S32 Design Studio for ARM v2018.R1 许可证已过期 你好, 我的S32 Design Studio for ARM v2018.R1许可证已过期。 请问您能否帮我延长一下许可证期限? 激活码:9D31-3A20-FFB1-F104 Re: S32 Design Studio for ARM v2018.R1 license expired 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
View full article
EB Tresos 29 的当前许可证缺少一些功能。 你好! 最近过期的 EB Tresos Studio 29 许可证包含的功能比当前可用的许可证要多得多。 以前的: 当前的: 值得注意的是,操作系统配置器和除一个导入器之外的所有导入器都已不再可用。 是否可以获得恢复缺失功能的新许可证? Re: EB Tresos 29 features missing from current license 嗨@johrehn 本案例中没有任何缺失的功能。比较的是两种不同产品的许可证。 功能集较大的产品是 EB tresos AutoCore,而功能较少的产品是 EB tresos Studio / AUTOSAR 配置工具。 BR,VaneB
View full article
i.MX93:ウォッチドッグはCortex-A55だけをリセットし、Cortex-M33を稼働させ続けることは可能ですか? カスタムのi.mx93ボードを使っていますが、主にEVKの設計とPMICに従っています。ソフトウェアではNXP BSPベースのYocto(walnascar-6.12.34-2.1.0)を使っています。支店)。 ウォッチドッグタイムアウトで、Cortex-A55だけをリセットし、Cortex-M33(Zephyr)を稼働させておきたいです。そうすればM33がA55を監視し、障害時にデータをバッファリングできます。 リファレンス・マニュアルで見つけたのですが、 - セクション32.2.10では、wdog4_ca55_rst_bおよびwdog5_ca55_rst_bをコールドリセットソースとして記載しています。 - セクション32.2.12.2ではCA55はウォームリセットができず、電源オフ、CPU待機、電源オン、リリースの手順が説明されています。 - WDOG第69章では、タイムアウトによって何がリセットされるかについては記載されていません。 devmem2を使用して、SRCベース0x44460000のレジスタをダンプしました。 +0x18 (マスクのリセット): 0x00000FBF。ビット6(CSU)はクリアで、WDOGビット(WDOG5(ビット4)を含む)は設定されているため、これらのソースはマスクされています。 WDOG4やWDOG5のマスクを解除し、リセットモードをCA55スライスのみに設定して、A55がリセットされる一方でM33が動作し続けるのはサポートされていますか?もしそうなら、A55を再始動させるために他に必要なものはありますか?申請書や例はありますか? アドバイスをいただければ幸いです。 よろしくお願いします Linux Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? SRCはM33ドメインを選択しなくてもWDOG4/5のリセットをA55ドメインにルーティングできますが、それだけではM33が動作し続ける間にA55が電源を再開し、再起動しLinuxを起動するわけではありません。A55の再起動シーケンスと、ウォッチドッグによってトリガーされるPMICのリセットについても考慮する必要があります。あなたのBSPでその完全なフローを実装しているNXPの例は見つかりませんでした。 また、マスクビットの読み取り値が間違っているようです。SRMASKでは、WDOG4とWDOG5はビット19と20であり、ビット3と4ではありません。レジスタフィールドを変更する前に、再度確認してください。 Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? 迅速なご返信ありがとうございます。 私のSRMASK図(スクリーンショットを添付)では、WDOG4とWDOG5がビット3と4に、WDOG1からWDOG3がビット0から2に割り当てられており、リセット値は0xFBFです。それは起動時に私が読んだ内容と一致します。 私はIMX93RM.pdfを読んでいます牧師7、2026年2月10日。 どの文書と改訂版を読んでいるのか確認していただけますか? 私の疑問は再起動についてです。このリセット後、CPUWAITが保持され、リセットベクタが設定された状態で、A55を再び動作させるためのサポートされている手順は何ですか?RMによるとCA55はウォームリセットできず、電源のサイクルが必要だと言われています。M33から電源を再投入する、サポートされている方法はありますか? ありがとう。 よろしくお願いします Re: i.MX93: can a watchdog reset only the Cortex-A55 and leave the Cortex-M33 running? SRMASKについては、あなたの言う通りです。図のビット位置ラベルを読み間違えていました。 再起動の場合、A55リセットだけでは手順として文書化されていません。セクション32.2.12.2ではCA55はウォームリセットできないと明記されており、以下は以下の通りです:CA55の電源を落とす。CPUn_WAIT CA55_CPUWAITビットを1に設定する。CA55の電源を入れる。そしてWAITを解除してコアを動作させる。したがって、リセットベクタを設定してCPUWAITを保持するだけでは、必要な電源サイクルは実行されません。 SRCスライスを電源サイクルするソフトウェア機構が文書化されており、M33ファームウェアで使用可能とされています。§32.2.8はMEM_CTRL[MEM_LP_EN]を有効にし、スライスのSLICE_SW_CTRL[PDN_SOFT]を1に設定して電源を入れ、0にクリアして電源を入れることについて説明しています。ソフトウェアスライス制御はAUTHEN_CTRL[LPM_MODE] = 0の場合にのみ許可されます;スライスのAUTHEN_CTRL[WHITE_LIST]はまた、どのTRDCドメインがレジスタを書き込めるかも決定します。RMは別々のA55コアとプラットフォームスライスを識別するため、これは適切なCA55パワードメインに適用しなければなりません。WDOGリセットがそれらにルーティングされる際に必ずしもそうなるとは限りません。 RMのCA55電源オフ→CPUWAIT→電源オン→WAIT解除のシーケンスを使用してください。ウォッチドッグリセットルーティングだけでは、A55の完全な再起動は確立されません。
View full article
Analog Front End Layout I am designing a PCB based around a TI CC1310. I plan to operate it around 915 MHz with an SMA connected whip antenna. Ideally, I would like to get 4-5 kilometers line-of-sight range at 50 kbs or lower, which seems doable if I have a decent RF frontend. However, RF is definitely not my expertise, so my plan was just to copy the CC1310 balun and filter layout as closely as possible. Unfortunately, that's going to be more complicated and expensive than I had anticipated, so I'm wondering how much wiggle room I have when it comes to layout before I totally destroy my performance. In particular, TI used a stack-up that is 0.175 mm between the ground and top signal plane. I can save some money if I extend that to 0.21 mm, which I don't think will affect performance much, but I'm not sure. I can also save some effort by swapping out some of the passive components with those from another company, but I'm not sure how risky that is. I noticed that even the same part numbers have different footprints than what were used on the TI board. I assume that won't affect too much though. Finally, I would like to shorten the trace between the end of the filter and the antenna connector/blocking capacitor, which I assume won't affect much as long as I keep it 50 Ohms. Assuming I keep the components pretty close together and the layout symmetrical, how much can I alter the layout before I have to worry about performance being degraded? Should I plan on having to select new frontend components if I make any of the changes mentioned? Level Shifters Re: Analog Front End Layout Hi s1hukla What can I do for your about NXP products support! Thanks!
View full article
模拟前端布局 我正在设计一款基于TI CC1310的PCB。我计划使用 SMA 连接的鞭状天线,在 915 MHz 左右的频率下运行。理想情况下,我希望在 50 kbs 或更低的速度下获得 4-5 公里的视距传输距离,如果我有一个不错的射频前端,这似乎是可以实现的。然而,射频绝对不是我的专长,所以我的计划就是尽可能地复制 CC1310 平衡-不平衡转换器和滤波器的布局。不幸的是,这比我预想的要复杂和昂贵得多,所以我很想知道在布局方面我还有多少回旋余地,以免彻底毁掉我的演出。 具体来说,TI 采用了一种堆叠结构,其接地层和顶部信号层之间的厚度为 0.175 毫米。如果我把尺寸扩大到 0.21 毫米,就能省下一些钱,我觉得这不会对性能产生太大影响,但我也不确定。我也可以通过更换一些被动元器件来节省一些精力,但我不知道这样做有多大风险。我注意到,即使是相同的零件编号,其封装尺寸也与TI电路板上使用的尺寸不同。我想这应该不会造成太大影响。最后,我想缩短滤波器末端与天线连接器/阻隔电容之间的线路,我估计只要保持阻抗为 50 欧姆,就不会有太大影响。 假设我将元器件保持得非常接近,并且布局对称,那么在不必担心性能下降的情况下,我可以对布局进行多大的改变?如果我进行上述任何更改,是否需要选择新的前端组件? 电平位移器 Re: Analog Front End Layout 你好s1hukla 关于NXP产品支持,我能为您做些什么? 谢谢您!
View full article
Request for hardware design source documents of IMX95_19x19_LP4x_EVK We are looking for an LP4x evaluation board based on the 19×19 mm package i.MX95. Could you advise if there are any related evaluation boards and reference designs available? At present, we have only obtained the hardware design source files for the FRDM-IMX95 board. Its supported speed is limited to 4000 Mbps, which does not meet our requirements. Could you please check if there is an LP4x evaluation board based on the 19×19 mm package i.MX95, along with its design source files for our reference? Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK i.MX 95 19x19 LPDD4x CPU is not public. You could contact your local FAE to see if you could access it. Also, you could refer to https://docs.nxp.com/bundle/UG10210/page/topics/imx_95_19x19mm_lpddr4x-4266_routing_recommendation.html and https://docs.nxp.com/bundle/UG10210/page/topics/lpddr4x-4266_routing_example_imx_95_19x19mm.html as your design guide. Thanks Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK Thanks for your reply. We are looking for an i.MX95_19x19mm EVK with LPDDR4. The board you referred to is based on LPDDR5, which does not fit our needs. Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK Hello @D_flash , have you checked this? i.MX 95 19mm x 19mm Evaluation Kit | NXP Semiconductors Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK OK,I will do it, thank you!
View full article
ARM v2018用のS32 Design Studio。R1ライセンスが切れました こんにちは、 私の S32 Design Studio for ARM v2018について。R1 ライセンスは期限切れです。 免許を延長してもらえますか? アクティベーションコード:9D31-3A20-FFB1-F104 Re: S32 Design Studio for ARM v2018.R1 license expired こんにちは、 お客様のS32DSライセンスが延長されました。以前のコードを使用して、S32DSを再度有効化してください。
View full article
S32DS3.4 インストール済みファイルの紛失 报错如下: インストールするアイテムを収集中にエラーが発生しました。セッションコンテキストは次のとおりです:(profile=DefaultProfile、phase=org.eclipse.equinox.internal.p2.engine.phases.Collect、operand=、action=)。アーティファクトのダウンロードに関する問題: osgi.bundle、com.iar.dmgr、1.1.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar ファイルの署名プロセッシング中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile8984369696384064703.jar アーティファクトのダウンロードに問題あり:org.eclipse.update.feature,com.iar.dmgr.feature,1.1.0.202505161156。署名付きコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar ファイルの署名処理中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile2215016743562443700.jar アーティファクトのダウンロードに問題がありました:osgi.bundle,com.iar.dmgr.jna,3.4.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar ファイルの署名プロセッシング中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile3084560555014788452.jar アーティファクトのダウンロードに問題ありました:osgi.bundle,com.iar.dmgr.ui,1.1.0.202505161156。署名済みコンテンツの読み取りエラー:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jarファイルの署名処理中にエラーが発生しました:C:\Users\vboxuser\AppData\Local\Temp\signatureFile5078090908682208579.jar 回复: S32DS3.4 安装iar插件失败 こんにちは、クリス 現在、S32DS3.5にIARプラグインをインストールする際に問題が発生しています。インストール先は公式ウェブサイト(https://eclipse-update.iar.com/plugin-manager/1.0 )からダウンロードしたパスです。 インストールと再起動後、「IAR EMBEDED workbench plugin manager」オプションがヘルプメニューに表示されなくなります。 IARのバージョンは9.32.2です。 回复: S32DS3.4 安装iar插件失败 S32DS v3.5はeclipse-iar-arm-8.0プラグインを使用できます。 S32DSの一部のバージョン(Eclipseの異なるバージョンに対応)では、IARプラグインをオフラインでインストールしてみてください。 https://eclipse-update.iar.com/updatesites.html 回复: S32DS3.4 安装iar插件失败 3.5以上であれば問題ありません。 回复: S32DS3.4 安装iar插件失败 わかりました。IARプラグインをインストールできるバージョンを教えていただけますか? 回复: S32DS3.4 安装iar插件失败 以前問い合わせたところ、IARプラグインのアップグレードは古いバージョンのEclipseをサポートしていないことが分かりました。
View full article
EB Tresos 29の機能が現在のライセンスに含まれていません こんにちは! 最近期限切れとなったEB Tresos Studio 29のライセンスには、現在入手可能なライセンスよりもはるかに多くの機能が含まれています。 前の: 現在: 特に、OSコンフィギュレーターと、インポートツールのほとんど(1つを除く)が利用できなくなっている。 欠落していた機能が復元された新しいライセンスを取得することは可能でしょうか? Re: EB Tresos 29 features missing from current license こんにちは、 @johrehnさん この場合、欠けている特徴はありません。比較は2つの異なる製品のライセンスを比較しています。 機能セットが豊富な製品はEB tresos AutoCoreで、機能が少ないのはEB tresos Studio / AUTOSAR Configuration Toolです。 BR、VaneB
View full article
请求提供 IMX95_19x19_LP4x_EVK 的硬件设计源文档 我们正在寻找基于 19×19 毫米封装 i.MX95 的 LP4x 评估板。请问是否有相关的评估板和参考设计可供参考? 目前,我们只获得了 FRDM-IMX95 板的硬件设计源文件。它支持的速度上限为 4000 Mbps,这不符合我们的要求。 请问是否有基于 19×19 毫米封装的 i.MX95 的 LP4x 评估板,以及其设计源文件供我们参考? Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK i.MX 95 19x19 LPDD4x CPU 未公开。您可以联系当地的FAE(现场应用工程师),看看您是否可以访问它。 此外,您还可以参考https://docs.nxp.com/bundle/UG10210/page/topics/imx_95_19x19mm_lpddr4x-4266_routing_recommendation.html和https://docs.nxp.com/bundle/UG10210/page/topics/lpddr4x-4266_routing_example_imx_95_19x19mm.html作为您的设计指南。 谢谢! Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK 谢谢你的回复。我们正在寻找一款配备 LPDDR4 的 i.MX95_19x19mm EVK。您提到的那款主板是基于 LPDDR5 的,这不符合我们的需求。 Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK @D_flash你好,你检查过这个问题吗? i.MX 95 19mm x 19mm 评估套件 | 恩智浦半导体 Re: Request for hardware design source documents of IMX95_19x19_LP4x_EVK 好的,我会照做的,谢谢!
View full article