perform commutation twice consecutively in the CommutationSetStarting function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

perform commutation twice consecutively in the CommutationSetStarting function

跳至解决方案
958 次查看
TQF
Contributor I

Why does the source code for the BLDC motor with BEMF Zero Crossing using ADC application switch from the alignment state to the start state and perform two commutations consecutively?

Reference code link:

https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSP56F8BLDCAZC-3-Phase-BLDC-w-Sensorless-B...

TQF_0-1747714929939.png

 

0 项奖励
回复
1 解答
928 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
929 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------
0 项奖励
回复