perform commutation twice consecutively in the CommutationSetStarting function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

perform commutation twice consecutively in the CommutationSetStarting function

Jump to solution
2,442 Views
TQF
Contributor I

Why does the source code for the BLDC motor with BEMF Zero Crossing using ADC application switch from the alignment state to the start state and perform two commutations consecutively?

Reference code link:

https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSP56F8BLDCAZC-3-Phase-BLDC-w-Sensorless-B...

TQF_0-1747714929939.png

 

0 Kudos
Reply
1 Solution
2,412 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,413 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------
0 Kudos
Reply