perform commutation twice consecutively in the CommutationSetStarting function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

perform commutation twice consecutively in the CommutationSetStarting function

ソリューションへジャンプ
992件の閲覧回数
TQF
Contributor I

Why does the source code for the BLDC motor with BEMF Zero Crossing using ADC application switch from the alignment state to the start state and perform two commutations consecutively?

Reference code link:

https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/RDDSP56F8BLDCAZC-3-Phase-BLDC-w-Sensorless-B...

TQF_0-1747714929939.png

 

0 件の賞賛
返信
1 解決策
962件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
963件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @TQF ,

Thanks for your post.

Please refer to the DRM026.pdf attached to the website you mentioned. (RDDSP56F8BLDCAZC: 3-Phase BLDC w/Sensorless Back-EMF ADC Zero Crossing Sensor for 56F80X or 56F8300 ...

Celeste_Liu_2-1747901645619.png


In Section 3.3.4.5 "Starting (Back-EMF Acquisition)", an explanation is provided:
 
Celeste_Liu_0-1747901534265.png
Celeste_Liu_3-1747901953085.png

 

Hope it can help you.

 

BRs,
Celeste
 
------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
------------------------------------------------------------------------------------------------------
0 件の賞賛
返信