Register symbol value and reset value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Register symbol value and reset value

跳至解决方案
6,507 次查看
YangHF
Contributor II

Hello community,

I want to use MC33774 to monitor the battery cell status, and I already have the file MC33774A Data sheet (0.1). I would like to ask some questions, please.

In ALLM_ In the CFG register, the value of bit 0 MEASEN is 0. Will writing 1 make it impossible to measure or meaningless?

The reset value of MEASEN is also 0. Can I not write value to ALLM_ In the CFG register always and IC automatically run with this register default values?

Additionally, I feel that the bit of the BALPAUSELEN signal is written incorrectly, it should be bit2, and bit15:2 should be reserved.

Best wishes, thank you.

1 解答
6,440 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Please see the info below about the usage of ALLM registers.

From the AN12913 (MC33775A and MC33774A measurement):

Capture.JPG

From the MC33774 datasheet:

Capture 1.JPG

Using the ALLM registers results not only in fewer write commands, but also ensures synchronicity between the measurement chains.

So if you set the MEASEN bit in the ALLM_CFG register, the MEASEN bit in both the PRMM_CFG and SECM_CFG registers will be set at the same time and the data acquisition enabled.

Capture 2.JPG

The same applies to the BALPAUSELEN[15:2] bits.

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,483 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

I am not sure I fully understand your question.

First off, I would recommend you to download the latest (Rev. 1) MC33774A datasheet which is classified as a Secure file requiring an NDA.

Regarding the MEASEN bit, please see below.

Table 16.JPG

As for the BALPAUSELEN [15:2] bits, please see below.

BALPAUSELEN.JPG

BR, Tomas

0 项奖励
回复
6,445 次查看
YangHF
Contributor II

Hi Tomas,

I have downloaded 33774 datasheetV1.0. In the screenshot below, the value of "MEASEN" is oniy "0". Can I set "MEASEN" to "1"? What will be the result of this?And  the "BALPAUSELEN" in the screenshot is not described in detail. Does it have the same meaning as the "BALPAUSELEN" you replied to me on Wednesday?

YangHF_0-1697190543663.png

Thank you! Best wishes!

0 项奖励
回复
6,441 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Please see the info below about the usage of ALLM registers.

From the AN12913 (MC33775A and MC33774A measurement):

Capture.JPG

From the MC33774 datasheet:

Capture 1.JPG

Using the ALLM registers results not only in fewer write commands, but also ensures synchronicity between the measurement chains.

So if you set the MEASEN bit in the ALLM_CFG register, the MEASEN bit in both the PRMM_CFG and SECM_CFG registers will be set at the same time and the data acquisition enabled.

Capture 2.JPG

The same applies to the BALPAUSELEN[15:2] bits.

BR, Tomas

0 项奖励
回复
6,347 次查看
YangHF
Contributor II

Hi Tomas,

Is my viewpoint below correct? In ALLM_CFG register, when "MEASEN" =1 , enable all measurement, When "MEASEN" =0, disable all measurement. And when "BALPAUSECYCMODEN" =1 , enable all balancing pause, When "BALPAUSECYCMODEN" =1, disable all balancing pause.

YangHF_1-1697509103765.png

If there is a sudden power outage, which registers of 33774 will not lose data? I didn't see relevant content in the datasheet. Could you tell me? Thank you!

Best wishes!

0 项奖励
回复
6,467 次查看
YangHF
Contributor II

Hi Tomas,

I'm very sorry to bother you again. I didn't find the latest version date sheet. Can you give me a website address to get this document? I will check my NDA level. Thank you!

Best wishes!

0 项奖励
回复
6,459 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The MC33774A datasheet (Rev. 1) is available under Secure Files on the following website:

https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/18-channel...

Capture.JPG

Please make sure you are signed in to nxp.com. If you do not see the MC33774A datasheet, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. 

For more information about secure access rights, please refer to this website:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS

BR, Tomas

0 项奖励
回复
6,478 次查看
YangHF
Contributor II
Hello Tomas,
Thank you very much. I will get the latest (Rev. 1) MC33774A datasheet.
Best wishes
0 项奖励
回复