s32k39. Disable CAN FD on the CAN4 port.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k39. Disable CAN FD on the CAN4 port.

跳至解决方案
618 次查看
MaMM
Contributor III

Hi.

I'm having a problem configuring the CAN4 port in the s32k396. I copied the same configuration from CAN0 and CAN1, into CAN4, but the configuration gets an error explaining that I should disable CANFD in CAN4. I have tried, but I cannot find where to disable the options. (I'm using tresos Studio).

Thanks in advance.

0 项奖励
回复
1 解答
602 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @MaMM 

Could you please check this article? https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

It contains a step by step guide on how to configure CAN component options, providing an overview of the main settings available in the configuration tool.

Hope this helps,

Irina

在原帖中查看解决方案

0 项奖励
回复
2 回复数
603 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @MaMM 

Could you please check this article? https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

It contains a step by step guide on how to configure CAN component options, providing an overview of the main settings available in the configuration tool.

Hope this helps,

Irina

0 项奖励
回复
590 次查看
MaMM
Contributor III

Hi Irina.

Since I am using Tresos, it was not so clear how to disable the option you mentioned. I was finally able to delete that part of the configuration and configure CAN4. Once compiled, I was able to see messages through CAN4.

Just to mention, the CAN4 of the processor board is connected to the CAN2 of the MB board, and the CAN2 of the processor board needs to be connected via cable routing to a transceiver on the MB, as I mentioned in another post.

Miguel.

标记 (1)