s32k39. Disable CAN FD on the CAN4 port.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k39. Disable CAN FD on the CAN4 port.

Jump to solution
614 Views
MaMM
Contributor III

Hi.

I'm having a problem configuring the CAN4 port in the s32k396. I copied the same configuration from CAN0 and CAN1, into CAN4, but the configuration gets an error explaining that I should disable CANFD in CAN4. I have tried, but I cannot find where to disable the options. (I'm using tresos Studio).

Thanks in advance.

0 Kudos
Reply
1 Solution
598 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @MaMM 

Could you please check this article? https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

It contains a step by step guide on how to configure CAN component options, providing an overview of the main settings available in the configuration tool.

Hope this helps,

Irina

View solution in original post

0 Kudos
Reply
2 Replies
599 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @MaMM 

Could you please check this article? https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

It contains a step by step guide on how to configure CAN component options, providing an overview of the main settings available in the configuration tool.

Hope this helps,

Irina

0 Kudos
Reply
586 Views
MaMM
Contributor III

Hi Irina.

Since I am using Tresos, it was not so clear how to disable the option you mentioned. I was finally able to delete that part of the configuration and configure CAN4. Once compiled, I was able to see messages through CAN4.

Just to mention, the CAN4 of the processor board is connected to the CAN2 of the MB board, and the CAN2 of the processor board needs to be connected via cable routing to a transceiver on the MB, as I mentioned in another post.

Miguel.

Tags (1)