Update R2017b

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Update R2017b

跳至解决方案
5,055 次查看
lethuer
Contributor V

Hello,

after the Installation of R2017b I get this error after I want to build a model.

Undefined function 'slsfnagctlr' for input arguments of type 'char'.

The Simulation runs successfully.

With R2017a Release the build of the model works.

Does anybody know this error and could help ?

Best regards

Leon

0 项奖励
回复
1 解答
4,386 次查看
lethuer
Contributor V

I do not have exactly such a path...

But I copied it to the following Folder and the build process is works now !

C:\MCToolbox\mctbx_Kinetis\mctbx_kv4xf\mctbx_kv4xf\mscripts

Thank you for Support !

Best regards

Leon

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,386 次查看
lethuer
Contributor V

Is there also a Hotfix for S32K v2.0 on Release R2017b ?

Unbenannt.PNG

0 项奖励
回复
4,386 次查看
Daniel_Popa
NXP Employee
NXP Employee

There is no fix for v2.0.0 since it has been replaced by https://community.nxp.com/docs/DOC-335555 

0 项奖励
回复
4,386 次查看
lethuer
Contributor V

Hello,

I'm using the Kinetis Toolbox.

Best regards

Leon

0 项奖励
回复
4,385 次查看
constantinrazva
NXP Employee
NXP Employee

Hi lethuer‌, 

Please do the following:

copy slsfnagctlr.p file from attached zip into {YOUR_KINETIS_TOOLBOX_ROOT}\mctbx_kv*xf\mscripts

This should do the trick.

Let me know if you encounter other problems with the new Matlab version.

Kind regards,

Razvan.

0 项奖励
回复
4,387 次查看
lethuer
Contributor V

I do not have exactly such a path...

But I copied it to the following Folder and the build process is works now !

C:\MCToolbox\mctbx_Kinetis\mctbx_kv4xf\mctbx_kv4xf\mscripts

Thank you for Support !

Best regards

Leon

0 项奖励
回复
4,385 次查看
constantinrazva
NXP Employee
NXP Employee

Hello lethuer‌,

You did it right. I used * in mctbx_kv*xf\mscripts as I did not know if you had kv3, kv4 or other KV board.

Best regards,

Razvan.

0 项奖励
回复
4,385 次查看
constantinrazva
NXP Employee
NXP Employee

Hi lethuer‌,

Can you tell us what toolbox are you using?

For example, we have a fix for MPC564xL available here: HotFix: MBD Toolbox rev1.3.0 for MPC564xL .

Kind regards,

Razvan.

0 项奖励
回复