HotFix: MBD Toolbox rev1.3.0 for MPC564xL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HotFix: MBD Toolbox rev1.3.0 for MPC564xL

5,588 Views
paulvlase
NXP Employee
NXP Employee

HotFix_1: Fix "Undefined function 'slsfnagctlr'..." when trying to generate code on R2016b/R2017a

 

NXP Tracking number: AST-527

 

Problem: If you try to generate code for any model on R2016b/R2017a, you will receive this error: "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

 

Root Cause: Matlab API change.

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}\rappid564xl\rappid564xl\mscripts folder slsfnagctlr.p file

 

Customer Report: BUG report

Special thanks to Michael Verrecchia for reporting this issue.

Labels (1)
Tags (1)
4 Replies

4,717 Views
paulvlase
NXP Employee
NXP Employee

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking number: AST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the rappid_hostid.p file attached in the following folder 

{Toolbox install dir}\rappid564xl\rappid564xl\mscripts

 

Customer Report: Undefined function or variable 'lic_err'.

0 Kudos
Reply

4,717 Views
jjacp
Contributor III

Hi paulvlase‌,

Is this fix available for the MBD v2.0.0 Toolbox for the MPC5744P (Panther)? I'm running R2018a and am getting the slsfnagctlr error.

Thanks!

0 Kudos
Reply

4,715 Views
constantinrazva
NXP Employee
NXP Employee

Hello jjacp‌,

Yes, there is a fix available for Panther (MPC5744P). I have attached it here.

Please move slsfnagctlr.p file into 

   {TOOLBOX_TOOL_ROOT}\mbdtbx_pnt\mbdtbx_pnt\mscripts

Kind regards,

Razvan.

4,715 Views
jjacp
Contributor III

Thanks constantinrazvan.chivu! It works!

0 Kudos
Reply